1 /*
2 * SPDX-License-Identifier: MIT
3 *
4 * Copyright � 2008-2018 Intel Corporation
5 */
7 #ifndef _I915_GPU_ERROR_H_
8 #define _I915_GPU_ERROR_H_
10 #include <linux/kref.h>
11 #include <linux/ktime.h>
12 #include <linux/sched.h>
14 #include <drm/drm_mm.h>
16 #include "intel_device_info.h"
17 #include "intel_ringbuffer.h"
18 #include "intel_uc_fw.h"
20 #include "i915_gem.h"
21 #include "i915_gem_gtt.h"
22 #include "i915_params.h"
23 #include "i915_scheduler.h"
25 struct drm_i915_private;
26 struct intel_overlay_error_state;
27 struct intel_display_error_state;
29 struct i915_gpu_state {
30 struct kref ref;
31 ktime_t time;
32 ktime_t boottime;
33 ktime_t uptime;
34 unsigned long capture;
35 unsigned long epoch;
37 struct drm_i915_private *i915;
39 char error_msg[128];
40 bool simulated;
41 bool awake;
42 bool wakelock;
43 bool suspended;
44 int iommu;
45 u32 reset_count;
46 u32 suspend_count;
47 struct intel_device_info device_info;
48 struct intel_driver_caps driver_caps;
49 struct i915_params params;
51 struct i915_error_uc {
52 struct intel_uc_fw guc_fw;
53 struct intel_uc_fw huc_fw;
54 struct drm_i915_error_object *guc_log;
55 } uc;
57 /* Generic register state */
58 u32 eir;
59 u32 pgtbl_er;
60 u32 ier;
61 u32 gtier[6], ngtier;
62 u32 ccid;
63 u32 derrmr;
64 u32 forcewake;
65 u32 error; /* gen6+ */
66 u32 err_int; /* gen7 */
67 u32 fault_data0; /* gen8, gen9 */
68 u32 fault_data1; /* gen8, gen9 */
69 u32 done_reg;
70 u32 gac_eco;
71 u32 gam_ecochk;
72 u32 gab_ctl;
73 u32 gfx_mode;
75 u32 nfence;
76 u64 fence[I915_MAX_NUM_FENCES];
77 struct intel_overlay_error_state *overlay;
78 struct intel_display_error_state *display;
80 struct drm_i915_error_engine {
81 int engine_id;
82 /* Software tracked state */
83 bool idle;
84 bool waiting;
85 int num_waiters;
86 unsigned long hangcheck_timestamp;
87 bool hangcheck_stalled;
88 enum intel_engine_hangcheck_action hangcheck_action;
89 struct i915_address_space *vm;
90 int num_requests;
91 u32 reset_count;
93 /* position of active request inside the ring */
94 u32 rq_head, rq_post, rq_tail;
96 /* our own tracking of ring head and tail */
97 u32 cpu_ring_head;
98 u32 cpu_ring_tail;
100 u32 last_seqno;
102 /* Register state */
103 u32 start;
104 u32 tail;
105 u32 head;
106 u32 ctl;
107 u32 mode;
108 u32 hws;
109 u32 ipeir;
110 u32 ipehr;
111 u32 bbstate;
112 u32 instpm;
113 u32 instps;
114 u32 seqno;
115 u64 bbaddr;
116 u64 acthd;
117 u32 fault_reg;
118 u64 faddr;
119 u32 rc_psmi; /* sleep state */
120 u32 semaphore_mboxes[I915_NUM_ENGINES - 1];
121 struct intel_instdone instdone;
123 struct drm_i915_error_context {
124 char comm[TASK_COMM_LEN];
125 pid_t pid;
126 u32 handle;
127 u32 hw_id;
128 int ban_score;
129 int active;
130 int guilty;
131 bool bannable;
132 struct i915_sched_attr sched_attr;
133 } context;
135 struct drm_i915_error_object {
136 u64 gtt_offset;
137 u64 gtt_size;
138 int num_pages;
139 int page_count;
140 int unused;
141 u32 *pages[0];
142 } *ringbuffer, *batchbuffer, *wa_batchbuffer, *ctx, *hws_page;
144 struct drm_i915_error_object **user_bo;
145 long user_bo_count;
147 struct drm_i915_error_object *wa_ctx;
148 struct drm_i915_error_object *default_state;
150 struct drm_i915_error_request {
151 long jiffies;
152 pid_t pid;
153 u32 context;
154 int ban_score;
155 u32 seqno;
156 u32 start;
157 u32 head;
158 u32 tail;
159 struct i915_sched_attr sched_attr;
160 } *requests, execlist[EXECLIST_MAX_PORTS];
161 unsigned int num_ports;
163 struct drm_i915_error_waiter {
164 char comm[TASK_COMM_LEN];
165 pid_t pid;
166 u32 seqno;
167 } *waiters;
169 struct {
170 u32 gfx_mode;
171 union {
172 u64 pdp[4];
173 u32 pp_dir_base;
174 };
175 } vm_info;
176 } engine[I915_NUM_ENGINES];
178 struct drm_i915_error_buffer {
179 u32 size;
180 u32 name;
181 u32 wseqno;
182 u64 gtt_offset;
183 u32 read_domains;
184 u32 write_domain;
185 s32 fence_reg:I915_MAX_NUM_FENCE_BITS;
186 u32 tiling:2;
187 u32 dirty:1;
188 u32 purgeable:1;
189 u32 userptr:1;
190 s32 engine:4;
191 u32 cache_level:3;
192 } *active_bo[I915_NUM_ENGINES], *pinned_bo;
193 u32 active_bo_count[I915_NUM_ENGINES], pinned_bo_count;
194 struct i915_address_space *active_vm[I915_NUM_ENGINES];
195 };
197 struct i915_gpu_error {
198 /* For hangcheck timer */
199 #define DRM_I915_HANGCHECK_PERIOD 1500 /* in ms */
200 #define DRM_I915_HANGCHECK_JIFFIES msecs_to_jiffies(DRM_I915_HANGCHECK_PERIOD)
202 struct delayed_work hangcheck_work;
204 /* For reset and error_state handling. */
205 spinlock_t lock;
206 /* Protected by the above dev->gpu_error.lock. */
207 struct i915_gpu_state *first_error;
209 atomic_t pending_fb_pin;
211 unsigned long missed_irq_rings;
213 /**
214 * State variable controlling the reset flow and count
215 *
216 * This is a counter which gets incremented when reset is triggered,
217 *
218 * Before the reset commences, the I915_RESET_BACKOFF bit is set
219 * meaning that any waiters holding onto the struct_mutex should
220 * relinquish the lock immediately in order for the reset to start.
221 *
222 * If reset is not completed successfully, the I915_WEDGE bit is
223 * set meaning that hardware is terminally sour and there is no
224 * recovery. All waiters on the reset_queue will be woken when
225 * that happens.
226 *
227 * This counter is used by the wait_seqno code to notice that reset
228 * event happened and it needs to restart the entire ioctl (since most
229 * likely the seqno it waited for won't ever signal anytime soon).
230 *
231 * This is important for lock-free wait paths, where no contended lock
232 * naturally enforces the correct ordering between the bail-out of the
233 * waiter and the gpu reset work code.
234 */
235 unsigned long reset_count;
237 /**
238 * flags: Control various stages of the GPU reset
239 *
240 * #I915_RESET_BACKOFF - When we start a reset, we want to stop any
241 * other users acquiring the struct_mutex. To do this we set the
242 * #I915_RESET_BACKOFF bit in the error flags when we detect a reset
243 * and then check for that bit before acquiring the struct_mutex (in
244 * i915_mutex_lock_interruptible()?). I915_RESET_BACKOFF serves a
245 * secondary role in preventing two concurrent global reset attempts.
246 *
247 * #I915_RESET_HANDOFF - To perform the actual GPU reset, we need the
248 * struct_mutex. We try to acquire the struct_mutex in the reset worker,
249 * but it may be held by some long running waiter (that we cannot
250 * interrupt without causing trouble). Once we are ready to do the GPU
251 * reset, we set the I915_RESET_HANDOFF bit and wakeup any waiters. If
252 * they already hold the struct_mutex and want to participate they can
253 * inspect the bit and do the reset directly, otherwise the worker
254 * waits for the struct_mutex.
255 *
256 * #I915_RESET_ENGINE[num_engines] - Since the driver doesn't need to
257 * acquire the struct_mutex to reset an engine, we need an explicit
258 * flag to prevent two concurrent reset attempts in the same engine.
259 * As the number of engines continues to grow, allocate the flags from
260 * the most significant bits.
261 *
262 * #I915_WEDGED - If reset fails and we can no longer use the GPU,
263 * we set the #I915_WEDGED bit. Prior to command submission, e.g.
264 * i915_request_alloc(), this bit is checked and the sequence
265 * aborted (with -EIO reported to userspace) if set.
266 */
267 unsigned long flags;
268 #define I915_RESET_BACKOFF 0
269 #define I915_RESET_HANDOFF 1
270 #define I915_RESET_MODESET 2
271 #define I915_WEDGED (BITS_PER_LONG - 1)
272 #define I915_RESET_ENGINE (I915_WEDGED - I915_NUM_ENGINES)
274 /** Number of times an engine has been reset */
275 u32 reset_engine_count[I915_NUM_ENGINES];
277 /** Set of stalled engines with guilty requests, in the current reset */
278 u32 stalled_mask;
280 /** Reason for the current *global* reset */
281 const char *reason;
283 /**
284 * Waitqueue to signal when a hang is detected. Used to for waiters
285 * to release the struct_mutex for the reset to procede.
286 */
287 wait_queue_head_t wait_queue;
289 /**
290 * Waitqueue to signal when the reset has completed. Used by clients
291 * that wait for dev_priv->mm.wedged to settle.
292 */
293 wait_queue_head_t reset_queue;
295 /* For missed irq/seqno simulation. */
296 unsigned long test_irq_rings;
297 };
299 struct drm_i915_error_state_buf {
300 struct drm_i915_private *i915;
301 unsigned int bytes;
302 unsigned int size;
303 int err;
304 u8 *buf;
305 loff_t start;
306 loff_t pos;
307 };
309 #if IS_ENABLED(CONFIG_DRM_I915_CAPTURE_ERROR)
311 __printf(2, 3)
312 void i915_error_printf(struct drm_i915_error_state_buf *e, const char *f, ...);
313 int i915_error_state_to_str(struct drm_i915_error_state_buf *estr,
314 const struct i915_gpu_state *gpu);
315 int i915_error_state_buf_init(struct drm_i915_error_state_buf *eb,
316 struct drm_i915_private *i915,
317 size_t count, loff_t pos);
319 static inline void
320 i915_error_state_buf_release(struct drm_i915_error_state_buf *eb)
321 {
322 kfree(eb->buf);
323 }
325 struct i915_gpu_state *i915_capture_gpu_state(struct drm_i915_private *i915);
326 void i915_capture_error_state(struct drm_i915_private *dev_priv,
327 u32 engine_mask,
328 const char *error_msg);
330 static inline struct i915_gpu_state *
331 i915_gpu_state_get(struct i915_gpu_state *gpu)
332 {
333 kref_get(&gpu->ref);
334 return gpu;
335 }
337 void __i915_gpu_state_free(struct kref *kref);
338 static inline void i915_gpu_state_put(struct i915_gpu_state *gpu)
339 {
340 if (gpu)
341 kref_put(&gpu->ref, __i915_gpu_state_free);
342 }
344 struct i915_gpu_state *i915_first_error_state(struct drm_i915_private *i915);
345 void i915_reset_error_state(struct drm_i915_private *i915);
347 #else
349 static inline void i915_capture_error_state(struct drm_i915_private *dev_priv,
350 u32 engine_mask,
351 const char *error_msg)
352 {
353 }
355 static inline struct i915_gpu_state *
356 i915_first_error_state(struct drm_i915_private *i915)
357 {
358 return NULL;
359 }
361 static inline void i915_reset_error_state(struct drm_i915_private *i915)
362 {
363 }
365 #endif /* IS_ENABLED(CONFIG_DRM_I915_CAPTURE_ERROR) */
367 #endif /* _I915_GPU_ERROR_H_ */