1 /*
2 * vga_switcheroo.c - Support for laptop with dual GPU using one set of outputs
3 *
4 * Copyright (c) 2010 Red Hat Inc.
5 * Author : Dave Airlie <airlied@redhat.com>
6 *
7 * Copyright (c) 2015 Lukas Wunner <lukas@wunner.de>
8 *
9 * Permission is hereby granted, free of charge, to any person obtaining a
10 * copy of this software and associated documentation files (the "Software"),
11 * to deal in the Software without restriction, including without limitation
12 * the rights to use, copy, modify, merge, publish, distribute, sublicense,
13 * and/or sell copies of the Software, and to permit persons to whom the
14 * Software is furnished to do so, subject to the following conditions:
15 *
16 * The above copyright notice and this permission notice (including the next
17 * paragraph) shall be included in all copies or substantial portions of the
18 * Software.
19 *
20 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
21 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
22 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL
23 * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
24 * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING
25 * FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER
26 * DEALINGS
27 * IN THE SOFTWARE.
28 *
29 */
31 #define pr_fmt(fmt) "vga_switcheroo: " fmt
33 #include <linux/apple-gmux.h>
34 #include <linux/console.h>
35 #include <linux/debugfs.h>
36 #include <linux/fb.h>
37 #include <linux/fs.h>
38 #include <linux/module.h>
39 #include <linux/pci.h>
40 #include <linux/pm_domain.h>
41 #include <linux/pm_runtime.h>
42 #include <linux/seq_file.h>
43 #include <linux/uaccess.h>
44 #include <linux/vgaarb.h>
45 #include <linux/vga_switcheroo.h>
47 /**
48 * DOC: Overview
49 *
50 * vga_switcheroo is the Linux subsystem for laptop hybrid graphics.
51 * These come in two flavors:
52 *
53 * * muxed: Dual GPUs with a multiplexer chip to switch outputs between GPUs.
54 * * muxless: Dual GPUs but only one of them is connected to outputs.
55 * The other one is merely used to offload rendering, its results
56 * are copied over PCIe into the framebuffer. On Linux this is
57 * supported with DRI PRIME.
58 *
59 * Hybrid graphics started to appear in the late Naughties and were initially
60 * all muxed. Newer laptops moved to a muxless architecture for cost reasons.
61 * A notable exception is the MacBook Pro which continues to use a mux.
62 * Muxes come with varying capabilities: Some switch only the panel, others
63 * can also switch external displays. Some switch all display pins at once
64 * while others can switch just the DDC lines. (To allow EDID probing
65 * for the inactive GPU.) Also, muxes are often used to cut power to the
66 * discrete GPU while it is not used.
67 *
68 * DRM drivers register GPUs with vga_switcheroo, these are henceforth called
69 * clients. The mux is called the handler. Muxless machines also register a
70 * handler to control the power state of the discrete GPU, its ->switchto
71 * callback is a no-op for obvious reasons. The discrete GPU is often equipped
72 * with an HDA controller for the HDMI/DP audio signal, this will also
73 * register as a client so that vga_switcheroo can take care of the correct
74 * suspend/resume order when changing the discrete GPU's power state. In total
75 * there can thus be up to three clients: Two vga clients (GPUs) and one audio
76 * client (on the discrete GPU). The code is mostly prepared to support
77 * machines with more than two GPUs should they become available.
78 *
79 * The GPU to which the outputs are currently switched is called the
80 * active client in vga_switcheroo parlance. The GPU not in use is the
81 * inactive client. When the inactive client's DRM driver is loaded,
82 * it will be unable to probe the panel's EDID and hence depends on
83 * VBIOS to provide its display modes. If the VBIOS modes are bogus or
84 * if there is no VBIOS at all (which is common on the MacBook Pro),
85 * a client may alternatively request that the DDC lines are temporarily
86 * switched to it, provided that the handler supports this. Switching
87 * only the DDC lines and not the entire output avoids unnecessary
88 * flickering.
89 */
91 /**
92 * struct vga_switcheroo_client - registered client
93 * @pdev: client pci device
94 * @fb_info: framebuffer to which console is remapped on switching
95 * @pwr_state: current power state if manual power control is used.
96 * For driver power control, call vga_switcheroo_pwr_state().
97 * @ops: client callbacks
98 * @id: client identifier. Determining the id requires the handler,
99 * so gpus are initially assigned VGA_SWITCHEROO_UNKNOWN_ID
100 * and later given their true id in vga_switcheroo_enable()
101 * @active: whether the outputs are currently switched to this client
102 * @driver_power_control: whether power state is controlled by the driver's
103 * runtime pm. If true, writing ON and OFF to the vga_switcheroo debugfs
104 * interface is a no-op so as not to interfere with runtime pm
105 * @list: client list
106 * @vga_dev: pci device, indicate which GPU is bound to current audio client
107 *
108 * Registered client. A client can be either a GPU or an audio device on a GPU.
109 * For audio clients, the @fb_info and @active members are bogus. For GPU
110 * clients, the @vga_dev is bogus.
111 */
112 struct vga_switcheroo_client {
113 struct pci_dev *pdev;
114 struct fb_info *fb_info;
115 enum vga_switcheroo_state pwr_state;
116 const struct vga_switcheroo_client_ops *ops;
117 enum vga_switcheroo_client_id id;
118 bool active;
119 bool driver_power_control;
120 struct list_head list;
121 struct pci_dev *vga_dev;
122 };
124 /*
125 * protects access to struct vgasr_priv
126 */
127 static DEFINE_MUTEX(vgasr_mutex);
129 /**
130 * struct vgasr_priv - vga_switcheroo private data
131 * @active: whether vga_switcheroo is enabled.
132 * Prerequisite is the registration of two GPUs and a handler
133 * @delayed_switch_active: whether a delayed switch is pending
134 * @delayed_client_id: client to which a delayed switch is pending
135 * @debugfs_root: directory for vga_switcheroo debugfs interface
136 * @switch_file: file for vga_switcheroo debugfs interface
137 * @registered_clients: number of registered GPUs
138 * (counting only vga clients, not audio clients)
139 * @clients: list of registered clients
140 * @handler: registered handler
141 * @handler_flags: flags of registered handler
142 * @mux_hw_lock: protects mux state
143 * (in particular while DDC lines are temporarily switched)
144 * @old_ddc_owner: client to which DDC lines will be switched back on unlock
145 *
146 * vga_switcheroo private data. Currently only one vga_switcheroo instance
147 * per system is supported.
148 */
149 struct vgasr_priv {
150 bool active;
151 bool delayed_switch_active;
152 enum vga_switcheroo_client_id delayed_client_id;
154 struct dentry *debugfs_root;
155 struct dentry *switch_file;
157 int registered_clients;
158 struct list_head clients;
160 const struct vga_switcheroo_handler *handler;
161 enum vga_switcheroo_handler_flags_t handler_flags;
162 struct mutex mux_hw_lock;
163 int old_ddc_owner;
164 };
166 #define ID_BIT_AUDIO 0x100
167 #define client_is_audio(c) ((c)->id & ID_BIT_AUDIO)
168 #define client_is_vga(c) (!client_is_audio(c))
169 #define client_id(c) ((c)->id & ~ID_BIT_AUDIO)
171 static int vga_switcheroo_debugfs_init(struct vgasr_priv *priv);
172 static void vga_switcheroo_debugfs_fini(struct vgasr_priv *priv);
174 /* only one switcheroo per system */
175 static struct vgasr_priv vgasr_priv = {
176 .clients = LIST_HEAD_INIT(vgasr_priv.clients),
177 .mux_hw_lock = __MUTEX_INITIALIZER(vgasr_priv.mux_hw_lock),
178 };
180 static bool vga_switcheroo_ready(void)
181 {
182 /* we're ready if we get two clients + handler */
183 return !vgasr_priv.active &&
184 vgasr_priv.registered_clients == 2 && vgasr_priv.handler;
185 }
187 static void vga_switcheroo_enable(void)
188 {
189 int ret;
190 struct vga_switcheroo_client *client;
192 /* call the handler to init */
193 if (vgasr_priv.handler->init)
194 vgasr_priv.handler->init();
196 list_for_each_entry(client, &vgasr_priv.clients, list) {
197 if (!client_is_vga(client) ||
198 client_id(client) != VGA_SWITCHEROO_UNKNOWN_ID)
199 continue;
201 ret = vgasr_priv.handler->get_client_id(client->pdev);
202 if (ret < 0)
203 return;
205 client->id = ret;
206 }
208 list_for_each_entry(client, &vgasr_priv.clients, list) {
209 if (!client_is_audio(client) ||
210 client_id(client) != VGA_SWITCHEROO_UNKNOWN_ID)
211 continue;
213 ret = vgasr_priv.handler->get_client_id(client->vga_dev);
214 if (ret < 0)
215 return;
217 client->id = ret | ID_BIT_AUDIO;
218 if (client->ops->gpu_bound)
219 client->ops->gpu_bound(client->pdev, ret);
220 }
222 vga_switcheroo_debugfs_init(&vgasr_priv);
223 vgasr_priv.active = true;
224 }
226 /**
227 * vga_switcheroo_register_handler() - register handler
228 * @handler: handler callbacks
229 * @handler_flags: handler flags
230 *
231 * Register handler. Enable vga_switcheroo if two vga clients have already
232 * registered.
233 *
234 * Return: 0 on success, -EINVAL if a handler was already registered.
235 */
236 int vga_switcheroo_register_handler(
237 const struct vga_switcheroo_handler *handler,
238 enum vga_switcheroo_handler_flags_t handler_flags)
239 {
240 mutex_lock(&vgasr_mutex);
241 if (vgasr_priv.handler) {
242 mutex_unlock(&vgasr_mutex);
243 return -EINVAL;
244 }
246 vgasr_priv.handler = handler;
247 vgasr_priv.handler_flags = handler_flags;
248 if (vga_switcheroo_ready()) {
249 pr_info("enabled\n");
250 vga_switcheroo_enable();
251 }
252 mutex_unlock(&vgasr_mutex);
253 return 0;
254 }
255 EXPORT_SYMBOL(vga_switcheroo_register_handler);
257 /**
258 * vga_switcheroo_unregister_handler() - unregister handler
259 *
260 * Unregister handler. Disable vga_switcheroo.
261 */
262 void vga_switcheroo_unregister_handler(void)
263 {
264 mutex_lock(&vgasr_mutex);
265 mutex_lock(&vgasr_priv.mux_hw_lock);
266 vgasr_priv.handler_flags = 0;
267 vgasr_priv.handler = NULL;
268 if (vgasr_priv.active) {
269 pr_info("disabled\n");
270 vga_switcheroo_debugfs_fini(&vgasr_priv);
271 vgasr_priv.active = false;
272 }
273 mutex_unlock(&vgasr_priv.mux_hw_lock);
274 mutex_unlock(&vgasr_mutex);
275 }
276 EXPORT_SYMBOL(vga_switcheroo_unregister_handler);
278 /**
279 * vga_switcheroo_handler_flags() - obtain handler flags
280 *
281 * Helper for clients to obtain the handler flags bitmask.
282 *
283 * Return: Handler flags. A value of 0 means that no handler is registered
284 * or that the handler has no special capabilities.
285 */
286 enum vga_switcheroo_handler_flags_t vga_switcheroo_handler_flags(void)
287 {
288 return vgasr_priv.handler_flags;
289 }
290 EXPORT_SYMBOL(vga_switcheroo_handler_flags);
292 static int register_client(struct pci_dev *pdev,
293 const struct vga_switcheroo_client_ops *ops,
294 enum vga_switcheroo_client_id id,
295 struct pci_dev *vga_dev,
296 bool active,
297 bool driver_power_control)
298 {
299 struct vga_switcheroo_client *client;
301 client = kzalloc(sizeof(*client), GFP_KERNEL);
302 if (!client)
303 return -ENOMEM;
305 client->pwr_state = VGA_SWITCHEROO_ON;
306 client->pdev = pdev;
307 client->ops = ops;
308 client->id = id;
309 client->active = active;
310 client->driver_power_control = driver_power_control;
311 client->vga_dev = vga_dev;
313 mutex_lock(&vgasr_mutex);
314 list_add_tail(&client->list, &vgasr_priv.clients);
315 if (client_is_vga(client))
316 vgasr_priv.registered_clients++;
318 if (vga_switcheroo_ready()) {
319 pr_info("enabled\n");
320 vga_switcheroo_enable();
321 }
322 mutex_unlock(&vgasr_mutex);
323 return 0;
324 }
326 /**
327 * vga_switcheroo_register_client - register vga client
328 * @pdev: client pci device
329 * @ops: client callbacks
330 * @driver_power_control: whether power state is controlled by the driver's
331 * runtime pm
332 *
333 * Register vga client (GPU). Enable vga_switcheroo if another GPU and a
334 * handler have already registered. The power state of the client is assumed
335 * to be ON. Beforehand, vga_switcheroo_client_probe_defer() shall be called
336 * to ensure that all prerequisites are met.
337 *
338 * Return: 0 on success, -ENOMEM on memory allocation error.
339 */
340 int vga_switcheroo_register_client(struct pci_dev *pdev,
341 const struct vga_switcheroo_client_ops *ops,
342 bool driver_power_control)
343 {
344 return register_client(pdev, ops, VGA_SWITCHEROO_UNKNOWN_ID, NULL,
345 pdev == vga_default_device(),
346 driver_power_control);
347 }
348 EXPORT_SYMBOL(vga_switcheroo_register_client);
350 /**
351 * vga_switcheroo_register_audio_client - register audio client
352 * @pdev: client pci device
353 * @ops: client callbacks
354 * @vga_dev: pci device which is bound to current audio client
355 *
356 * Register audio client (audio device on a GPU). The client is assumed
357 * to use runtime PM. Beforehand, vga_switcheroo_client_probe_defer()
358 * shall be called to ensure that all prerequisites are met.
359 *
360 * Return: 0 on success, -ENOMEM on memory allocation error, -EINVAL on getting
361 * client id error.
362 */
363 int vga_switcheroo_register_audio_client(struct pci_dev *pdev,
364 const struct vga_switcheroo_client_ops *ops,
365 struct pci_dev *vga_dev)
366 {
367 enum vga_switcheroo_client_id id = VGA_SWITCHEROO_UNKNOWN_ID;
369 /*
370 * if vga_switcheroo has enabled, that mean two GPU clients and also
371 * handler are registered. Get audio client id from bound GPU client
372 * id directly, otherwise, set it as VGA_SWITCHEROO_UNKNOWN_ID,
373 * it will set to correct id in later when vga_switcheroo_enable()
374 * is called.
375 */
376 mutex_lock(&vgasr_mutex);
377 if (vgasr_priv.active) {
378 id = vgasr_priv.handler->get_client_id(vga_dev);
379 if (id < 0) {
380 mutex_unlock(&vgasr_mutex);
381 return -EINVAL;
382 }
383 }
384 mutex_unlock(&vgasr_mutex);
386 return register_client(pdev, ops, id | ID_BIT_AUDIO, vga_dev,
387 false, true);
388 }
389 EXPORT_SYMBOL(vga_switcheroo_register_audio_client);
391 static struct vga_switcheroo_client *
392 find_client_from_pci(struct list_head *head, struct pci_dev *pdev)
393 {
394 struct vga_switcheroo_client *client;
396 list_for_each_entry(client, head, list)
397 if (client->pdev == pdev)
398 return client;
399 return NULL;
400 }
402 static struct vga_switcheroo_client *
403 find_client_from_id(struct list_head *head,
404 enum vga_switcheroo_client_id client_id)
405 {
406 struct vga_switcheroo_client *client;
408 list_for_each_entry(client, head, list)
409 if (client->id == client_id)
410 return client;
411 return NULL;
412 }
414 static struct vga_switcheroo_client *
415 find_active_client(struct list_head *head)
416 {
417 struct vga_switcheroo_client *client;
419 list_for_each_entry(client, head, list)
420 if (client->active)
421 return client;
422 return NULL;
423 }
425 /**
426 * vga_switcheroo_client_probe_defer() - whether to defer probing a given client
427 * @pdev: client pci device
428 *
429 * Determine whether any prerequisites are not fulfilled to probe a given
430 * client. Drivers shall invoke this early on in their ->probe callback
431 * and return %-EPROBE_DEFER if it evaluates to %true. Thou shalt not
432 * register the client ere thou hast called this.
433 *
434 * Return: %true if probing should be deferred, otherwise %false.
435 */
436 bool vga_switcheroo_client_probe_defer(struct pci_dev *pdev)
437 {
438 if ((pdev->class >> 16) == PCI_BASE_CLASS_DISPLAY) {
439 /*
440 * apple-gmux is needed on pre-retina MacBook Pro
441 * to probe the panel if pdev is the inactive GPU.
442 */
443 if (apple_gmux_present() && pdev != vga_default_device() &&
444 !vgasr_priv.handler_flags)
445 return true;
446 }
448 return false;
449 }
450 EXPORT_SYMBOL(vga_switcheroo_client_probe_defer);
452 static enum vga_switcheroo_state
453 vga_switcheroo_pwr_state(struct vga_switcheroo_client *client)
454 {
455 if (client->driver_power_control)
456 if (pm_runtime_enabled(&client->pdev->dev) &&
457 pm_runtime_active(&client->pdev->dev))
458 return VGA_SWITCHEROO_ON;
459 else
460 return VGA_SWITCHEROO_OFF;
461 else
462 return client->pwr_state;
463 }
465 /**
466 * vga_switcheroo_get_client_state() - obtain power state of a given client
467 * @pdev: client pci device
468 *
469 * Obtain power state of a given client as seen from vga_switcheroo.
470 * The function is only called from hda_intel.c.
471 *
472 * Return: Power state.
473 */
474 enum vga_switcheroo_state vga_switcheroo_get_client_state(struct pci_dev *pdev)
475 {
476 struct vga_switcheroo_client *client;
477 enum vga_switcheroo_state ret;
479 mutex_lock(&vgasr_mutex);
480 client = find_client_from_pci(&vgasr_priv.clients, pdev);
481 if (!client)
482 ret = VGA_SWITCHEROO_NOT_FOUND;
483 else
484 ret = vga_switcheroo_pwr_state(client);
485 mutex_unlock(&vgasr_mutex);
486 return ret;
487 }
488 EXPORT_SYMBOL(vga_switcheroo_get_client_state);
490 /**
491 * vga_switcheroo_unregister_client() - unregister client
492 * @pdev: client pci device
493 *
494 * Unregister client. Disable vga_switcheroo if this is a vga client (GPU).
495 */
496 void vga_switcheroo_unregister_client(struct pci_dev *pdev)
497 {
498 struct vga_switcheroo_client *client;
500 mutex_lock(&vgasr_mutex);
501 client = find_client_from_pci(&vgasr_priv.clients, pdev);
502 if (client) {
503 if (client_is_vga(client))
504 vgasr_priv.registered_clients--;
505 list_del(&client->list);
506 kfree(client);
507 }
508 if (vgasr_priv.active && vgasr_priv.registered_clients < 2) {
509 pr_info("disabled\n");
510 vga_switcheroo_debugfs_fini(&vgasr_priv);
511 vgasr_priv.active = false;
512 }
513 mutex_unlock(&vgasr_mutex);
514 }
515 EXPORT_SYMBOL(vga_switcheroo_unregister_client);
517 /**
518 * vga_switcheroo_client_fb_set() - set framebuffer of a given client
519 * @pdev: client pci device
520 * @info: framebuffer
521 *
522 * Set framebuffer of a given client. The console will be remapped to this
523 * on switching.
524 */
525 void vga_switcheroo_client_fb_set(struct pci_dev *pdev,
526 struct fb_info *info)
527 {
528 struct vga_switcheroo_client *client;
530 mutex_lock(&vgasr_mutex);
531 client = find_client_from_pci(&vgasr_priv.clients, pdev);
532 if (client)
533 client->fb_info = info;
534 mutex_unlock(&vgasr_mutex);
535 }
536 EXPORT_SYMBOL(vga_switcheroo_client_fb_set);
538 /**
539 * vga_switcheroo_lock_ddc() - temporarily switch DDC lines to a given client
540 * @pdev: client pci device
541 *
542 * Temporarily switch DDC lines to the client identified by @pdev
543 * (but leave the outputs otherwise switched to where they are).
544 * This allows the inactive client to probe EDID. The DDC lines must
545 * afterwards be switched back by calling vga_switcheroo_unlock_ddc(),
546 * even if this function returns an error.
547 *
548 * Return: Previous DDC owner on success or a negative int on error.
549 * Specifically, %-ENODEV if no handler has registered or if the handler
550 * does not support switching the DDC lines. Also, a negative value
551 * returned by the handler is propagated back to the caller.
552 * The return value has merely an informational purpose for any caller
553 * which might be interested in it. It is acceptable to ignore the return
554 * value and simply rely on the result of the subsequent EDID probe,
555 * which will be %NULL if DDC switching failed.
556 */
557 int vga_switcheroo_lock_ddc(struct pci_dev *pdev)
558 {
559 enum vga_switcheroo_client_id id;
561 mutex_lock(&vgasr_priv.mux_hw_lock);
562 if (!vgasr_priv.handler || !vgasr_priv.handler->switch_ddc) {
563 vgasr_priv.old_ddc_owner = -ENODEV;
564 return -ENODEV;
565 }
567 id = vgasr_priv.handler->get_client_id(pdev);
568 vgasr_priv.old_ddc_owner = vgasr_priv.handler->switch_ddc(id);
569 return vgasr_priv.old_ddc_owner;
570 }
571 EXPORT_SYMBOL(vga_switcheroo_lock_ddc);
573 /**
574 * vga_switcheroo_unlock_ddc() - switch DDC lines back to previous owner
575 * @pdev: client pci device
576 *
577 * Switch DDC lines back to the previous owner after calling
578 * vga_switcheroo_lock_ddc(). This must be called even if
579 * vga_switcheroo_lock_ddc() returned an error.
580 *
581 * Return: Previous DDC owner on success (i.e. the client identifier of @pdev)
582 * or a negative int on error.
583 * Specifically, %-ENODEV if no handler has registered or if the handler
584 * does not support switching the DDC lines. Also, a negative value
585 * returned by the handler is propagated back to the caller.
586 * Finally, invoking this function without calling vga_switcheroo_lock_ddc()
587 * first is not allowed and will result in %-EINVAL.
588 */
589 int vga_switcheroo_unlock_ddc(struct pci_dev *pdev)
590 {
591 enum vga_switcheroo_client_id id;
592 int ret = vgasr_priv.old_ddc_owner;
594 if (WARN_ON_ONCE(!mutex_is_locked(&vgasr_priv.mux_hw_lock)))
595 return -EINVAL;
597 if (vgasr_priv.old_ddc_owner >= 0) {
598 id = vgasr_priv.handler->get_client_id(pdev);
599 if (vgasr_priv.old_ddc_owner != id)
600 ret = vgasr_priv.handler->switch_ddc(
601 vgasr_priv.old_ddc_owner);
602 }
603 mutex_unlock(&vgasr_priv.mux_hw_lock);
604 return ret;
605 }
606 EXPORT_SYMBOL(vga_switcheroo_unlock_ddc);
608 /**
609 * DOC: Manual switching and manual power control
610 *
611 * In this mode of use, the file /sys/kernel/debug/vgaswitcheroo/switch
612 * can be read to retrieve the current vga_switcheroo state and commands
613 * can be written to it to change the state. The file appears as soon as
614 * two GPU drivers and one handler have registered with vga_switcheroo.
615 * The following commands are understood:
616 *
617 * * OFF: Power off the device not in use.
618 * * ON: Power on the device not in use.
619 * * IGD: Switch to the integrated graphics device.
620 * Power on the integrated GPU if necessary, power off the discrete GPU.
621 * Prerequisite is that no user space processes (e.g. Xorg, alsactl)
622 * have opened device files of the GPUs or the audio client. If the
623 * switch fails, the user may invoke lsof(8) or fuser(1) on /dev/dri/
624 * and /dev/snd/controlC1 to identify processes blocking the switch.
625 * * DIS: Switch to the discrete graphics device.
626 * * DIGD: Delayed switch to the integrated graphics device.
627 * This will perform the switch once the last user space process has
628 * closed the device files of the GPUs and the audio client.
629 * * DDIS: Delayed switch to the discrete graphics device.
630 * * MIGD: Mux-only switch to the integrated graphics device.
631 * Does not remap console or change the power state of either gpu.
632 * If the integrated GPU is currently off, the screen will turn black.
633 * If it is on, the screen will show whatever happens to be in VRAM.
634 * Either way, the user has to blindly enter the command to switch back.
635 * * MDIS: Mux-only switch to the discrete graphics device.
636 *
637 * For GPUs whose power state is controlled by the driver's runtime pm,
638 * the ON and OFF commands are a no-op (see next section).
639 *
640 * For muxless machines, the IGD/DIS, DIGD/DDIS and MIGD/MDIS commands
641 * should not be used.
642 */
644 static int vga_switcheroo_show(struct seq_file *m, void *v)
645 {
646 struct vga_switcheroo_client *client;
647 int i = 0;
649 mutex_lock(&vgasr_mutex);
650 list_for_each_entry(client, &vgasr_priv.clients, list) {
651 seq_printf(m, "%d:%s%s:%c:%s%s:%s\n", i,
652 client_id(client) == VGA_SWITCHEROO_DIS ? "DIS" :
653 "IGD",
654 client_is_vga(client) ? "" : "-Audio",
655 client->active ? '+' : ' ',
656 client->driver_power_control ? "Dyn" : "",
657 vga_switcheroo_pwr_state(client) ? "Pwr" : "Off",
658 pci_name(client->pdev));
659 i++;
660 }
661 mutex_unlock(&vgasr_mutex);
662 return 0;
663 }
665 static int vga_switcheroo_debugfs_open(struct inode *inode, struct file *file)
666 {
667 return single_open(file, vga_switcheroo_show, NULL);
668 }
670 static int vga_switchon(struct vga_switcheroo_client *client)
671 {
672 if (client->driver_power_control)
673 return 0;
674 if (vgasr_priv.handler->power_state)
675 vgasr_priv.handler->power_state(client->id, VGA_SWITCHEROO_ON);
676 /* call the driver callback to turn on device */
677 client->ops->set_gpu_state(client->pdev, VGA_SWITCHEROO_ON);
678 client->pwr_state = VGA_SWITCHEROO_ON;
679 return 0;
680 }
682 static int vga_switchoff(struct vga_switcheroo_client *client)
683 {
684 if (client->driver_power_control)
685 return 0;
686 /* call the driver callback to turn off device */
687 client->ops->set_gpu_state(client->pdev, VGA_SWITCHEROO_OFF);
688 if (vgasr_priv.handler->power_state)
689 vgasr_priv.handler->power_state(client->id, VGA_SWITCHEROO_OFF);
690 client->pwr_state = VGA_SWITCHEROO_OFF;
691 return 0;
692 }
694 static void set_audio_state(enum vga_switcheroo_client_id id,
695 enum vga_switcheroo_state state)
696 {
697 struct vga_switcheroo_client *client;
699 client = find_client_from_id(&vgasr_priv.clients, id | ID_BIT_AUDIO);
700 if (client)
701 client->ops->set_gpu_state(client->pdev, state);
702 }
704 /* stage one happens before delay */
705 static int vga_switchto_stage1(struct vga_switcheroo_client *new_client)
706 {
707 struct vga_switcheroo_client *active;
709 active = find_active_client(&vgasr_priv.clients);
710 if (!active)
711 return 0;
713 if (vga_switcheroo_pwr_state(new_client) == VGA_SWITCHEROO_OFF)
714 vga_switchon(new_client);
716 vga_set_default_device(new_client->pdev);
717 return 0;
718 }
720 /* post delay */
721 static int vga_switchto_stage2(struct vga_switcheroo_client *new_client)
722 {
723 int ret;
724 struct vga_switcheroo_client *active;
726 active = find_active_client(&vgasr_priv.clients);
727 if (!active)
728 return 0;
730 active->active = false;
732 /* let HDA controller autosuspend if GPU uses driver power control */
733 if (!active->driver_power_control)
734 set_audio_state(active->id, VGA_SWITCHEROO_OFF);
736 if (new_client->fb_info) {
737 struct fb_event event;
739 console_lock();
740 event.info = new_client->fb_info;
741 fb_notifier_call_chain(FB_EVENT_REMAP_ALL_CONSOLE, &event);
742 console_unlock();
743 }
745 mutex_lock(&vgasr_priv.mux_hw_lock);
746 ret = vgasr_priv.handler->switchto(new_client->id);
747 mutex_unlock(&vgasr_priv.mux_hw_lock);
748 if (ret)
749 return ret;
751 if (new_client->ops->reprobe)
752 new_client->ops->reprobe(new_client->pdev);
754 if (vga_switcheroo_pwr_state(active) == VGA_SWITCHEROO_ON)
755 vga_switchoff(active);
757 /* let HDA controller autoresume if GPU uses driver power control */
758 if (!new_client->driver_power_control)
759 set_audio_state(new_client->id, VGA_SWITCHEROO_ON);
761 new_client->active = true;
762 return 0;
763 }
765 static bool check_can_switch(void)
766 {
767 struct vga_switcheroo_client *client;
769 list_for_each_entry(client, &vgasr_priv.clients, list) {
770 if (!client->ops->can_switch(client->pdev)) {
771 pr_err("client %x refused switch\n", client->id);
772 return false;
773 }
774 }
775 return true;
776 }
778 static ssize_t
779 vga_switcheroo_debugfs_write(struct file *filp, const char __user *ubuf,
780 size_t cnt, loff_t *ppos)
781 {
782 char usercmd[64];
783 int ret;
784 bool delay = false, can_switch;
785 bool just_mux = false;
786 enum vga_switcheroo_client_id client_id = VGA_SWITCHEROO_UNKNOWN_ID;
787 struct vga_switcheroo_client *client = NULL;
789 if (cnt > 63)
790 cnt = 63;
792 if (copy_from_user(usercmd, ubuf, cnt))
793 return -EFAULT;
795 mutex_lock(&vgasr_mutex);
797 if (!vgasr_priv.active) {
798 cnt = -EINVAL;
799 goto out;
800 }
802 /* pwr off the device not in use */
803 if (strncmp(usercmd, "OFF", 3) == 0) {
804 list_for_each_entry(client, &vgasr_priv.clients, list) {
805 if (client->active || client_is_audio(client))
806 continue;
807 if (client->driver_power_control)
808 continue;
809 set_audio_state(client->id, VGA_SWITCHEROO_OFF);
810 if (client->pwr_state == VGA_SWITCHEROO_ON)
811 vga_switchoff(client);
812 }
813 goto out;
814 }
815 /* pwr on the device not in use */
816 if (strncmp(usercmd, "ON", 2) == 0) {
817 list_for_each_entry(client, &vgasr_priv.clients, list) {
818 if (client->active || client_is_audio(client))
819 continue;
820 if (client->driver_power_control)
821 continue;
822 if (client->pwr_state == VGA_SWITCHEROO_OFF)
823 vga_switchon(client);
824 set_audio_state(client->id, VGA_SWITCHEROO_ON);
825 }
826 goto out;
827 }
829 /* request a delayed switch - test can we switch now */
830 if (strncmp(usercmd, "DIGD", 4) == 0) {
831 client_id = VGA_SWITCHEROO_IGD;
832 delay = true;
833 }
835 if (strncmp(usercmd, "DDIS", 4) == 0) {
836 client_id = VGA_SWITCHEROO_DIS;
837 delay = true;
838 }
840 if (strncmp(usercmd, "IGD", 3) == 0)
841 client_id = VGA_SWITCHEROO_IGD;
843 if (strncmp(usercmd, "DIS", 3) == 0)
844 client_id = VGA_SWITCHEROO_DIS;
846 if (strncmp(usercmd, "MIGD", 4) == 0) {
847 just_mux = true;
848 client_id = VGA_SWITCHEROO_IGD;
849 }
850 if (strncmp(usercmd, "MDIS", 4) == 0) {
851 just_mux = true;
852 client_id = VGA_SWITCHEROO_DIS;
853 }
855 if (client_id == VGA_SWITCHEROO_UNKNOWN_ID)
856 goto out;
857 client = find_client_from_id(&vgasr_priv.clients, client_id);
858 if (!client)
859 goto out;
861 vgasr_priv.delayed_switch_active = false;
863 if (just_mux) {
864 mutex_lock(&vgasr_priv.mux_hw_lock);
865 ret = vgasr_priv.handler->switchto(client_id);
866 mutex_unlock(&vgasr_priv.mux_hw_lock);
867 goto out;
868 }
870 if (client->active)
871 goto out;
873 /* okay we want a switch - test if devices are willing to switch */
874 can_switch = check_can_switch();
876 if (can_switch == false && delay == false)
877 goto out;
879 if (can_switch) {
880 ret = vga_switchto_stage1(client);
881 if (ret)
882 pr_err("switching failed stage 1 %d\n", ret);
884 ret = vga_switchto_stage2(client);
885 if (ret)
886 pr_err("switching failed stage 2 %d\n", ret);
888 } else {
889 pr_info("setting delayed switch to client %d\n", client->id);
890 vgasr_priv.delayed_switch_active = true;
891 vgasr_priv.delayed_client_id = client_id;
893 ret = vga_switchto_stage1(client);
894 if (ret)
895 pr_err("delayed switching stage 1 failed %d\n", ret);
896 }
898 out:
899 mutex_unlock(&vgasr_mutex);
900 return cnt;
901 }
903 static const struct file_operations vga_switcheroo_debugfs_fops = {
904 .owner = THIS_MODULE,
905 .open = vga_switcheroo_debugfs_open,
906 .write = vga_switcheroo_debugfs_write,
907 .read = seq_read,
908 .llseek = seq_lseek,
909 .release = single_release,
910 };
912 static void vga_switcheroo_debugfs_fini(struct vgasr_priv *priv)
913 {
914 debugfs_remove(priv->switch_file);
915 priv->switch_file = NULL;
917 debugfs_remove(priv->debugfs_root);
918 priv->debugfs_root = NULL;
919 }
921 static int vga_switcheroo_debugfs_init(struct vgasr_priv *priv)
922 {
923 static const char mp[] = "/sys/kernel/debug";
925 /* already initialised */
926 if (priv->debugfs_root)
927 return 0;
928 priv->debugfs_root = debugfs_create_dir("vgaswitcheroo", NULL);
930 if (!priv->debugfs_root) {
931 pr_err("Cannot create %s/vgaswitcheroo\n", mp);
932 goto fail;
933 }
935 priv->switch_file = debugfs_create_file("switch", 0644,
936 priv->debugfs_root, NULL,
937 &vga_switcheroo_debugfs_fops);
938 if (!priv->switch_file) {
939 pr_err("cannot create %s/vgaswitcheroo/switch\n", mp);
940 goto fail;
941 }
942 return 0;
943 fail:
944 vga_switcheroo_debugfs_fini(priv);
945 return -1;
946 }
948 /**
949 * vga_switcheroo_process_delayed_switch() - helper for delayed switching
950 *
951 * Process a delayed switch if one is pending. DRM drivers should call this
952 * from their ->lastclose callback.
953 *
954 * Return: 0 on success. -EINVAL if no delayed switch is pending, if the client
955 * has unregistered in the meantime or if there are other clients blocking the
956 * switch. If the actual switch fails, an error is reported and 0 is returned.
957 */
958 int vga_switcheroo_process_delayed_switch(void)
959 {
960 struct vga_switcheroo_client *client;
961 int ret;
962 int err = -EINVAL;
964 mutex_lock(&vgasr_mutex);
965 if (!vgasr_priv.delayed_switch_active)
966 goto err;
968 pr_info("processing delayed switch to %d\n",
969 vgasr_priv.delayed_client_id);
971 client = find_client_from_id(&vgasr_priv.clients,
972 vgasr_priv.delayed_client_id);
973 if (!client || !check_can_switch())
974 goto err;
976 ret = vga_switchto_stage2(client);
977 if (ret)
978 pr_err("delayed switching failed stage 2 %d\n", ret);
980 vgasr_priv.delayed_switch_active = false;
981 err = 0;
982 err:
983 mutex_unlock(&vgasr_mutex);
984 return err;
985 }
986 EXPORT_SYMBOL(vga_switcheroo_process_delayed_switch);
988 /**
989 * DOC: Driver power control
990 *
991 * In this mode of use, the discrete GPU automatically powers up and down at
992 * the discretion of the driver's runtime pm. On muxed machines, the user may
993 * still influence the muxer state by way of the debugfs interface, however
994 * the ON and OFF commands become a no-op for the discrete GPU.
995 *
996 * This mode is the default on Nvidia HybridPower/Optimus and ATI PowerXpress.
997 * Specifying nouveau.runpm=0, radeon.runpm=0 or amdgpu.runpm=0 on the kernel
998 * command line disables it.
999 *
1000 * After the GPU has been suspended, the handler needs to be called to cut
1001 * power to the GPU. Likewise it needs to reinstate power before the GPU
1002 * can resume. This is achieved by vga_switcheroo_init_domain_pm_ops(),
1003 * which augments the GPU's suspend/resume functions by the requisite
1004 * calls to the handler.
1005 *
1006 * When the audio device resumes, the GPU needs to be woken. This is achieved
1007 * by a PCI quirk which calls device_link_add() to declare a dependency on the
1008 * GPU. That way, the GPU is kept awake whenever and as long as the audio
1009 * device is in use.
1010 *
1011 * On muxed machines, if the mux is initially switched to the discrete GPU,
1012 * the user ends up with a black screen when the GPU powers down after boot.
1013 * As a workaround, the mux is forced to the integrated GPU on runtime suspend,
1014 * cf. https://bugs.freedesktop.org/show_bug.cgi?id=75917
1015 */
1017 static void vga_switcheroo_power_switch(struct pci_dev *pdev,
1018 enum vga_switcheroo_state state)
1019 {
1020 struct vga_switcheroo_client *client;
1022 if (!vgasr_priv.handler->power_state)
1023 return;
1025 client = find_client_from_pci(&vgasr_priv.clients, pdev);
1026 if (!client)
1027 return;
1029 if (!client->driver_power_control)
1030 return;
1032 vgasr_priv.handler->power_state(client->id, state);
1033 }
1035 /* switcheroo power domain */
1036 static int vga_switcheroo_runtime_suspend(struct device *dev)
1037 {
1038 struct pci_dev *pdev = to_pci_dev(dev);
1039 int ret;
1041 ret = dev->bus->pm->runtime_suspend(dev);
1042 if (ret)
1043 return ret;
1044 mutex_lock(&vgasr_mutex);
1045 if (vgasr_priv.handler->switchto) {
1046 mutex_lock(&vgasr_priv.mux_hw_lock);
1047 vgasr_priv.handler->switchto(VGA_SWITCHEROO_IGD);
1048 mutex_unlock(&vgasr_priv.mux_hw_lock);
1049 }
1050 pci_bus_set_current_state(pdev->bus, PCI_D3cold);
1051 vga_switcheroo_power_switch(pdev, VGA_SWITCHEROO_OFF);
1052 mutex_unlock(&vgasr_mutex);
1053 return 0;
1054 }
1056 static int vga_switcheroo_runtime_resume(struct device *dev)
1057 {
1058 struct pci_dev *pdev = to_pci_dev(dev);
1059 int ret;
1061 mutex_lock(&vgasr_mutex);
1062 vga_switcheroo_power_switch(pdev, VGA_SWITCHEROO_ON);
1063 mutex_unlock(&vgasr_mutex);
1064 pci_wakeup_bus(pdev->bus);
1065 ret = dev->bus->pm->runtime_resume(dev);
1066 if (ret)
1067 return ret;
1069 return 0;
1070 }
1072 /**
1073 * vga_switcheroo_init_domain_pm_ops() - helper for driver power control
1074 * @dev: vga client device
1075 * @domain: power domain
1076 *
1077 * Helper for GPUs whose power state is controlled by the driver's runtime pm.
1078 * After the GPU has been suspended, the handler needs to be called to cut
1079 * power to the GPU. Likewise it needs to reinstate power before the GPU
1080 * can resume. To this end, this helper augments the suspend/resume functions
1081 * by the requisite calls to the handler. It needs only be called on platforms
1082 * where the power switch is separate to the device being powered down.
1083 */
1084 int vga_switcheroo_init_domain_pm_ops(struct device *dev,
1085 struct dev_pm_domain *domain)
1086 {
1087 /* copy over all the bus versions */
1088 if (dev->bus && dev->bus->pm) {
1089 domain->ops = *dev->bus->pm;
1090 domain->ops.runtime_suspend = vga_switcheroo_runtime_suspend;
1091 domain->ops.runtime_resume = vga_switcheroo_runtime_resume;
1093 dev_pm_domain_set(dev, domain);
1094 return 0;
1095 }
1096 dev_pm_domain_set(dev, NULL);
1097 return -EINVAL;
1098 }
1099 EXPORT_SYMBOL(vga_switcheroo_init_domain_pm_ops);
1101 void vga_switcheroo_fini_domain_pm_ops(struct device *dev)
1102 {
1103 dev_pm_domain_set(dev, NULL);
1104 }
1105 EXPORT_SYMBOL(vga_switcheroo_fini_domain_pm_ops);