1 // SPDX-License-Identifier: GPL-2.0 OR Linux-OpenIB
2 /*
3 * Copyright (c) 2017, Mellanox Technologies inc. All rights reserved.
4 */
5 #include <rdma/uverbs_ioctl.h>
6 #include <rdma/rdma_user_ioctl.h>
7 #include <linux/bitops.h>
8 #include "rdma_core.h"
9 #include "uverbs.h"
11 static void *uapi_add_elm(struct uverbs_api *uapi, u32 key, size_t alloc_size)
12 {
13 void *elm;
14 int rc;
16 if (key == UVERBS_API_KEY_ERR)
17 return ERR_PTR(-EOVERFLOW);
19 elm = kzalloc(alloc_size, GFP_KERNEL);
20 rc = radix_tree_insert(&uapi->radix, key, elm);
21 if (rc) {
22 kfree(elm);
23 return ERR_PTR(rc);
24 }
26 return elm;
27 }
29 static int uapi_merge_method(struct uverbs_api *uapi,
30 struct uverbs_api_object *obj_elm, u32 obj_key,
31 const struct uverbs_method_def *method,
32 bool is_driver)
33 {
34 u32 method_key = obj_key | uapi_key_ioctl_method(method->id);
35 struct uverbs_api_ioctl_method *method_elm;
36 unsigned int i;
38 if (!method->attrs)
39 return 0;
41 method_elm = uapi_add_elm(uapi, method_key, sizeof(*method_elm));
42 if (IS_ERR(method_elm)) {
43 if (method_elm != ERR_PTR(-EEXIST))
44 return PTR_ERR(method_elm);
46 /*
47 * This occurs when a driver uses ADD_UVERBS_ATTRIBUTES_SIMPLE
48 */
49 if (WARN_ON(method->handler))
50 return -EINVAL;
51 method_elm = radix_tree_lookup(&uapi->radix, method_key);
52 if (WARN_ON(!method_elm))
53 return -EINVAL;
54 } else {
55 WARN_ON(!method->handler);
56 rcu_assign_pointer(method_elm->handler, method->handler);
57 if (method->handler != uverbs_destroy_def_handler)
58 method_elm->driver_method = is_driver;
59 }
61 for (i = 0; i != method->num_attrs; i++) {
62 const struct uverbs_attr_def *attr = (*method->attrs)[i];
63 struct uverbs_api_attr *attr_slot;
65 if (!attr)
66 continue;
68 /*
69 * ENUM_IN contains the 'ids' pointer to the driver's .rodata,
70 * so if it is specified by a driver then it always makes this
71 * into a driver method.
72 */
73 if (attr->attr.type == UVERBS_ATTR_TYPE_ENUM_IN)
74 method_elm->driver_method |= is_driver;
76 attr_slot =
77 uapi_add_elm(uapi, method_key | uapi_key_attr(attr->id),
78 sizeof(*attr_slot));
79 /* Attributes are not allowed to be modified by drivers */
80 if (IS_ERR(attr_slot))
81 return PTR_ERR(attr_slot);
83 attr_slot->spec = attr->attr;
84 }
86 return 0;
87 }
89 static int uapi_merge_tree(struct uverbs_api *uapi,
90 const struct uverbs_object_tree_def *tree,
91 bool is_driver)
92 {
93 unsigned int i, j;
94 int rc;
96 if (!tree->objects)
97 return 0;
99 for (i = 0; i != tree->num_objects; i++) {
100 const struct uverbs_object_def *obj = (*tree->objects)[i];
101 struct uverbs_api_object *obj_elm;
102 u32 obj_key;
104 if (!obj)
105 continue;
107 obj_key = uapi_key_obj(obj->id);
108 obj_elm = uapi_add_elm(uapi, obj_key, sizeof(*obj_elm));
109 if (IS_ERR(obj_elm)) {
110 if (obj_elm != ERR_PTR(-EEXIST))
111 return PTR_ERR(obj_elm);
113 /* This occurs when a driver uses ADD_UVERBS_METHODS */
114 if (WARN_ON(obj->type_attrs))
115 return -EINVAL;
116 obj_elm = radix_tree_lookup(&uapi->radix, obj_key);
117 if (WARN_ON(!obj_elm))
118 return -EINVAL;
119 } else {
120 obj_elm->type_attrs = obj->type_attrs;
121 if (obj->type_attrs) {
122 obj_elm->type_class =
123 obj->type_attrs->type_class;
124 /*
125 * Today drivers are only permitted to use
126 * idr_class types. They cannot use FD types
127 * because we currently have no way to revoke
128 * the fops pointer after device
129 * disassociation.
130 */
131 if (WARN_ON(is_driver &&
132 obj->type_attrs->type_class !=
133 &uverbs_idr_class))
134 return -EINVAL;
135 }
136 }
138 if (!obj->methods)
139 continue;
141 for (j = 0; j != obj->num_methods; j++) {
142 const struct uverbs_method_def *method =
143 (*obj->methods)[j];
144 if (!method)
145 continue;
147 rc = uapi_merge_method(uapi, obj_elm, obj_key, method,
148 is_driver);
149 if (rc)
150 return rc;
151 }
152 }
154 return 0;
155 }
157 static int
158 uapi_finalize_ioctl_method(struct uverbs_api *uapi,
159 struct uverbs_api_ioctl_method *method_elm,
160 u32 method_key)
161 {
162 struct radix_tree_iter iter;
163 unsigned int num_attrs = 0;
164 unsigned int max_bkey = 0;
165 bool single_uobj = false;
166 void __rcu **slot;
168 method_elm->destroy_bkey = UVERBS_API_ATTR_BKEY_LEN;
169 radix_tree_for_each_slot (slot, &uapi->radix, &iter,
170 uapi_key_attrs_start(method_key)) {
171 struct uverbs_api_attr *elm =
172 rcu_dereference_protected(*slot, true);
173 u32 attr_key = iter.index & UVERBS_API_ATTR_KEY_MASK;
174 u32 attr_bkey = uapi_bkey_attr(attr_key);
175 u8 type = elm->spec.type;
177 if (uapi_key_attr_to_method(iter.index) !=
178 uapi_key_attr_to_method(method_key))
179 break;
181 if (elm->spec.mandatory)
182 __set_bit(attr_bkey, method_elm->attr_mandatory);
184 if (type == UVERBS_ATTR_TYPE_IDR ||
185 type == UVERBS_ATTR_TYPE_FD) {
186 u8 access = elm->spec.u.obj.access;
188 /*
189 * Verbs specs may only have one NEW/DESTROY, we don't
190 * have the infrastructure to abort multiple NEW's or
191 * cope with multiple DESTROY failure.
192 */
193 if (access == UVERBS_ACCESS_NEW ||
194 access == UVERBS_ACCESS_DESTROY) {
195 if (WARN_ON(single_uobj))
196 return -EINVAL;
198 single_uobj = true;
199 if (WARN_ON(!elm->spec.mandatory))
200 return -EINVAL;
201 }
203 if (access == UVERBS_ACCESS_DESTROY)
204 method_elm->destroy_bkey = attr_bkey;
205 }
207 max_bkey = max(max_bkey, attr_bkey);
208 num_attrs++;
209 }
211 method_elm->key_bitmap_len = max_bkey + 1;
212 WARN_ON(method_elm->key_bitmap_len > UVERBS_API_ATTR_BKEY_LEN);
214 uapi_compute_bundle_size(method_elm, num_attrs);
215 return 0;
216 }
218 static int uapi_finalize(struct uverbs_api *uapi)
219 {
220 struct radix_tree_iter iter;
221 void __rcu **slot;
222 int rc;
224 radix_tree_for_each_slot (slot, &uapi->radix, &iter, 0) {
225 struct uverbs_api_ioctl_method *method_elm =
226 rcu_dereference_protected(*slot, true);
228 if (uapi_key_is_ioctl_method(iter.index)) {
229 rc = uapi_finalize_ioctl_method(uapi, method_elm,
230 iter.index);
231 if (rc)
232 return rc;
233 }
234 }
236 return 0;
237 }
239 void uverbs_destroy_api(struct uverbs_api *uapi)
240 {
241 struct radix_tree_iter iter;
242 void __rcu **slot;
244 if (!uapi)
245 return;
247 radix_tree_for_each_slot (slot, &uapi->radix, &iter, 0) {
248 kfree(rcu_dereference_protected(*slot, true));
249 radix_tree_iter_delete(&uapi->radix, &iter, slot);
250 }
251 kfree(uapi);
252 }
254 struct uverbs_api *uverbs_alloc_api(
255 const struct uverbs_object_tree_def *const *driver_specs,
256 enum rdma_driver_id driver_id)
257 {
258 struct uverbs_api *uapi;
259 int rc;
261 uapi = kzalloc(sizeof(*uapi), GFP_KERNEL);
262 if (!uapi)
263 return ERR_PTR(-ENOMEM);
265 INIT_RADIX_TREE(&uapi->radix, GFP_KERNEL);
266 uapi->driver_id = driver_id;
268 rc = uapi_merge_tree(uapi, uverbs_default_get_objects(), false);
269 if (rc)
270 goto err;
272 for (; driver_specs && *driver_specs; driver_specs++) {
273 rc = uapi_merge_tree(uapi, *driver_specs, true);
274 if (rc)
275 goto err;
276 }
278 rc = uapi_finalize(uapi);
279 if (rc)
280 goto err;
282 return uapi;
283 err:
284 if (rc != -ENOMEM)
285 pr_err("Setup of uverbs_api failed, kernel parsing tree description is not valid (%d)??\n",
286 rc);
288 uverbs_destroy_api(uapi);
289 return ERR_PTR(rc);
290 }
292 /*
293 * The pre version is done before destroying the HW objects, it only blocks
294 * off method access. All methods that require the ib_dev or the module data
295 * must test one of these assignments prior to continuing.
296 */
297 void uverbs_disassociate_api_pre(struct ib_uverbs_device *uverbs_dev)
298 {
299 struct uverbs_api *uapi = uverbs_dev->uapi;
300 struct radix_tree_iter iter;
301 void __rcu **slot;
303 rcu_assign_pointer(uverbs_dev->ib_dev, NULL);
305 radix_tree_for_each_slot (slot, &uapi->radix, &iter, 0) {
306 if (uapi_key_is_ioctl_method(iter.index)) {
307 struct uverbs_api_ioctl_method *method_elm =
308 rcu_dereference_protected(*slot, true);
310 if (method_elm->driver_method)
311 rcu_assign_pointer(method_elm->handler, NULL);
312 }
313 }
315 synchronize_srcu(&uverbs_dev->disassociate_srcu);
316 }
318 /*
319 * Called when a driver disassociates from the ib_uverbs_device. The
320 * assumption is that the driver module will unload after. Replace everything
321 * related to the driver with NULL as a safety measure.
322 */
323 void uverbs_disassociate_api(struct uverbs_api *uapi)
324 {
325 struct radix_tree_iter iter;
326 void __rcu **slot;
328 radix_tree_for_each_slot (slot, &uapi->radix, &iter, 0) {
329 if (uapi_key_is_object(iter.index)) {
330 struct uverbs_api_object *object_elm =
331 rcu_dereference_protected(*slot, true);
333 /*
334 * Some type_attrs are in the driver module. We don't
335 * bother to keep track of which since there should be
336 * no use of this after disassociate.
337 */
338 object_elm->type_attrs = NULL;
339 } else if (uapi_key_is_attr(iter.index)) {
340 struct uverbs_api_attr *elm =
341 rcu_dereference_protected(*slot, true);
343 if (elm->spec.type == UVERBS_ATTR_TYPE_ENUM_IN)
344 elm->spec.u2.enum_def.ids = NULL;
345 }
346 }
347 }