mmc: omap_hsmmc: use the generic config for omap2plus devices
[rpmsg/rpmsg.git] / drivers / mmc / host / Kconfig
1 #
2 # MMC/SD host controller drivers
3 #
5 comment "MMC/SD/SDIO Host Controller Drivers"
7 config MMC_ARMMMCI
8         tristate "ARM AMBA Multimedia Card Interface support"
9         depends on ARM_AMBA
10         help
11           This selects the ARM(R) AMBA(R) PrimeCell Multimedia Card
12           Interface (PL180 and PL181) support.  If you have an ARM(R)
13           platform with a Multimedia Card slot, say Y or M here.
15           If unsure, say N.
17 config MMC_PXA
18         tristate "Intel PXA25x/26x/27x Multimedia Card Interface support"
19         depends on ARCH_PXA
20         help
21           This selects the Intel(R) PXA(R) Multimedia card Interface.
22           If you have a PXA(R) platform with a Multimedia Card slot,
23           say Y or M here.
25           If unsure, say N.
27 config MMC_SDHCI
28         tristate "Secure Digital Host Controller Interface support"
29         depends on HAS_DMA
30         help
31           This selects the generic Secure Digital Host Controller Interface.
32           It is used by manufacturers such as Texas Instruments(R), Ricoh(R)
33           and Toshiba(R). Most controllers found in laptops are of this type.
35           If you have a controller with this interface, say Y or M here. You
36           also need to enable an appropriate bus interface.
38           If unsure, say N.
40 config MMC_SDHCI_IO_ACCESSORS
41         bool
42         depends on MMC_SDHCI
43         help
44           This is silent Kconfig symbol that is selected by the drivers that
45           need to overwrite SDHCI IO memory accessors.
47 config MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
48         bool
49         select MMC_SDHCI_IO_ACCESSORS
50         help
51           This option is selected by drivers running on big endian hosts
52           and performing I/O to a SDHCI controller through a bus that
53           implements a hardware byte swapper using a 32-bit datum.
54           This endian mapping mode is called "data invariance" and
55           has the effect of scrambling the addresses and formats of data
56           accessed in sizes other than the datum size.
58           This is the case for the Freescale eSDHC and Nintendo Wii SDHCI.
60 config MMC_SDHCI_PCI
61         tristate "SDHCI support on PCI bus"
62         depends on MMC_SDHCI && PCI
63         help
64           This selects the PCI Secure Digital Host Controller Interface.
65           Most controllers found today are PCI devices.
67           If you have a controller with this interface, say Y or M here.
69           If unsure, say N.
71 config MMC_RICOH_MMC
72         bool "Ricoh MMC Controller Disabler"
73         depends on MMC_SDHCI_PCI
74         help
75           This adds a pci quirk to disable Ricoh MMC Controller. This
76           proprietary controller is unnecessary because the SDHCI driver
77           supports MMC cards on the SD controller, but if it is not
78           disabled, it will steal the MMC cards away - rendering them
79           useless. It is safe to select this even if you don't
80           have a Ricoh based card reader.
82           If unsure, say Y.
84 config MMC_SDHCI_ACPI
85         tristate "SDHCI support for ACPI enumerated SDHCI controllers"
86         depends on MMC_SDHCI && ACPI
87         help
88           This selects support for ACPI enumerated SDHCI controllers,
89           identified by ACPI Compatibility ID PNP0D40 or specific
90           ACPI Hardware IDs.
92           If you have a controller with this interface, say Y or M here.
94           If unsure, say N.
96 config MMC_SDHCI_PLTFM
97         tristate "SDHCI platform and OF driver helper"
98         depends on MMC_SDHCI
99         help
100           This selects the common helper functions support for Secure Digital
101           Host Controller Interface based platform and OF drivers.
103           If you have a controller with this interface, say Y or M here.
105           If unsure, say N.
107 config MMC_SDHCI_OF_ESDHC
108         tristate "SDHCI OF support for the Freescale eSDHC controller"
109         depends on MMC_SDHCI_PLTFM
110         depends on PPC_OF
111         select MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
112         help
113           This selects the Freescale eSDHC controller support.
115           If you have a controller with this interface, say Y or M here.
117           If unsure, say N.
119 config MMC_SDHCI_OF_HLWD
120         tristate "SDHCI OF support for the Nintendo Wii SDHCI controllers"
121         depends on MMC_SDHCI_PLTFM
122         depends on PPC_OF
123         select MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
124         help
125           This selects the Secure Digital Host Controller Interface (SDHCI)
126           found in the "Hollywood" chipset of the Nintendo Wii video game
127           console.
129           If you have a controller with this interface, say Y or M here.
131           If unsure, say N.
133 config MMC_SDHCI_CNS3XXX
134         tristate "SDHCI support on the Cavium Networks CNS3xxx SoC"
135         depends on ARCH_CNS3XXX
136         depends on MMC_SDHCI_PLTFM
137         help
138           This selects the SDHCI support for CNS3xxx System-on-Chip devices.
140           If you have a controller with this interface, say Y or M here.
142           If unsure, say N.
144 config MMC_SDHCI_ESDHC_IMX
145         tristate "SDHCI support for the Freescale eSDHC/uSDHC i.MX controller"
146         depends on ARCH_MXC
147         depends on MMC_SDHCI_PLTFM
148         select MMC_SDHCI_IO_ACCESSORS
149         help
150           This selects the Freescale eSDHC/uSDHC controller support
151           found on i.MX25, i.MX35 i.MX5x and i.MX6x.
153           If you have a controller with this interface, say Y or M here.
155           If unsure, say N.
157 config MMC_SDHCI_DOVE
158         tristate "SDHCI support on Marvell's Dove SoC"
159         depends on ARCH_DOVE
160         depends on MMC_SDHCI_PLTFM
161         select MMC_SDHCI_IO_ACCESSORS
162         help
163           This selects the Secure Digital Host Controller Interface in
164           Marvell's Dove SoC.
166           If you have a controller with this interface, say Y or M here.
168           If unsure, say N.
170 config MMC_SDHCI_TEGRA
171         tristate "SDHCI platform support for the Tegra SD/MMC Controller"
172         depends on ARCH_TEGRA
173         depends on MMC_SDHCI_PLTFM
174         select MMC_SDHCI_IO_ACCESSORS
175         help
176           This selects the Tegra SD/MMC controller. If you have a Tegra
177           platform with SD or MMC devices, say Y or M here.
179           If unsure, say N.
181 config MMC_SDHCI_S3C
182         tristate "SDHCI support on Samsung S3C SoC"
183         depends on MMC_SDHCI && PLAT_SAMSUNG
184         help
185           This selects the Secure Digital Host Controller Interface (SDHCI)
186           often referrered to as the HSMMC block in some of the Samsung S3C
187           range of SoC.
189           If you have a controller with this interface, say Y or M here.
191           If unsure, say N.
193 config MMC_SDHCI_SIRF
194         tristate "SDHCI support on CSR SiRFprimaII and SiRFmarco SoCs"
195         depends on ARCH_SIRF
196         depends on MMC_SDHCI_PLTFM
197         help
198           This selects the SDHCI support for SiRF System-on-Chip devices.
200           If you have a controller with this interface, say Y or M here.
202           If unsure, say N.
204 config MMC_SDHCI_PXAV3
205         tristate "Marvell MMP2 SD Host Controller support (PXAV3)"
206         depends on CLKDEV_LOOKUP
207         select MMC_SDHCI
208         select MMC_SDHCI_PLTFM
209         default CPU_MMP2
210         help
211           This selects the Marvell(R) PXAV3 SD Host Controller.
212           If you have a MMP2 platform with SD Host Controller
213           and a card slot, say Y or M here.
215           If unsure, say N.
217 config MMC_SDHCI_PXAV2
218         tristate "Marvell PXA9XX SD Host Controller support (PXAV2)"
219         depends on CLKDEV_LOOKUP
220         select MMC_SDHCI
221         select MMC_SDHCI_PLTFM
222         default CPU_PXA910
223         help
224           This selects the Marvell(R) PXAV2 SD Host Controller.
225           If you have a PXA9XX platform with SD Host Controller
226           and a card slot, say Y or M here.
228           If unsure, say N.
230 config MMC_SDHCI_SPEAR
231         tristate "SDHCI support on ST SPEAr platform"
232         depends on MMC_SDHCI && PLAT_SPEAR
233         help
234           This selects the Secure Digital Host Controller Interface (SDHCI)
235           often referrered to as the HSMMC block in some of the ST SPEAR range
236           of SoC
238           If you have a controller with this interface, say Y or M here.
240           If unsure, say N.
242 config MMC_SDHCI_S3C_DMA
243         bool "DMA support on S3C SDHCI"
244         depends on MMC_SDHCI_S3C
245         help
246           Enable DMA support on the Samsung S3C SDHCI glue. The DMA
247           has proved to be problematic if the controller encounters
248           certain errors, and thus should be treated with care.
250           YMMV.
252 config MMC_SDHCI_BCM_KONA
253         tristate "SDHCI support on Broadcom KONA platform"
254         depends on ARCH_BCM
255         select MMC_SDHCI_PLTFM
256         help
257           This selects the Broadcom Kona Secure Digital Host Controller
258           Interface(SDHCI) support.
259           This is used in Broadcom mobile SoCs.
261           If you have a controller with this interface, say Y or M here.
263 config MMC_SDHCI_BCM2835
264         tristate "SDHCI platform support for the BCM2835 SD/MMC Controller"
265         depends on ARCH_BCM2835
266         depends on MMC_SDHCI_PLTFM
267         select MMC_SDHCI_IO_ACCESSORS
268         help
269           This selects the BCM2835 SD/MMC controller. If you have a BCM2835
270           platform with SD or MMC devices, say Y or M here.
272           If unsure, say N.
274 config MMC_OMAP
275         tristate "TI OMAP Multimedia Card Interface support"
276         depends on ARCH_OMAP
277         select TPS65010 if MACH_OMAP_H2
278         help
279           This selects the TI OMAP Multimedia card Interface.
280           If you have an OMAP board with a Multimedia Card slot,
281           say Y or M here.
283           If unsure, say N.
285 config MMC_OMAP_HS
286         tristate "TI OMAP High Speed Multimedia Card Interface support"
287         depends on ARCH_OMAP2PLUS || COMPILE_TEST
288         help
289           This selects the TI OMAP High Speed Multimedia card Interface.
290           If you have an omap2plus board with a Multimedia Card slot,
291           say Y or M here.
293           If unsure, say N.
295 config MMC_WBSD
296         tristate "Winbond W83L51xD SD/MMC Card Interface support"
297         depends on ISA_DMA_API
298         help
299           This selects the Winbond(R) W83L51xD Secure digital and
300           Multimedia card Interface.
301           If you have a machine with a integrated W83L518D or W83L519D
302           SD/MMC card reader, say Y or M here.
304           If unsure, say N.
306 config MMC_AU1X
307         tristate "Alchemy AU1XX0 MMC Card Interface support"
308         depends on MIPS_ALCHEMY
309         help
310           This selects the AMD Alchemy(R) Multimedia card interface.
311           If you have a Alchemy platform with a MMC slot, say Y or M here.
313           If unsure, say N.
315 config MMC_ATMELMCI
316         tristate "Atmel SD/MMC Driver (Multimedia Card Interface)"
317         depends on AVR32 || ARCH_AT91
318         help
319           This selects the Atmel Multimedia Card Interface driver. If
320           you have an AT32 (AVR32) or AT91 platform with a Multimedia
321           Card slot, say Y or M here.
323           If unsure, say N.
325 config MMC_MSM
326         tristate "Qualcomm SDCC Controller Support"
327         depends on MMC && ARCH_MSM
328         help
329           This provides support for the SD/MMC cell found in the
330           MSM and QSD SOCs from Qualcomm. The controller also has
331           support for SDIO devices.
333 config MMC_MXC
334         tristate "Freescale i.MX21/27/31 or MPC512x Multimedia Card support"
335         depends on ARCH_MXC || PPC_MPC512x
336         help
337           This selects the Freescale i.MX21, i.MX27, i.MX31 or MPC512x
338           Multimedia Card Interface. If you have an i.MX or MPC512x platform
339           with a Multimedia Card slot, say Y or M here.
341           If unsure, say N.
343 config MMC_MXS
344         tristate "Freescale MXS Multimedia Card Interface support"
345         depends on ARCH_MXS && MXS_DMA
346         help
347           This selects the Freescale SSP MMC controller found on MXS based
348           platforms like mx23/28.
350           If unsure, say N.
352 config MMC_TIFM_SD
353         tristate "TI Flash Media MMC/SD Interface support"
354         depends on PCI
355         select TIFM_CORE
356         help
357           Say Y here if you want to be able to access MMC/SD cards with
358           the Texas Instruments(R) Flash Media card reader, found in many
359           laptops.
360           This option 'selects' (turns on, enables) 'TIFM_CORE', but you
361           probably also need appropriate card reader host adapter, such as
362           'Misc devices: TI Flash Media PCI74xx/PCI76xx host adapter support
363           (TIFM_7XX1)'.
365           To compile this driver as a module, choose M here: the
366           module will be called tifm_sd.
368 config MMC_MVSDIO
369         tristate "Marvell MMC/SD/SDIO host driver"
370         depends on PLAT_ORION
371         ---help---
372           This selects the Marvell SDIO host driver.
373           SDIO may currently be found on the Kirkwood 88F6281 and 88F6192
374           SoC controllers.
376           To compile this driver as a module, choose M here: the
377           module will be called mvsdio.
379 config MMC_DAVINCI
380         tristate "TI DAVINCI Multimedia Card Interface support"
381         depends on ARCH_DAVINCI
382         help
383           This selects the TI DAVINCI Multimedia card Interface.
384           If you have an DAVINCI board with a Multimedia Card slot,
385           say Y or M here.  If unsure, say N.
387 config MMC_GOLDFISH
388         tristate "goldfish qemu Multimedia Card Interface support"
389         depends on GOLDFISH
390         help
391           This selects the Goldfish Multimedia card Interface emulation
392           found on the Goldfish Android virtual device emulation.
394 config MMC_SPI
395         tristate "MMC/SD/SDIO over SPI"
396         depends on SPI_MASTER && !HIGHMEM && HAS_DMA
397         select CRC7
398         select CRC_ITU_T
399         help
400           Some systems access MMC/SD/SDIO cards using a SPI controller
401           instead of using a "native" MMC/SD/SDIO controller.  This has a
402           disadvantage of being relatively high overhead, but a compensating
403           advantage of working on many systems without dedicated MMC/SD/SDIO
404           controllers.
406           If unsure, or if your system has no SPI master driver, say N.
408 config MMC_S3C
409         tristate "Samsung S3C SD/MMC Card Interface support"
410         depends on ARCH_S3C24XX
411         help
412           This selects a driver for the MCI interface found in
413           Samsung's S3C2410, S3C2412, S3C2440, S3C2442 CPUs.
414           If you have a board based on one of those and a MMC/SD
415           slot, say Y or M here.
417           If unsure, say N.
419 config MMC_S3C_HW_SDIO_IRQ
420        bool "Hardware support for SDIO IRQ"
421        depends on MMC_S3C
422        help
423          Enable the hardware support for SDIO interrupts instead of using
424          the generic polling code.
426 choice
427         prompt "Samsung S3C SD/MMC transfer code"
428         depends on MMC_S3C
430 config MMC_S3C_PIO
431         bool "Use PIO transfers only"
432         help
433           Use PIO to transfer data between memory and the hardware.
435           PIO is slower than DMA as it requires CPU instructions to
436           move the data. This has been the traditional default for
437           the S3C MCI driver.
439 config MMC_S3C_DMA
440         bool "Use DMA transfers only"
441         help
442           Use DMA to transfer data between memory and the hardare.
444           Currently, the DMA support in this driver seems to not be
445           working properly and needs to be debugged before this
446           option is useful.
448 config MMC_S3C_PIODMA
449         bool "Support for both PIO and DMA"
450         help
451           Compile both the PIO and DMA transfer routines into the
452           driver and let the platform select at run-time which one
453           is best.
455           See notes for the DMA option.
457 endchoice
459 config MMC_SDRICOH_CS
460         tristate "MMC/SD driver for Ricoh Bay1Controllers"
461         depends on PCI && PCMCIA
462         help
463           Say Y here if your Notebook reports a Ricoh Bay1Controller PCMCIA
464           card whenever you insert a MMC or SD card into the card slot.
466           To compile this driver as a module, choose M here: the
467           module will be called sdricoh_cs.
469 config MMC_TMIO_CORE
470         tristate
472 config MMC_TMIO
473         tristate "Toshiba Mobile IO Controller (TMIO) MMC/SD function support"
474         depends on MFD_TMIO || MFD_ASIC3
475         select MMC_TMIO_CORE
476         help
477           This provides support for the SD/MMC cell found in TC6393XB,
478           T7L66XB and also HTC ASIC3
480 config MMC_SDHI
481         tristate "SH-Mobile SDHI SD/SDIO controller support"
482         depends on SUPERH || ARCH_SHMOBILE
483         select MMC_TMIO_CORE
484         help
485           This provides support for the SDHI SD/SDIO controller found in
486           SuperH and ARM SH-Mobile SoCs
488 config MMC_CB710
489         tristate "ENE CB710 MMC/SD Interface support"
490         depends on PCI && GENERIC_HARDIRQS
491         select CB710_CORE
492         help
493           This option enables support for MMC/SD part of ENE CB710/720 Flash
494           memory card reader found in some laptops (ie. some versions of
495           HP Compaq nx9500).
497           This driver can also be built as a module. If so, the module
498           will be called cb710-mmc.
500 config MMC_VIA_SDMMC
501         tristate "VIA SD/MMC Card Reader Driver"
502         depends on PCI
503         help
504           This selects the VIA SD/MMC Card Reader driver, say Y or M here.
505           VIA provides one multi-functional card reader which integrated into
506           some motherboards manufactured by VIA. This card reader supports
507           SD/MMC/SDHC.
508           If you have a controller with this interface, say Y or M here.
510           If unsure, say N.
512 config SDH_BFIN
513         tristate "Blackfin Secure Digital Host support"
514         depends on (BF54x && !BF544) || (BF51x && !BF512)
515         help
516           If you say yes here you will get support for the Blackfin on-chip
517           Secure Digital Host interface.  This includes support for MMC and
518           SD cards.
520           To compile this driver as a module, choose M here: the
521           module will be called bfin_sdh.
523           If unsure, say N.
525 config SDH_BFIN_MISSING_CMD_PULLUP_WORKAROUND
526         bool "Blackfin EZkit Missing SDH_CMD Pull Up Resistor Workaround"
527         depends on SDH_BFIN
528         help
529           If you say yes here SD-Cards may work on the EZkit.
531 config MMC_DW
532         tristate "Synopsys DesignWare Memory Card Interface"
533         depends on ARM
534         help
535           This selects support for the Synopsys DesignWare Mobile Storage IP
536           block, this provides host support for SD and MMC interfaces, in both
537           PIO and external DMA modes.
539 config MMC_DW_IDMAC
540         bool "Internal DMAC interface"
541         depends on MMC_DW
542         help
543           This selects support for the internal DMAC block within the Synopsys
544           Designware Mobile Storage IP block. This disables the external DMA
545           interface.
547 config MMC_DW_PLTFM
548         tristate "Synopsys Designware MCI Support as platform device"
549         depends on MMC_DW
550         default y
551         help
552           This selects the common helper functions support for Host Controller
553           Interface based platform driver. Please select this option if the IP
554           is present as a platform device. This is the common interface for the
555           Synopsys Designware IP.
557           If you have a controller with this interface, say Y or M here.
559           If unsure, say Y.
561 config MMC_DW_EXYNOS
562         tristate "Exynos specific extensions for Synopsys DW Memory Card Interface"
563         depends on MMC_DW
564         select MMC_DW_PLTFM
565         help
566           This selects support for Samsung Exynos SoC specific extensions to the
567           Synopsys DesignWare Memory Card Interface driver. Select this option
568           for platforms based on Exynos4 and Exynos5 SoC's.
570 config MMC_DW_SOCFPGA
571         tristate "SOCFPGA specific extensions for Synopsys DW Memory Card Interface"
572         depends on MMC_DW && MFD_SYSCON
573         select MMC_DW_PLTFM
574         help
575           This selects support for Altera SoCFPGA specific extensions to the
576           Synopsys DesignWare Memory Card Interface driver.
578 config MMC_DW_PCI
579         tristate "Synopsys Designware MCI support on PCI bus"
580         depends on MMC_DW && PCI
581         help
582           This selects the PCI bus for the Synopsys Designware Mobile Storage IP.
583           Select this option if the IP is present on PCI platform.
585           If you have a controller with this interface, say Y or M here.
587           If unsure, say N.
589 config MMC_SH_MMCIF
590         tristate "SuperH Internal MMCIF support"
591         depends on MMC_BLOCK && (SUPERH || ARCH_SHMOBILE)
592         help
593           This selects the MMC Host Interface controller (MMCIF).
595           This driver supports MMCIF in sh7724/sh7757/sh7372.
597 config MMC_JZ4740
598         tristate "JZ4740 SD/Multimedia Card Interface support"
599         depends on MACH_JZ4740
600         help
601           This selects support for the SD/MMC controller on Ingenic JZ4740
602           SoCs.
603           If you have a board based on such a SoC and with a SD/MMC slot,
604           say Y or M here.
606 config MMC_VUB300
607         tristate "VUB300 USB to SDIO/SD/MMC Host Controller support"
608         depends on USB
609         help
610           This selects support for Elan Digital Systems' VUB300 chip.
612           The VUB300 is a USB-SDIO Host Controller Interface chip
613           that enables the host computer to use SDIO/SD/MMC cards
614           via a USB 2.0 or USB 1.1 host.
616           The VUB300 chip will be found in both physically separate
617           USB to SDIO/SD/MMC adapters and embedded on some motherboards.
619           The VUB300 chip supports SD and MMC memory cards in addition
620           to single and multifunction SDIO cards.
622           Some SDIO cards will need a firmware file to be loaded and
623           sent to VUB300 chip in order to achieve better data throughput.
624           Download these "Offload Pseudocode" from Elan Digital Systems'
625           web-site http://www.elandigitalsystems.com/support/downloads.php
626           and put them in /lib/firmware. Note that without these additional
627           firmware files the VUB300 chip will still function, but not at
628           the best obtainable data rate.
630           To compile this mmc host controller driver as a module,
631           choose M here: the module will be called vub300.
633           If you have a computer with an embedded VUB300 chip
634           or if you intend connecting a USB adapter based on a
635           VUB300 chip say Y or M here.
637 config MMC_USHC
638         tristate "USB SD Host Controller (USHC) support"
639         depends on USB
640         help
641           This selects support for USB SD Host Controllers based on
642           the Cypress Astoria chip with firmware compliant with CSR's
643           USB SD Host Controller specification (CS-118793-SP).
645           CSR boards with this device include: USB<>SDIO (M1985v2),
646           and Ultrasira.
648           Note: These controllers only support SDIO cards and do not
649           support MMC or SD memory cards.
651 config MMC_WMT
652         tristate "Wondermedia SD/MMC Host Controller support"
653         depends on ARCH_VT8500
654         default y
655         help
656           This selects support for the SD/MMC Host Controller on
657           Wondermedia WM8505/WM8650 based SoCs.
659           To compile this driver as a module, choose M here: the
660           module will be called wmt-sdmmc.
662 config MMC_REALTEK_PCI
663         tristate "Realtek PCI-E SD/MMC Card Interface Driver"
664         depends on MFD_RTSX_PCI
665         help
666           Say Y here to include driver code to support SD/MMC card interface
667           of Realtek PCI-E card reader