]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/mmc/host/Kconfig
Merge tag 'gpio-for-linus' of git://git.secretlab.ca/git/linux
[rpmsg/rpmsg.git] / drivers / mmc / host / Kconfig
1 #
2 # MMC/SD host controller drivers
3 #
5 comment "MMC/SD/SDIO Host Controller Drivers"
7 config MMC_ARMMMCI
8         tristate "ARM AMBA Multimedia Card Interface support"
9         depends on ARM_AMBA
10         help
11           This selects the ARM(R) AMBA(R) PrimeCell Multimedia Card
12           Interface (PL180 and PL181) support.  If you have an ARM(R)
13           platform with a Multimedia Card slot, say Y or M here.
15           If unsure, say N.
17 config MMC_PXA
18         tristate "Intel PXA25x/26x/27x Multimedia Card Interface support"
19         depends on ARCH_PXA
20         help
21           This selects the Intel(R) PXA(R) Multimedia card Interface.
22           If you have a PXA(R) platform with a Multimedia Card slot,
23           say Y or M here.
25           If unsure, say N.
27 config MMC_SDHCI
28         tristate "Secure Digital Host Controller Interface support"
29         depends on HAS_DMA
30         help
31           This selects the generic Secure Digital Host Controller Interface.
32           It is used by manufacturers such as Texas Instruments(R), Ricoh(R)
33           and Toshiba(R). Most controllers found in laptops are of this type.
35           If you have a controller with this interface, say Y or M here. You
36           also need to enable an appropriate bus interface.
38           If unsure, say N.
40 config MMC_SDHCI_IO_ACCESSORS
41         bool
42         depends on MMC_SDHCI
43         help
44           This is silent Kconfig symbol that is selected by the drivers that
45           need to overwrite SDHCI IO memory accessors.
47 config MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
48         bool
49         select MMC_SDHCI_IO_ACCESSORS
50         help
51           This option is selected by drivers running on big endian hosts
52           and performing I/O to a SDHCI controller through a bus that
53           implements a hardware byte swapper using a 32-bit datum.
54           This endian mapping mode is called "data invariance" and
55           has the effect of scrambling the addresses and formats of data
56           accessed in sizes other than the datum size.
58           This is the case for the Freescale eSDHC and Nintendo Wii SDHCI.
60 config MMC_SDHCI_PCI
61         tristate "SDHCI support on PCI bus"
62         depends on MMC_SDHCI && PCI
63         help
64           This selects the PCI Secure Digital Host Controller Interface.
65           Most controllers found today are PCI devices.
67           If you have a controller with this interface, say Y or M here.
69           If unsure, say N.
71 config MMC_RICOH_MMC
72         bool "Ricoh MMC Controller Disabler"
73         depends on MMC_SDHCI_PCI
74         help
75           This adds a pci quirk to disable Ricoh MMC Controller. This
76           proprietary controller is unnecessary because the SDHCI driver
77           supports MMC cards on the SD controller, but if it is not
78           disabled, it will steal the MMC cards away - rendering them
79           useless. It is safe to select this even if you don't
80           have a Ricoh based card reader.
82           If unsure, say Y.
84 config MMC_SDHCI_ACPI
85         tristate "SDHCI support for ACPI enumerated SDHCI controllers"
86         depends on MMC_SDHCI && ACPI
87         help
88           This selects support for ACPI enumerated SDHCI controllers,
89           identified by ACPI Compatibility ID PNP0D40 or specific
90           ACPI Hardware IDs.
92           If you have a controller with this interface, say Y or M here.
94           If unsure, say N.
96 config MMC_SDHCI_PLTFM
97         tristate "SDHCI platform and OF driver helper"
98         depends on MMC_SDHCI
99         help
100           This selects the common helper functions support for Secure Digital
101           Host Controller Interface based platform and OF drivers.
103           If you have a controller with this interface, say Y or M here.
105           If unsure, say N.
107 config MMC_SDHCI_OF_ESDHC
108         tristate "SDHCI OF support for the Freescale eSDHC controller"
109         depends on MMC_SDHCI_PLTFM
110         depends on PPC_OF
111         select MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
112         help
113           This selects the Freescale eSDHC controller support.
115           If you have a controller with this interface, say Y or M here.
117           If unsure, say N.
119 config MMC_SDHCI_OF_HLWD
120         tristate "SDHCI OF support for the Nintendo Wii SDHCI controllers"
121         depends on MMC_SDHCI_PLTFM
122         depends on PPC_OF
123         select MMC_SDHCI_BIG_ENDIAN_32BIT_BYTE_SWAPPER
124         help
125           This selects the Secure Digital Host Controller Interface (SDHCI)
126           found in the "Hollywood" chipset of the Nintendo Wii video game
127           console.
129           If you have a controller with this interface, say Y or M here.
131           If unsure, say N.
133 config MMC_SDHCI_CNS3XXX
134         tristate "SDHCI support on the Cavium Networks CNS3xxx SoC"
135         depends on ARCH_CNS3XXX
136         depends on MMC_SDHCI_PLTFM
137         help
138           This selects the SDHCI support for CNS3xxx System-on-Chip devices.
140           If you have a controller with this interface, say Y or M here.
142           If unsure, say N.
144 config MMC_SDHCI_ESDHC_IMX
145         tristate "SDHCI support for the Freescale eSDHC/uSDHC i.MX controller"
146         depends on ARCH_MXC
147         depends on MMC_SDHCI_PLTFM
148         select MMC_SDHCI_IO_ACCESSORS
149         help
150           This selects the Freescale eSDHC/uSDHC controller support
151           found on i.MX25, i.MX35 i.MX5x and i.MX6x.
153           If you have a controller with this interface, say Y or M here.
155           If unsure, say N.
157 config MMC_SDHCI_DOVE
158         tristate "SDHCI support on Marvell's Dove SoC"
159         depends on ARCH_DOVE
160         depends on MMC_SDHCI_PLTFM
161         select MMC_SDHCI_IO_ACCESSORS
162         help
163           This selects the Secure Digital Host Controller Interface in
164           Marvell's Dove SoC.
166           If you have a controller with this interface, say Y or M here.
168           If unsure, say N.
170 config MMC_SDHCI_TEGRA
171         tristate "SDHCI platform support for the Tegra SD/MMC Controller"
172         depends on ARCH_TEGRA
173         depends on MMC_SDHCI_PLTFM
174         select MMC_SDHCI_IO_ACCESSORS
175         help
176           This selects the Tegra SD/MMC controller. If you have a Tegra
177           platform with SD or MMC devices, say Y or M here.
179           If unsure, say N.
181 config MMC_SDHCI_S3C
182         tristate "SDHCI support on Samsung S3C SoC"
183         depends on MMC_SDHCI && PLAT_SAMSUNG
184         help
185           This selects the Secure Digital Host Controller Interface (SDHCI)
186           often referrered to as the HSMMC block in some of the Samsung S3C
187           range of SoC.
189           If you have a controller with this interface, say Y or M here.
191           If unsure, say N.
193 config MMC_SDHCI_SIRF
194         tristate "SDHCI support on CSR SiRFprimaII and SiRFmarco SoCs"
195         depends on ARCH_SIRF
196         depends on MMC_SDHCI_PLTFM
197         help
198           This selects the SDHCI support for SiRF System-on-Chip devices.
200           If you have a controller with this interface, say Y or M here.
202           If unsure, say N.
204 config MMC_SDHCI_PXAV3
205         tristate "Marvell MMP2 SD Host Controller support (PXAV3)"
206         depends on CLKDEV_LOOKUP
207         select MMC_SDHCI
208         select MMC_SDHCI_PLTFM
209         default CPU_MMP2
210         help
211           This selects the Marvell(R) PXAV3 SD Host Controller.
212           If you have a MMP2 platform with SD Host Controller
213           and a card slot, say Y or M here.
215           If unsure, say N.
217 config MMC_SDHCI_PXAV2
218         tristate "Marvell PXA9XX SD Host Controller support (PXAV2)"
219         depends on CLKDEV_LOOKUP
220         select MMC_SDHCI
221         select MMC_SDHCI_PLTFM
222         default CPU_PXA910
223         help
224           This selects the Marvell(R) PXAV2 SD Host Controller.
225           If you have a PXA9XX platform with SD Host Controller
226           and a card slot, say Y or M here.
228           If unsure, say N.
230 config MMC_SDHCI_SPEAR
231         tristate "SDHCI support on ST SPEAr platform"
232         depends on MMC_SDHCI && PLAT_SPEAR
233         help
234           This selects the Secure Digital Host Controller Interface (SDHCI)
235           often referrered to as the HSMMC block in some of the ST SPEAR range
236           of SoC
238           If you have a controller with this interface, say Y or M here.
240           If unsure, say N.
242 config MMC_SDHCI_S3C_DMA
243         bool "DMA support on S3C SDHCI"
244         depends on MMC_SDHCI_S3C
245         help
246           Enable DMA support on the Samsung S3C SDHCI glue. The DMA
247           has proved to be problematic if the controller encounters
248           certain errors, and thus should be treated with care.
250           YMMV.
252 config MMC_SDHCI_BCM2835
253         tristate "SDHCI platform support for the BCM2835 SD/MMC Controller"
254         depends on ARCH_BCM2835
255         depends on MMC_SDHCI_PLTFM
256         select MMC_SDHCI_IO_ACCESSORS
257         help
258           This selects the BCM2835 SD/MMC controller. If you have a BCM2835
259           platform with SD or MMC devices, say Y or M here.
261           If unsure, say N.
263 config MMC_OMAP
264         tristate "TI OMAP Multimedia Card Interface support"
265         depends on ARCH_OMAP
266         select TPS65010 if MACH_OMAP_H2
267         help
268           This selects the TI OMAP Multimedia card Interface.
269           If you have an OMAP board with a Multimedia Card slot,
270           say Y or M here.
272           If unsure, say N.
274 config MMC_OMAP_HS
275         tristate "TI OMAP High Speed Multimedia Card Interface support"
276         depends on SOC_OMAP2430 || ARCH_OMAP3 || ARCH_OMAP4
277         help
278           This selects the TI OMAP High Speed Multimedia card Interface.
279           If you have an OMAP2430 or OMAP3 board or OMAP4 board with a
280           Multimedia Card slot, say Y or M here.
282           If unsure, say N.
284 config MMC_WBSD
285         tristate "Winbond W83L51xD SD/MMC Card Interface support"
286         depends on ISA_DMA_API
287         help
288           This selects the Winbond(R) W83L51xD Secure digital and
289           Multimedia card Interface.
290           If you have a machine with a integrated W83L518D or W83L519D
291           SD/MMC card reader, say Y or M here.
293           If unsure, say N.
295 config MMC_AU1X
296         tristate "Alchemy AU1XX0 MMC Card Interface support"
297         depends on MIPS_ALCHEMY
298         help
299           This selects the AMD Alchemy(R) Multimedia card interface.
300           If you have a Alchemy platform with a MMC slot, say Y or M here.
302           If unsure, say N.
304 config MMC_ATMELMCI
305         tristate "Atmel SD/MMC Driver (Multimedia Card Interface)"
306         depends on AVR32 || ARCH_AT91
307         help
308           This selects the Atmel Multimedia Card Interface driver. If
309           you have an AT32 (AVR32) or AT91 platform with a Multimedia
310           Card slot, say Y or M here.
312           If unsure, say N.
314 config MMC_MSM
315         tristate "Qualcomm SDCC Controller Support"
316         depends on MMC && ARCH_MSM
317         help
318           This provides support for the SD/MMC cell found in the
319           MSM and QSD SOCs from Qualcomm. The controller also has
320           support for SDIO devices.
322 config MMC_MXC
323         tristate "Freescale i.MX21/27/31 or MPC512x Multimedia Card support"
324         depends on ARCH_MXC || PPC_MPC512x
325         help
326           This selects the Freescale i.MX21, i.MX27, i.MX31 or MPC512x
327           Multimedia Card Interface. If you have an i.MX or MPC512x platform
328           with a Multimedia Card slot, say Y or M here.
330           If unsure, say N.
332 config MMC_MXS
333         tristate "Freescale MXS Multimedia Card Interface support"
334         depends on ARCH_MXS && MXS_DMA
335         help
336           This selects the Freescale SSP MMC controller found on MXS based
337           platforms like mx23/28.
339           If unsure, say N.
341 config MMC_TIFM_SD
342         tristate "TI Flash Media MMC/SD Interface support"
343         depends on PCI
344         select TIFM_CORE
345         help
346           Say Y here if you want to be able to access MMC/SD cards with
347           the Texas Instruments(R) Flash Media card reader, found in many
348           laptops.
349           This option 'selects' (turns on, enables) 'TIFM_CORE', but you
350           probably also need appropriate card reader host adapter, such as
351           'Misc devices: TI Flash Media PCI74xx/PCI76xx host adapter support
352           (TIFM_7XX1)'.
354           To compile this driver as a module, choose M here: the
355           module will be called tifm_sd.
357 config MMC_MVSDIO
358         tristate "Marvell MMC/SD/SDIO host driver"
359         depends on PLAT_ORION
360         ---help---
361           This selects the Marvell SDIO host driver.
362           SDIO may currently be found on the Kirkwood 88F6281 and 88F6192
363           SoC controllers.
365           To compile this driver as a module, choose M here: the
366           module will be called mvsdio.
368 config MMC_DAVINCI
369         tristate "TI DAVINCI Multimedia Card Interface support"
370         depends on ARCH_DAVINCI
371         help
372           This selects the TI DAVINCI Multimedia card Interface.
373           If you have an DAVINCI board with a Multimedia Card slot,
374           say Y or M here.  If unsure, say N.
376 config MMC_GOLDFISH
377         tristate "goldfish qemu Multimedia Card Interface support"
378         depends on GOLDFISH
379         help
380           This selects the Goldfish Multimedia card Interface emulation
381           found on the Goldfish Android virtual device emulation.
383 config MMC_SPI
384         tristate "MMC/SD/SDIO over SPI"
385         depends on SPI_MASTER && !HIGHMEM && HAS_DMA
386         select CRC7
387         select CRC_ITU_T
388         help
389           Some systems access MMC/SD/SDIO cards using a SPI controller
390           instead of using a "native" MMC/SD/SDIO controller.  This has a
391           disadvantage of being relatively high overhead, but a compensating
392           advantage of working on many systems without dedicated MMC/SD/SDIO
393           controllers.
395           If unsure, or if your system has no SPI master driver, say N.
397 config MMC_S3C
398         tristate "Samsung S3C SD/MMC Card Interface support"
399         depends on ARCH_S3C24XX
400         help
401           This selects a driver for the MCI interface found in
402           Samsung's S3C2410, S3C2412, S3C2440, S3C2442 CPUs.
403           If you have a board based on one of those and a MMC/SD
404           slot, say Y or M here.
406           If unsure, say N.
408 config MMC_S3C_HW_SDIO_IRQ
409        bool "Hardware support for SDIO IRQ"
410        depends on MMC_S3C
411        help
412          Enable the hardware support for SDIO interrupts instead of using
413          the generic polling code.
415 choice
416         prompt "Samsung S3C SD/MMC transfer code"
417         depends on MMC_S3C
419 config MMC_S3C_PIO
420         bool "Use PIO transfers only"
421         help
422           Use PIO to transfer data between memory and the hardware.
424           PIO is slower than DMA as it requires CPU instructions to
425           move the data. This has been the traditional default for
426           the S3C MCI driver.
428 config MMC_S3C_DMA
429         bool "Use DMA transfers only"
430         help
431           Use DMA to transfer data between memory and the hardare.
433           Currently, the DMA support in this driver seems to not be
434           working properly and needs to be debugged before this
435           option is useful.
437 config MMC_S3C_PIODMA
438         bool "Support for both PIO and DMA"
439         help
440           Compile both the PIO and DMA transfer routines into the
441           driver and let the platform select at run-time which one
442           is best.
444           See notes for the DMA option.
446 endchoice
448 config MMC_SDRICOH_CS
449         tristate "MMC/SD driver for Ricoh Bay1Controllers"
450         depends on PCI && PCMCIA
451         help
452           Say Y here if your Notebook reports a Ricoh Bay1Controller PCMCIA
453           card whenever you insert a MMC or SD card into the card slot.
455           To compile this driver as a module, choose M here: the
456           module will be called sdricoh_cs.
458 config MMC_TMIO_CORE
459         tristate
461 config MMC_TMIO
462         tristate "Toshiba Mobile IO Controller (TMIO) MMC/SD function support"
463         depends on MFD_TMIO || MFD_ASIC3
464         select MMC_TMIO_CORE
465         help
466           This provides support for the SD/MMC cell found in TC6393XB,
467           T7L66XB and also HTC ASIC3
469 config MMC_SDHI
470         tristate "SH-Mobile SDHI SD/SDIO controller support"
471         depends on SUPERH || ARCH_SHMOBILE
472         select MMC_TMIO_CORE
473         help
474           This provides support for the SDHI SD/SDIO controller found in
475           SuperH and ARM SH-Mobile SoCs
477 config MMC_CB710
478         tristate "ENE CB710 MMC/SD Interface support"
479         depends on PCI && GENERIC_HARDIRQS
480         select CB710_CORE
481         help
482           This option enables support for MMC/SD part of ENE CB710/720 Flash
483           memory card reader found in some laptops (ie. some versions of
484           HP Compaq nx9500).
486           This driver can also be built as a module. If so, the module
487           will be called cb710-mmc.
489 config MMC_VIA_SDMMC
490         tristate "VIA SD/MMC Card Reader Driver"
491         depends on PCI
492         help
493           This selects the VIA SD/MMC Card Reader driver, say Y or M here.
494           VIA provides one multi-functional card reader which integrated into
495           some motherboards manufactured by VIA. This card reader supports
496           SD/MMC/SDHC.
497           If you have a controller with this interface, say Y or M here.
499           If unsure, say N.
501 config SDH_BFIN
502         tristate "Blackfin Secure Digital Host support"
503         depends on (BF54x && !BF544) || (BF51x && !BF512)
504         help
505           If you say yes here you will get support for the Blackfin on-chip
506           Secure Digital Host interface.  This includes support for MMC and
507           SD cards.
509           To compile this driver as a module, choose M here: the
510           module will be called bfin_sdh.
512           If unsure, say N.
514 config SDH_BFIN_MISSING_CMD_PULLUP_WORKAROUND
515         bool "Blackfin EZkit Missing SDH_CMD Pull Up Resistor Workaround"
516         depends on SDH_BFIN
517         help
518           If you say yes here SD-Cards may work on the EZkit.
520 config MMC_DW
521         tristate "Synopsys DesignWare Memory Card Interface"
522         depends on ARM
523         help
524           This selects support for the Synopsys DesignWare Mobile Storage IP
525           block, this provides host support for SD and MMC interfaces, in both
526           PIO and external DMA modes.
528 config MMC_DW_IDMAC
529         bool "Internal DMAC interface"
530         depends on MMC_DW
531         help
532           This selects support for the internal DMAC block within the Synopsys
533           Designware Mobile Storage IP block. This disables the external DMA
534           interface.
536 config MMC_DW_PLTFM
537         tristate "Synopsys Designware MCI Support as platform device"
538         depends on MMC_DW
539         default y
540         help
541           This selects the common helper functions support for Host Controller
542           Interface based platform driver. Please select this option if the IP
543           is present as a platform device. This is the common interface for the
544           Synopsys Designware IP.
546           If you have a controller with this interface, say Y or M here.
548           If unsure, say Y.
550 config MMC_DW_EXYNOS
551         tristate "Exynos specific extensions for Synopsys DW Memory Card Interface"
552         depends on MMC_DW
553         select MMC_DW_PLTFM
554         help
555           This selects support for Samsung Exynos SoC specific extensions to the
556           Synopsys DesignWare Memory Card Interface driver. Select this option
557           for platforms based on Exynos4 and Exynos5 SoC's.
559 config MMC_DW_PCI
560         tristate "Synopsys Designware MCI support on PCI bus"
561         depends on MMC_DW && PCI
562         help
563           This selects the PCI bus for the Synopsys Designware Mobile Storage IP.
564           Select this option if the IP is present on PCI platform.
566           If you have a controller with this interface, say Y or M here.
568           If unsure, say N.
570 config MMC_SH_MMCIF
571         tristate "SuperH Internal MMCIF support"
572         depends on MMC_BLOCK && (SUPERH || ARCH_SHMOBILE)
573         help
574           This selects the MMC Host Interface controller (MMCIF).
576           This driver supports MMCIF in sh7724/sh7757/sh7372.
578 config MMC_JZ4740
579         tristate "JZ4740 SD/Multimedia Card Interface support"
580         depends on MACH_JZ4740
581         help
582           This selects support for the SD/MMC controller on Ingenic JZ4740
583           SoCs.
584           If you have a board based on such a SoC and with a SD/MMC slot,
585           say Y or M here.
587 config MMC_VUB300
588         tristate "VUB300 USB to SDIO/SD/MMC Host Controller support"
589         depends on USB
590         help
591           This selects support for Elan Digital Systems' VUB300 chip.
593           The VUB300 is a USB-SDIO Host Controller Interface chip
594           that enables the host computer to use SDIO/SD/MMC cards
595           via a USB 2.0 or USB 1.1 host.
597           The VUB300 chip will be found in both physically separate
598           USB to SDIO/SD/MMC adapters and embedded on some motherboards.
600           The VUB300 chip supports SD and MMC memory cards in addition
601           to single and multifunction SDIO cards.
603           Some SDIO cards will need a firmware file to be loaded and
604           sent to VUB300 chip in order to achieve better data throughput.
605           Download these "Offload Pseudocode" from Elan Digital Systems'
606           web-site http://www.elandigitalsystems.com/support/downloads.php
607           and put them in /lib/firmware. Note that without these additional
608           firmware files the VUB300 chip will still function, but not at
609           the best obtainable data rate.
611           To compile this mmc host controller driver as a module,
612           choose M here: the module will be called vub300.
614           If you have a computer with an embedded VUB300 chip
615           or if you intend connecting a USB adapter based on a
616           VUB300 chip say Y or M here.
618 config MMC_USHC
619         tristate "USB SD Host Controller (USHC) support"
620         depends on USB
621         help
622           This selects support for USB SD Host Controllers based on
623           the Cypress Astoria chip with firmware compliant with CSR's
624           USB SD Host Controller specification (CS-118793-SP).
626           CSR boards with this device include: USB<>SDIO (M1985v2),
627           and Ultrasira.
629           Note: These controllers only support SDIO cards and do not
630           support MMC or SD memory cards.
632 config MMC_WMT
633         tristate "Wondermedia SD/MMC Host Controller support"
634         depends on ARCH_VT8500
635         default y
636         help
637           This selects support for the SD/MMC Host Controller on
638           Wondermedia WM8505/WM8650 based SoCs.
640           To compile this driver as a module, choose M here: the
641           module will be called wmt-sdmmc.
643 config MMC_REALTEK_PCI
644         tristate "Realtek PCI-E SD/MMC Card Interface Driver"
645         depends on MFD_RTSX_PCI
646         help
647           Say Y here to include driver code to support SD/MMC card interface
648           of Realtek PCI-E card reader