1 /* mac89x0.c: A Crystal Semiconductor CS89[02]0 driver for linux. */
2 /*
3 Written 1996 by Russell Nelson, with reference to skeleton.c
4 written 1993-1994 by Donald Becker.
6 This software may be used and distributed according to the terms
7 of the GNU General Public License, incorporated herein by reference.
9 The author may be reached at nelson@crynwr.com, Crynwr
10 Software, 11 Grant St., Potsdam, NY 13676
12 Changelog:
14 Mike Cruse : mcruse@cti-ltd.com
15 : Changes for Linux 2.0 compatibility.
16 : Added dev_id parameter in net_interrupt(),
17 : request_irq() and free_irq(). Just NULL for now.
19 Mike Cruse : Added MOD_INC_USE_COUNT and MOD_DEC_USE_COUNT macros
20 : in net_open() and net_close() so kerneld would know
21 : that the module is in use and wouldn't eject the
22 : driver prematurely.
24 Mike Cruse : Rewrote init_module() and cleanup_module using 8390.c
25 : as an example. Disabled autoprobing in init_module(),
26 : not a good thing to do to other devices while Linux
27 : is running from all accounts.
29 Alan Cox : Removed 1.2 support, added 2.1 extra counters.
31 David Huggins-Daines <dhd@debian.org>
33 Split this off into mac89x0.c, and gutted it of all parts which are
34 not relevant to the existing CS8900 cards on the Macintosh
35 (i.e. basically the Daynaport CS and LC cards). To be precise:
37 * Removed all the media-detection stuff, because these cards are
38 TP-only.
40 * Lobotomized the ISA interrupt bogosity, because these cards use
41 a hardwired NuBus interrupt and a magic ISAIRQ value in the card.
43 * Basically eliminated everything not relevant to getting the
44 cards minimally functioning on the Macintosh.
46 I might add that these cards are badly designed even from the Mac
47 standpoint, in that Dayna, in their infinite wisdom, used NuBus slot
48 I/O space and NuBus interrupts for these cards, but neglected to
49 provide anything even remotely resembling a NuBus ROM. Therefore we
50 have to probe for them in a brain-damaged ISA-like fashion.
52 Arnaldo Carvalho de Melo <acme@conectiva.com.br> - 11/01/2001
53 check kmalloc and release the allocated memory on failure in
54 mac89x0_probe and in init_module
55 use local_irq_{save,restore}(flags) in net_get_stat, not just
56 local_irq_{dis,en}able()
57 */
59 #define pr_fmt(fmt) KBUILD_MODNAME ": " fmt
61 static const char version[] =
62 "cs89x0.c:v1.02 11/26/96 Russell Nelson <nelson@crynwr.com>\n";
64 #include <linux/module.h>
66 /*
67 Sources:
69 Crynwr packet driver epktisa.
71 Crystal Semiconductor data sheets.
73 */
75 #include <linux/kernel.h>
76 #include <linux/types.h>
77 #include <linux/fcntl.h>
78 #include <linux/interrupt.h>
79 #include <linux/ioport.h>
80 #include <linux/in.h>
81 #include <linux/string.h>
82 #include <linux/nubus.h>
83 #include <linux/errno.h>
84 #include <linux/init.h>
85 #include <linux/netdevice.h>
86 #include <linux/platform_device.h>
87 #include <linux/etherdevice.h>
88 #include <linux/skbuff.h>
89 #include <linux/delay.h>
90 #include <linux/bitops.h>
91 #include <linux/gfp.h>
93 #include <asm/io.h>
94 #include <asm/hwtest.h>
95 #include <asm/macints.h>
97 #include "cs89x0.h"
99 static int debug = -1;
100 module_param(debug, int, 0);
101 MODULE_PARM_DESC(debug, "debug message level");
103 /* Information that need to be kept for each board. */
104 struct net_local {
105 int msg_enable;
106 int chip_type; /* one of: CS8900, CS8920, CS8920M */
107 char chip_revision; /* revision letter of the chip ('A'...) */
108 int send_cmd; /* the propercommand used to send a packet. */
109 int rx_mode;
110 int curr_rx_cfg;
111 int send_underrun; /* keep track of how many underruns in a row we get */
112 };
114 /* Index to functions, as function prototypes. */
115 static int net_open(struct net_device *dev);
116 static netdev_tx_t net_send_packet(struct sk_buff *skb, struct net_device *dev);
117 static irqreturn_t net_interrupt(int irq, void *dev_id);
118 static void set_multicast_list(struct net_device *dev);
119 static void net_rx(struct net_device *dev);
120 static int net_close(struct net_device *dev);
121 static struct net_device_stats *net_get_stats(struct net_device *dev);
122 static int set_mac_address(struct net_device *dev, void *addr);
124 /* For reading/writing registers ISA-style */
125 static inline int
126 readreg_io(struct net_device *dev, int portno)
127 {
128 nubus_writew(swab16(portno), dev->base_addr + ADD_PORT);
129 return swab16(nubus_readw(dev->base_addr + DATA_PORT));
130 }
132 static inline void
133 writereg_io(struct net_device *dev, int portno, int value)
134 {
135 nubus_writew(swab16(portno), dev->base_addr + ADD_PORT);
136 nubus_writew(swab16(value), dev->base_addr + DATA_PORT);
137 }
139 /* These are for reading/writing registers in shared memory */
140 static inline int
141 readreg(struct net_device *dev, int portno)
142 {
143 return swab16(nubus_readw(dev->mem_start + portno));
144 }
146 static inline void
147 writereg(struct net_device *dev, int portno, int value)
148 {
149 nubus_writew(swab16(value), dev->mem_start + portno);
150 }
152 static const struct net_device_ops mac89x0_netdev_ops = {
153 .ndo_open = net_open,
154 .ndo_stop = net_close,
155 .ndo_start_xmit = net_send_packet,
156 .ndo_get_stats = net_get_stats,
157 .ndo_set_rx_mode = set_multicast_list,
158 .ndo_set_mac_address = set_mac_address,
159 .ndo_validate_addr = eth_validate_addr,
160 };
162 /* Probe for the CS8900 card in slot E. We won't bother looking
163 anywhere else until we have a really good reason to do so. */
164 static int mac89x0_device_probe(struct platform_device *pdev)
165 {
166 struct net_device *dev;
167 struct net_local *lp;
168 int i, slot;
169 unsigned rev_type = 0;
170 unsigned long ioaddr;
171 unsigned short sig;
172 int err = -ENODEV;
173 struct nubus_rsrc *fres;
175 dev = alloc_etherdev(sizeof(struct net_local));
176 if (!dev)
177 return -ENOMEM;
179 /* We might have to parameterize this later */
180 slot = 0xE;
181 /* Get out now if there's a real NuBus card in slot E */
182 for_each_func_rsrc(fres)
183 if (fres->board->slot == slot)
184 goto out;
186 /* The pseudo-ISA bits always live at offset 0x300 (gee,
187 wonder why...) */
188 ioaddr = (unsigned long)
189 nubus_slot_addr(slot) | (((slot&0xf) << 20) + DEFAULTIOBASE);
190 {
191 int card_present;
193 card_present = (hwreg_present((void *)ioaddr + 4) &&
194 hwreg_present((void *)ioaddr + DATA_PORT));
195 if (!card_present)
196 goto out;
197 }
199 nubus_writew(0, ioaddr + ADD_PORT);
200 sig = nubus_readw(ioaddr + DATA_PORT);
201 if (sig != swab16(CHIP_EISA_ID_SIG))
202 goto out;
204 SET_NETDEV_DEV(dev, &pdev->dev);
206 /* Initialize the net_device structure. */
207 lp = netdev_priv(dev);
209 lp->msg_enable = netif_msg_init(debug, 0);
211 /* Fill in the 'dev' fields. */
212 dev->base_addr = ioaddr;
213 dev->mem_start = (unsigned long)
214 nubus_slot_addr(slot) | (((slot&0xf) << 20) + MMIOBASE);
215 dev->mem_end = dev->mem_start + 0x1000;
217 /* Turn on shared memory */
218 writereg_io(dev, PP_BusCTL, MEMORY_ON);
220 /* get the chip type */
221 rev_type = readreg(dev, PRODUCT_ID_ADD);
222 lp->chip_type = rev_type &~ REVISON_BITS;
223 lp->chip_revision = ((rev_type & REVISON_BITS) >> 8) + 'A';
225 /* Check the chip type and revision in order to set the correct send command
226 CS8920 revision C and CS8900 revision F can use the faster send. */
227 lp->send_cmd = TX_AFTER_381;
228 if (lp->chip_type == CS8900 && lp->chip_revision >= 'F')
229 lp->send_cmd = TX_NOW;
230 if (lp->chip_type != CS8900 && lp->chip_revision >= 'C')
231 lp->send_cmd = TX_NOW;
233 netif_dbg(lp, drv, dev, "%s", version);
235 pr_info("cs89%c0%s rev %c found at %#8lx\n",
236 lp->chip_type == CS8900 ? '0' : '2',
237 lp->chip_type == CS8920M ? "M" : "",
238 lp->chip_revision, dev->base_addr);
240 /* Try to read the MAC address */
241 if ((readreg(dev, PP_SelfST) & (EEPROM_PRESENT | EEPROM_OK)) == 0) {
242 pr_info("No EEPROM, giving up now.\n");
243 goto out1;
244 } else {
245 for (i = 0; i < ETH_ALEN; i += 2) {
246 /* Big-endian (why??!) */
247 unsigned short s = readreg(dev, PP_IA + i);
248 dev->dev_addr[i] = s >> 8;
249 dev->dev_addr[i+1] = s & 0xff;
250 }
251 }
253 dev->irq = SLOT2IRQ(slot);
255 /* print the IRQ and ethernet address. */
257 pr_info("MAC %pM, IRQ %d\n", dev->dev_addr, dev->irq);
259 dev->netdev_ops = &mac89x0_netdev_ops;
261 err = register_netdev(dev);
262 if (err)
263 goto out1;
265 platform_set_drvdata(pdev, dev);
266 return 0;
267 out1:
268 nubus_writew(0, dev->base_addr + ADD_PORT);
269 out:
270 free_netdev(dev);
271 return err;
272 }
274 /* Open/initialize the board. This is called (in the current kernel)
275 sometime after booting when the 'ifconfig' program is run.
277 This routine should set everything up anew at each open, even
278 registers that "should" only need to be set once at boot, so that
279 there is non-reboot way to recover if something goes wrong.
280 */
281 static int
282 net_open(struct net_device *dev)
283 {
284 struct net_local *lp = netdev_priv(dev);
285 int i;
287 /* Disable the interrupt for now */
288 writereg(dev, PP_BusCTL, readreg(dev, PP_BusCTL) & ~ENABLE_IRQ);
290 /* Grab the interrupt */
291 if (request_irq(dev->irq, net_interrupt, 0, "cs89x0", dev))
292 return -EAGAIN;
294 /* Set up the IRQ - Apparently magic */
295 if (lp->chip_type == CS8900)
296 writereg(dev, PP_CS8900_ISAINT, 0);
297 else
298 writereg(dev, PP_CS8920_ISAINT, 0);
300 /* set the Ethernet address */
301 for (i=0; i < ETH_ALEN/2; i++)
302 writereg(dev, PP_IA+i*2, dev->dev_addr[i*2] | (dev->dev_addr[i*2+1] << 8));
304 /* Turn on both receive and transmit operations */
305 writereg(dev, PP_LineCTL, readreg(dev, PP_LineCTL) | SERIAL_RX_ON | SERIAL_TX_ON);
307 /* Receive only error free packets addressed to this card */
308 lp->rx_mode = 0;
309 writereg(dev, PP_RxCTL, DEF_RX_ACCEPT);
311 lp->curr_rx_cfg = RX_OK_ENBL | RX_CRC_ERROR_ENBL;
313 writereg(dev, PP_RxCFG, lp->curr_rx_cfg);
315 writereg(dev, PP_TxCFG, TX_LOST_CRS_ENBL | TX_SQE_ERROR_ENBL | TX_OK_ENBL |
316 TX_LATE_COL_ENBL | TX_JBR_ENBL | TX_ANY_COL_ENBL | TX_16_COL_ENBL);
318 writereg(dev, PP_BufCFG, READY_FOR_TX_ENBL | RX_MISS_COUNT_OVRFLOW_ENBL |
319 TX_COL_COUNT_OVRFLOW_ENBL | TX_UNDERRUN_ENBL);
321 /* now that we've got our act together, enable everything */
322 writereg(dev, PP_BusCTL, readreg(dev, PP_BusCTL) | ENABLE_IRQ);
323 netif_start_queue(dev);
324 return 0;
325 }
327 static netdev_tx_t
328 net_send_packet(struct sk_buff *skb, struct net_device *dev)
329 {
330 struct net_local *lp = netdev_priv(dev);
331 unsigned long flags;
333 netif_dbg(lp, tx_queued, dev, "sent %d byte packet of type %x\n",
334 skb->len, skb->data[ETH_ALEN + ETH_ALEN] << 8 |
335 skb->data[ETH_ALEN + ETH_ALEN + 1]);
337 /* keep the upload from being interrupted, since we
338 ask the chip to start transmitting before the
339 whole packet has been completely uploaded. */
340 local_irq_save(flags);
341 netif_stop_queue(dev);
343 /* initiate a transmit sequence */
344 writereg(dev, PP_TxCMD, lp->send_cmd);
345 writereg(dev, PP_TxLength, skb->len);
347 /* Test to see if the chip has allocated memory for the packet */
348 if ((readreg(dev, PP_BusST) & READY_FOR_TX_NOW) == 0) {
349 /* Gasp! It hasn't. But that shouldn't happen since
350 we're waiting for TxOk, so return 1 and requeue this packet. */
351 local_irq_restore(flags);
352 return NETDEV_TX_BUSY;
353 }
355 /* Write the contents of the packet */
356 skb_copy_from_linear_data(skb, (void *)(dev->mem_start + PP_TxFrame),
357 skb->len+1);
359 local_irq_restore(flags);
360 dev_kfree_skb (skb);
362 return NETDEV_TX_OK;
363 }
365 /* The typical workload of the driver:
366 Handle the network interface interrupts. */
367 static irqreturn_t net_interrupt(int irq, void *dev_id)
368 {
369 struct net_device *dev = dev_id;
370 struct net_local *lp;
371 int ioaddr, status;
373 ioaddr = dev->base_addr;
374 lp = netdev_priv(dev);
376 /* we MUST read all the events out of the ISQ, otherwise we'll never
377 get interrupted again. As a consequence, we can't have any limit
378 on the number of times we loop in the interrupt handler. The
379 hardware guarantees that eventually we'll run out of events. Of
380 course, if you're on a slow machine, and packets are arriving
381 faster than you can read them off, you're screwed. Hasta la
382 vista, baby! */
383 while ((status = swab16(nubus_readw(dev->base_addr + ISQ_PORT)))) {
384 netif_dbg(lp, intr, dev, "status=%04x\n", status);
385 switch(status & ISQ_EVENT_MASK) {
386 case ISQ_RECEIVER_EVENT:
387 /* Got a packet(s). */
388 net_rx(dev);
389 break;
390 case ISQ_TRANSMITTER_EVENT:
391 dev->stats.tx_packets++;
392 netif_wake_queue(dev);
393 if ((status & TX_OK) == 0)
394 dev->stats.tx_errors++;
395 if (status & TX_LOST_CRS)
396 dev->stats.tx_carrier_errors++;
397 if (status & TX_SQE_ERROR)
398 dev->stats.tx_heartbeat_errors++;
399 if (status & TX_LATE_COL)
400 dev->stats.tx_window_errors++;
401 if (status & TX_16_COL)
402 dev->stats.tx_aborted_errors++;
403 break;
404 case ISQ_BUFFER_EVENT:
405 if (status & READY_FOR_TX) {
406 /* we tried to transmit a packet earlier,
407 but inexplicably ran out of buffers.
408 That shouldn't happen since we only ever
409 load one packet. Shrug. Do the right
410 thing anyway. */
411 netif_wake_queue(dev);
412 }
413 if (status & TX_UNDERRUN) {
414 netif_dbg(lp, tx_err, dev, "transmit underrun\n");
415 lp->send_underrun++;
416 if (lp->send_underrun == 3) lp->send_cmd = TX_AFTER_381;
417 else if (lp->send_underrun == 6) lp->send_cmd = TX_AFTER_ALL;
418 }
419 break;
420 case ISQ_RX_MISS_EVENT:
421 dev->stats.rx_missed_errors += (status >> 6);
422 break;
423 case ISQ_TX_COL_EVENT:
424 dev->stats.collisions += (status >> 6);
425 break;
426 }
427 }
428 return IRQ_HANDLED;
429 }
431 /* We have a good packet(s), get it/them out of the buffers. */
432 static void
433 net_rx(struct net_device *dev)
434 {
435 struct net_local *lp = netdev_priv(dev);
436 struct sk_buff *skb;
437 int status, length;
439 status = readreg(dev, PP_RxStatus);
440 if ((status & RX_OK) == 0) {
441 dev->stats.rx_errors++;
442 if (status & RX_RUNT)
443 dev->stats.rx_length_errors++;
444 if (status & RX_EXTRA_DATA)
445 dev->stats.rx_length_errors++;
446 if ((status & RX_CRC_ERROR) &&
447 !(status & (RX_EXTRA_DATA|RX_RUNT)))
448 /* per str 172 */
449 dev->stats.rx_crc_errors++;
450 if (status & RX_DRIBBLE)
451 dev->stats.rx_frame_errors++;
452 return;
453 }
455 length = readreg(dev, PP_RxLength);
456 /* Malloc up new buffer. */
457 skb = alloc_skb(length, GFP_ATOMIC);
458 if (skb == NULL) {
459 dev->stats.rx_dropped++;
460 return;
461 }
462 skb_put(skb, length);
464 skb_copy_to_linear_data(skb, (void *)(dev->mem_start + PP_RxFrame),
465 length);
467 netif_dbg(lp, rx_status, dev, "received %d byte packet of type %x\n",
468 length, skb->data[ETH_ALEN + ETH_ALEN] << 8 |
469 skb->data[ETH_ALEN + ETH_ALEN + 1]);
471 skb->protocol=eth_type_trans(skb,dev);
472 netif_rx(skb);
473 dev->stats.rx_packets++;
474 dev->stats.rx_bytes += length;
475 }
477 /* The inverse routine to net_open(). */
478 static int
479 net_close(struct net_device *dev)
480 {
482 writereg(dev, PP_RxCFG, 0);
483 writereg(dev, PP_TxCFG, 0);
484 writereg(dev, PP_BufCFG, 0);
485 writereg(dev, PP_BusCTL, 0);
487 netif_stop_queue(dev);
489 free_irq(dev->irq, dev);
491 /* Update the statistics here. */
493 return 0;
495 }
497 /* Get the current statistics. This may be called with the card open or
498 closed. */
499 static struct net_device_stats *
500 net_get_stats(struct net_device *dev)
501 {
502 unsigned long flags;
504 local_irq_save(flags);
505 /* Update the statistics from the device registers. */
506 dev->stats.rx_missed_errors += (readreg(dev, PP_RxMiss) >> 6);
507 dev->stats.collisions += (readreg(dev, PP_TxCol) >> 6);
508 local_irq_restore(flags);
510 return &dev->stats;
511 }
513 static void set_multicast_list(struct net_device *dev)
514 {
515 struct net_local *lp = netdev_priv(dev);
517 if(dev->flags&IFF_PROMISC)
518 {
519 lp->rx_mode = RX_ALL_ACCEPT;
520 } else if ((dev->flags & IFF_ALLMULTI) || !netdev_mc_empty(dev)) {
521 /* The multicast-accept list is initialized to accept-all, and we
522 rely on higher-level filtering for now. */
523 lp->rx_mode = RX_MULTCAST_ACCEPT;
524 }
525 else
526 lp->rx_mode = 0;
528 writereg(dev, PP_RxCTL, DEF_RX_ACCEPT | lp->rx_mode);
530 /* in promiscuous mode, we accept errored packets, so we have to enable interrupts on them also */
531 writereg(dev, PP_RxCFG, lp->curr_rx_cfg |
532 (lp->rx_mode == RX_ALL_ACCEPT? (RX_CRC_ERROR_ENBL|RX_RUNT_ENBL|RX_EXTRA_DATA_ENBL) : 0));
533 }
536 static int set_mac_address(struct net_device *dev, void *addr)
537 {
538 struct sockaddr *saddr = addr;
539 int i;
541 if (!is_valid_ether_addr(saddr->sa_data))
542 return -EADDRNOTAVAIL;
544 memcpy(dev->dev_addr, saddr->sa_data, ETH_ALEN);
545 netdev_info(dev, "Setting MAC address to %pM\n", dev->dev_addr);
547 /* set the Ethernet address */
548 for (i=0; i < ETH_ALEN/2; i++)
549 writereg(dev, PP_IA+i*2, dev->dev_addr[i*2] | (dev->dev_addr[i*2+1] << 8));
551 return 0;
552 }
554 MODULE_LICENSE("GPL");
556 static int mac89x0_device_remove(struct platform_device *pdev)
557 {
558 struct net_device *dev = platform_get_drvdata(pdev);
560 unregister_netdev(dev);
561 nubus_writew(0, dev->base_addr + ADD_PORT);
562 free_netdev(dev);
563 return 0;
564 }
566 static struct platform_driver mac89x0_platform_driver = {
567 .probe = mac89x0_device_probe,
568 .remove = mac89x0_device_remove,
569 .driver = {
570 .name = "mac89x0",
571 },
572 };
574 module_platform_driver(mac89x0_platform_driver);