1 config STMMAC_ETH
2 tristate "STMicroelectronics 10/100/1000/EQOS Ethernet driver"
3 depends on HAS_IOMEM && HAS_DMA
4 select MII
5 select PHYLIB
6 select CRC32
7 imply PTP_1588_CLOCK
8 select RESET_CONTROLLER
9 ---help---
10 This is the driver for the Ethernet IPs built around a
11 Synopsys IP Core.
13 if STMMAC_ETH
15 config STMMAC_PLATFORM
16 tristate "STMMAC Platform bus support"
17 depends on STMMAC_ETH
18 select MFD_SYSCON
19 default y
20 ---help---
21 This selects the platform specific bus support for the stmmac driver.
22 This is the driver used on several SoCs:
23 STi, Allwinner, Amlogic Meson, Altera SOCFPGA.
25 If you have a controller with this interface, say Y or M here.
27 If unsure, say N.
29 if STMMAC_PLATFORM
31 config DWMAC_DWC_QOS_ETH
32 tristate "Support for snps,dwc-qos-ethernet.txt DT binding."
33 select PHYLIB
34 select CRC32
35 select MII
36 depends on OF && HAS_DMA
37 help
38 Support for chips using the snps,dwc-qos-ethernet.txt DT binding.
40 config DWMAC_GENERIC
41 tristate "Generic driver for DWMAC"
42 default STMMAC_PLATFORM
43 ---help---
44 Generic DWMAC driver for platforms that don't require any
45 platform specific code to function or is using platform
46 data for setup.
48 config DWMAC_ANARION
49 tristate "Adaptrum Anarion GMAC support"
50 default ARC
51 depends on OF && (ARC || COMPILE_TEST)
52 help
53 Support for Adaptrum Anarion GMAC Ethernet controller.
55 This selects the Anarion SoC glue layer support for the stmmac driver.
57 config DWMAC_IPQ806X
58 tristate "QCA IPQ806x DWMAC support"
59 default ARCH_QCOM
60 depends on OF && (ARCH_QCOM || COMPILE_TEST)
61 select MFD_SYSCON
62 help
63 Support for QCA IPQ806X DWMAC Ethernet.
65 This selects the IPQ806x SoC glue layer support for the stmmac
66 device driver. This driver does not use any of the hardware
67 acceleration features available on this SoC. Network devices
68 will behave like standard non-accelerated ethernet interfaces.
70 config DWMAC_LPC18XX
71 tristate "NXP LPC18xx/43xx DWMAC support"
72 default ARCH_LPC18XX
73 depends on OF && (ARCH_LPC18XX || COMPILE_TEST)
74 select MFD_SYSCON
75 ---help---
76 Support for NXP LPC18xx/43xx DWMAC Ethernet.
78 config DWMAC_MESON
79 tristate "Amlogic Meson dwmac support"
80 default ARCH_MESON
81 depends on OF && COMMON_CLK && (ARCH_MESON || COMPILE_TEST)
82 help
83 Support for Ethernet controller on Amlogic Meson SoCs.
85 This selects the Amlogic Meson SoC glue layer support for
86 the stmmac device driver. This driver is used for Meson6,
87 Meson8, Meson8b and GXBB SoCs.
89 config DWMAC_OXNAS
90 tristate "Oxford Semiconductor OXNAS dwmac support"
91 default ARCH_OXNAS
92 depends on OF && COMMON_CLK && (ARCH_OXNAS || COMPILE_TEST)
93 select MFD_SYSCON
94 help
95 Support for Ethernet controller on Oxford Semiconductor OXNAS SoCs.
97 This selects the Oxford Semiconductor OXNASSoC glue layer support for
98 the stmmac device driver. This driver is used for OX820.
100 config DWMAC_ROCKCHIP
101 tristate "Rockchip dwmac support"
102 default ARCH_ROCKCHIP
103 depends on OF && (ARCH_ROCKCHIP || COMPILE_TEST)
104 select MFD_SYSCON
105 help
106 Support for Ethernet controller on Rockchip RK3288 SoC.
108 This selects the Rockchip RK3288 SoC glue layer support for
109 the stmmac device driver.
111 config DWMAC_SOCFPGA
112 tristate "SOCFPGA dwmac support"
113 default (ARCH_SOCFPGA || ARCH_STRATIX10)
114 depends on OF && (ARCH_SOCFPGA || ARCH_STRATIX10 || COMPILE_TEST)
115 select MFD_SYSCON
116 help
117 Support for ethernet controller on Altera SOCFPGA
119 This selects the Altera SOCFPGA SoC glue layer support
120 for the stmmac device driver. This driver is used for
121 arria5 and cyclone5 FPGA SoCs.
123 config DWMAC_STI
124 tristate "STi GMAC support"
125 default ARCH_STI
126 depends on OF && (ARCH_STI || COMPILE_TEST)
127 select MFD_SYSCON
128 ---help---
129 Support for ethernet controller on STi SOCs.
131 This selects STi SoC glue layer support for the stmmac
132 device driver. This driver is used on for the STi series
133 SOCs GMAC ethernet controller.
135 config DWMAC_STM32
136 tristate "STM32 DWMAC support"
137 default ARCH_STM32
138 depends on OF && HAS_IOMEM && (ARCH_STM32 || COMPILE_TEST)
139 select MFD_SYSCON
140 ---help---
141 Support for ethernet controller on STM32 SOCs.
143 This selects STM32 SoC glue layer support for the stmmac
144 device driver. This driver is used on for the STM32 series
145 SOCs GMAC ethernet controller.
147 config DWMAC_SUNXI
148 tristate "Allwinner GMAC support"
149 default ARCH_SUNXI
150 depends on OF && (ARCH_SUNXI || COMPILE_TEST)
151 ---help---
152 Support for Allwinner A20/A31 GMAC ethernet controllers.
154 This selects Allwinner SoC glue layer support for the
155 stmmac device driver. This driver is used for A20/A31
156 GMAC ethernet controller.
158 config DWMAC_SUN8I
159 tristate "Allwinner sun8i GMAC support"
160 default ARCH_SUNXI
161 depends on OF && (ARCH_SUNXI || COMPILE_TEST)
162 select MDIO_BUS_MUX
163 ---help---
164 Support for Allwinner H3 A83T A64 EMAC ethernet controllers.
166 This selects Allwinner SoC glue layer support for the
167 stmmac device driver. This driver is used for H3/A83T/A64
168 EMAC ethernet controller.
169 endif
171 config STMMAC_PCI
172 tristate "STMMAC PCI bus support"
173 depends on STMMAC_ETH && PCI
174 ---help---
175 This selects the platform specific bus support for the stmmac driver.
176 This driver was tested on XLINX XC2V3000 FF1152AMT0221
177 D1215994A VIRTEX FPGA board and SNPS QoS IPK Prototyping Kit.
179 If you have a controller with this interface, say Y or M here.
181 If unsure, say N.
182 endif