1 /*******************************************************************************
2 This contains the functions to handle the platform driver.
4 Copyright (C) 2007-2011 STMicroelectronics Ltd
6 This program is free software; you can redistribute it and/or modify it
7 under the terms and conditions of the GNU General Public License,
8 version 2, as published by the Free Software Foundation.
10 This program is distributed in the hope it will be useful, but WITHOUT
11 ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
12 FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
13 more details.
15 The full GNU General Public License is included in this distribution in
16 the file called "COPYING".
18 Author: Giuseppe Cavallaro <peppe.cavallaro@st.com>
19 *******************************************************************************/
21 #include <linux/platform_device.h>
22 #include <linux/module.h>
23 #include <linux/io.h>
24 #include <linux/of.h>
25 #include <linux/of_net.h>
26 #include <linux/of_device.h>
27 #include <linux/of_mdio.h>
29 #include "stmmac.h"
30 #include "stmmac_platform.h"
32 #ifdef CONFIG_OF
34 /**
35 * dwmac1000_validate_mcast_bins - validates the number of Multicast filter bins
36 * @mcast_bins: Multicast filtering bins
37 * Description:
38 * this function validates the number of Multicast filtering bins specified
39 * by the configuration through the device tree. The Synopsys GMAC supports
40 * 64 bins, 128 bins, or 256 bins. "bins" refer to the division of CRC
41 * number space. 64 bins correspond to 6 bits of the CRC, 128 corresponds
42 * to 7 bits, and 256 refers to 8 bits of the CRC. Any other setting is
43 * invalid and will cause the filtering algorithm to use Multicast
44 * promiscuous mode.
45 */
46 static int dwmac1000_validate_mcast_bins(int mcast_bins)
47 {
48 int x = mcast_bins;
50 switch (x) {
51 case HASH_TABLE_SIZE:
52 case 128:
53 case 256:
54 break;
55 default:
56 x = 0;
57 pr_info("Hash table entries set to unexpected value %d",
58 mcast_bins);
59 break;
60 }
61 return x;
62 }
64 /**
65 * dwmac1000_validate_ucast_entries - validate the Unicast address entries
66 * @ucast_entries: number of Unicast address entries
67 * Description:
68 * This function validates the number of Unicast address entries supported
69 * by a particular Synopsys 10/100/1000 controller. The Synopsys controller
70 * supports 1..32, 64, or 128 Unicast filter entries for it's Unicast filter
71 * logic. This function validates a valid, supported configuration is
72 * selected, and defaults to 1 Unicast address if an unsupported
73 * configuration is selected.
74 */
75 static int dwmac1000_validate_ucast_entries(int ucast_entries)
76 {
77 int x = ucast_entries;
79 switch (x) {
80 case 1 ... 32:
81 case 64:
82 case 128:
83 break;
84 default:
85 x = 1;
86 pr_info("Unicast table entries set to unexpected value %d\n",
87 ucast_entries);
88 break;
89 }
90 return x;
91 }
93 /**
94 * stmmac_axi_setup - parse DT parameters for programming the AXI register
95 * @pdev: platform device
96 * Description:
97 * if required, from device-tree the AXI internal register can be tuned
98 * by using platform parameters.
99 */
100 static struct stmmac_axi *stmmac_axi_setup(struct platform_device *pdev)
101 {
102 struct device_node *np;
103 struct stmmac_axi *axi;
105 np = of_parse_phandle(pdev->dev.of_node, "snps,axi-config", 0);
106 if (!np)
107 return NULL;
109 axi = devm_kzalloc(&pdev->dev, sizeof(*axi), GFP_KERNEL);
110 if (!axi) {
111 of_node_put(np);
112 return ERR_PTR(-ENOMEM);
113 }
115 axi->axi_lpi_en = of_property_read_bool(np, "snps,lpi_en");
116 axi->axi_xit_frm = of_property_read_bool(np, "snps,xit_frm");
117 axi->axi_kbbe = of_property_read_bool(np, "snps,axi_kbbe");
118 axi->axi_fb = of_property_read_bool(np, "snps,axi_fb");
119 axi->axi_mb = of_property_read_bool(np, "snps,axi_mb");
120 axi->axi_rb = of_property_read_bool(np, "snps,axi_rb");
122 if (of_property_read_u32(np, "snps,wr_osr_lmt", &axi->axi_wr_osr_lmt))
123 axi->axi_wr_osr_lmt = 1;
124 if (of_property_read_u32(np, "snps,rd_osr_lmt", &axi->axi_rd_osr_lmt))
125 axi->axi_rd_osr_lmt = 1;
126 of_property_read_u32_array(np, "snps,blen", axi->axi_blen, AXI_BLEN);
127 of_node_put(np);
129 return axi;
130 }
132 /**
133 * stmmac_mtl_setup - parse DT parameters for multiple queues configuration
134 * @pdev: platform device
135 */
136 static int stmmac_mtl_setup(struct platform_device *pdev,
137 struct plat_stmmacenet_data *plat)
138 {
139 struct device_node *q_node;
140 struct device_node *rx_node;
141 struct device_node *tx_node;
142 u8 queue = 0;
143 int ret = 0;
145 /* For backwards-compatibility with device trees that don't have any
146 * snps,mtl-rx-config or snps,mtl-tx-config properties, we fall back
147 * to one RX and TX queues each.
148 */
149 plat->rx_queues_to_use = 1;
150 plat->tx_queues_to_use = 1;
152 /* First Queue must always be in DCB mode. As MTL_QUEUE_DCB = 1 we need
153 * to always set this, otherwise Queue will be classified as AVB
154 * (because MTL_QUEUE_AVB = 0).
155 */
156 plat->rx_queues_cfg[0].mode_to_use = MTL_QUEUE_DCB;
157 plat->tx_queues_cfg[0].mode_to_use = MTL_QUEUE_DCB;
159 rx_node = of_parse_phandle(pdev->dev.of_node, "snps,mtl-rx-config", 0);
160 if (!rx_node)
161 return ret;
163 tx_node = of_parse_phandle(pdev->dev.of_node, "snps,mtl-tx-config", 0);
164 if (!tx_node) {
165 of_node_put(rx_node);
166 return ret;
167 }
169 /* Processing RX queues common config */
170 if (of_property_read_u32(rx_node, "snps,rx-queues-to-use",
171 &plat->rx_queues_to_use))
172 plat->rx_queues_to_use = 1;
174 if (of_property_read_bool(rx_node, "snps,rx-sched-sp"))
175 plat->rx_sched_algorithm = MTL_RX_ALGORITHM_SP;
176 else if (of_property_read_bool(rx_node, "snps,rx-sched-wsp"))
177 plat->rx_sched_algorithm = MTL_RX_ALGORITHM_WSP;
178 else
179 plat->rx_sched_algorithm = MTL_RX_ALGORITHM_SP;
181 /* Processing individual RX queue config */
182 for_each_child_of_node(rx_node, q_node) {
183 if (queue >= plat->rx_queues_to_use)
184 break;
186 if (of_property_read_bool(q_node, "snps,dcb-algorithm"))
187 plat->rx_queues_cfg[queue].mode_to_use = MTL_QUEUE_DCB;
188 else if (of_property_read_bool(q_node, "snps,avb-algorithm"))
189 plat->rx_queues_cfg[queue].mode_to_use = MTL_QUEUE_AVB;
190 else
191 plat->rx_queues_cfg[queue].mode_to_use = MTL_QUEUE_DCB;
193 if (of_property_read_u32(q_node, "snps,map-to-dma-channel",
194 &plat->rx_queues_cfg[queue].chan))
195 plat->rx_queues_cfg[queue].chan = queue;
196 /* TODO: Dynamic mapping to be included in the future */
198 if (of_property_read_u32(q_node, "snps,priority",
199 &plat->rx_queues_cfg[queue].prio)) {
200 plat->rx_queues_cfg[queue].prio = 0;
201 plat->rx_queues_cfg[queue].use_prio = false;
202 } else {
203 plat->rx_queues_cfg[queue].use_prio = true;
204 }
206 /* RX queue specific packet type routing */
207 if (of_property_read_bool(q_node, "snps,route-avcp"))
208 plat->rx_queues_cfg[queue].pkt_route = PACKET_AVCPQ;
209 else if (of_property_read_bool(q_node, "snps,route-ptp"))
210 plat->rx_queues_cfg[queue].pkt_route = PACKET_PTPQ;
211 else if (of_property_read_bool(q_node, "snps,route-dcbcp"))
212 plat->rx_queues_cfg[queue].pkt_route = PACKET_DCBCPQ;
213 else if (of_property_read_bool(q_node, "snps,route-up"))
214 plat->rx_queues_cfg[queue].pkt_route = PACKET_UPQ;
215 else if (of_property_read_bool(q_node, "snps,route-multi-broad"))
216 plat->rx_queues_cfg[queue].pkt_route = PACKET_MCBCQ;
217 else
218 plat->rx_queues_cfg[queue].pkt_route = 0x0;
220 queue++;
221 }
222 if (queue != plat->rx_queues_to_use) {
223 ret = -EINVAL;
224 dev_err(&pdev->dev, "Not all RX queues were configured\n");
225 goto out;
226 }
228 /* Processing TX queues common config */
229 if (of_property_read_u32(tx_node, "snps,tx-queues-to-use",
230 &plat->tx_queues_to_use))
231 plat->tx_queues_to_use = 1;
233 if (of_property_read_bool(tx_node, "snps,tx-sched-wrr"))
234 plat->tx_sched_algorithm = MTL_TX_ALGORITHM_WRR;
235 else if (of_property_read_bool(tx_node, "snps,tx-sched-wfq"))
236 plat->tx_sched_algorithm = MTL_TX_ALGORITHM_WFQ;
237 else if (of_property_read_bool(tx_node, "snps,tx-sched-dwrr"))
238 plat->tx_sched_algorithm = MTL_TX_ALGORITHM_DWRR;
239 else if (of_property_read_bool(tx_node, "snps,tx-sched-sp"))
240 plat->tx_sched_algorithm = MTL_TX_ALGORITHM_SP;
241 else
242 plat->tx_sched_algorithm = MTL_TX_ALGORITHM_SP;
244 queue = 0;
246 /* Processing individual TX queue config */
247 for_each_child_of_node(tx_node, q_node) {
248 if (queue >= plat->tx_queues_to_use)
249 break;
251 if (of_property_read_u32(q_node, "snps,weight",
252 &plat->tx_queues_cfg[queue].weight))
253 plat->tx_queues_cfg[queue].weight = 0x10 + queue;
255 if (of_property_read_bool(q_node, "snps,dcb-algorithm")) {
256 plat->tx_queues_cfg[queue].mode_to_use = MTL_QUEUE_DCB;
257 } else if (of_property_read_bool(q_node,
258 "snps,avb-algorithm")) {
259 plat->tx_queues_cfg[queue].mode_to_use = MTL_QUEUE_AVB;
261 /* Credit Base Shaper parameters used by AVB */
262 if (of_property_read_u32(q_node, "snps,send_slope",
263 &plat->tx_queues_cfg[queue].send_slope))
264 plat->tx_queues_cfg[queue].send_slope = 0x0;
265 if (of_property_read_u32(q_node, "snps,idle_slope",
266 &plat->tx_queues_cfg[queue].idle_slope))
267 plat->tx_queues_cfg[queue].idle_slope = 0x0;
268 if (of_property_read_u32(q_node, "snps,high_credit",
269 &plat->tx_queues_cfg[queue].high_credit))
270 plat->tx_queues_cfg[queue].high_credit = 0x0;
271 if (of_property_read_u32(q_node, "snps,low_credit",
272 &plat->tx_queues_cfg[queue].low_credit))
273 plat->tx_queues_cfg[queue].low_credit = 0x0;
274 } else {
275 plat->tx_queues_cfg[queue].mode_to_use = MTL_QUEUE_DCB;
276 }
278 if (of_property_read_u32(q_node, "snps,priority",
279 &plat->tx_queues_cfg[queue].prio)) {
280 plat->tx_queues_cfg[queue].prio = 0;
281 plat->tx_queues_cfg[queue].use_prio = false;
282 } else {
283 plat->tx_queues_cfg[queue].use_prio = true;
284 }
286 queue++;
287 }
288 if (queue != plat->tx_queues_to_use) {
289 ret = -EINVAL;
290 dev_err(&pdev->dev, "Not all TX queues were configured\n");
291 goto out;
292 }
294 out:
295 of_node_put(rx_node);
296 of_node_put(tx_node);
297 of_node_put(q_node);
299 return ret;
300 }
302 /**
303 * stmmac_dt_phy - parse device-tree driver parameters to allocate PHY resources
304 * @plat: driver data platform structure
305 * @np: device tree node
306 * @dev: device pointer
307 * Description:
308 * The mdio bus will be allocated in case of a phy transceiver is on board;
309 * it will be NULL if the fixed-link is configured.
310 * If there is the "snps,dwmac-mdio" sub-node the mdio will be allocated
311 * in any case (for DSA, mdio must be registered even if fixed-link).
312 * The table below sums the supported configurations:
313 * -------------------------------
314 * snps,phy-addr | Y
315 * -------------------------------
316 * phy-handle | Y
317 * -------------------------------
318 * fixed-link | N
319 * -------------------------------
320 * snps,dwmac-mdio |
321 * even if | Y
322 * fixed-link |
323 * -------------------------------
324 *
325 * It returns 0 in case of success otherwise -ENODEV.
326 */
327 static int stmmac_dt_phy(struct plat_stmmacenet_data *plat,
328 struct device_node *np, struct device *dev)
329 {
330 bool mdio = true;
331 static const struct of_device_id need_mdio_ids[] = {
332 { .compatible = "snps,dwc-qos-ethernet-4.10" },
333 {},
334 };
336 /* If phy-handle property is passed from DT, use it as the PHY */
337 plat->phy_node = of_parse_phandle(np, "phy-handle", 0);
338 if (plat->phy_node)
339 dev_dbg(dev, "Found phy-handle subnode\n");
341 /* If phy-handle is not specified, check if we have a fixed-phy */
342 if (!plat->phy_node && of_phy_is_fixed_link(np)) {
343 if ((of_phy_register_fixed_link(np) < 0))
344 return -ENODEV;
346 dev_dbg(dev, "Found fixed-link subnode\n");
347 plat->phy_node = of_node_get(np);
348 mdio = false;
349 }
351 if (of_match_node(need_mdio_ids, np)) {
352 plat->mdio_node = of_get_child_by_name(np, "mdio");
353 } else {
354 /**
355 * If snps,dwmac-mdio is passed from DT, always register
356 * the MDIO
357 */
358 for_each_child_of_node(np, plat->mdio_node) {
359 if (of_device_is_compatible(plat->mdio_node,
360 "snps,dwmac-mdio"))
361 break;
362 }
363 }
365 if (plat->mdio_node) {
366 dev_dbg(dev, "Found MDIO subnode\n");
367 mdio = true;
368 }
370 if (mdio)
371 plat->mdio_bus_data =
372 devm_kzalloc(dev, sizeof(struct stmmac_mdio_bus_data),
373 GFP_KERNEL);
374 return 0;
375 }
377 /**
378 * stmmac_probe_config_dt - parse device-tree driver parameters
379 * @pdev: platform_device structure
380 * @mac: MAC address to use
381 * Description:
382 * this function is to read the driver parameters from device-tree and
383 * set some private fields that will be used by the main at runtime.
384 */
385 struct plat_stmmacenet_data *
386 stmmac_probe_config_dt(struct platform_device *pdev, const char **mac)
387 {
388 struct device_node *np = pdev->dev.of_node;
389 struct plat_stmmacenet_data *plat;
390 struct stmmac_dma_cfg *dma_cfg;
391 int rc;
393 plat = devm_kzalloc(&pdev->dev, sizeof(*plat), GFP_KERNEL);
394 if (!plat)
395 return ERR_PTR(-ENOMEM);
397 *mac = of_get_mac_address(np);
398 plat->interface = of_get_phy_mode(np);
400 /* Get max speed of operation from device tree */
401 if (of_property_read_u32(np, "max-speed", &plat->max_speed))
402 plat->max_speed = -1;
404 plat->bus_id = of_alias_get_id(np, "ethernet");
405 if (plat->bus_id < 0)
406 plat->bus_id = 0;
408 /* Default to phy auto-detection */
409 plat->phy_addr = -1;
411 /* "snps,phy-addr" is not a standard property. Mark it as deprecated
412 * and warn of its use. Remove this when phy node support is added.
413 */
414 if (of_property_read_u32(np, "snps,phy-addr", &plat->phy_addr) == 0)
415 dev_warn(&pdev->dev, "snps,phy-addr property is deprecated\n");
417 /* To Configure PHY by using all device-tree supported properties */
418 rc = stmmac_dt_phy(plat, np, &pdev->dev);
419 if (rc)
420 return ERR_PTR(rc);
422 of_property_read_u32(np, "tx-fifo-depth", &plat->tx_fifo_size);
424 of_property_read_u32(np, "rx-fifo-depth", &plat->rx_fifo_size);
426 plat->force_sf_dma_mode =
427 of_property_read_bool(np, "snps,force_sf_dma_mode");
429 plat->en_tx_lpi_clockgating =
430 of_property_read_bool(np, "snps,en-tx-lpi-clockgating");
432 /* Set the maxmtu to a default of JUMBO_LEN in case the
433 * parameter is not present in the device tree.
434 */
435 plat->maxmtu = JUMBO_LEN;
437 /* Set default value for multicast hash bins */
438 plat->multicast_filter_bins = HASH_TABLE_SIZE;
440 /* Set default value for unicast filter entries */
441 plat->unicast_filter_entries = 1;
443 /*
444 * Currently only the properties needed on SPEAr600
445 * are provided. All other properties should be added
446 * once needed on other platforms.
447 */
448 if (of_device_is_compatible(np, "st,spear600-gmac") ||
449 of_device_is_compatible(np, "snps,dwmac-3.50a") ||
450 of_device_is_compatible(np, "snps,dwmac-3.70a") ||
451 of_device_is_compatible(np, "snps,dwmac")) {
452 /* Note that the max-frame-size parameter as defined in the
453 * ePAPR v1.1 spec is defined as max-frame-size, it's
454 * actually used as the IEEE definition of MAC Client
455 * data, or MTU. The ePAPR specification is confusing as
456 * the definition is max-frame-size, but usage examples
457 * are clearly MTUs
458 */
459 of_property_read_u32(np, "max-frame-size", &plat->maxmtu);
460 of_property_read_u32(np, "snps,multicast-filter-bins",
461 &plat->multicast_filter_bins);
462 of_property_read_u32(np, "snps,perfect-filter-entries",
463 &plat->unicast_filter_entries);
464 plat->unicast_filter_entries = dwmac1000_validate_ucast_entries(
465 plat->unicast_filter_entries);
466 plat->multicast_filter_bins = dwmac1000_validate_mcast_bins(
467 plat->multicast_filter_bins);
468 plat->has_gmac = 1;
469 plat->pmt = 1;
470 }
472 if (of_device_is_compatible(np, "snps,dwmac-4.00") ||
473 of_device_is_compatible(np, "snps,dwmac-4.10a") ||
474 of_device_is_compatible(np, "snps,dwmac-4.20a")) {
475 plat->has_gmac4 = 1;
476 plat->has_gmac = 0;
477 plat->pmt = 1;
478 plat->tso_en = of_property_read_bool(np, "snps,tso");
479 }
481 if (of_device_is_compatible(np, "snps,dwmac-3.610") ||
482 of_device_is_compatible(np, "snps,dwmac-3.710")) {
483 plat->enh_desc = 1;
484 plat->bugged_jumbo = 1;
485 plat->force_sf_dma_mode = 1;
486 }
488 if (of_device_is_compatible(np, "snps,dwxgmac")) {
489 plat->has_xgmac = 1;
490 plat->pmt = 1;
491 plat->tso_en = of_property_read_bool(np, "snps,tso");
492 }
494 dma_cfg = devm_kzalloc(&pdev->dev, sizeof(*dma_cfg),
495 GFP_KERNEL);
496 if (!dma_cfg) {
497 stmmac_remove_config_dt(pdev, plat);
498 return ERR_PTR(-ENOMEM);
499 }
500 plat->dma_cfg = dma_cfg;
502 of_property_read_u32(np, "snps,pbl", &dma_cfg->pbl);
503 if (!dma_cfg->pbl)
504 dma_cfg->pbl = DEFAULT_DMA_PBL;
505 of_property_read_u32(np, "snps,txpbl", &dma_cfg->txpbl);
506 of_property_read_u32(np, "snps,rxpbl", &dma_cfg->rxpbl);
507 dma_cfg->pblx8 = !of_property_read_bool(np, "snps,no-pbl-x8");
509 dma_cfg->aal = of_property_read_bool(np, "snps,aal");
510 dma_cfg->fixed_burst = of_property_read_bool(np, "snps,fixed-burst");
511 dma_cfg->mixed_burst = of_property_read_bool(np, "snps,mixed-burst");
513 plat->force_thresh_dma_mode = of_property_read_bool(np, "snps,force_thresh_dma_mode");
514 if (plat->force_thresh_dma_mode) {
515 plat->force_sf_dma_mode = 0;
516 pr_warn("force_sf_dma_mode is ignored if force_thresh_dma_mode is set.");
517 }
519 of_property_read_u32(np, "snps,ps-speed", &plat->mac_port_sel_speed);
521 plat->axi = stmmac_axi_setup(pdev);
523 rc = stmmac_mtl_setup(pdev, plat);
524 if (rc) {
525 stmmac_remove_config_dt(pdev, plat);
526 return ERR_PTR(rc);
527 }
529 /* clock setup */
530 plat->stmmac_clk = devm_clk_get(&pdev->dev,
531 STMMAC_RESOURCE_NAME);
532 if (IS_ERR(plat->stmmac_clk)) {
533 dev_warn(&pdev->dev, "Cannot get CSR clock\n");
534 plat->stmmac_clk = NULL;
535 }
536 clk_prepare_enable(plat->stmmac_clk);
538 plat->pclk = devm_clk_get(&pdev->dev, "pclk");
539 if (IS_ERR(plat->pclk)) {
540 if (PTR_ERR(plat->pclk) == -EPROBE_DEFER)
541 goto error_pclk_get;
543 plat->pclk = NULL;
544 }
545 clk_prepare_enable(plat->pclk);
547 /* Fall-back to main clock in case of no PTP ref is passed */
548 plat->clk_ptp_ref = devm_clk_get(&pdev->dev, "ptp_ref");
549 if (IS_ERR(plat->clk_ptp_ref)) {
550 plat->clk_ptp_rate = clk_get_rate(plat->stmmac_clk);
551 plat->clk_ptp_ref = NULL;
552 dev_warn(&pdev->dev, "PTP uses main clock\n");
553 } else {
554 plat->clk_ptp_rate = clk_get_rate(plat->clk_ptp_ref);
555 dev_dbg(&pdev->dev, "PTP rate %d\n", plat->clk_ptp_rate);
556 }
558 plat->stmmac_rst = devm_reset_control_get(&pdev->dev,
559 STMMAC_RESOURCE_NAME);
560 if (IS_ERR(plat->stmmac_rst)) {
561 if (PTR_ERR(plat->stmmac_rst) == -EPROBE_DEFER)
562 goto error_hw_init;
564 dev_info(&pdev->dev, "no reset control found\n");
565 plat->stmmac_rst = NULL;
566 }
568 return plat;
570 error_hw_init:
571 clk_disable_unprepare(plat->pclk);
572 error_pclk_get:
573 clk_disable_unprepare(plat->stmmac_clk);
575 return ERR_PTR(-EPROBE_DEFER);
576 }
578 /**
579 * stmmac_remove_config_dt - undo the effects of stmmac_probe_config_dt()
580 * @pdev: platform_device structure
581 * @plat: driver data platform structure
582 *
583 * Release resources claimed by stmmac_probe_config_dt().
584 */
585 void stmmac_remove_config_dt(struct platform_device *pdev,
586 struct plat_stmmacenet_data *plat)
587 {
588 struct device_node *np = pdev->dev.of_node;
590 if (of_phy_is_fixed_link(np))
591 of_phy_deregister_fixed_link(np);
592 of_node_put(plat->phy_node);
593 of_node_put(plat->mdio_node);
594 }
595 #else
596 struct plat_stmmacenet_data *
597 stmmac_probe_config_dt(struct platform_device *pdev, const char **mac)
598 {
599 return ERR_PTR(-EINVAL);
600 }
602 void stmmac_remove_config_dt(struct platform_device *pdev,
603 struct plat_stmmacenet_data *plat)
604 {
605 }
606 #endif /* CONFIG_OF */
607 EXPORT_SYMBOL_GPL(stmmac_probe_config_dt);
608 EXPORT_SYMBOL_GPL(stmmac_remove_config_dt);
610 int stmmac_get_platform_resources(struct platform_device *pdev,
611 struct stmmac_resources *stmmac_res)
612 {
613 struct resource *res;
615 memset(stmmac_res, 0, sizeof(*stmmac_res));
617 /* Get IRQ information early to have an ability to ask for deferred
618 * probe if needed before we went too far with resource allocation.
619 */
620 stmmac_res->irq = platform_get_irq_byname(pdev, "macirq");
621 if (stmmac_res->irq < 0) {
622 if (stmmac_res->irq != -EPROBE_DEFER) {
623 dev_err(&pdev->dev,
624 "MAC IRQ configuration information not found\n");
625 }
626 return stmmac_res->irq;
627 }
629 /* On some platforms e.g. SPEAr the wake up irq differs from the mac irq
630 * The external wake up irq can be passed through the platform code
631 * named as "eth_wake_irq"
632 *
633 * In case the wake up interrupt is not passed from the platform
634 * so the driver will continue to use the mac irq (ndev->irq)
635 */
636 stmmac_res->wol_irq = platform_get_irq_byname(pdev, "eth_wake_irq");
637 if (stmmac_res->wol_irq < 0) {
638 if (stmmac_res->wol_irq == -EPROBE_DEFER)
639 return -EPROBE_DEFER;
640 stmmac_res->wol_irq = stmmac_res->irq;
641 }
643 stmmac_res->lpi_irq = platform_get_irq_byname(pdev, "eth_lpi");
644 if (stmmac_res->lpi_irq == -EPROBE_DEFER)
645 return -EPROBE_DEFER;
647 res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
648 stmmac_res->addr = devm_ioremap_resource(&pdev->dev, res);
650 return PTR_ERR_OR_ZERO(stmmac_res->addr);
651 }
652 EXPORT_SYMBOL_GPL(stmmac_get_platform_resources);
654 /**
655 * stmmac_pltfr_remove
656 * @pdev: platform device pointer
657 * Description: this function calls the main to free the net resources
658 * and calls the platforms hook and release the resources (e.g. mem).
659 */
660 int stmmac_pltfr_remove(struct platform_device *pdev)
661 {
662 struct net_device *ndev = platform_get_drvdata(pdev);
663 struct stmmac_priv *priv = netdev_priv(ndev);
664 struct plat_stmmacenet_data *plat = priv->plat;
665 int ret = stmmac_dvr_remove(&pdev->dev);
667 if (plat->exit)
668 plat->exit(pdev, plat->bsp_priv);
670 stmmac_remove_config_dt(pdev, plat);
672 return ret;
673 }
674 EXPORT_SYMBOL_GPL(stmmac_pltfr_remove);
676 #ifdef CONFIG_PM_SLEEP
677 /**
678 * stmmac_pltfr_suspend
679 * @dev: device pointer
680 * Description: this function is invoked when suspend the driver and it direcly
681 * call the main suspend function and then, if required, on some platform, it
682 * can call an exit helper.
683 */
684 static int stmmac_pltfr_suspend(struct device *dev)
685 {
686 int ret;
687 struct net_device *ndev = dev_get_drvdata(dev);
688 struct stmmac_priv *priv = netdev_priv(ndev);
689 struct platform_device *pdev = to_platform_device(dev);
691 ret = stmmac_suspend(dev);
692 if (priv->plat->exit)
693 priv->plat->exit(pdev, priv->plat->bsp_priv);
695 return ret;
696 }
698 /**
699 * stmmac_pltfr_resume
700 * @dev: device pointer
701 * Description: this function is invoked when resume the driver before calling
702 * the main resume function, on some platforms, it can call own init helper
703 * if required.
704 */
705 static int stmmac_pltfr_resume(struct device *dev)
706 {
707 struct net_device *ndev = dev_get_drvdata(dev);
708 struct stmmac_priv *priv = netdev_priv(ndev);
709 struct platform_device *pdev = to_platform_device(dev);
711 if (priv->plat->init)
712 priv->plat->init(pdev, priv->plat->bsp_priv);
714 return stmmac_resume(dev);
715 }
716 #endif /* CONFIG_PM_SLEEP */
718 SIMPLE_DEV_PM_OPS(stmmac_pltfr_pm_ops, stmmac_pltfr_suspend,
719 stmmac_pltfr_resume);
720 EXPORT_SYMBOL_GPL(stmmac_pltfr_pm_ops);
722 MODULE_DESCRIPTION("STMMAC 10/100/1000 Ethernet platform support");
723 MODULE_AUTHOR("Giuseppe Cavallaro <peppe.cavallaro@st.com>");
724 MODULE_LICENSE("GPL");