1 #
2 # TI device configuration
3 #
5 config NET_VENDOR_TI
6 bool "Texas Instruments (TI) devices"
7 default y
8 depends on PCI || EISA || AR7 || ARCH_DAVINCI || ARCH_OMAP2PLUS || ARCH_KEYSTONE
9 ---help---
10 If you have a network (Ethernet) card belonging to this class, say Y.
12 Note that the answer to this question doesn't directly affect the
13 kernel: saying N will just cause the configurator to skip all
14 the questions about TI devices. If you say Y, you will be asked for
15 your specific card in the following questions.
17 if NET_VENDOR_TI
19 config TI_DAVINCI_EMAC
20 tristate "TI DaVinci EMAC Support"
21 depends on ARM && ( ARCH_DAVINCI || ARCH_OMAP3 ) || COMPILE_TEST
22 select TI_DAVINCI_MDIO
23 select TI_DAVINCI_CPDMA
24 select PHYLIB
25 ---help---
26 This driver supports TI's DaVinci Ethernet .
28 To compile this driver as a module, choose M here: the module
29 will be called davinci_emac_driver. This is recommended.
31 config TI_DAVINCI_MDIO
32 tristate "TI DaVinci MDIO Support"
33 depends on ARCH_DAVINCI || ARCH_OMAP2PLUS || ARCH_KEYSTONE || COMPILE_TEST
34 select PHYLIB
35 ---help---
36 This driver supports TI's DaVinci MDIO module.
38 To compile this driver as a module, choose M here: the module
39 will be called davinci_mdio. This is recommended.
41 config TI_DAVINCI_CPDMA
42 tristate "TI DaVinci CPDMA Support"
43 depends on ARCH_DAVINCI || ARCH_OMAP2PLUS || COMPILE_TEST
44 select GENERIC_ALLOCATOR
45 ---help---
46 This driver supports TI's DaVinci CPDMA dma engine.
48 To compile this driver as a module, choose M here: the module
49 will be called davinci_cpdma. This is recommended.
51 config TI_CPSW_PHY_SEL
52 bool
53 ---help---
54 This driver supports configuring of the phy mode connected to
55 the CPSW.
57 config TI_CPSW_ALE
58 tristate "TI CPSW ALE Support"
59 ---help---
60 This driver supports TI's CPSW ALE module.
62 config TI_CPSW
63 tristate "TI CPSW Switch Support"
64 depends on ARCH_DAVINCI || ARCH_OMAP2PLUS || COMPILE_TEST
65 select TI_DAVINCI_CPDMA
66 select TI_DAVINCI_MDIO
67 select TI_CPSW_PHY_SEL
68 select TI_CPSW_ALE
69 select MFD_SYSCON
70 select REGMAP
71 ---help---
72 This driver supports TI's CPSW Ethernet Switch.
74 To compile this driver as a module, choose M here: the module
75 will be called cpsw.
77 config TI_CPTS
78 bool "TI Common Platform Time Sync (CPTS) Support"
79 depends on TI_CPSW || TI_KEYSTONE_NETCP || COMPILE_TEST
80 depends on POSIX_TIMERS
81 ---help---
82 This driver supports the Common Platform Time Sync unit of
83 the CPSW Ethernet Switch and Keystone 2 1g/10g Switch Subsystem.
84 The unit can time stamp PTP UDP/IPv4 and Layer 2 packets, and the
85 driver offers a PTP Hardware Clock.
87 config TI_CPTS_MOD
88 tristate
89 depends on TI_CPTS
90 default y if TI_CPSW=y || TI_KEYSTONE_NETCP=y
91 select NET_PTP_CLASSIFY
92 imply PTP_1588_CLOCK
93 default m
95 config TI_KEYSTONE_NETCP
96 tristate "TI Keystone NETCP Core Support"
97 select TI_CPSW_ALE
98 select TI_DAVINCI_MDIO
99 depends on OF
100 depends on KEYSTONE_NAVIGATOR_DMA && KEYSTONE_NAVIGATOR_QMSS
101 ---help---
102 This driver supports TI's Keystone NETCP Core.
104 To compile this driver as a module, choose M here: the module
105 will be called keystone_netcp.
107 config TI_KEYSTONE_NETCP_ETHSS
108 depends on TI_KEYSTONE_NETCP
109 tristate "TI Keystone NETCP Ethernet subsystem Support"
110 ---help---
112 To compile this driver as a module, choose M here: the module
113 will be called keystone_netcp_ethss.
115 config TLAN
116 tristate "TI ThunderLAN support"
117 depends on (PCI || EISA)
118 ---help---
119 If you have a PCI Ethernet network card based on the ThunderLAN chip
120 which is supported by this driver, say Y here.
122 Devices currently supported by this driver are Compaq Netelligent,
123 Compaq NetFlex and Olicom cards. Please read the file
124 <file:Documentation/networking/tlan.txt> for more details.
126 To compile this driver as a module, choose M here. The module
127 will be called tlan.
129 Please email feedback to <torben.mathiasen@compaq.com>.
131 config CPMAC
132 tristate "TI AR7 CPMAC Ethernet support"
133 depends on AR7
134 select PHYLIB
135 ---help---
136 TI AR7 CPMAC Ethernet support
138 endif # NET_VENDOR_TI