1 /*
2 * ASIX AX8817X based USB 2.0 Ethernet Devices
3 * Copyright (C) 2003-2006 David Hollis <dhollis@davehollis.com>
4 * Copyright (C) 2005 Phil Chang <pchang23@sbcglobal.net>
5 * Copyright (C) 2006 James Painter <jamie.painter@iname.com>
6 * Copyright (c) 2002-2003 TiVo Inc.
7 *
8 * This program is free software; you can redistribute it and/or modify
9 * it under the terms of the GNU General Public License as published by
10 * the Free Software Foundation; either version 2 of the License, or
11 * (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, see <http://www.gnu.org/licenses/>.
20 */
22 #include "asix.h"
24 int asix_read_cmd(struct usbnet *dev, u8 cmd, u16 value, u16 index,
25 u16 size, void *data, int in_pm)
26 {
27 int ret;
28 int (*fn)(struct usbnet *, u8, u8, u16, u16, void *, u16);
30 BUG_ON(!dev);
32 if (!in_pm)
33 fn = usbnet_read_cmd;
34 else
35 fn = usbnet_read_cmd_nopm;
37 ret = fn(dev, cmd, USB_DIR_IN | USB_TYPE_VENDOR | USB_RECIP_DEVICE,
38 value, index, data, size);
40 if (unlikely(ret < 0))
41 netdev_warn(dev->net, "Failed to read reg index 0x%04x: %d\n",
42 index, ret);
44 return ret;
45 }
47 int asix_write_cmd(struct usbnet *dev, u8 cmd, u16 value, u16 index,
48 u16 size, void *data, int in_pm)
49 {
50 int ret;
51 int (*fn)(struct usbnet *, u8, u8, u16, u16, const void *, u16);
53 BUG_ON(!dev);
55 if (!in_pm)
56 fn = usbnet_write_cmd;
57 else
58 fn = usbnet_write_cmd_nopm;
60 ret = fn(dev, cmd, USB_DIR_OUT | USB_TYPE_VENDOR | USB_RECIP_DEVICE,
61 value, index, data, size);
63 if (unlikely(ret < 0))
64 netdev_warn(dev->net, "Failed to write reg index 0x%04x: %d\n",
65 index, ret);
67 return ret;
68 }
70 void asix_write_cmd_async(struct usbnet *dev, u8 cmd, u16 value, u16 index,
71 u16 size, void *data)
72 {
73 usbnet_write_cmd_async(dev, cmd,
74 USB_DIR_OUT | USB_TYPE_VENDOR | USB_RECIP_DEVICE,
75 value, index, data, size);
76 }
78 static void reset_asix_rx_fixup_info(struct asix_rx_fixup_info *rx)
79 {
80 /* Reset the variables that have a lifetime outside of
81 * asix_rx_fixup_internal() so that future processing starts from a
82 * known set of initial conditions.
83 */
85 if (rx->ax_skb) {
86 /* Discard any incomplete Ethernet frame in the netdev buffer */
87 kfree_skb(rx->ax_skb);
88 rx->ax_skb = NULL;
89 }
91 /* Assume the Data header 32-bit word is at the start of the current
92 * or next URB socket buffer so reset all the state variables.
93 */
94 rx->remaining = 0;
95 rx->split_head = false;
96 rx->header = 0;
97 }
99 int asix_rx_fixup_internal(struct usbnet *dev, struct sk_buff *skb,
100 struct asix_rx_fixup_info *rx)
101 {
102 int offset = 0;
103 u16 size;
105 /* When an Ethernet frame spans multiple URB socket buffers,
106 * do a sanity test for the Data header synchronisation.
107 * Attempt to detect the situation of the previous socket buffer having
108 * been truncated or a socket buffer was missing. These situations
109 * cause a discontinuity in the data stream and therefore need to avoid
110 * appending bad data to the end of the current netdev socket buffer.
111 * Also avoid unnecessarily discarding a good current netdev socket
112 * buffer.
113 */
114 if (rx->remaining && (rx->remaining + sizeof(u32) <= skb->len)) {
115 offset = ((rx->remaining + 1) & 0xfffe);
116 rx->header = get_unaligned_le32(skb->data + offset);
117 offset = 0;
119 size = (u16)(rx->header & 0x7ff);
120 if (size != ((~rx->header >> 16) & 0x7ff)) {
121 netdev_err(dev->net, "asix_rx_fixup() Data Header synchronisation was lost, remaining %d\n",
122 rx->remaining);
123 reset_asix_rx_fixup_info(rx);
124 }
125 }
127 while (offset + sizeof(u16) <= skb->len) {
128 u16 copy_length;
130 if (!rx->remaining) {
131 if (skb->len - offset == sizeof(u16)) {
132 rx->header = get_unaligned_le16(
133 skb->data + offset);
134 rx->split_head = true;
135 offset += sizeof(u16);
136 break;
137 }
139 if (rx->split_head == true) {
140 rx->header |= (get_unaligned_le16(
141 skb->data + offset) << 16);
142 rx->split_head = false;
143 offset += sizeof(u16);
144 } else {
145 rx->header = get_unaligned_le32(skb->data +
146 offset);
147 offset += sizeof(u32);
148 }
150 /* take frame length from Data header 32-bit word */
151 size = (u16)(rx->header & 0x7ff);
152 if (size != ((~rx->header >> 16) & 0x7ff)) {
153 netdev_err(dev->net, "asix_rx_fixup() Bad Header Length 0x%x, offset %d\n",
154 rx->header, offset);
155 reset_asix_rx_fixup_info(rx);
156 return 0;
157 }
158 if (size > dev->net->mtu + ETH_HLEN + VLAN_HLEN) {
159 netdev_dbg(dev->net, "asix_rx_fixup() Bad RX Length %d\n",
160 size);
161 reset_asix_rx_fixup_info(rx);
162 return 0;
163 }
165 /* Sometimes may fail to get a netdev socket buffer but
166 * continue to process the URB socket buffer so that
167 * synchronisation of the Ethernet frame Data header
168 * word is maintained.
169 */
170 rx->ax_skb = netdev_alloc_skb_ip_align(dev->net, size);
172 rx->remaining = size;
173 }
175 if (rx->remaining > skb->len - offset) {
176 copy_length = skb->len - offset;
177 rx->remaining -= copy_length;
178 } else {
179 copy_length = rx->remaining;
180 rx->remaining = 0;
181 }
183 if (rx->ax_skb) {
184 skb_put_data(rx->ax_skb, skb->data + offset,
185 copy_length);
186 if (!rx->remaining) {
187 usbnet_skb_return(dev, rx->ax_skb);
188 rx->ax_skb = NULL;
189 }
190 }
192 offset += (copy_length + 1) & 0xfffe;
193 }
195 if (skb->len != offset) {
196 netdev_err(dev->net, "asix_rx_fixup() Bad SKB Length %d, %d\n",
197 skb->len, offset);
198 reset_asix_rx_fixup_info(rx);
199 return 0;
200 }
202 return 1;
203 }
205 int asix_rx_fixup_common(struct usbnet *dev, struct sk_buff *skb)
206 {
207 struct asix_common_private *dp = dev->driver_priv;
208 struct asix_rx_fixup_info *rx = &dp->rx_fixup_info;
210 return asix_rx_fixup_internal(dev, skb, rx);
211 }
213 void asix_rx_fixup_common_free(struct asix_common_private *dp)
214 {
215 struct asix_rx_fixup_info *rx;
217 if (!dp)
218 return;
220 rx = &dp->rx_fixup_info;
222 if (rx->ax_skb) {
223 kfree_skb(rx->ax_skb);
224 rx->ax_skb = NULL;
225 }
226 }
228 struct sk_buff *asix_tx_fixup(struct usbnet *dev, struct sk_buff *skb,
229 gfp_t flags)
230 {
231 int padlen;
232 int headroom = skb_headroom(skb);
233 int tailroom = skb_tailroom(skb);
234 u32 packet_len;
235 u32 padbytes = 0xffff0000;
237 padlen = ((skb->len + 4) & (dev->maxpacket - 1)) ? 0 : 4;
239 /* We need to push 4 bytes in front of frame (packet_len)
240 * and maybe add 4 bytes after the end (if padlen is 4)
241 *
242 * Avoid skb_copy_expand() expensive call, using following rules :
243 * - We are allowed to push 4 bytes in headroom if skb_header_cloned()
244 * is false (and if we have 4 bytes of headroom)
245 * - We are allowed to put 4 bytes at tail if skb_cloned()
246 * is false (and if we have 4 bytes of tailroom)
247 *
248 * TCP packets for example are cloned, but __skb_header_release()
249 * was called in tcp stack, allowing us to use headroom for our needs.
250 */
251 if (!skb_header_cloned(skb) &&
252 !(padlen && skb_cloned(skb)) &&
253 headroom + tailroom >= 4 + padlen) {
254 /* following should not happen, but better be safe */
255 if (headroom < 4 ||
256 tailroom < padlen) {
257 skb->data = memmove(skb->head + 4, skb->data, skb->len);
258 skb_set_tail_pointer(skb, skb->len);
259 }
260 } else {
261 struct sk_buff *skb2;
263 skb2 = skb_copy_expand(skb, 4, padlen, flags);
264 dev_kfree_skb_any(skb);
265 skb = skb2;
266 if (!skb)
267 return NULL;
268 }
270 packet_len = ((skb->len ^ 0x0000ffff) << 16) + skb->len;
271 skb_push(skb, 4);
272 cpu_to_le32s(&packet_len);
273 skb_copy_to_linear_data(skb, &packet_len, sizeof(packet_len));
275 if (padlen) {
276 cpu_to_le32s(&padbytes);
277 memcpy(skb_tail_pointer(skb), &padbytes, sizeof(padbytes));
278 skb_put(skb, sizeof(padbytes));
279 }
281 usbnet_set_skb_tx_stats(skb, 1, 0);
282 return skb;
283 }
285 int asix_set_sw_mii(struct usbnet *dev, int in_pm)
286 {
287 int ret;
288 ret = asix_write_cmd(dev, AX_CMD_SET_SW_MII, 0x0000, 0, 0, NULL, in_pm);
290 if (ret < 0)
291 netdev_err(dev->net, "Failed to enable software MII access\n");
292 return ret;
293 }
295 int asix_set_hw_mii(struct usbnet *dev, int in_pm)
296 {
297 int ret;
298 ret = asix_write_cmd(dev, AX_CMD_SET_HW_MII, 0x0000, 0, 0, NULL, in_pm);
299 if (ret < 0)
300 netdev_err(dev->net, "Failed to enable hardware MII access\n");
301 return ret;
302 }
304 int asix_read_phy_addr(struct usbnet *dev, int internal)
305 {
306 int offset = (internal ? 1 : 0);
307 u8 buf[2];
308 int ret = asix_read_cmd(dev, AX_CMD_READ_PHY_ID, 0, 0, 2, buf, 0);
310 netdev_dbg(dev->net, "asix_get_phy_addr()\n");
312 if (ret < 0) {
313 netdev_err(dev->net, "Error reading PHYID register: %02x\n", ret);
314 goto out;
315 }
316 netdev_dbg(dev->net, "asix_get_phy_addr() returning 0x%04x\n",
317 *((__le16 *)buf));
318 ret = buf[offset];
320 out:
321 return ret;
322 }
324 int asix_get_phy_addr(struct usbnet *dev)
325 {
326 /* return the address of the internal phy */
327 return asix_read_phy_addr(dev, 1);
328 }
331 int asix_sw_reset(struct usbnet *dev, u8 flags, int in_pm)
332 {
333 int ret;
335 ret = asix_write_cmd(dev, AX_CMD_SW_RESET, flags, 0, 0, NULL, in_pm);
336 if (ret < 0)
337 netdev_err(dev->net, "Failed to send software reset: %02x\n", ret);
339 return ret;
340 }
342 u16 asix_read_rx_ctl(struct usbnet *dev, int in_pm)
343 {
344 __le16 v;
345 int ret = asix_read_cmd(dev, AX_CMD_READ_RX_CTL, 0, 0, 2, &v, in_pm);
347 if (ret < 0) {
348 netdev_err(dev->net, "Error reading RX_CTL register: %02x\n", ret);
349 goto out;
350 }
351 ret = le16_to_cpu(v);
352 out:
353 return ret;
354 }
356 int asix_write_rx_ctl(struct usbnet *dev, u16 mode, int in_pm)
357 {
358 int ret;
360 netdev_dbg(dev->net, "asix_write_rx_ctl() - mode = 0x%04x\n", mode);
361 ret = asix_write_cmd(dev, AX_CMD_WRITE_RX_CTL, mode, 0, 0, NULL, in_pm);
362 if (ret < 0)
363 netdev_err(dev->net, "Failed to write RX_CTL mode to 0x%04x: %02x\n",
364 mode, ret);
366 return ret;
367 }
369 u16 asix_read_medium_status(struct usbnet *dev, int in_pm)
370 {
371 __le16 v;
372 int ret = asix_read_cmd(dev, AX_CMD_READ_MEDIUM_STATUS,
373 0, 0, 2, &v, in_pm);
375 if (ret < 0) {
376 netdev_err(dev->net, "Error reading Medium Status register: %02x\n",
377 ret);
378 return ret; /* TODO: callers not checking for error ret */
379 }
381 return le16_to_cpu(v);
383 }
385 int asix_write_medium_mode(struct usbnet *dev, u16 mode, int in_pm)
386 {
387 int ret;
389 netdev_dbg(dev->net, "asix_write_medium_mode() - mode = 0x%04x\n", mode);
390 ret = asix_write_cmd(dev, AX_CMD_WRITE_MEDIUM_MODE,
391 mode, 0, 0, NULL, in_pm);
392 if (ret < 0)
393 netdev_err(dev->net, "Failed to write Medium Mode mode to 0x%04x: %02x\n",
394 mode, ret);
396 return ret;
397 }
399 int asix_write_gpio(struct usbnet *dev, u16 value, int sleep, int in_pm)
400 {
401 int ret;
403 netdev_dbg(dev->net, "asix_write_gpio() - value = 0x%04x\n", value);
404 ret = asix_write_cmd(dev, AX_CMD_WRITE_GPIOS, value, 0, 0, NULL, in_pm);
405 if (ret < 0)
406 netdev_err(dev->net, "Failed to write GPIO value 0x%04x: %02x\n",
407 value, ret);
409 if (sleep)
410 msleep(sleep);
412 return ret;
413 }
415 /*
416 * AX88772 & AX88178 have a 16-bit RX_CTL value
417 */
418 void asix_set_multicast(struct net_device *net)
419 {
420 struct usbnet *dev = netdev_priv(net);
421 struct asix_data *data = (struct asix_data *)&dev->data;
422 u16 rx_ctl = AX_DEFAULT_RX_CTL;
424 if (net->flags & IFF_PROMISC) {
425 rx_ctl |= AX_RX_CTL_PRO;
426 } else if (net->flags & IFF_ALLMULTI ||
427 netdev_mc_count(net) > AX_MAX_MCAST) {
428 rx_ctl |= AX_RX_CTL_AMALL;
429 } else if (netdev_mc_empty(net)) {
430 /* just broadcast and directed */
431 } else {
432 /* We use the 20 byte dev->data
433 * for our 8 byte filter buffer
434 * to avoid allocating memory that
435 * is tricky to free later */
436 struct netdev_hw_addr *ha;
437 u32 crc_bits;
439 memset(data->multi_filter, 0, AX_MCAST_FILTER_SIZE);
441 /* Build the multicast hash filter. */
442 netdev_for_each_mc_addr(ha, net) {
443 crc_bits = ether_crc(ETH_ALEN, ha->addr) >> 26;
444 data->multi_filter[crc_bits >> 3] |=
445 1 << (crc_bits & 7);
446 }
448 asix_write_cmd_async(dev, AX_CMD_WRITE_MULTI_FILTER, 0, 0,
449 AX_MCAST_FILTER_SIZE, data->multi_filter);
451 rx_ctl |= AX_RX_CTL_AM;
452 }
454 asix_write_cmd_async(dev, AX_CMD_WRITE_RX_CTL, rx_ctl, 0, 0, NULL);
455 }
457 int asix_mdio_read(struct net_device *netdev, int phy_id, int loc)
458 {
459 struct usbnet *dev = netdev_priv(netdev);
460 __le16 res;
461 u8 smsr;
462 int i = 0;
463 int ret;
465 mutex_lock(&dev->phy_mutex);
466 do {
467 ret = asix_set_sw_mii(dev, 0);
468 if (ret == -ENODEV || ret == -ETIMEDOUT)
469 break;
470 usleep_range(1000, 1100);
471 ret = asix_read_cmd(dev, AX_CMD_STATMNGSTS_REG,
472 0, 0, 1, &smsr, 0);
473 } while (!(smsr & AX_HOST_EN) && (i++ < 30) && (ret != -ENODEV));
474 if (ret == -ENODEV || ret == -ETIMEDOUT) {
475 mutex_unlock(&dev->phy_mutex);
476 return ret;
477 }
479 asix_read_cmd(dev, AX_CMD_READ_MII_REG, phy_id,
480 (__u16)loc, 2, &res, 0);
481 asix_set_hw_mii(dev, 0);
482 mutex_unlock(&dev->phy_mutex);
484 netdev_dbg(dev->net, "asix_mdio_read() phy_id=0x%02x, loc=0x%02x, returns=0x%04x\n",
485 phy_id, loc, le16_to_cpu(res));
487 return le16_to_cpu(res);
488 }
490 void asix_mdio_write(struct net_device *netdev, int phy_id, int loc, int val)
491 {
492 struct usbnet *dev = netdev_priv(netdev);
493 __le16 res = cpu_to_le16(val);
494 u8 smsr;
495 int i = 0;
496 int ret;
498 netdev_dbg(dev->net, "asix_mdio_write() phy_id=0x%02x, loc=0x%02x, val=0x%04x\n",
499 phy_id, loc, val);
501 mutex_lock(&dev->phy_mutex);
502 do {
503 ret = asix_set_sw_mii(dev, 0);
504 if (ret == -ENODEV)
505 break;
506 usleep_range(1000, 1100);
507 ret = asix_read_cmd(dev, AX_CMD_STATMNGSTS_REG,
508 0, 0, 1, &smsr, 0);
509 } while (!(smsr & AX_HOST_EN) && (i++ < 30) && (ret != -ENODEV));
510 if (ret == -ENODEV) {
511 mutex_unlock(&dev->phy_mutex);
512 return;
513 }
515 asix_write_cmd(dev, AX_CMD_WRITE_MII_REG, phy_id,
516 (__u16)loc, 2, &res, 0);
517 asix_set_hw_mii(dev, 0);
518 mutex_unlock(&dev->phy_mutex);
519 }
521 int asix_mdio_read_nopm(struct net_device *netdev, int phy_id, int loc)
522 {
523 struct usbnet *dev = netdev_priv(netdev);
524 __le16 res;
525 u8 smsr;
526 int i = 0;
527 int ret;
529 mutex_lock(&dev->phy_mutex);
530 do {
531 ret = asix_set_sw_mii(dev, 1);
532 if (ret == -ENODEV || ret == -ETIMEDOUT)
533 break;
534 usleep_range(1000, 1100);
535 ret = asix_read_cmd(dev, AX_CMD_STATMNGSTS_REG,
536 0, 0, 1, &smsr, 1);
537 } while (!(smsr & AX_HOST_EN) && (i++ < 30) && (ret != -ENODEV));
538 if (ret == -ENODEV || ret == -ETIMEDOUT) {
539 mutex_unlock(&dev->phy_mutex);
540 return ret;
541 }
543 asix_read_cmd(dev, AX_CMD_READ_MII_REG, phy_id,
544 (__u16)loc, 2, &res, 1);
545 asix_set_hw_mii(dev, 1);
546 mutex_unlock(&dev->phy_mutex);
548 netdev_dbg(dev->net, "asix_mdio_read_nopm() phy_id=0x%02x, loc=0x%02x, returns=0x%04x\n",
549 phy_id, loc, le16_to_cpu(res));
551 return le16_to_cpu(res);
552 }
554 void
555 asix_mdio_write_nopm(struct net_device *netdev, int phy_id, int loc, int val)
556 {
557 struct usbnet *dev = netdev_priv(netdev);
558 __le16 res = cpu_to_le16(val);
559 u8 smsr;
560 int i = 0;
561 int ret;
563 netdev_dbg(dev->net, "asix_mdio_write() phy_id=0x%02x, loc=0x%02x, val=0x%04x\n",
564 phy_id, loc, val);
566 mutex_lock(&dev->phy_mutex);
567 do {
568 ret = asix_set_sw_mii(dev, 1);
569 if (ret == -ENODEV)
570 break;
571 usleep_range(1000, 1100);
572 ret = asix_read_cmd(dev, AX_CMD_STATMNGSTS_REG,
573 0, 0, 1, &smsr, 1);
574 } while (!(smsr & AX_HOST_EN) && (i++ < 30) && (ret != -ENODEV));
575 if (ret == -ENODEV) {
576 mutex_unlock(&dev->phy_mutex);
577 return;
578 }
580 asix_write_cmd(dev, AX_CMD_WRITE_MII_REG, phy_id,
581 (__u16)loc, 2, &res, 1);
582 asix_set_hw_mii(dev, 1);
583 mutex_unlock(&dev->phy_mutex);
584 }
586 void asix_get_wol(struct net_device *net, struct ethtool_wolinfo *wolinfo)
587 {
588 struct usbnet *dev = netdev_priv(net);
589 u8 opt;
591 if (asix_read_cmd(dev, AX_CMD_READ_MONITOR_MODE,
592 0, 0, 1, &opt, 0) < 0) {
593 wolinfo->supported = 0;
594 wolinfo->wolopts = 0;
595 return;
596 }
597 wolinfo->supported = WAKE_PHY | WAKE_MAGIC;
598 wolinfo->wolopts = 0;
599 if (opt & AX_MONITOR_LINK)
600 wolinfo->wolopts |= WAKE_PHY;
601 if (opt & AX_MONITOR_MAGIC)
602 wolinfo->wolopts |= WAKE_MAGIC;
603 }
605 int asix_set_wol(struct net_device *net, struct ethtool_wolinfo *wolinfo)
606 {
607 struct usbnet *dev = netdev_priv(net);
608 u8 opt = 0;
610 if (wolinfo->wolopts & ~(WAKE_PHY | WAKE_MAGIC))
611 return -EINVAL;
613 if (wolinfo->wolopts & WAKE_PHY)
614 opt |= AX_MONITOR_LINK;
615 if (wolinfo->wolopts & WAKE_MAGIC)
616 opt |= AX_MONITOR_MAGIC;
618 if (asix_write_cmd(dev, AX_CMD_WRITE_MONITOR_MODE,
619 opt, 0, 0, NULL, 0) < 0)
620 return -EINVAL;
622 return 0;
623 }
625 int asix_get_eeprom_len(struct net_device *net)
626 {
627 return AX_EEPROM_LEN;
628 }
630 int asix_get_eeprom(struct net_device *net, struct ethtool_eeprom *eeprom,
631 u8 *data)
632 {
633 struct usbnet *dev = netdev_priv(net);
634 u16 *eeprom_buff;
635 int first_word, last_word;
636 int i;
638 if (eeprom->len == 0)
639 return -EINVAL;
641 eeprom->magic = AX_EEPROM_MAGIC;
643 first_word = eeprom->offset >> 1;
644 last_word = (eeprom->offset + eeprom->len - 1) >> 1;
646 eeprom_buff = kmalloc_array(last_word - first_word + 1, sizeof(u16),
647 GFP_KERNEL);
648 if (!eeprom_buff)
649 return -ENOMEM;
651 /* ax8817x returns 2 bytes from eeprom on read */
652 for (i = first_word; i <= last_word; i++) {
653 if (asix_read_cmd(dev, AX_CMD_READ_EEPROM, i, 0, 2,
654 &eeprom_buff[i - first_word], 0) < 0) {
655 kfree(eeprom_buff);
656 return -EIO;
657 }
658 }
660 memcpy(data, (u8 *)eeprom_buff + (eeprom->offset & 1), eeprom->len);
661 kfree(eeprom_buff);
662 return 0;
663 }
665 int asix_set_eeprom(struct net_device *net, struct ethtool_eeprom *eeprom,
666 u8 *data)
667 {
668 struct usbnet *dev = netdev_priv(net);
669 u16 *eeprom_buff;
670 int first_word, last_word;
671 int i;
672 int ret;
674 netdev_dbg(net, "write EEPROM len %d, offset %d, magic 0x%x\n",
675 eeprom->len, eeprom->offset, eeprom->magic);
677 if (eeprom->len == 0)
678 return -EINVAL;
680 if (eeprom->magic != AX_EEPROM_MAGIC)
681 return -EINVAL;
683 first_word = eeprom->offset >> 1;
684 last_word = (eeprom->offset + eeprom->len - 1) >> 1;
686 eeprom_buff = kmalloc_array(last_word - first_word + 1, sizeof(u16),
687 GFP_KERNEL);
688 if (!eeprom_buff)
689 return -ENOMEM;
691 /* align data to 16 bit boundaries, read the missing data from
692 the EEPROM */
693 if (eeprom->offset & 1) {
694 ret = asix_read_cmd(dev, AX_CMD_READ_EEPROM, first_word, 0, 2,
695 &eeprom_buff[0], 0);
696 if (ret < 0) {
697 netdev_err(net, "Failed to read EEPROM at offset 0x%02x.\n", first_word);
698 goto free;
699 }
700 }
702 if ((eeprom->offset + eeprom->len) & 1) {
703 ret = asix_read_cmd(dev, AX_CMD_READ_EEPROM, last_word, 0, 2,
704 &eeprom_buff[last_word - first_word], 0);
705 if (ret < 0) {
706 netdev_err(net, "Failed to read EEPROM at offset 0x%02x.\n", last_word);
707 goto free;
708 }
709 }
711 memcpy((u8 *)eeprom_buff + (eeprom->offset & 1), data, eeprom->len);
713 /* write data to EEPROM */
714 ret = asix_write_cmd(dev, AX_CMD_WRITE_ENABLE, 0x0000, 0, 0, NULL, 0);
715 if (ret < 0) {
716 netdev_err(net, "Failed to enable EEPROM write\n");
717 goto free;
718 }
719 msleep(20);
721 for (i = first_word; i <= last_word; i++) {
722 netdev_dbg(net, "write to EEPROM at offset 0x%02x, data 0x%04x\n",
723 i, eeprom_buff[i - first_word]);
724 ret = asix_write_cmd(dev, AX_CMD_WRITE_EEPROM, i,
725 eeprom_buff[i - first_word], 0, NULL, 0);
726 if (ret < 0) {
727 netdev_err(net, "Failed to write EEPROM at offset 0x%02x.\n",
728 i);
729 goto free;
730 }
731 msleep(20);
732 }
734 ret = asix_write_cmd(dev, AX_CMD_WRITE_DISABLE, 0x0000, 0, 0, NULL, 0);
735 if (ret < 0) {
736 netdev_err(net, "Failed to disable EEPROM write\n");
737 goto free;
738 }
740 ret = 0;
741 free:
742 kfree(eeprom_buff);
743 return ret;
744 }
746 void asix_get_drvinfo(struct net_device *net, struct ethtool_drvinfo *info)
747 {
748 /* Inherit standard device info */
749 usbnet_get_drvinfo(net, info);
750 strlcpy(info->driver, DRIVER_NAME, sizeof(info->driver));
751 strlcpy(info->version, DRIVER_VERSION, sizeof(info->version));
752 }
754 int asix_set_mac_address(struct net_device *net, void *p)
755 {
756 struct usbnet *dev = netdev_priv(net);
757 struct asix_data *data = (struct asix_data *)&dev->data;
758 struct sockaddr *addr = p;
760 if (netif_running(net))
761 return -EBUSY;
762 if (!is_valid_ether_addr(addr->sa_data))
763 return -EADDRNOTAVAIL;
765 memcpy(net->dev_addr, addr->sa_data, ETH_ALEN);
767 /* We use the 20 byte dev->data
768 * for our 6 byte mac buffer
769 * to avoid allocating memory that
770 * is tricky to free later */
771 memcpy(data->mac_addr, addr->sa_data, ETH_ALEN);
772 asix_write_cmd_async(dev, AX_CMD_WRITE_NODE_ID, 0, 0, ETH_ALEN,
773 data->mac_addr);
775 return 0;
776 }