1 /*
2 * OMAP Remote Processor driver
3 *
4 * Copyright (C) 2011 Texas Instruments, Inc.
5 * Copyright (C) 2011 Google, Inc.
6 *
7 * Ohad Ben-Cohen <ohad@wizery.com>
8 * Brian Swetland <swetland@google.com>
9 * Fernando Guzman Lugo <fernando.lugo@ti.com>
10 * Mark Grosen <mgrosen@ti.com>
11 * Suman Anna <s-anna@ti.com>
12 * Hari Kanigeri <h-kanigeri2@ti.com>
13 *
14 * This program is free software; you can redistribute it and/or
15 * modify it under the terms of the GNU General Public License
16 * version 2 as published by the Free Software Foundation.
17 *
18 * This program is distributed in the hope that it will be useful,
19 * but WITHOUT ANY WARRANTY; without even the implied warranty of
20 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
21 * GNU General Public License for more details.
22 */
24 #include <linux/kernel.h>
25 #include <linux/module.h>
26 #include <linux/err.h>
27 #include <linux/platform_device.h>
28 #include <linux/dma-mapping.h>
29 #include <linux/remoteproc.h>
30 #include <linux/mailbox_client.h>
31 #include <linux/omap-mailbox.h>
33 #include <linux/platform_data/remoteproc-omap.h>
35 #include "omap_remoteproc.h"
36 #include "remoteproc_internal.h"
38 /**
39 * struct omap_rproc - omap remote processor state
40 * @mbox: mailbox channel handle
41 * @client: mailbox client to request the mailbox channel
42 * @rproc: rproc handle
43 */
44 struct omap_rproc {
45 struct mbox_chan *mbox;
46 struct mbox_client client;
47 struct rproc *rproc;
48 };
50 /**
51 * omap_rproc_mbox_callback() - inbound mailbox message handler
52 * @client: mailbox client pointer used for requesting the mailbox channel
53 * @data: mailbox payload
54 *
55 * This handler is invoked by omap's mailbox driver whenever a mailbox
56 * message is received. Usually, the mailbox payload simply contains
57 * the index of the virtqueue that is kicked by the remote processor,
58 * and we let remoteproc core handle it.
59 *
60 * In addition to virtqueue indices, we also have some out-of-band values
61 * that indicates different events. Those values are deliberately very
62 * big so they don't coincide with virtqueue indices.
63 */
64 static void omap_rproc_mbox_callback(struct mbox_client *client, void *data)
65 {
66 struct omap_rproc *oproc = container_of(client, struct omap_rproc,
67 client);
68 struct device *dev = oproc->rproc->dev.parent;
69 const char *name = oproc->rproc->name;
70 u32 msg = (u32)data;
72 dev_dbg(dev, "mbox msg: 0x%x\n", msg);
74 switch (msg) {
75 case RP_MBOX_CRASH:
76 /* just log this for now. later, we'll also do recovery */
77 dev_err(dev, "omap rproc %s crashed\n", name);
78 break;
79 case RP_MBOX_ECHO_REPLY:
80 dev_info(dev, "received echo reply from %s\n", name);
81 break;
82 default:
83 /* msg contains the index of the triggered vring */
84 if (rproc_vq_interrupt(oproc->rproc, msg) == IRQ_NONE)
85 dev_dbg(dev, "no message was found in vqid %d\n", msg);
86 }
87 }
89 /* kick a virtqueue */
90 static void omap_rproc_kick(struct rproc *rproc, int vqid)
91 {
92 struct omap_rproc *oproc = rproc->priv;
93 struct device *dev = rproc->dev.parent;
94 int ret;
96 /* send the index of the triggered virtqueue in the mailbox payload */
97 ret = mbox_send_message(oproc->mbox, (void *)vqid);
98 if (ret < 0)
99 dev_err(dev, "failed to send mailbox message, status = %d\n",
100 ret);
101 }
103 /*
104 * Power up the remote processor.
105 *
106 * This function will be invoked only after the firmware for this rproc
107 * was loaded, parsed successfully, and all of its resource requirements
108 * were met.
109 */
110 static int omap_rproc_start(struct rproc *rproc)
111 {
112 struct omap_rproc *oproc = rproc->priv;
113 struct device *dev = rproc->dev.parent;
114 struct platform_device *pdev = to_platform_device(dev);
115 struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
116 int ret;
117 struct mbox_client *client = &oproc->client;
119 if (pdata->set_bootaddr)
120 pdata->set_bootaddr(rproc->bootaddr);
122 client->dev = dev;
123 client->tx_done = NULL;
124 client->rx_callback = omap_rproc_mbox_callback;
125 client->tx_block = false;
126 client->knows_txdone = false;
128 oproc->mbox = omap_mbox_request_channel(client, pdata->mbox_name);
129 if (IS_ERR(oproc->mbox)) {
130 ret = -EBUSY;
131 dev_err(dev, "mbox_request_channel failed: %ld\n",
132 PTR_ERR(oproc->mbox));
133 return ret;
134 }
136 /*
137 * Ping the remote processor. this is only for sanity-sake;
138 * there is no functional effect whatsoever.
139 *
140 * Note that the reply will _not_ arrive immediately: this message
141 * will wait in the mailbox fifo until the remote processor is booted.
142 */
143 ret = mbox_send_message(oproc->mbox, (void *)RP_MBOX_ECHO_REQUEST);
144 if (ret < 0) {
145 dev_err(dev, "mbox_send_message failed: %d\n", ret);
146 goto put_mbox;
147 }
149 ret = pdata->device_enable(pdev);
150 if (ret) {
151 dev_err(dev, "omap_device_enable failed: %d\n", ret);
152 goto put_mbox;
153 }
155 return 0;
157 put_mbox:
158 mbox_free_channel(oproc->mbox);
159 return ret;
160 }
162 /* power off the remote processor */
163 static int omap_rproc_stop(struct rproc *rproc)
164 {
165 struct device *dev = rproc->dev.parent;
166 struct platform_device *pdev = to_platform_device(dev);
167 struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
168 struct omap_rproc *oproc = rproc->priv;
169 int ret;
171 ret = pdata->device_shutdown(pdev);
172 if (ret)
173 return ret;
175 mbox_free_channel(oproc->mbox);
177 return 0;
178 }
180 static const struct rproc_ops omap_rproc_ops = {
181 .start = omap_rproc_start,
182 .stop = omap_rproc_stop,
183 .kick = omap_rproc_kick,
184 };
186 static int omap_rproc_probe(struct platform_device *pdev)
187 {
188 struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
189 struct omap_rproc *oproc;
190 struct rproc *rproc;
191 int ret;
193 ret = dma_set_coherent_mask(&pdev->dev, DMA_BIT_MASK(32));
194 if (ret) {
195 dev_err(&pdev->dev, "dma_set_coherent_mask: %d\n", ret);
196 return ret;
197 }
199 rproc = rproc_alloc(&pdev->dev, pdata->name, &omap_rproc_ops,
200 pdata->firmware, sizeof(*oproc));
201 if (!rproc)
202 return -ENOMEM;
204 oproc = rproc->priv;
205 oproc->rproc = rproc;
206 /* All existing OMAP IPU and DSP processors have an MMU */
207 rproc->has_iommu = true;
209 platform_set_drvdata(pdev, rproc);
211 ret = rproc_add(rproc);
212 if (ret)
213 goto free_rproc;
215 return 0;
217 free_rproc:
218 rproc_free(rproc);
219 return ret;
220 }
222 static int omap_rproc_remove(struct platform_device *pdev)
223 {
224 struct rproc *rproc = platform_get_drvdata(pdev);
226 rproc_del(rproc);
227 rproc_free(rproc);
229 return 0;
230 }
232 static struct platform_driver omap_rproc_driver = {
233 .probe = omap_rproc_probe,
234 .remove = omap_rproc_remove,
235 .driver = {
236 .name = "omap-rproc",
237 },
238 };
240 module_platform_driver(omap_rproc_driver);
242 MODULE_LICENSE("GPL v2");
243 MODULE_DESCRIPTION("OMAP Remote Processor control driver");