]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/remoteproc/omap_remoteproc.c
Merge remote-tracking branches 'asoc/topic/cs35l35', 'asoc/topic/cs53l30', 'asoc...
[rpmsg/rpmsg.git] / drivers / remoteproc / omap_remoteproc.c
1 /*
2  * OMAP Remote Processor driver
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  * Copyright (C) 2011 Google, Inc.
6  *
7  * Ohad Ben-Cohen <ohad@wizery.com>
8  * Brian Swetland <swetland@google.com>
9  * Fernando Guzman Lugo <fernando.lugo@ti.com>
10  * Mark Grosen <mgrosen@ti.com>
11  * Suman Anna <s-anna@ti.com>
12  * Hari Kanigeri <h-kanigeri2@ti.com>
13  *
14  * This program is free software; you can redistribute it and/or
15  * modify it under the terms of the GNU General Public License
16  * version 2 as published by the Free Software Foundation.
17  *
18  * This program is distributed in the hope that it will be useful,
19  * but WITHOUT ANY WARRANTY; without even the implied warranty of
20  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
21  * GNU General Public License for more details.
22  */
24 #include <linux/kernel.h>
25 #include <linux/module.h>
26 #include <linux/err.h>
27 #include <linux/platform_device.h>
28 #include <linux/dma-mapping.h>
29 #include <linux/remoteproc.h>
30 #include <linux/mailbox_client.h>
31 #include <linux/omap-mailbox.h>
33 #include <linux/platform_data/remoteproc-omap.h>
35 #include "omap_remoteproc.h"
36 #include "remoteproc_internal.h"
38 /**
39  * struct omap_rproc - omap remote processor state
40  * @mbox: mailbox channel handle
41  * @client: mailbox client to request the mailbox channel
42  * @rproc: rproc handle
43  */
44 struct omap_rproc {
45         struct mbox_chan *mbox;
46         struct mbox_client client;
47         struct rproc *rproc;
48 };
50 /**
51  * omap_rproc_mbox_callback() - inbound mailbox message handler
52  * @client: mailbox client pointer used for requesting the mailbox channel
53  * @data: mailbox payload
54  *
55  * This handler is invoked by omap's mailbox driver whenever a mailbox
56  * message is received. Usually, the mailbox payload simply contains
57  * the index of the virtqueue that is kicked by the remote processor,
58  * and we let remoteproc core handle it.
59  *
60  * In addition to virtqueue indices, we also have some out-of-band values
61  * that indicates different events. Those values are deliberately very
62  * big so they don't coincide with virtqueue indices.
63  */
64 static void omap_rproc_mbox_callback(struct mbox_client *client, void *data)
65 {
66         struct omap_rproc *oproc = container_of(client, struct omap_rproc,
67                                                 client);
68         struct device *dev = oproc->rproc->dev.parent;
69         const char *name = oproc->rproc->name;
70         u32 msg = (u32)data;
72         dev_dbg(dev, "mbox msg: 0x%x\n", msg);
74         switch (msg) {
75         case RP_MBOX_CRASH:
76                 /* just log this for now. later, we'll also do recovery */
77                 dev_err(dev, "omap rproc %s crashed\n", name);
78                 break;
79         case RP_MBOX_ECHO_REPLY:
80                 dev_info(dev, "received echo reply from %s\n", name);
81                 break;
82         default:
83                 /* msg contains the index of the triggered vring */
84                 if (rproc_vq_interrupt(oproc->rproc, msg) == IRQ_NONE)
85                         dev_dbg(dev, "no message was found in vqid %d\n", msg);
86         }
87 }
89 /* kick a virtqueue */
90 static void omap_rproc_kick(struct rproc *rproc, int vqid)
91 {
92         struct omap_rproc *oproc = rproc->priv;
93         struct device *dev = rproc->dev.parent;
94         int ret;
96         /* send the index of the triggered virtqueue in the mailbox payload */
97         ret = mbox_send_message(oproc->mbox, (void *)vqid);
98         if (ret < 0)
99                 dev_err(dev, "failed to send mailbox message, status = %d\n",
100                         ret);
103 /*
104  * Power up the remote processor.
105  *
106  * This function will be invoked only after the firmware for this rproc
107  * was loaded, parsed successfully, and all of its resource requirements
108  * were met.
109  */
110 static int omap_rproc_start(struct rproc *rproc)
112         struct omap_rproc *oproc = rproc->priv;
113         struct device *dev = rproc->dev.parent;
114         struct platform_device *pdev = to_platform_device(dev);
115         struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
116         int ret;
117         struct mbox_client *client = &oproc->client;
119         if (pdata->set_bootaddr)
120                 pdata->set_bootaddr(rproc->bootaddr);
122         client->dev = dev;
123         client->tx_done = NULL;
124         client->rx_callback = omap_rproc_mbox_callback;
125         client->tx_block = false;
126         client->knows_txdone = false;
128         oproc->mbox = omap_mbox_request_channel(client, pdata->mbox_name);
129         if (IS_ERR(oproc->mbox)) {
130                 ret = -EBUSY;
131                 dev_err(dev, "mbox_request_channel failed: %ld\n",
132                         PTR_ERR(oproc->mbox));
133                 return ret;
134         }
136         /*
137          * Ping the remote processor. this is only for sanity-sake;
138          * there is no functional effect whatsoever.
139          *
140          * Note that the reply will _not_ arrive immediately: this message
141          * will wait in the mailbox fifo until the remote processor is booted.
142          */
143         ret = mbox_send_message(oproc->mbox, (void *)RP_MBOX_ECHO_REQUEST);
144         if (ret < 0) {
145                 dev_err(dev, "mbox_send_message failed: %d\n", ret);
146                 goto put_mbox;
147         }
149         ret = pdata->device_enable(pdev);
150         if (ret) {
151                 dev_err(dev, "omap_device_enable failed: %d\n", ret);
152                 goto put_mbox;
153         }
155         return 0;
157 put_mbox:
158         mbox_free_channel(oproc->mbox);
159         return ret;
162 /* power off the remote processor */
163 static int omap_rproc_stop(struct rproc *rproc)
165         struct device *dev = rproc->dev.parent;
166         struct platform_device *pdev = to_platform_device(dev);
167         struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
168         struct omap_rproc *oproc = rproc->priv;
169         int ret;
171         ret = pdata->device_shutdown(pdev);
172         if (ret)
173                 return ret;
175         mbox_free_channel(oproc->mbox);
177         return 0;
180 static const struct rproc_ops omap_rproc_ops = {
181         .start          = omap_rproc_start,
182         .stop           = omap_rproc_stop,
183         .kick           = omap_rproc_kick,
184 };
186 static int omap_rproc_probe(struct platform_device *pdev)
188         struct omap_rproc_pdata *pdata = pdev->dev.platform_data;
189         struct omap_rproc *oproc;
190         struct rproc *rproc;
191         int ret;
193         ret = dma_set_coherent_mask(&pdev->dev, DMA_BIT_MASK(32));
194         if (ret) {
195                 dev_err(&pdev->dev, "dma_set_coherent_mask: %d\n", ret);
196                 return ret;
197         }
199         rproc = rproc_alloc(&pdev->dev, pdata->name, &omap_rproc_ops,
200                             pdata->firmware, sizeof(*oproc));
201         if (!rproc)
202                 return -ENOMEM;
204         oproc = rproc->priv;
205         oproc->rproc = rproc;
206         /* All existing OMAP IPU and DSP processors have an MMU */
207         rproc->has_iommu = true;
209         platform_set_drvdata(pdev, rproc);
211         ret = rproc_add(rproc);
212         if (ret)
213                 goto free_rproc;
215         return 0;
217 free_rproc:
218         rproc_free(rproc);
219         return ret;
222 static int omap_rproc_remove(struct platform_device *pdev)
224         struct rproc *rproc = platform_get_drvdata(pdev);
226         rproc_del(rproc);
227         rproc_free(rproc);
229         return 0;
232 static struct platform_driver omap_rproc_driver = {
233         .probe = omap_rproc_probe,
234         .remove = omap_rproc_remove,
235         .driver = {
236                 .name = "omap-rproc",
237         },
238 };
240 module_platform_driver(omap_rproc_driver);
242 MODULE_LICENSE("GPL v2");
243 MODULE_DESCRIPTION("OMAP Remote Processor control driver");