]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/remoteproc/remoteproc_core.c
Merge tag 'powerpc-4.19-2' of git://git.kernel.org/pub/scm/linux/kernel/git/powerpc...
[rpmsg/rpmsg.git] / drivers / remoteproc / remoteproc_core.c
1 /*
2  * Remote Processor Framework
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  * Copyright (C) 2011 Google, Inc.
6  *
7  * Ohad Ben-Cohen <ohad@wizery.com>
8  * Brian Swetland <swetland@google.com>
9  * Mark Grosen <mgrosen@ti.com>
10  * Fernando Guzman Lugo <fernando.lugo@ti.com>
11  * Suman Anna <s-anna@ti.com>
12  * Robert Tivy <rtivy@ti.com>
13  * Armando Uribe De Leon <x0095078@ti.com>
14  *
15  * This program is free software; you can redistribute it and/or
16  * modify it under the terms of the GNU General Public License
17  * version 2 as published by the Free Software Foundation.
18  *
19  * This program is distributed in the hope that it will be useful,
20  * but WITHOUT ANY WARRANTY; without even the implied warranty of
21  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
22  * GNU General Public License for more details.
23  */
25 #define pr_fmt(fmt)    "%s: " fmt, __func__
27 #include <linux/kernel.h>
28 #include <linux/module.h>
29 #include <linux/device.h>
30 #include <linux/slab.h>
31 #include <linux/mutex.h>
32 #include <linux/dma-mapping.h>
33 #include <linux/firmware.h>
34 #include <linux/string.h>
35 #include <linux/debugfs.h>
36 #include <linux/devcoredump.h>
37 #include <linux/remoteproc.h>
38 #include <linux/iommu.h>
39 #include <linux/idr.h>
40 #include <linux/elf.h>
41 #include <linux/crc32.h>
42 #include <linux/virtio_ids.h>
43 #include <linux/virtio_ring.h>
44 #include <asm/byteorder.h>
46 #include "remoteproc_internal.h"
48 static DEFINE_MUTEX(rproc_list_mutex);
49 static LIST_HEAD(rproc_list);
51 typedef int (*rproc_handle_resources_t)(struct rproc *rproc,
52                                 struct resource_table *table, int len);
53 typedef int (*rproc_handle_resource_t)(struct rproc *rproc,
54                                  void *, int offset, int avail);
56 /* Unique indices for remoteproc devices */
57 static DEFINE_IDA(rproc_dev_index);
59 static const char * const rproc_crash_names[] = {
60         [RPROC_MMUFAULT]        = "mmufault",
61         [RPROC_WATCHDOG]        = "watchdog",
62         [RPROC_FATAL_ERROR]     = "fatal error",
63 };
65 /* translate rproc_crash_type to string */
66 static const char *rproc_crash_to_string(enum rproc_crash_type type)
67 {
68         if (type < ARRAY_SIZE(rproc_crash_names))
69                 return rproc_crash_names[type];
70         return "unknown";
71 }
73 /*
74  * This is the IOMMU fault handler we register with the IOMMU API
75  * (when relevant; not all remote processors access memory through
76  * an IOMMU).
77  *
78  * IOMMU core will invoke this handler whenever the remote processor
79  * will try to access an unmapped device address.
80  */
81 static int rproc_iommu_fault(struct iommu_domain *domain, struct device *dev,
82                              unsigned long iova, int flags, void *token)
83 {
84         struct rproc *rproc = token;
86         dev_err(dev, "iommu fault: da 0x%lx flags 0x%x\n", iova, flags);
88         rproc_report_crash(rproc, RPROC_MMUFAULT);
90         /*
91          * Let the iommu core know we're not really handling this fault;
92          * we just used it as a recovery trigger.
93          */
94         return -ENOSYS;
95 }
97 static int rproc_enable_iommu(struct rproc *rproc)
98 {
99         struct iommu_domain *domain;
100         struct device *dev = rproc->dev.parent;
101         int ret;
103         if (!rproc->has_iommu) {
104                 dev_dbg(dev, "iommu not present\n");
105                 return 0;
106         }
108         domain = iommu_domain_alloc(dev->bus);
109         if (!domain) {
110                 dev_err(dev, "can't alloc iommu domain\n");
111                 return -ENOMEM;
112         }
114         iommu_set_fault_handler(domain, rproc_iommu_fault, rproc);
116         ret = iommu_attach_device(domain, dev);
117         if (ret) {
118                 dev_err(dev, "can't attach iommu device: %d\n", ret);
119                 goto free_domain;
120         }
122         rproc->domain = domain;
124         return 0;
126 free_domain:
127         iommu_domain_free(domain);
128         return ret;
131 static void rproc_disable_iommu(struct rproc *rproc)
133         struct iommu_domain *domain = rproc->domain;
134         struct device *dev = rproc->dev.parent;
136         if (!domain)
137                 return;
139         iommu_detach_device(domain, dev);
140         iommu_domain_free(domain);
143 /**
144  * rproc_da_to_va() - lookup the kernel virtual address for a remoteproc address
145  * @rproc: handle of a remote processor
146  * @da: remoteproc device address to translate
147  * @len: length of the memory region @da is pointing to
148  *
149  * Some remote processors will ask us to allocate them physically contiguous
150  * memory regions (which we call "carveouts"), and map them to specific
151  * device addresses (which are hardcoded in the firmware). They may also have
152  * dedicated memory regions internal to the processors, and use them either
153  * exclusively or alongside carveouts.
154  *
155  * They may then ask us to copy objects into specific device addresses (e.g.
156  * code/data sections) or expose us certain symbols in other device address
157  * (e.g. their trace buffer).
158  *
159  * This function is a helper function with which we can go over the allocated
160  * carveouts and translate specific device addresses to kernel virtual addresses
161  * so we can access the referenced memory. This function also allows to perform
162  * translations on the internal remoteproc memory regions through a platform
163  * implementation specific da_to_va ops, if present.
164  *
165  * The function returns a valid kernel address on success or NULL on failure.
166  *
167  * Note: phys_to_virt(iommu_iova_to_phys(rproc->domain, da)) will work too,
168  * but only on kernel direct mapped RAM memory. Instead, we're just using
169  * here the output of the DMA API for the carveouts, which should be more
170  * correct.
171  */
172 void *rproc_da_to_va(struct rproc *rproc, u64 da, int len)
174         struct rproc_mem_entry *carveout;
175         void *ptr = NULL;
177         if (rproc->ops->da_to_va) {
178                 ptr = rproc->ops->da_to_va(rproc, da, len);
179                 if (ptr)
180                         goto out;
181         }
183         list_for_each_entry(carveout, &rproc->carveouts, node) {
184                 int offset = da - carveout->da;
186                 /* try next carveout if da is too small */
187                 if (offset < 0)
188                         continue;
190                 /* try next carveout if da is too large */
191                 if (offset + len > carveout->len)
192                         continue;
194                 ptr = carveout->va + offset;
196                 break;
197         }
199 out:
200         return ptr;
202 EXPORT_SYMBOL(rproc_da_to_va);
204 int rproc_alloc_vring(struct rproc_vdev *rvdev, int i)
206         struct rproc *rproc = rvdev->rproc;
207         struct device *dev = &rproc->dev;
208         struct rproc_vring *rvring = &rvdev->vring[i];
209         struct fw_rsc_vdev *rsc;
210         dma_addr_t dma;
211         void *va;
212         int ret, size, notifyid;
214         /* actual size of vring (in bytes) */
215         size = PAGE_ALIGN(vring_size(rvring->len, rvring->align));
217         /*
218          * Allocate non-cacheable memory for the vring. In the future
219          * this call will also configure the IOMMU for us
220          */
221         va = dma_alloc_coherent(dev->parent, size, &dma, GFP_KERNEL);
222         if (!va) {
223                 dev_err(dev->parent, "dma_alloc_coherent failed\n");
224                 return -EINVAL;
225         }
227         /*
228          * Assign an rproc-wide unique index for this vring
229          * TODO: assign a notifyid for rvdev updates as well
230          * TODO: support predefined notifyids (via resource table)
231          */
232         ret = idr_alloc(&rproc->notifyids, rvring, 0, 0, GFP_KERNEL);
233         if (ret < 0) {
234                 dev_err(dev, "idr_alloc failed: %d\n", ret);
235                 dma_free_coherent(dev->parent, size, va, dma);
236                 return ret;
237         }
238         notifyid = ret;
240         /* Potentially bump max_notifyid */
241         if (notifyid > rproc->max_notifyid)
242                 rproc->max_notifyid = notifyid;
244         dev_dbg(dev, "vring%d: va %pK dma %pad size 0x%x idr %d\n",
245                 i, va, &dma, size, notifyid);
247         rvring->va = va;
248         rvring->dma = dma;
249         rvring->notifyid = notifyid;
251         /*
252          * Let the rproc know the notifyid and da of this vring.
253          * Not all platforms use dma_alloc_coherent to automatically
254          * set up the iommu. In this case the device address (da) will
255          * hold the physical address and not the device address.
256          */
257         rsc = (void *)rproc->table_ptr + rvdev->rsc_offset;
258         rsc->vring[i].da = dma;
259         rsc->vring[i].notifyid = notifyid;
260         return 0;
263 static int
264 rproc_parse_vring(struct rproc_vdev *rvdev, struct fw_rsc_vdev *rsc, int i)
266         struct rproc *rproc = rvdev->rproc;
267         struct device *dev = &rproc->dev;
268         struct fw_rsc_vdev_vring *vring = &rsc->vring[i];
269         struct rproc_vring *rvring = &rvdev->vring[i];
271         dev_dbg(dev, "vdev rsc: vring%d: da 0x%x, qsz %d, align %d\n",
272                 i, vring->da, vring->num, vring->align);
274         /* verify queue size and vring alignment are sane */
275         if (!vring->num || !vring->align) {
276                 dev_err(dev, "invalid qsz (%d) or alignment (%d)\n",
277                         vring->num, vring->align);
278                 return -EINVAL;
279         }
281         rvring->len = vring->num;
282         rvring->align = vring->align;
283         rvring->rvdev = rvdev;
285         return 0;
288 void rproc_free_vring(struct rproc_vring *rvring)
290         int size = PAGE_ALIGN(vring_size(rvring->len, rvring->align));
291         struct rproc *rproc = rvring->rvdev->rproc;
292         int idx = rvring->rvdev->vring - rvring;
293         struct fw_rsc_vdev *rsc;
295         dma_free_coherent(rproc->dev.parent, size, rvring->va, rvring->dma);
296         idr_remove(&rproc->notifyids, rvring->notifyid);
298         /* reset resource entry info */
299         rsc = (void *)rproc->table_ptr + rvring->rvdev->rsc_offset;
300         rsc->vring[idx].da = 0;
301         rsc->vring[idx].notifyid = -1;
304 static int rproc_vdev_do_start(struct rproc_subdev *subdev)
306         struct rproc_vdev *rvdev = container_of(subdev, struct rproc_vdev, subdev);
308         return rproc_add_virtio_dev(rvdev, rvdev->id);
311 static void rproc_vdev_do_stop(struct rproc_subdev *subdev, bool crashed)
313         struct rproc_vdev *rvdev = container_of(subdev, struct rproc_vdev, subdev);
315         rproc_remove_virtio_dev(rvdev);
318 /**
319  * rproc_handle_vdev() - handle a vdev fw resource
320  * @rproc: the remote processor
321  * @rsc: the vring resource descriptor
322  * @avail: size of available data (for sanity checking the image)
323  *
324  * This resource entry requests the host to statically register a virtio
325  * device (vdev), and setup everything needed to support it. It contains
326  * everything needed to make it possible: the virtio device id, virtio
327  * device features, vrings information, virtio config space, etc...
328  *
329  * Before registering the vdev, the vrings are allocated from non-cacheable
330  * physically contiguous memory. Currently we only support two vrings per
331  * remote processor (temporary limitation). We might also want to consider
332  * doing the vring allocation only later when ->find_vqs() is invoked, and
333  * then release them upon ->del_vqs().
334  *
335  * Note: @da is currently not really handled correctly: we dynamically
336  * allocate it using the DMA API, ignoring requested hard coded addresses,
337  * and we don't take care of any required IOMMU programming. This is all
338  * going to be taken care of when the generic iommu-based DMA API will be
339  * merged. Meanwhile, statically-addressed iommu-based firmware images should
340  * use RSC_DEVMEM resource entries to map their required @da to the physical
341  * address of their base CMA region (ouch, hacky!).
342  *
343  * Returns 0 on success, or an appropriate error code otherwise
344  */
345 static int rproc_handle_vdev(struct rproc *rproc, struct fw_rsc_vdev *rsc,
346                              int offset, int avail)
348         struct device *dev = &rproc->dev;
349         struct rproc_vdev *rvdev;
350         int i, ret;
352         /* make sure resource isn't truncated */
353         if (sizeof(*rsc) + rsc->num_of_vrings * sizeof(struct fw_rsc_vdev_vring)
354                         + rsc->config_len > avail) {
355                 dev_err(dev, "vdev rsc is truncated\n");
356                 return -EINVAL;
357         }
359         /* make sure reserved bytes are zeroes */
360         if (rsc->reserved[0] || rsc->reserved[1]) {
361                 dev_err(dev, "vdev rsc has non zero reserved bytes\n");
362                 return -EINVAL;
363         }
365         dev_dbg(dev, "vdev rsc: id %d, dfeatures 0x%x, cfg len %d, %d vrings\n",
366                 rsc->id, rsc->dfeatures, rsc->config_len, rsc->num_of_vrings);
368         /* we currently support only two vrings per rvdev */
369         if (rsc->num_of_vrings > ARRAY_SIZE(rvdev->vring)) {
370                 dev_err(dev, "too many vrings: %d\n", rsc->num_of_vrings);
371                 return -EINVAL;
372         }
374         rvdev = kzalloc(sizeof(*rvdev), GFP_KERNEL);
375         if (!rvdev)
376                 return -ENOMEM;
378         kref_init(&rvdev->refcount);
380         rvdev->id = rsc->id;
381         rvdev->rproc = rproc;
383         /* parse the vrings */
384         for (i = 0; i < rsc->num_of_vrings; i++) {
385                 ret = rproc_parse_vring(rvdev, rsc, i);
386                 if (ret)
387                         goto free_rvdev;
388         }
390         /* remember the resource offset*/
391         rvdev->rsc_offset = offset;
393         /* allocate the vring resources */
394         for (i = 0; i < rsc->num_of_vrings; i++) {
395                 ret = rproc_alloc_vring(rvdev, i);
396                 if (ret)
397                         goto unwind_vring_allocations;
398         }
400         list_add_tail(&rvdev->node, &rproc->rvdevs);
402         rvdev->subdev.start = rproc_vdev_do_start;
403         rvdev->subdev.stop = rproc_vdev_do_stop;
405         rproc_add_subdev(rproc, &rvdev->subdev);
407         return 0;
409 unwind_vring_allocations:
410         for (i--; i >= 0; i--)
411                 rproc_free_vring(&rvdev->vring[i]);
412 free_rvdev:
413         kfree(rvdev);
414         return ret;
417 void rproc_vdev_release(struct kref *ref)
419         struct rproc_vdev *rvdev = container_of(ref, struct rproc_vdev, refcount);
420         struct rproc_vring *rvring;
421         struct rproc *rproc = rvdev->rproc;
422         int id;
424         for (id = 0; id < ARRAY_SIZE(rvdev->vring); id++) {
425                 rvring = &rvdev->vring[id];
426                 if (!rvring->va)
427                         continue;
429                 rproc_free_vring(rvring);
430         }
432         rproc_remove_subdev(rproc, &rvdev->subdev);
433         list_del(&rvdev->node);
434         kfree(rvdev);
437 /**
438  * rproc_handle_trace() - handle a shared trace buffer resource
439  * @rproc: the remote processor
440  * @rsc: the trace resource descriptor
441  * @avail: size of available data (for sanity checking the image)
442  *
443  * In case the remote processor dumps trace logs into memory,
444  * export it via debugfs.
445  *
446  * Currently, the 'da' member of @rsc should contain the device address
447  * where the remote processor is dumping the traces. Later we could also
448  * support dynamically allocating this address using the generic
449  * DMA API (but currently there isn't a use case for that).
450  *
451  * Returns 0 on success, or an appropriate error code otherwise
452  */
453 static int rproc_handle_trace(struct rproc *rproc, struct fw_rsc_trace *rsc,
454                               int offset, int avail)
456         struct rproc_mem_entry *trace;
457         struct device *dev = &rproc->dev;
458         void *ptr;
459         char name[15];
461         if (sizeof(*rsc) > avail) {
462                 dev_err(dev, "trace rsc is truncated\n");
463                 return -EINVAL;
464         }
466         /* make sure reserved bytes are zeroes */
467         if (rsc->reserved) {
468                 dev_err(dev, "trace rsc has non zero reserved bytes\n");
469                 return -EINVAL;
470         }
472         /* what's the kernel address of this resource ? */
473         ptr = rproc_da_to_va(rproc, rsc->da, rsc->len);
474         if (!ptr) {
475                 dev_err(dev, "erroneous trace resource entry\n");
476                 return -EINVAL;
477         }
479         trace = kzalloc(sizeof(*trace), GFP_KERNEL);
480         if (!trace)
481                 return -ENOMEM;
483         /* set the trace buffer dma properties */
484         trace->len = rsc->len;
485         trace->va = ptr;
487         /* make sure snprintf always null terminates, even if truncating */
488         snprintf(name, sizeof(name), "trace%d", rproc->num_traces);
490         /* create the debugfs entry */
491         trace->priv = rproc_create_trace_file(name, rproc, trace);
492         if (!trace->priv) {
493                 trace->va = NULL;
494                 kfree(trace);
495                 return -EINVAL;
496         }
498         list_add_tail(&trace->node, &rproc->traces);
500         rproc->num_traces++;
502         dev_dbg(dev, "%s added: va %pK, da 0x%x, len 0x%x\n",
503                 name, ptr, rsc->da, rsc->len);
505         return 0;
508 /**
509  * rproc_handle_devmem() - handle devmem resource entry
510  * @rproc: remote processor handle
511  * @rsc: the devmem resource entry
512  * @avail: size of available data (for sanity checking the image)
513  *
514  * Remote processors commonly need to access certain on-chip peripherals.
515  *
516  * Some of these remote processors access memory via an iommu device,
517  * and might require us to configure their iommu before they can access
518  * the on-chip peripherals they need.
519  *
520  * This resource entry is a request to map such a peripheral device.
521  *
522  * These devmem entries will contain the physical address of the device in
523  * the 'pa' member. If a specific device address is expected, then 'da' will
524  * contain it (currently this is the only use case supported). 'len' will
525  * contain the size of the physical region we need to map.
526  *
527  * Currently we just "trust" those devmem entries to contain valid physical
528  * addresses, but this is going to change: we want the implementations to
529  * tell us ranges of physical addresses the firmware is allowed to request,
530  * and not allow firmwares to request access to physical addresses that
531  * are outside those ranges.
532  */
533 static int rproc_handle_devmem(struct rproc *rproc, struct fw_rsc_devmem *rsc,
534                                int offset, int avail)
536         struct rproc_mem_entry *mapping;
537         struct device *dev = &rproc->dev;
538         int ret;
540         /* no point in handling this resource without a valid iommu domain */
541         if (!rproc->domain)
542                 return -EINVAL;
544         if (sizeof(*rsc) > avail) {
545                 dev_err(dev, "devmem rsc is truncated\n");
546                 return -EINVAL;
547         }
549         /* make sure reserved bytes are zeroes */
550         if (rsc->reserved) {
551                 dev_err(dev, "devmem rsc has non zero reserved bytes\n");
552                 return -EINVAL;
553         }
555         mapping = kzalloc(sizeof(*mapping), GFP_KERNEL);
556         if (!mapping)
557                 return -ENOMEM;
559         ret = iommu_map(rproc->domain, rsc->da, rsc->pa, rsc->len, rsc->flags);
560         if (ret) {
561                 dev_err(dev, "failed to map devmem: %d\n", ret);
562                 goto out;
563         }
565         /*
566          * We'll need this info later when we'll want to unmap everything
567          * (e.g. on shutdown).
568          *
569          * We can't trust the remote processor not to change the resource
570          * table, so we must maintain this info independently.
571          */
572         mapping->da = rsc->da;
573         mapping->len = rsc->len;
574         list_add_tail(&mapping->node, &rproc->mappings);
576         dev_dbg(dev, "mapped devmem pa 0x%x, da 0x%x, len 0x%x\n",
577                 rsc->pa, rsc->da, rsc->len);
579         return 0;
581 out:
582         kfree(mapping);
583         return ret;
586 /**
587  * rproc_handle_carveout() - handle phys contig memory allocation requests
588  * @rproc: rproc handle
589  * @rsc: the resource entry
590  * @avail: size of available data (for image validation)
591  *
592  * This function will handle firmware requests for allocation of physically
593  * contiguous memory regions.
594  *
595  * These request entries should come first in the firmware's resource table,
596  * as other firmware entries might request placing other data objects inside
597  * these memory regions (e.g. data/code segments, trace resource entries, ...).
598  *
599  * Allocating memory this way helps utilizing the reserved physical memory
600  * (e.g. CMA) more efficiently, and also minimizes the number of TLB entries
601  * needed to map it (in case @rproc is using an IOMMU). Reducing the TLB
602  * pressure is important; it may have a substantial impact on performance.
603  */
604 static int rproc_handle_carveout(struct rproc *rproc,
605                                  struct fw_rsc_carveout *rsc,
606                                  int offset, int avail)
608         struct rproc_mem_entry *carveout, *mapping;
609         struct device *dev = &rproc->dev;
610         dma_addr_t dma;
611         void *va;
612         int ret;
614         if (sizeof(*rsc) > avail) {
615                 dev_err(dev, "carveout rsc is truncated\n");
616                 return -EINVAL;
617         }
619         /* make sure reserved bytes are zeroes */
620         if (rsc->reserved) {
621                 dev_err(dev, "carveout rsc has non zero reserved bytes\n");
622                 return -EINVAL;
623         }
625         dev_dbg(dev, "carveout rsc: name: %s, da 0x%x, pa 0x%x, len 0x%x, flags 0x%x\n",
626                 rsc->name, rsc->da, rsc->pa, rsc->len, rsc->flags);
628         carveout = kzalloc(sizeof(*carveout), GFP_KERNEL);
629         if (!carveout)
630                 return -ENOMEM;
632         va = dma_alloc_coherent(dev->parent, rsc->len, &dma, GFP_KERNEL);
633         if (!va) {
634                 dev_err(dev->parent,
635                         "failed to allocate dma memory: len 0x%x\n", rsc->len);
636                 ret = -ENOMEM;
637                 goto free_carv;
638         }
640         dev_dbg(dev, "carveout va %pK, dma %pad, len 0x%x\n",
641                 va, &dma, rsc->len);
643         /*
644          * Ok, this is non-standard.
645          *
646          * Sometimes we can't rely on the generic iommu-based DMA API
647          * to dynamically allocate the device address and then set the IOMMU
648          * tables accordingly, because some remote processors might
649          * _require_ us to use hard coded device addresses that their
650          * firmware was compiled with.
651          *
652          * In this case, we must use the IOMMU API directly and map
653          * the memory to the device address as expected by the remote
654          * processor.
655          *
656          * Obviously such remote processor devices should not be configured
657          * to use the iommu-based DMA API: we expect 'dma' to contain the
658          * physical address in this case.
659          */
660         if (rproc->domain) {
661                 mapping = kzalloc(sizeof(*mapping), GFP_KERNEL);
662                 if (!mapping) {
663                         ret = -ENOMEM;
664                         goto dma_free;
665                 }
667                 ret = iommu_map(rproc->domain, rsc->da, dma, rsc->len,
668                                 rsc->flags);
669                 if (ret) {
670                         dev_err(dev, "iommu_map failed: %d\n", ret);
671                         goto free_mapping;
672                 }
674                 /*
675                  * We'll need this info later when we'll want to unmap
676                  * everything (e.g. on shutdown).
677                  *
678                  * We can't trust the remote processor not to change the
679                  * resource table, so we must maintain this info independently.
680                  */
681                 mapping->da = rsc->da;
682                 mapping->len = rsc->len;
683                 list_add_tail(&mapping->node, &rproc->mappings);
685                 dev_dbg(dev, "carveout mapped 0x%x to %pad\n",
686                         rsc->da, &dma);
687         }
689         /*
690          * Some remote processors might need to know the pa
691          * even though they are behind an IOMMU. E.g., OMAP4's
692          * remote M3 processor needs this so it can control
693          * on-chip hardware accelerators that are not behind
694          * the IOMMU, and therefor must know the pa.
695          *
696          * Generally we don't want to expose physical addresses
697          * if we don't have to (remote processors are generally
698          * _not_ trusted), so we might want to do this only for
699          * remote processor that _must_ have this (e.g. OMAP4's
700          * dual M3 subsystem).
701          *
702          * Non-IOMMU processors might also want to have this info.
703          * In this case, the device address and the physical address
704          * are the same.
705          */
706         rsc->pa = dma;
708         carveout->va = va;
709         carveout->len = rsc->len;
710         carveout->dma = dma;
711         carveout->da = rsc->da;
713         list_add_tail(&carveout->node, &rproc->carveouts);
715         return 0;
717 free_mapping:
718         kfree(mapping);
719 dma_free:
720         dma_free_coherent(dev->parent, rsc->len, va, dma);
721 free_carv:
722         kfree(carveout);
723         return ret;
726 /*
727  * A lookup table for resource handlers. The indices are defined in
728  * enum fw_resource_type.
729  */
730 static rproc_handle_resource_t rproc_loading_handlers[RSC_LAST] = {
731         [RSC_CARVEOUT] = (rproc_handle_resource_t)rproc_handle_carveout,
732         [RSC_DEVMEM] = (rproc_handle_resource_t)rproc_handle_devmem,
733         [RSC_TRACE] = (rproc_handle_resource_t)rproc_handle_trace,
734         [RSC_VDEV] = (rproc_handle_resource_t)rproc_handle_vdev,
735 };
737 /* handle firmware resource entries before booting the remote processor */
738 static int rproc_handle_resources(struct rproc *rproc,
739                                   rproc_handle_resource_t handlers[RSC_LAST])
741         struct device *dev = &rproc->dev;
742         rproc_handle_resource_t handler;
743         int ret = 0, i;
745         if (!rproc->table_ptr)
746                 return 0;
748         for (i = 0; i < rproc->table_ptr->num; i++) {
749                 int offset = rproc->table_ptr->offset[i];
750                 struct fw_rsc_hdr *hdr = (void *)rproc->table_ptr + offset;
751                 int avail = rproc->table_sz - offset - sizeof(*hdr);
752                 void *rsc = (void *)hdr + sizeof(*hdr);
754                 /* make sure table isn't truncated */
755                 if (avail < 0) {
756                         dev_err(dev, "rsc table is truncated\n");
757                         return -EINVAL;
758                 }
760                 dev_dbg(dev, "rsc: type %d\n", hdr->type);
762                 if (hdr->type >= RSC_LAST) {
763                         dev_warn(dev, "unsupported resource %d\n", hdr->type);
764                         continue;
765                 }
767                 handler = handlers[hdr->type];
768                 if (!handler)
769                         continue;
771                 ret = handler(rproc, rsc, offset + sizeof(*hdr), avail);
772                 if (ret)
773                         break;
774         }
776         return ret;
779 static int rproc_prepare_subdevices(struct rproc *rproc)
781         struct rproc_subdev *subdev;
782         int ret;
784         list_for_each_entry(subdev, &rproc->subdevs, node) {
785                 if (subdev->prepare) {
786                         ret = subdev->prepare(subdev);
787                         if (ret)
788                                 goto unroll_preparation;
789                 }
790         }
792         return 0;
794 unroll_preparation:
795         list_for_each_entry_continue_reverse(subdev, &rproc->subdevs, node) {
796                 if (subdev->unprepare)
797                         subdev->unprepare(subdev);
798         }
800         return ret;
803 static int rproc_start_subdevices(struct rproc *rproc)
805         struct rproc_subdev *subdev;
806         int ret;
808         list_for_each_entry(subdev, &rproc->subdevs, node) {
809                 if (subdev->start) {
810                         ret = subdev->start(subdev);
811                         if (ret)
812                                 goto unroll_registration;
813                 }
814         }
816         return 0;
818 unroll_registration:
819         list_for_each_entry_continue_reverse(subdev, &rproc->subdevs, node) {
820                 if (subdev->stop)
821                         subdev->stop(subdev, true);
822         }
824         return ret;
827 static void rproc_stop_subdevices(struct rproc *rproc, bool crashed)
829         struct rproc_subdev *subdev;
831         list_for_each_entry_reverse(subdev, &rproc->subdevs, node) {
832                 if (subdev->stop)
833                         subdev->stop(subdev, crashed);
834         }
837 static void rproc_unprepare_subdevices(struct rproc *rproc)
839         struct rproc_subdev *subdev;
841         list_for_each_entry_reverse(subdev, &rproc->subdevs, node) {
842                 if (subdev->unprepare)
843                         subdev->unprepare(subdev);
844         }
847 /**
848  * rproc_coredump_cleanup() - clean up dump_segments list
849  * @rproc: the remote processor handle
850  */
851 static void rproc_coredump_cleanup(struct rproc *rproc)
853         struct rproc_dump_segment *entry, *tmp;
855         list_for_each_entry_safe(entry, tmp, &rproc->dump_segments, node) {
856                 list_del(&entry->node);
857                 kfree(entry);
858         }
861 /**
862  * rproc_resource_cleanup() - clean up and free all acquired resources
863  * @rproc: rproc handle
864  *
865  * This function will free all resources acquired for @rproc, and it
866  * is called whenever @rproc either shuts down or fails to boot.
867  */
868 static void rproc_resource_cleanup(struct rproc *rproc)
870         struct rproc_mem_entry *entry, *tmp;
871         struct rproc_vdev *rvdev, *rvtmp;
872         struct device *dev = &rproc->dev;
874         /* clean up debugfs trace entries */
875         list_for_each_entry_safe(entry, tmp, &rproc->traces, node) {
876                 rproc_remove_trace_file(entry->priv);
877                 rproc->num_traces--;
878                 list_del(&entry->node);
879                 kfree(entry);
880         }
882         /* clean up iommu mapping entries */
883         list_for_each_entry_safe(entry, tmp, &rproc->mappings, node) {
884                 size_t unmapped;
886                 unmapped = iommu_unmap(rproc->domain, entry->da, entry->len);
887                 if (unmapped != entry->len) {
888                         /* nothing much to do besides complaining */
889                         dev_err(dev, "failed to unmap %u/%zu\n", entry->len,
890                                 unmapped);
891                 }
893                 list_del(&entry->node);
894                 kfree(entry);
895         }
897         /* clean up carveout allocations */
898         list_for_each_entry_safe(entry, tmp, &rproc->carveouts, node) {
899                 dma_free_coherent(dev->parent, entry->len, entry->va,
900                                   entry->dma);
901                 list_del(&entry->node);
902                 kfree(entry);
903         }
905         /* clean up remote vdev entries */
906         list_for_each_entry_safe(rvdev, rvtmp, &rproc->rvdevs, node)
907                 kref_put(&rvdev->refcount, rproc_vdev_release);
909         rproc_coredump_cleanup(rproc);
912 static int rproc_start(struct rproc *rproc, const struct firmware *fw)
914         struct resource_table *loaded_table;
915         struct device *dev = &rproc->dev;
916         int ret;
918         /* load the ELF segments to memory */
919         ret = rproc_load_segments(rproc, fw);
920         if (ret) {
921                 dev_err(dev, "Failed to load program segments: %d\n", ret);
922                 return ret;
923         }
925         /*
926          * The starting device has been given the rproc->cached_table as the
927          * resource table. The address of the vring along with the other
928          * allocated resources (carveouts etc) is stored in cached_table.
929          * In order to pass this information to the remote device we must copy
930          * this information to device memory. We also update the table_ptr so
931          * that any subsequent changes will be applied to the loaded version.
932          */
933         loaded_table = rproc_find_loaded_rsc_table(rproc, fw);
934         if (loaded_table) {
935                 memcpy(loaded_table, rproc->cached_table, rproc->table_sz);
936                 rproc->table_ptr = loaded_table;
937         }
939         ret = rproc_prepare_subdevices(rproc);
940         if (ret) {
941                 dev_err(dev, "failed to prepare subdevices for %s: %d\n",
942                         rproc->name, ret);
943                 goto reset_table_ptr;
944         }
946         /* power up the remote processor */
947         ret = rproc->ops->start(rproc);
948         if (ret) {
949                 dev_err(dev, "can't start rproc %s: %d\n", rproc->name, ret);
950                 goto unprepare_subdevices;
951         }
953         /* Start any subdevices for the remote processor */
954         ret = rproc_start_subdevices(rproc);
955         if (ret) {
956                 dev_err(dev, "failed to probe subdevices for %s: %d\n",
957                         rproc->name, ret);
958                 goto stop_rproc;
959         }
961         rproc->state = RPROC_RUNNING;
963         dev_info(dev, "remote processor %s is now up\n", rproc->name);
965         return 0;
967 stop_rproc:
968         rproc->ops->stop(rproc);
969 unprepare_subdevices:
970         rproc_unprepare_subdevices(rproc);
971 reset_table_ptr:
972         rproc->table_ptr = rproc->cached_table;
974         return ret;
977 /*
978  * take a firmware and boot a remote processor with it.
979  */
980 static int rproc_fw_boot(struct rproc *rproc, const struct firmware *fw)
982         struct device *dev = &rproc->dev;
983         const char *name = rproc->firmware;
984         int ret;
986         ret = rproc_fw_sanity_check(rproc, fw);
987         if (ret)
988                 return ret;
990         dev_info(dev, "Booting fw image %s, size %zd\n", name, fw->size);
992         /*
993          * if enabling an IOMMU isn't relevant for this rproc, this is
994          * just a nop
995          */
996         ret = rproc_enable_iommu(rproc);
997         if (ret) {
998                 dev_err(dev, "can't enable iommu: %d\n", ret);
999                 return ret;
1000         }
1002         rproc->bootaddr = rproc_get_boot_addr(rproc, fw);
1004         /* Load resource table, core dump segment list etc from the firmware */
1005         ret = rproc_parse_fw(rproc, fw);
1006         if (ret)
1007                 goto disable_iommu;
1009         /* reset max_notifyid */
1010         rproc->max_notifyid = -1;
1012         /* handle fw resources which are required to boot rproc */
1013         ret = rproc_handle_resources(rproc, rproc_loading_handlers);
1014         if (ret) {
1015                 dev_err(dev, "Failed to process resources: %d\n", ret);
1016                 goto clean_up_resources;
1017         }
1019         ret = rproc_start(rproc, fw);
1020         if (ret)
1021                 goto clean_up_resources;
1023         return 0;
1025 clean_up_resources:
1026         rproc_resource_cleanup(rproc);
1027         kfree(rproc->cached_table);
1028         rproc->cached_table = NULL;
1029         rproc->table_ptr = NULL;
1030 disable_iommu:
1031         rproc_disable_iommu(rproc);
1032         return ret;
1035 /*
1036  * take a firmware and boot it up.
1037  *
1038  * Note: this function is called asynchronously upon registration of the
1039  * remote processor (so we must wait until it completes before we try
1040  * to unregister the device. one other option is just to use kref here,
1041  * that might be cleaner).
1042  */
1043 static void rproc_auto_boot_callback(const struct firmware *fw, void *context)
1045         struct rproc *rproc = context;
1047         rproc_boot(rproc);
1049         release_firmware(fw);
1052 static int rproc_trigger_auto_boot(struct rproc *rproc)
1054         int ret;
1056         /*
1057          * We're initiating an asynchronous firmware loading, so we can
1058          * be built-in kernel code, without hanging the boot process.
1059          */
1060         ret = request_firmware_nowait(THIS_MODULE, FW_ACTION_HOTPLUG,
1061                                       rproc->firmware, &rproc->dev, GFP_KERNEL,
1062                                       rproc, rproc_auto_boot_callback);
1063         if (ret < 0)
1064                 dev_err(&rproc->dev, "request_firmware_nowait err: %d\n", ret);
1066         return ret;
1069 static int rproc_stop(struct rproc *rproc, bool crashed)
1071         struct device *dev = &rproc->dev;
1072         int ret;
1074         /* Stop any subdevices for the remote processor */
1075         rproc_stop_subdevices(rproc, crashed);
1077         /* the installed resource table is no longer accessible */
1078         rproc->table_ptr = rproc->cached_table;
1080         /* power off the remote processor */
1081         ret = rproc->ops->stop(rproc);
1082         if (ret) {
1083                 dev_err(dev, "can't stop rproc: %d\n", ret);
1084                 return ret;
1085         }
1087         rproc_unprepare_subdevices(rproc);
1089         rproc->state = RPROC_OFFLINE;
1091         dev_info(dev, "stopped remote processor %s\n", rproc->name);
1093         return 0;
1096 /**
1097  * rproc_coredump_add_segment() - add segment of device memory to coredump
1098  * @rproc:      handle of a remote processor
1099  * @da:         device address
1100  * @size:       size of segment
1101  *
1102  * Add device memory to the list of segments to be included in a coredump for
1103  * the remoteproc.
1104  *
1105  * Return: 0 on success, negative errno on error.
1106  */
1107 int rproc_coredump_add_segment(struct rproc *rproc, dma_addr_t da, size_t size)
1109         struct rproc_dump_segment *segment;
1111         segment = kzalloc(sizeof(*segment), GFP_KERNEL);
1112         if (!segment)
1113                 return -ENOMEM;
1115         segment->da = da;
1116         segment->size = size;
1118         list_add_tail(&segment->node, &rproc->dump_segments);
1120         return 0;
1122 EXPORT_SYMBOL(rproc_coredump_add_segment);
1124 /**
1125  * rproc_coredump() - perform coredump
1126  * @rproc:      rproc handle
1127  *
1128  * This function will generate an ELF header for the registered segments
1129  * and create a devcoredump device associated with rproc.
1130  */
1131 static void rproc_coredump(struct rproc *rproc)
1133         struct rproc_dump_segment *segment;
1134         struct elf32_phdr *phdr;
1135         struct elf32_hdr *ehdr;
1136         size_t data_size;
1137         size_t offset;
1138         void *data;
1139         void *ptr;
1140         int phnum = 0;
1142         if (list_empty(&rproc->dump_segments))
1143                 return;
1145         data_size = sizeof(*ehdr);
1146         list_for_each_entry(segment, &rproc->dump_segments, node) {
1147                 data_size += sizeof(*phdr) + segment->size;
1149                 phnum++;
1150         }
1152         data = vmalloc(data_size);
1153         if (!data)
1154                 return;
1156         ehdr = data;
1158         memset(ehdr, 0, sizeof(*ehdr));
1159         memcpy(ehdr->e_ident, ELFMAG, SELFMAG);
1160         ehdr->e_ident[EI_CLASS] = ELFCLASS32;
1161         ehdr->e_ident[EI_DATA] = ELFDATA2LSB;
1162         ehdr->e_ident[EI_VERSION] = EV_CURRENT;
1163         ehdr->e_ident[EI_OSABI] = ELFOSABI_NONE;
1164         ehdr->e_type = ET_CORE;
1165         ehdr->e_machine = EM_NONE;
1166         ehdr->e_version = EV_CURRENT;
1167         ehdr->e_entry = rproc->bootaddr;
1168         ehdr->e_phoff = sizeof(*ehdr);
1169         ehdr->e_ehsize = sizeof(*ehdr);
1170         ehdr->e_phentsize = sizeof(*phdr);
1171         ehdr->e_phnum = phnum;
1173         phdr = data + ehdr->e_phoff;
1174         offset = ehdr->e_phoff + sizeof(*phdr) * ehdr->e_phnum;
1175         list_for_each_entry(segment, &rproc->dump_segments, node) {
1176                 memset(phdr, 0, sizeof(*phdr));
1177                 phdr->p_type = PT_LOAD;
1178                 phdr->p_offset = offset;
1179                 phdr->p_vaddr = segment->da;
1180                 phdr->p_paddr = segment->da;
1181                 phdr->p_filesz = segment->size;
1182                 phdr->p_memsz = segment->size;
1183                 phdr->p_flags = PF_R | PF_W | PF_X;
1184                 phdr->p_align = 0;
1186                 ptr = rproc_da_to_va(rproc, segment->da, segment->size);
1187                 if (!ptr) {
1188                         dev_err(&rproc->dev,
1189                                 "invalid coredump segment (%pad, %zu)\n",
1190                                 &segment->da, segment->size);
1191                         memset(data + offset, 0xff, segment->size);
1192                 } else {
1193                         memcpy(data + offset, ptr, segment->size);
1194                 }
1196                 offset += phdr->p_filesz;
1197                 phdr++;
1198         }
1200         dev_coredumpv(&rproc->dev, data, data_size, GFP_KERNEL);
1203 /**
1204  * rproc_trigger_recovery() - recover a remoteproc
1205  * @rproc: the remote processor
1206  *
1207  * The recovery is done by resetting all the virtio devices, that way all the
1208  * rpmsg drivers will be reseted along with the remote processor making the
1209  * remoteproc functional again.
1210  *
1211  * This function can sleep, so it cannot be called from atomic context.
1212  */
1213 int rproc_trigger_recovery(struct rproc *rproc)
1215         const struct firmware *firmware_p;
1216         struct device *dev = &rproc->dev;
1217         int ret;
1219         dev_err(dev, "recovering %s\n", rproc->name);
1221         ret = mutex_lock_interruptible(&rproc->lock);
1222         if (ret)
1223                 return ret;
1225         ret = rproc_stop(rproc, true);
1226         if (ret)
1227                 goto unlock_mutex;
1229         /* generate coredump */
1230         rproc_coredump(rproc);
1232         /* load firmware */
1233         ret = request_firmware(&firmware_p, rproc->firmware, dev);
1234         if (ret < 0) {
1235                 dev_err(dev, "request_firmware failed: %d\n", ret);
1236                 goto unlock_mutex;
1237         }
1239         /* boot the remote processor up again */
1240         ret = rproc_start(rproc, firmware_p);
1242         release_firmware(firmware_p);
1244 unlock_mutex:
1245         mutex_unlock(&rproc->lock);
1246         return ret;
1249 /**
1250  * rproc_crash_handler_work() - handle a crash
1251  *
1252  * This function needs to handle everything related to a crash, like cpu
1253  * registers and stack dump, information to help to debug the fatal error, etc.
1254  */
1255 static void rproc_crash_handler_work(struct work_struct *work)
1257         struct rproc *rproc = container_of(work, struct rproc, crash_handler);
1258         struct device *dev = &rproc->dev;
1260         dev_dbg(dev, "enter %s\n", __func__);
1262         mutex_lock(&rproc->lock);
1264         if (rproc->state == RPROC_CRASHED || rproc->state == RPROC_OFFLINE) {
1265                 /* handle only the first crash detected */
1266                 mutex_unlock(&rproc->lock);
1267                 return;
1268         }
1270         rproc->state = RPROC_CRASHED;
1271         dev_err(dev, "handling crash #%u in %s\n", ++rproc->crash_cnt,
1272                 rproc->name);
1274         mutex_unlock(&rproc->lock);
1276         if (!rproc->recovery_disabled)
1277                 rproc_trigger_recovery(rproc);
1280 /**
1281  * rproc_boot() - boot a remote processor
1282  * @rproc: handle of a remote processor
1283  *
1284  * Boot a remote processor (i.e. load its firmware, power it on, ...).
1285  *
1286  * If the remote processor is already powered on, this function immediately
1287  * returns (successfully).
1288  *
1289  * Returns 0 on success, and an appropriate error value otherwise.
1290  */
1291 int rproc_boot(struct rproc *rproc)
1293         const struct firmware *firmware_p;
1294         struct device *dev;
1295         int ret;
1297         if (!rproc) {
1298                 pr_err("invalid rproc handle\n");
1299                 return -EINVAL;
1300         }
1302         dev = &rproc->dev;
1304         ret = mutex_lock_interruptible(&rproc->lock);
1305         if (ret) {
1306                 dev_err(dev, "can't lock rproc %s: %d\n", rproc->name, ret);
1307                 return ret;
1308         }
1310         if (rproc->state == RPROC_DELETED) {
1311                 ret = -ENODEV;
1312                 dev_err(dev, "can't boot deleted rproc %s\n", rproc->name);
1313                 goto unlock_mutex;
1314         }
1316         /* skip the boot process if rproc is already powered up */
1317         if (atomic_inc_return(&rproc->power) > 1) {
1318                 ret = 0;
1319                 goto unlock_mutex;
1320         }
1322         dev_info(dev, "powering up %s\n", rproc->name);
1324         /* load firmware */
1325         ret = request_firmware(&firmware_p, rproc->firmware, dev);
1326         if (ret < 0) {
1327                 dev_err(dev, "request_firmware failed: %d\n", ret);
1328                 goto downref_rproc;
1329         }
1331         ret = rproc_fw_boot(rproc, firmware_p);
1333         release_firmware(firmware_p);
1335 downref_rproc:
1336         if (ret)
1337                 atomic_dec(&rproc->power);
1338 unlock_mutex:
1339         mutex_unlock(&rproc->lock);
1340         return ret;
1342 EXPORT_SYMBOL(rproc_boot);
1344 /**
1345  * rproc_shutdown() - power off the remote processor
1346  * @rproc: the remote processor
1347  *
1348  * Power off a remote processor (previously booted with rproc_boot()).
1349  *
1350  * In case @rproc is still being used by an additional user(s), then
1351  * this function will just decrement the power refcount and exit,
1352  * without really powering off the device.
1353  *
1354  * Every call to rproc_boot() must (eventually) be accompanied by a call
1355  * to rproc_shutdown(). Calling rproc_shutdown() redundantly is a bug.
1356  *
1357  * Notes:
1358  * - we're not decrementing the rproc's refcount, only the power refcount.
1359  *   which means that the @rproc handle stays valid even after rproc_shutdown()
1360  *   returns, and users can still use it with a subsequent rproc_boot(), if
1361  *   needed.
1362  */
1363 void rproc_shutdown(struct rproc *rproc)
1365         struct device *dev = &rproc->dev;
1366         int ret;
1368         ret = mutex_lock_interruptible(&rproc->lock);
1369         if (ret) {
1370                 dev_err(dev, "can't lock rproc %s: %d\n", rproc->name, ret);
1371                 return;
1372         }
1374         /* if the remote proc is still needed, bail out */
1375         if (!atomic_dec_and_test(&rproc->power))
1376                 goto out;
1378         ret = rproc_stop(rproc, false);
1379         if (ret) {
1380                 atomic_inc(&rproc->power);
1381                 goto out;
1382         }
1384         /* clean up all acquired resources */
1385         rproc_resource_cleanup(rproc);
1387         rproc_disable_iommu(rproc);
1389         /* Free the copy of the resource table */
1390         kfree(rproc->cached_table);
1391         rproc->cached_table = NULL;
1392         rproc->table_ptr = NULL;
1393 out:
1394         mutex_unlock(&rproc->lock);
1396 EXPORT_SYMBOL(rproc_shutdown);
1398 /**
1399  * rproc_get_by_phandle() - find a remote processor by phandle
1400  * @phandle: phandle to the rproc
1401  *
1402  * Finds an rproc handle using the remote processor's phandle, and then
1403  * return a handle to the rproc.
1404  *
1405  * This function increments the remote processor's refcount, so always
1406  * use rproc_put() to decrement it back once rproc isn't needed anymore.
1407  *
1408  * Returns the rproc handle on success, and NULL on failure.
1409  */
1410 #ifdef CONFIG_OF
1411 struct rproc *rproc_get_by_phandle(phandle phandle)
1413         struct rproc *rproc = NULL, *r;
1414         struct device_node *np;
1416         np = of_find_node_by_phandle(phandle);
1417         if (!np)
1418                 return NULL;
1420         mutex_lock(&rproc_list_mutex);
1421         list_for_each_entry(r, &rproc_list, node) {
1422                 if (r->dev.parent && r->dev.parent->of_node == np) {
1423                         /* prevent underlying implementation from being removed */
1424                         if (!try_module_get(r->dev.parent->driver->owner)) {
1425                                 dev_err(&r->dev, "can't get owner\n");
1426                                 break;
1427                         }
1429                         rproc = r;
1430                         get_device(&rproc->dev);
1431                         break;
1432                 }
1433         }
1434         mutex_unlock(&rproc_list_mutex);
1436         of_node_put(np);
1438         return rproc;
1440 #else
1441 struct rproc *rproc_get_by_phandle(phandle phandle)
1443         return NULL;
1445 #endif
1446 EXPORT_SYMBOL(rproc_get_by_phandle);
1448 /**
1449  * rproc_add() - register a remote processor
1450  * @rproc: the remote processor handle to register
1451  *
1452  * Registers @rproc with the remoteproc framework, after it has been
1453  * allocated with rproc_alloc().
1454  *
1455  * This is called by the platform-specific rproc implementation, whenever
1456  * a new remote processor device is probed.
1457  *
1458  * Returns 0 on success and an appropriate error code otherwise.
1459  *
1460  * Note: this function initiates an asynchronous firmware loading
1461  * context, which will look for virtio devices supported by the rproc's
1462  * firmware.
1463  *
1464  * If found, those virtio devices will be created and added, so as a result
1465  * of registering this remote processor, additional virtio drivers might be
1466  * probed.
1467  */
1468 int rproc_add(struct rproc *rproc)
1470         struct device *dev = &rproc->dev;
1471         int ret;
1473         ret = device_add(dev);
1474         if (ret < 0)
1475                 return ret;
1477         dev_info(dev, "%s is available\n", rproc->name);
1479         /* create debugfs entries */
1480         rproc_create_debug_dir(rproc);
1482         /* if rproc is marked always-on, request it to boot */
1483         if (rproc->auto_boot) {
1484                 ret = rproc_trigger_auto_boot(rproc);
1485                 if (ret < 0)
1486                         return ret;
1487         }
1489         /* expose to rproc_get_by_phandle users */
1490         mutex_lock(&rproc_list_mutex);
1491         list_add(&rproc->node, &rproc_list);
1492         mutex_unlock(&rproc_list_mutex);
1494         return 0;
1496 EXPORT_SYMBOL(rproc_add);
1498 /**
1499  * rproc_type_release() - release a remote processor instance
1500  * @dev: the rproc's device
1501  *
1502  * This function should _never_ be called directly.
1503  *
1504  * It will be called by the driver core when no one holds a valid pointer
1505  * to @dev anymore.
1506  */
1507 static void rproc_type_release(struct device *dev)
1509         struct rproc *rproc = container_of(dev, struct rproc, dev);
1511         dev_info(&rproc->dev, "releasing %s\n", rproc->name);
1513         idr_destroy(&rproc->notifyids);
1515         if (rproc->index >= 0)
1516                 ida_simple_remove(&rproc_dev_index, rproc->index);
1518         kfree(rproc->firmware);
1519         kfree(rproc->ops);
1520         kfree(rproc);
1523 static const struct device_type rproc_type = {
1524         .name           = "remoteproc",
1525         .release        = rproc_type_release,
1526 };
1528 /**
1529  * rproc_alloc() - allocate a remote processor handle
1530  * @dev: the underlying device
1531  * @name: name of this remote processor
1532  * @ops: platform-specific handlers (mainly start/stop)
1533  * @firmware: name of firmware file to load, can be NULL
1534  * @len: length of private data needed by the rproc driver (in bytes)
1535  *
1536  * Allocates a new remote processor handle, but does not register
1537  * it yet. if @firmware is NULL, a default name is used.
1538  *
1539  * This function should be used by rproc implementations during initialization
1540  * of the remote processor.
1541  *
1542  * After creating an rproc handle using this function, and when ready,
1543  * implementations should then call rproc_add() to complete
1544  * the registration of the remote processor.
1545  *
1546  * On success the new rproc is returned, and on failure, NULL.
1547  *
1548  * Note: _never_ directly deallocate @rproc, even if it was not registered
1549  * yet. Instead, when you need to unroll rproc_alloc(), use rproc_free().
1550  */
1551 struct rproc *rproc_alloc(struct device *dev, const char *name,
1552                           const struct rproc_ops *ops,
1553                           const char *firmware, int len)
1555         struct rproc *rproc;
1556         char *p, *template = "rproc-%s-fw";
1557         int name_len;
1559         if (!dev || !name || !ops)
1560                 return NULL;
1562         if (!firmware) {
1563                 /*
1564                  * If the caller didn't pass in a firmware name then
1565                  * construct a default name.
1566                  */
1567                 name_len = strlen(name) + strlen(template) - 2 + 1;
1568                 p = kmalloc(name_len, GFP_KERNEL);
1569                 if (!p)
1570                         return NULL;
1571                 snprintf(p, name_len, template, name);
1572         } else {
1573                 p = kstrdup(firmware, GFP_KERNEL);
1574                 if (!p)
1575                         return NULL;
1576         }
1578         rproc = kzalloc(sizeof(struct rproc) + len, GFP_KERNEL);
1579         if (!rproc) {
1580                 kfree(p);
1581                 return NULL;
1582         }
1584         rproc->ops = kmemdup(ops, sizeof(*ops), GFP_KERNEL);
1585         if (!rproc->ops) {
1586                 kfree(p);
1587                 kfree(rproc);
1588                 return NULL;
1589         }
1591         rproc->firmware = p;
1592         rproc->name = name;
1593         rproc->priv = &rproc[1];
1594         rproc->auto_boot = true;
1596         device_initialize(&rproc->dev);
1597         rproc->dev.parent = dev;
1598         rproc->dev.type = &rproc_type;
1599         rproc->dev.class = &rproc_class;
1600         rproc->dev.driver_data = rproc;
1602         /* Assign a unique device index and name */
1603         rproc->index = ida_simple_get(&rproc_dev_index, 0, 0, GFP_KERNEL);
1604         if (rproc->index < 0) {
1605                 dev_err(dev, "ida_simple_get failed: %d\n", rproc->index);
1606                 put_device(&rproc->dev);
1607                 return NULL;
1608         }
1610         dev_set_name(&rproc->dev, "remoteproc%d", rproc->index);
1612         atomic_set(&rproc->power, 0);
1614         /* Default to ELF loader if no load function is specified */
1615         if (!rproc->ops->load) {
1616                 rproc->ops->load = rproc_elf_load_segments;
1617                 rproc->ops->parse_fw = rproc_elf_load_rsc_table;
1618                 rproc->ops->find_loaded_rsc_table = rproc_elf_find_loaded_rsc_table;
1619                 rproc->ops->sanity_check = rproc_elf_sanity_check;
1620                 rproc->ops->get_boot_addr = rproc_elf_get_boot_addr;
1621         }
1623         mutex_init(&rproc->lock);
1625         idr_init(&rproc->notifyids);
1627         INIT_LIST_HEAD(&rproc->carveouts);
1628         INIT_LIST_HEAD(&rproc->mappings);
1629         INIT_LIST_HEAD(&rproc->traces);
1630         INIT_LIST_HEAD(&rproc->rvdevs);
1631         INIT_LIST_HEAD(&rproc->subdevs);
1632         INIT_LIST_HEAD(&rproc->dump_segments);
1634         INIT_WORK(&rproc->crash_handler, rproc_crash_handler_work);
1636         rproc->state = RPROC_OFFLINE;
1638         return rproc;
1640 EXPORT_SYMBOL(rproc_alloc);
1642 /**
1643  * rproc_free() - unroll rproc_alloc()
1644  * @rproc: the remote processor handle
1645  *
1646  * This function decrements the rproc dev refcount.
1647  *
1648  * If no one holds any reference to rproc anymore, then its refcount would
1649  * now drop to zero, and it would be freed.
1650  */
1651 void rproc_free(struct rproc *rproc)
1653         put_device(&rproc->dev);
1655 EXPORT_SYMBOL(rproc_free);
1657 /**
1658  * rproc_put() - release rproc reference
1659  * @rproc: the remote processor handle
1660  *
1661  * This function decrements the rproc dev refcount.
1662  *
1663  * If no one holds any reference to rproc anymore, then its refcount would
1664  * now drop to zero, and it would be freed.
1665  */
1666 void rproc_put(struct rproc *rproc)
1668         module_put(rproc->dev.parent->driver->owner);
1669         put_device(&rproc->dev);
1671 EXPORT_SYMBOL(rproc_put);
1673 /**
1674  * rproc_del() - unregister a remote processor
1675  * @rproc: rproc handle to unregister
1676  *
1677  * This function should be called when the platform specific rproc
1678  * implementation decides to remove the rproc device. it should
1679  * _only_ be called if a previous invocation of rproc_add()
1680  * has completed successfully.
1681  *
1682  * After rproc_del() returns, @rproc isn't freed yet, because
1683  * of the outstanding reference created by rproc_alloc. To decrement that
1684  * one last refcount, one still needs to call rproc_free().
1685  *
1686  * Returns 0 on success and -EINVAL if @rproc isn't valid.
1687  */
1688 int rproc_del(struct rproc *rproc)
1690         if (!rproc)
1691                 return -EINVAL;
1693         /* if rproc is marked always-on, rproc_add() booted it */
1694         /* TODO: make sure this works with rproc->power > 1 */
1695         if (rproc->auto_boot)
1696                 rproc_shutdown(rproc);
1698         mutex_lock(&rproc->lock);
1699         rproc->state = RPROC_DELETED;
1700         mutex_unlock(&rproc->lock);
1702         rproc_delete_debug_dir(rproc);
1704         /* the rproc is downref'ed as soon as it's removed from the klist */
1705         mutex_lock(&rproc_list_mutex);
1706         list_del(&rproc->node);
1707         mutex_unlock(&rproc_list_mutex);
1709         device_del(&rproc->dev);
1711         return 0;
1713 EXPORT_SYMBOL(rproc_del);
1715 /**
1716  * rproc_add_subdev() - add a subdevice to a remoteproc
1717  * @rproc: rproc handle to add the subdevice to
1718  * @subdev: subdev handle to register
1719  *
1720  * Caller is responsible for populating optional subdevice function pointers.
1721  */
1722 void rproc_add_subdev(struct rproc *rproc, struct rproc_subdev *subdev)
1724         list_add_tail(&subdev->node, &rproc->subdevs);
1726 EXPORT_SYMBOL(rproc_add_subdev);
1728 /**
1729  * rproc_remove_subdev() - remove a subdevice from a remoteproc
1730  * @rproc: rproc handle to remove the subdevice from
1731  * @subdev: subdev handle, previously registered with rproc_add_subdev()
1732  */
1733 void rproc_remove_subdev(struct rproc *rproc, struct rproc_subdev *subdev)
1735         list_del(&subdev->node);
1737 EXPORT_SYMBOL(rproc_remove_subdev);
1739 /**
1740  * rproc_get_by_child() - acquire rproc handle of @dev's ancestor
1741  * @dev:        child device to find ancestor of
1742  *
1743  * Returns the ancestor rproc instance, or NULL if not found.
1744  */
1745 struct rproc *rproc_get_by_child(struct device *dev)
1747         for (dev = dev->parent; dev; dev = dev->parent) {
1748                 if (dev->type == &rproc_type)
1749                         return dev->driver_data;
1750         }
1752         return NULL;
1754 EXPORT_SYMBOL(rproc_get_by_child);
1756 /**
1757  * rproc_report_crash() - rproc crash reporter function
1758  * @rproc: remote processor
1759  * @type: crash type
1760  *
1761  * This function must be called every time a crash is detected by the low-level
1762  * drivers implementing a specific remoteproc. This should not be called from a
1763  * non-remoteproc driver.
1764  *
1765  * This function can be called from atomic/interrupt context.
1766  */
1767 void rproc_report_crash(struct rproc *rproc, enum rproc_crash_type type)
1769         if (!rproc) {
1770                 pr_err("NULL rproc pointer\n");
1771                 return;
1772         }
1774         dev_err(&rproc->dev, "crash detected in %s: type %s\n",
1775                 rproc->name, rproc_crash_to_string(type));
1777         /* create a new task to handle the error */
1778         schedule_work(&rproc->crash_handler);
1780 EXPORT_SYMBOL(rproc_report_crash);
1782 static int __init remoteproc_init(void)
1784         rproc_init_sysfs();
1785         rproc_init_debugfs();
1787         return 0;
1789 module_init(remoteproc_init);
1791 static void __exit remoteproc_exit(void)
1793         ida_destroy(&rproc_dev_index);
1795         rproc_exit_debugfs();
1796         rproc_exit_sysfs();
1798 module_exit(remoteproc_exit);
1800 MODULE_LICENSE("GPL v2");
1801 MODULE_DESCRIPTION("Generic Remote Processor Framework");