1 /*
2 * Remote Processor Framework Elf loader
3 *
4 * Copyright (C) 2011 Texas Instruments, Inc.
5 * Copyright (C) 2011 Google, Inc.
6 *
7 * Ohad Ben-Cohen <ohad@wizery.com>
8 * Brian Swetland <swetland@google.com>
9 * Mark Grosen <mgrosen@ti.com>
10 * Fernando Guzman Lugo <fernando.lugo@ti.com>
11 * Suman Anna <s-anna@ti.com>
12 * Robert Tivy <rtivy@ti.com>
13 * Armando Uribe De Leon <x0095078@ti.com>
14 * Sjur Brændeland <sjur.brandeland@stericsson.com>
15 *
16 * This program is free software; you can redistribute it and/or
17 * modify it under the terms of the GNU General Public License
18 * version 2 as published by the Free Software Foundation.
19 *
20 * This program is distributed in the hope that it will be useful,
21 * but WITHOUT ANY WARRANTY; without even the implied warranty of
22 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
23 * GNU General Public License for more details.
24 */
26 #define pr_fmt(fmt) "%s: " fmt, __func__
28 #include <linux/module.h>
29 #include <linux/firmware.h>
30 #include <linux/remoteproc.h>
31 #include <linux/elf.h>
33 #include "remoteproc_internal.h"
35 /**
36 * rproc_elf_sanity_check() - Sanity Check ELF firmware image
37 * @rproc: the remote processor handle
38 * @fw: the ELF firmware image
39 *
40 * Make sure this fw image is sane.
41 */
42 int rproc_elf_sanity_check(struct rproc *rproc, const struct firmware *fw)
43 {
44 const char *name = rproc->firmware;
45 struct device *dev = &rproc->dev;
46 struct elf32_hdr *ehdr;
47 char class;
49 if (!fw) {
50 dev_err(dev, "failed to load %s\n", name);
51 return -EINVAL;
52 }
54 if (fw->size < sizeof(struct elf32_hdr)) {
55 dev_err(dev, "Image is too small\n");
56 return -EINVAL;
57 }
59 ehdr = (struct elf32_hdr *)fw->data;
61 /* We only support ELF32 at this point */
62 class = ehdr->e_ident[EI_CLASS];
63 if (class != ELFCLASS32) {
64 dev_err(dev, "Unsupported class: %d\n", class);
65 return -EINVAL;
66 }
68 /* We assume the firmware has the same endianness as the host */
69 # ifdef __LITTLE_ENDIAN
70 if (ehdr->e_ident[EI_DATA] != ELFDATA2LSB) {
71 # else /* BIG ENDIAN */
72 if (ehdr->e_ident[EI_DATA] != ELFDATA2MSB) {
73 # endif
74 dev_err(dev, "Unsupported firmware endianness\n");
75 return -EINVAL;
76 }
78 if (fw->size < ehdr->e_shoff + sizeof(struct elf32_shdr)) {
79 dev_err(dev, "Image is too small\n");
80 return -EINVAL;
81 }
83 if (memcmp(ehdr->e_ident, ELFMAG, SELFMAG)) {
84 dev_err(dev, "Image is corrupted (bad magic)\n");
85 return -EINVAL;
86 }
88 if (ehdr->e_phnum == 0) {
89 dev_err(dev, "No loadable segments\n");
90 return -EINVAL;
91 }
93 if (ehdr->e_phoff > fw->size) {
94 dev_err(dev, "Firmware size is too small\n");
95 return -EINVAL;
96 }
98 return 0;
99 }
100 EXPORT_SYMBOL(rproc_elf_sanity_check);
102 /**
103 * rproc_elf_get_boot_addr() - Get rproc's boot address.
104 * @rproc: the remote processor handle
105 * @fw: the ELF firmware image
106 *
107 * This function returns the entry point address of the ELF
108 * image.
109 *
110 * Note that the boot address is not a configurable property of all remote
111 * processors. Some will always boot at a specific hard-coded address.
112 */
113 u32 rproc_elf_get_boot_addr(struct rproc *rproc, const struct firmware *fw)
114 {
115 struct elf32_hdr *ehdr = (struct elf32_hdr *)fw->data;
117 return ehdr->e_entry;
118 }
119 EXPORT_SYMBOL(rproc_elf_get_boot_addr);
121 /**
122 * rproc_elf_load_segments() - load firmware segments to memory
123 * @rproc: remote processor which will be booted using these fw segments
124 * @fw: the ELF firmware image
125 *
126 * This function loads the firmware segments to memory, where the remote
127 * processor expects them.
128 *
129 * Some remote processors will expect their code and data to be placed
130 * in specific device addresses, and can't have them dynamically assigned.
131 *
132 * We currently support only those kind of remote processors, and expect
133 * the program header's paddr member to contain those addresses. We then go
134 * through the physically contiguous "carveout" memory regions which we
135 * allocated (and mapped) earlier on behalf of the remote processor,
136 * and "translate" device address to kernel addresses, so we can copy the
137 * segments where they are expected.
138 *
139 * Currently we only support remote processors that required carveout
140 * allocations and got them mapped onto their iommus. Some processors
141 * might be different: they might not have iommus, and would prefer to
142 * directly allocate memory for every segment/resource. This is not yet
143 * supported, though.
144 */
145 int rproc_elf_load_segments(struct rproc *rproc, const struct firmware *fw)
146 {
147 struct device *dev = &rproc->dev;
148 struct elf32_hdr *ehdr;
149 struct elf32_phdr *phdr;
150 int i, ret = 0;
151 const u8 *elf_data = fw->data;
153 ehdr = (struct elf32_hdr *)elf_data;
154 phdr = (struct elf32_phdr *)(elf_data + ehdr->e_phoff);
156 /* go through the available ELF segments */
157 for (i = 0; i < ehdr->e_phnum; i++, phdr++) {
158 u32 da = phdr->p_paddr;
159 u32 memsz = phdr->p_memsz;
160 u32 filesz = phdr->p_filesz;
161 u32 offset = phdr->p_offset;
162 void *ptr;
164 if (phdr->p_type != PT_LOAD)
165 continue;
167 dev_dbg(dev, "phdr: type %d da 0x%x memsz 0x%x filesz 0x%x\n",
168 phdr->p_type, da, memsz, filesz);
170 if (filesz > memsz) {
171 dev_err(dev, "bad phdr filesz 0x%x memsz 0x%x\n",
172 filesz, memsz);
173 ret = -EINVAL;
174 break;
175 }
177 if (offset + filesz > fw->size) {
178 dev_err(dev, "truncated fw: need 0x%x avail 0x%zx\n",
179 offset + filesz, fw->size);
180 ret = -EINVAL;
181 break;
182 }
184 /* grab the kernel address for this device address */
185 ptr = rproc_da_to_va(rproc, da, memsz,
186 RPROC_FLAGS_ELF_PHDR | phdr->p_flags);
187 if (!ptr) {
188 dev_err(dev, "bad phdr da 0x%x mem 0x%x\n", da, memsz);
189 ret = -EINVAL;
190 break;
191 }
193 /* put the segment where the remote processor expects it */
194 if (phdr->p_filesz)
195 memcpy(ptr, elf_data + phdr->p_offset, filesz);
197 /*
198 * Zero out remaining memory for this segment.
199 *
200 * This isn't strictly required since dma_alloc_coherent already
201 * did this for us. albeit harmless, we may consider removing
202 * this.
203 */
204 if (memsz > filesz)
205 memset(ptr + filesz, 0, memsz - filesz);
206 }
208 return ret;
209 }
210 EXPORT_SYMBOL(rproc_elf_load_segments);
212 static struct elf32_shdr *
213 find_table(struct device *dev, struct elf32_hdr *ehdr, size_t fw_size)
214 {
215 struct elf32_shdr *shdr;
216 int i;
217 const char *name_table;
218 struct resource_table *table = NULL;
219 const u8 *elf_data = (void *)ehdr;
221 /* look for the resource table and handle it */
222 shdr = (struct elf32_shdr *)(elf_data + ehdr->e_shoff);
223 name_table = elf_data + shdr[ehdr->e_shstrndx].sh_offset;
225 for (i = 0; i < ehdr->e_shnum; i++, shdr++) {
226 u32 size = shdr->sh_size;
227 u32 offset = shdr->sh_offset;
229 if (strcmp(name_table + shdr->sh_name, ".resource_table"))
230 continue;
232 table = (struct resource_table *)(elf_data + offset);
234 /* make sure we have the entire table */
235 if (offset + size > fw_size || offset + size < size) {
236 dev_err(dev, "resource table truncated\n");
237 return NULL;
238 }
240 /* make sure table has at least the header */
241 if (sizeof(struct resource_table) > size) {
242 dev_err(dev, "header-less resource table\n");
243 return NULL;
244 }
246 /* we don't support any version beyond the first */
247 if (table->ver != 1) {
248 dev_err(dev, "unsupported fw ver: %d\n", table->ver);
249 return NULL;
250 }
252 /* make sure reserved bytes are zeroes */
253 if (table->reserved[0] || table->reserved[1]) {
254 dev_err(dev, "non zero reserved bytes\n");
255 return NULL;
256 }
258 /* make sure the offsets array isn't truncated */
259 if (table->num * sizeof(table->offset[0]) +
260 sizeof(struct resource_table) > size) {
261 dev_err(dev, "resource table incomplete\n");
262 return NULL;
263 }
265 return shdr;
266 }
268 return NULL;
269 }
271 /**
272 * rproc_elf_load_rsc_table() - load the resource table
273 * @rproc: the rproc handle
274 * @fw: the ELF firmware image
275 *
276 * This function finds the resource table inside the remote processor's
277 * firmware, load it into the @cached_table and update @table_ptr.
278 *
279 * Return: 0 on success, negative errno on failure.
280 */
281 int rproc_elf_load_rsc_table(struct rproc *rproc, const struct firmware *fw)
282 {
283 struct elf32_hdr *ehdr;
284 struct elf32_shdr *shdr;
285 struct device *dev = &rproc->dev;
286 struct resource_table *table = NULL;
287 const u8 *elf_data = fw->data;
288 size_t tablesz;
290 ehdr = (struct elf32_hdr *)elf_data;
292 shdr = find_table(dev, ehdr, fw->size);
293 if (!shdr)
294 return -EINVAL;
296 table = (struct resource_table *)(elf_data + shdr->sh_offset);
297 tablesz = shdr->sh_size;
299 /*
300 * Create a copy of the resource table. When a virtio device starts
301 * and calls vring_new_virtqueue() the address of the allocated vring
302 * will be stored in the cached_table. Before the device is started,
303 * cached_table will be copied into device memory.
304 */
305 rproc->cached_table = kmemdup(table, tablesz, GFP_KERNEL);
306 if (!rproc->cached_table)
307 return -ENOMEM;
309 rproc->table_ptr = rproc->cached_table;
310 rproc->table_sz = tablesz;
312 return 0;
313 }
314 EXPORT_SYMBOL(rproc_elf_load_rsc_table);
316 /**
317 * rproc_elf_find_loaded_rsc_table() - find the loaded resource table
318 * @rproc: the rproc handle
319 * @fw: the ELF firmware image
320 *
321 * This function finds the location of the loaded resource table. Don't
322 * call this function if the table wasn't loaded yet - it's a bug if you do.
323 *
324 * Returns the pointer to the resource table if it is found or NULL otherwise.
325 * If the table wasn't loaded yet the result is unspecified.
326 */
327 struct resource_table *rproc_elf_find_loaded_rsc_table(struct rproc *rproc,
328 const struct firmware *fw)
329 {
330 struct elf32_hdr *ehdr = (struct elf32_hdr *)fw->data;
331 struct elf32_shdr *shdr;
333 shdr = find_table(&rproc->dev, ehdr, fw->size);
334 if (!shdr)
335 return NULL;
337 return rproc_da_to_va(rproc, shdr->sh_addr, shdr->sh_size,
338 RPROC_FLAGS_ELF_SHDR | shdr->sh_flags);
339 }
340 EXPORT_SYMBOL(rproc_elf_find_loaded_rsc_table);