]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/remoteproc/remoteproc_internal.h
remoteproc: move rproc_da_to_va declaration to remoteproc.h
[rpmsg/rpmsg.git] / drivers / remoteproc / remoteproc_internal.h
1 /*
2  * Remote processor framework
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  * Copyright (C) 2011 Google, Inc.
6  *
7  * Ohad Ben-Cohen <ohad@wizery.com>
8  * Brian Swetland <swetland@google.com>
9  *
10  * This software is licensed under the terms of the GNU General Public
11  * License version 2, as published by the Free Software Foundation, and
12  * may be copied, distributed, and modified under those terms.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  */
20 #ifndef REMOTEPROC_INTERNAL_H
21 #define REMOTEPROC_INTERNAL_H
23 #include <linux/irqreturn.h>
24 #include <linux/firmware.h>
26 struct rproc;
28 /* from remoteproc_core.c */
29 void rproc_release(struct kref *kref);
30 irqreturn_t rproc_vq_interrupt(struct rproc *rproc, int vq_id);
31 void rproc_vdev_release(struct kref *ref);
33 /* from remoteproc_virtio.c */
34 int rproc_add_virtio_dev(struct rproc_vdev *rvdev, int id);
35 void rproc_remove_virtio_dev(struct rproc_vdev *rvdev);
37 /* from remoteproc_debugfs.c */
38 void rproc_remove_trace_file(struct dentry *tfile);
39 struct dentry *rproc_create_trace_file(const char *name, struct rproc *rproc,
40                                        struct rproc_mem_entry *trace);
41 void rproc_delete_debug_dir(struct rproc *rproc);
42 void rproc_create_debug_dir(struct rproc *rproc);
43 void rproc_init_debugfs(void);
44 void rproc_exit_debugfs(void);
46 /* from remoteproc_sysfs.c */
47 extern struct class rproc_class;
48 int rproc_init_sysfs(void);
49 void rproc_exit_sysfs(void);
51 void rproc_free_vring(struct rproc_vring *rvring);
52 int rproc_alloc_vring(struct rproc_vdev *rvdev, int i);
54 int rproc_trigger_recovery(struct rproc *rproc);
56 int rproc_elf_sanity_check(struct rproc *rproc, const struct firmware *fw);
57 u32 rproc_elf_get_boot_addr(struct rproc *rproc, const struct firmware *fw);
58 int rproc_elf_load_segments(struct rproc *rproc, const struct firmware *fw);
59 int rproc_elf_load_rsc_table(struct rproc *rproc, const struct firmware *fw);
60 struct resource_table *rproc_elf_find_loaded_rsc_table(struct rproc *rproc,
61                                                        const struct firmware *fw);
63 static inline
64 int rproc_fw_sanity_check(struct rproc *rproc, const struct firmware *fw)
65 {
66         if (rproc->ops->sanity_check)
67                 return rproc->ops->sanity_check(rproc, fw);
69         return 0;
70 }
72 static inline
73 u32 rproc_get_boot_addr(struct rproc *rproc, const struct firmware *fw)
74 {
75         if (rproc->ops->get_boot_addr)
76                 return rproc->ops->get_boot_addr(rproc, fw);
78         return 0;
79 }
81 static inline
82 int rproc_load_segments(struct rproc *rproc, const struct firmware *fw)
83 {
84         if (rproc->ops->load)
85                 return rproc->ops->load(rproc, fw);
87         return -EINVAL;
88 }
90 static inline int rproc_parse_fw(struct rproc *rproc, const struct firmware *fw)
91 {
92         if (rproc->ops->parse_fw)
93                 return rproc->ops->parse_fw(rproc, fw);
95         return 0;
96 }
98 static inline
99 struct resource_table *rproc_find_loaded_rsc_table(struct rproc *rproc,
100                                                    const struct firmware *fw)
102         if (rproc->ops->find_loaded_rsc_table)
103                 return rproc->ops->find_loaded_rsc_table(rproc, fw);
105         return NULL;
108 #endif /* REMOTEPROC_INTERNAL_H */