]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/rpmsg/rpmsg_rpc_sysfs.c
rpmsg: rpc: introduce a new rpmsg_rpc driver
[rpmsg/rpmsg.git] / drivers / rpmsg / rpmsg_rpc_sysfs.c
1 // SPDX-License-Identifier: GPL-2.0
2 /*
3  * Remote Processor Procedure Call Driver
4  *
5  * Copyright (C) 2012-2019 Texas Instruments Incorporated - http://www.ti.com/
6  *      Erik Rainey <erik.rainey@ti.com>
7  *      Suman Anna <s-anna@ti.com>
8  */
10 #include <linux/device.h>
11 #include <linux/slab.h>
12 #include <linux/rpmsg_rpc.h>
14 #include "rpmsg_rpc_internal.h"
16 static ssize_t show_numfuncs(struct device *dev, struct device_attribute *attr,
17                              char *buf)
18 {
19         struct rppc_device *rppcdev = dev_get_drvdata(dev);
21         return snprintf(buf, PAGE_SIZE, "%u\n", rppcdev->num_funcs - 1);
22 }
24 static ssize_t set_type_c(char *buf, uint32_t len,
25                           struct rppc_param_signature *psig)
26 {
27         char *isptr = (psig->type & RPPC_PARAM_PTR ? " *" : "");
29         switch (psig->type & RPPC_PARAM_MASK) {
30         case RPPC_PARAM_S08:
31                 return snprintf(buf, len, "int8_t%s", isptr);
32         case RPPC_PARAM_U08:
33                 return snprintf(buf, len, "uint8_t%s", isptr);
34         case RPPC_PARAM_S16:
35                 return snprintf(buf, len, "int16_t%s", isptr);
36         case RPPC_PARAM_U16:
37                 return snprintf(buf, len, "uint16_t%s", isptr);
38         case RPPC_PARAM_S32:
39                 return snprintf(buf, len, "int32_t%s", isptr);
40         case RPPC_PARAM_U32:
41                 return snprintf(buf, len, "uint32_t%s", isptr);
42         case RPPC_PARAM_S64:
43                 return snprintf(buf, len, "int64_t%s", isptr);
44         case RPPC_PARAM_U64:
45                 return snprintf(buf, len, "uint64_t%s", isptr);
46         default:
47                 return snprintf(buf, len, "<unknown>%s", isptr);
48         }
49 }
51 static ssize_t set_type_doxy(char *buf, uint32_t len,
52                              struct rppc_param_signature *psig)
53 {
54         char *isptr = (psig->type & RPPC_PARAM_PTR ? " *" : "");
55         char dir[10];
57         switch (psig->direction) {
58         case RPPC_PARAMDIR_IN:
59                 snprintf(dir, sizeof(dir), "[in]");
60                 break;
61         case RPPC_PARAMDIR_OUT:
62                 snprintf(dir, sizeof(dir), "[out]");
63                 break;
64         case RPPC_PARAMDIR_BI:
65                 snprintf(dir, sizeof(dir), "[in,out]");
66                 break;
67         default:
68                 snprintf(dir, sizeof(dir), "[unknown]");
69                 break;
70         }
72         switch (psig->type & RPPC_PARAM_MASK) {
73         case RPPC_PARAM_S08:
74                 return snprintf(buf, len, "%s int8_t%s", dir, isptr);
75         case RPPC_PARAM_U08:
76                 return snprintf(buf, len, "%s uint8_t%s", dir, isptr);
77         case RPPC_PARAM_S16:
78                 return snprintf(buf, len, "%s int16_t%s", dir, isptr);
79         case RPPC_PARAM_U16:
80                 return snprintf(buf, len, "%s uint16_t%s", dir, isptr);
81         case RPPC_PARAM_S32:
82                 return snprintf(buf, len, "%s int32_t%s", dir, isptr);
83         case RPPC_PARAM_U32:
84                 return snprintf(buf, len, "%s uint32_t%s", dir, isptr);
85         case RPPC_PARAM_S64:
86                 return snprintf(buf, len, "%s int64_t%s", dir, isptr);
87         case RPPC_PARAM_U64:
88                 return snprintf(buf, len, "%s uint64_t%s", dir, isptr);
89         default:
90                 return snprintf(buf, len, "%s <unknown>%s", dir, isptr);
91         }
92 }
94 static ssize_t show_c_function(struct device *dev,
95                                struct device_attribute *attr, char *buf)
96 {
97         struct rppc_device *rppcdev = dev_get_drvdata(dev);
98         char return_value[11]; /* longest string is strlen("uintXX_t *") = 10 */
99         char parameters[110]; /* longest string * 10 + 9(,) */
100         char comment[300];
101         int p;
102         ssize_t pidx = 0;
103         ssize_t cidx = 0;
104         __u32 index = 0;
106         if (sscanf(attr->attr.name, "c_function%u\n", &index) != 1)
107                 return -EIO;
109         memset(return_value, 0, sizeof(return_value));
110         memset(parameters, 0, sizeof(parameters));
112         strcpy(return_value, "void");
113         strcpy(parameters, "void");
114         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx, "/**\n");
115         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx,
116                 " * \\fn %s\n", rppcdev->signatures[index].name);
117         for (p = 0; p < rppcdev->signatures[index].num_param; p++) {
118                 if (p == 0) {
119                         set_type_c(return_value, sizeof(return_value),
120                                    &rppcdev->signatures[index].params[0]);
121                         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx,
122                                         " * \\return %s\n", return_value);
123                 } else {
124                         pidx += set_type_c(&parameters[pidx],
125                                         sizeof(parameters) - pidx,
126                                         &rppcdev->signatures[index].params[p]);
127                         if (p != rppcdev->signatures[index].num_param - 1)
128                                 parameters[pidx++] = ',';
129                         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx,
130                                                 " * \\param ");
131                         cidx += set_type_doxy(&comment[cidx],
132                                         sizeof(comment) - cidx,
133                                         &rppcdev->signatures[index].params[p]);
134                         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx,
135                                                 "\n");
136                 }
137         }
138         if (p <= 1)
139                 pidx += strlen("void");
140         if (pidx < sizeof(parameters))
141                 parameters[pidx] = '\0';
142         cidx += snprintf(&comment[cidx], sizeof(comment) - cidx, " */");
143         return snprintf(buf, PAGE_SIZE, "%s\nextern \"C\" %s %s(%s);\n",
144                         comment, return_value, rppcdev->signatures[index].name,
145                         parameters);
148 static struct device_attribute rppc_attrs[] = {
149         __ATTR(num_funcs, 0444, show_numfuncs, NULL),
150 };
152 /**
153  * rppc_create_sysfs - Creates the sysfs entry structures for the instance
154  * @rppcdev: the rppc device (remote server instance) handle
155  *
156  * Helper function to create all the sysfs entries associated with a rppc
157  * device. Each device is associated with a number of remote procedure
158  * functions. The number of such functions and the signatures of those
159  * functions are created in sysfs. Function is invoked after querying
160  * the remote side about the supported functions on this device.
161  *
162  * The entries are split into a set of static entries, which are common
163  * between all rppc devices, and a set of dynamic entries specific to
164  * each rppc device.
165  *
166  * Return: 0 on success, or an appropriate error code otherwise
167  */
168 int rppc_create_sysfs(struct rppc_device *rppcdev)
170         int i;
171         int ret;
173         rppcdev->sig_attr = kcalloc(rppcdev->num_funcs,
174                                     sizeof(*rppcdev->sig_attr), GFP_KERNEL);
175         if (!rppcdev->sig_attr)
176                 return -ENOMEM;
178         for (i = 0; i < ARRAY_SIZE(rppc_attrs); i++) {
179                 ret = device_create_file(rppcdev->dev, &rppc_attrs[i]);
180                 if (ret) {
181                         dev_err(rppcdev->dev, "failed to create sysfs entry\n");
182                         goto clean_static_entries;
183                 }
184         }
186         for (i = 1; i < rppcdev->num_funcs; i++) {
187                 sysfs_attr_init(&rppcdev->sig_attr[i].attr);
188                 rppcdev->sig_attr[i].attr.name =
189                                 kzalloc(RPPC_MAX_FUNC_NAMELEN, GFP_KERNEL);
190                 if (!rppcdev->sig_attr[i].attr.name) {
191                         ret = -ENOMEM;
192                         goto clean_dynamic_entries;
193                 }
194                 snprintf((char *)rppcdev->sig_attr[i].attr.name,
195                          RPPC_MAX_FUNC_NAMELEN, "c_function%u", i);
196                 rppcdev->sig_attr[i].attr.mode = 0444;
197                 rppcdev->sig_attr[i].show = show_c_function;
198                 rppcdev->sig_attr[i].store = NULL;
200                 ret = device_create_file(rppcdev->dev, &rppcdev->sig_attr[i]);
201                 if (ret) {
202                         dev_err(rppcdev->dev, "failed to create sysfs function entry (%d)\n",
203                                 ret);
204                         goto clean_dynamic_entries;
205                 }
206         }
207         return 0;
209 clean_dynamic_entries:
210         while (i-- > 1) {
211                 device_remove_file(rppcdev->dev, &rppcdev->sig_attr[i]);
212                 kfree(rppcdev->sig_attr[i].attr.name);
213         }
214         i = ARRAY_SIZE(rppc_attrs);
215 clean_static_entries:
216         while (i-- > 0)
217                 device_remove_file(rppcdev->dev, &rppc_attrs[i]);
218         kfree(rppcdev->sig_attr);
219         return ret;
222 /**
223  * rppc_remove_sysfs: Removes the sysfs entry structures for the instance
224  * @rppcdev: the rppc device (remote server instance) handle
225  *
226  * Helper function to remove all the sysfs entries associated with the
227  * rppc device.
228  *
229  * Return: 0 on success, or an appropriate error code otherwise
230  */
231 int rppc_remove_sysfs(struct rppc_device *rppcdev)
233         int i;
235         if (rppcdev->sig_attr) {
236                 for (i = 1; i < rppcdev->num_funcs; i++) {
237                         device_remove_file(rppcdev->dev, &rppcdev->sig_attr[i]);
238                         kfree(rppcdev->sig_attr[i].attr.name);
239                 }
240         }
241         kfree(rppcdev->sig_attr);
243         for (i = 0; i < ARRAY_SIZE(rppc_attrs); i++)
244                 device_remove_file(rppcdev->dev, &rppc_attrs[i]);
246         return 0;