]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/scsi/csiostor/csio_hw.h
Merge tag 'devicetree-fixes-for-4.19-3' of git://git.kernel.org/pub/scm/linux/kernel...
[rpmsg/rpmsg.git] / drivers / scsi / csiostor / csio_hw.h
1 /*
2  * This file is part of the Chelsio FCoE driver for Linux.
3  *
4  * Copyright (c) 2008-2012 Chelsio Communications, Inc. All rights reserved.
5  *
6  * This software is available to you under a choice of one of two
7  * licenses.  You may choose to be licensed under the terms of the GNU
8  * General Public License (GPL) Version 2, available from the file
9  * COPYING in the main directory of this source tree, or the
10  * OpenIB.org BSD license below:
11  *
12  *     Redistribution and use in source and binary forms, with or
13  *     without modification, are permitted provided that the following
14  *     conditions are met:
15  *
16  *      - Redistributions of source code must retain the above
17  *        copyright notice, this list of conditions and the following
18  *        disclaimer.
19  *
20  *      - Redistributions in binary form must reproduce the above
21  *        copyright notice, this list of conditions and the following
22  *        disclaimer in the documentation and/or other materials
23  *        provided with the distribution.
24  *
25  * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
26  * EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
27  * MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND
28  * NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS
29  * BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN
30  * ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN
31  * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
32  * SOFTWARE.
33  */
35 #ifndef __CSIO_HW_H__
36 #define __CSIO_HW_H__
38 #include <linux/kernel.h>
39 #include <linux/pci.h>
40 #include <linux/device.h>
41 #include <linux/workqueue.h>
42 #include <linux/compiler.h>
43 #include <linux/cdev.h>
44 #include <linux/list.h>
45 #include <linux/mempool.h>
46 #include <linux/io.h>
47 #include <linux/spinlock_types.h>
48 #include <scsi/scsi_device.h>
49 #include <scsi/scsi_transport_fc.h>
51 #include "t4_hw.h"
52 #include "csio_hw_chip.h"
53 #include "csio_wr.h"
54 #include "csio_mb.h"
55 #include "csio_scsi.h"
56 #include "csio_defs.h"
57 #include "t4_regs.h"
58 #include "t4_msg.h"
60 /*
61  * An error value used by host. Should not clash with FW defined return values.
62  */
63 #define FW_HOSTERROR                    255
65 #define CSIO_HW_NAME            "Chelsio FCoE Adapter"
66 #define CSIO_MAX_PFN            8
67 #define CSIO_MAX_PPORTS         4
69 #define CSIO_MAX_LUN            0xFFFF
70 #define CSIO_MAX_QUEUE          2048
71 #define CSIO_MAX_CMD_PER_LUN    32
72 #define CSIO_MAX_DDP_BUF_SIZE   (1024 * 1024)
73 #define CSIO_MAX_SECTOR_SIZE    128
74 #define CSIO_MIN_T6_FW          0x01102D00  /* FW 1.16.45.0 */
76 /* Interrupts */
77 #define CSIO_EXTRA_MSI_IQS      2       /* Extra iqs for INTX/MSI mode
78                                          * (Forward intr iq + fw iq) */
79 #define CSIO_EXTRA_VECS         2       /* non-data + FW evt */
80 #define CSIO_MAX_SCSI_CPU       128
81 #define CSIO_MAX_SCSI_QSETS     (CSIO_MAX_SCSI_CPU * CSIO_MAX_PPORTS)
82 #define CSIO_MAX_MSIX_VECS      (CSIO_MAX_SCSI_QSETS + CSIO_EXTRA_VECS)
84 /* Queues */
85 enum {
86         CSIO_INTR_WRSIZE = 128,
87         CSIO_INTR_IQSIZE = ((CSIO_MAX_MSIX_VECS + 1) * CSIO_INTR_WRSIZE),
88         CSIO_FWEVT_WRSIZE = 128,
89         CSIO_FWEVT_IQLEN = 128,
90         CSIO_FWEVT_FLBUFS = 64,
91         CSIO_FWEVT_IQSIZE = (CSIO_FWEVT_WRSIZE * CSIO_FWEVT_IQLEN),
92         CSIO_HW_NIQ = 1,
93         CSIO_HW_NFLQ = 1,
94         CSIO_HW_NEQ = 1,
95         CSIO_HW_NINTXQ = 1,
96 };
98 struct csio_msix_entries {
99         void            *dev_id;        /* Priv object associated w/ this msix*/
100         char            desc[24];       /* Description of this vector */
101 };
103 struct csio_scsi_qset {
104         int             iq_idx;         /* Ingress index */
105         int             eq_idx;         /* Egress index */
106         uint32_t        intr_idx;       /* MSIX Vector index */
107 };
109 struct csio_scsi_cpu_info {
110         int16_t max_cpus;
111 };
113 extern int csio_dbg_level;
114 extern unsigned int csio_port_mask;
115 extern int csio_msi;
117 #define CSIO_VENDOR_ID                          0x1425
118 #define CSIO_ASIC_DEVID_PROTO_MASK              0xFF00
119 #define CSIO_ASIC_DEVID_TYPE_MASK               0x00FF
121 #define CSIO_GLBL_INTR_MASK     (CIM_F | MPS_F | PL_F | PCIE_F | MC_F | \
122                                  EDC0_F | EDC1_F | LE_F | TP_F | MA_F | \
123                                  PM_TX_F | PM_RX_F | ULP_RX_F | \
124                                  CPL_SWITCH_F | SGE_F | ULP_TX_F | SF_F)
126 /*
127  * Hard parameters used to initialize the card in the absence of a
128  * configuration file.
129  */
130 enum {
131         /* General */
132         CSIO_SGE_DBFIFO_INT_THRESH      = 10,
134         CSIO_SGE_RX_DMA_OFFSET          = 2,
136         CSIO_SGE_FLBUF_SIZE1            = 65536,
137         CSIO_SGE_FLBUF_SIZE2            = 1536,
138         CSIO_SGE_FLBUF_SIZE3            = 9024,
139         CSIO_SGE_FLBUF_SIZE4            = 9216,
140         CSIO_SGE_FLBUF_SIZE5            = 2048,
141         CSIO_SGE_FLBUF_SIZE6            = 128,
142         CSIO_SGE_FLBUF_SIZE7            = 8192,
143         CSIO_SGE_FLBUF_SIZE8            = 16384,
145         CSIO_SGE_TIMER_VAL_0            = 5,
146         CSIO_SGE_TIMER_VAL_1            = 10,
147         CSIO_SGE_TIMER_VAL_2            = 20,
148         CSIO_SGE_TIMER_VAL_3            = 50,
149         CSIO_SGE_TIMER_VAL_4            = 100,
150         CSIO_SGE_TIMER_VAL_5            = 200,
152         CSIO_SGE_INT_CNT_VAL_0          = 1,
153         CSIO_SGE_INT_CNT_VAL_1          = 4,
154         CSIO_SGE_INT_CNT_VAL_2          = 8,
155         CSIO_SGE_INT_CNT_VAL_3          = 16,
156 };
158 /* Slowpath events */
159 enum csio_evt {
160         CSIO_EVT_FW  = 0,       /* FW event */
161         CSIO_EVT_MBX,           /* MBX event */
162         CSIO_EVT_SCN,           /* State change notification */
163         CSIO_EVT_DEV_LOSS,      /* Device loss event */
164         CSIO_EVT_MAX,           /* Max supported event */
165 };
167 #define CSIO_EVT_MSG_SIZE       512
168 #define CSIO_EVTQ_SIZE          512
170 /* Event msg  */
171 struct csio_evt_msg {
172         struct list_head        list;   /* evt queue*/
173         enum csio_evt           type;
174         uint8_t                 data[CSIO_EVT_MSG_SIZE];
175 };
177 enum {
178         SERNUM_LEN     = 16,    /* Serial # length */
179         EC_LEN         = 16,    /* E/C length */
180         ID_LEN         = 16,    /* ID length */
181 };
183 enum {
184         SF_SIZE = SF_SEC_SIZE * 16,   /* serial flash size */
185 };
187 /* serial flash and firmware constants */
188 enum {
189         SF_ATTEMPTS = 10,             /* max retries for SF operations */
191         /* flash command opcodes */
192         SF_PROG_PAGE    = 2,          /* program page */
193         SF_WR_DISABLE   = 4,          /* disable writes */
194         SF_RD_STATUS    = 5,          /* read status register */
195         SF_WR_ENABLE    = 6,          /* enable writes */
196         SF_RD_DATA_FAST = 0xb,        /* read flash */
197         SF_RD_ID        = 0x9f,       /* read ID */
198         SF_ERASE_SECTOR = 0xd8,       /* erase sector */
199 };
201 /* Management module */
202 enum {
203         CSIO_MGMT_EQ_WRSIZE = 512,
204         CSIO_MGMT_IQ_WRSIZE = 128,
205         CSIO_MGMT_EQLEN = 64,
206         CSIO_MGMT_IQLEN = 64,
207 };
209 #define CSIO_MGMT_EQSIZE        (CSIO_MGMT_EQLEN * CSIO_MGMT_EQ_WRSIZE)
210 #define CSIO_MGMT_IQSIZE        (CSIO_MGMT_IQLEN * CSIO_MGMT_IQ_WRSIZE)
212 /* mgmt module stats */
213 struct csio_mgmtm_stats {
214         uint32_t        n_abort_req;            /* Total abort request */
215         uint32_t        n_abort_rsp;            /* Total abort response */
216         uint32_t        n_close_req;            /* Total close request */
217         uint32_t        n_close_rsp;            /* Total close response */
218         uint32_t        n_err;                  /* Total Errors */
219         uint32_t        n_drop;                 /* Total request dropped */
220         uint32_t        n_active;               /* Count of active_q */
221         uint32_t        n_cbfn;                 /* Count of cbfn_q */
222 };
224 /* MGMT module */
225 struct csio_mgmtm {
226         struct  csio_hw         *hw;            /* Pointer to HW moduel */
227         int                     eq_idx;         /* Egress queue index */
228         int                     iq_idx;         /* Ingress queue index */
229         int                     msi_vec;        /* MSI vector */
230         struct list_head        active_q;       /* Outstanding ELS/CT */
231         struct list_head        abort_q;        /* Outstanding abort req */
232         struct list_head        cbfn_q;         /* Completion queue */
233         struct list_head        mgmt_req_freelist; /* Free poll of reqs */
234                                                 /* ELSCT request freelist*/
235         struct timer_list       mgmt_timer;     /* MGMT timer */
236         struct csio_mgmtm_stats stats;          /* ELS/CT stats */
237 };
239 struct csio_adap_desc {
240         char model_no[16];
241         char description[32];
242 };
244 struct pci_params {
245         uint16_t   vendor_id;
246         uint16_t   device_id;
247         int        vpd_cap_addr;
248         uint16_t   speed;
249         uint8_t    width;
250 };
252 /* User configurable hw parameters */
253 struct csio_hw_params {
254         uint32_t                sf_size;                /* serial flash
255                                                          * size in bytes
256                                                          */
257         uint32_t                sf_nsec;                /* # of flash sectors */
258         struct pci_params       pci;
259         uint32_t                log_level;              /* Module-level for
260                                                          * debug log.
261                                                          */
262 };
264 struct csio_vpd {
265         uint32_t cclk;
266         uint8_t ec[EC_LEN + 1];
267         uint8_t sn[SERNUM_LEN + 1];
268         uint8_t id[ID_LEN + 1];
269 };
271 /* Firmware Port Capabilities types. */
273 typedef u16 fw_port_cap16_t;    /* 16-bit Port Capabilities integral value */
274 typedef u32 fw_port_cap32_t;    /* 32-bit Port Capabilities integral value */
276 enum fw_caps {
277         FW_CAPS_UNKNOWN = 0,    /* 0'ed out initial state */
278         FW_CAPS16       = 1,    /* old Firmware: 16-bit Port Capabilities */
279         FW_CAPS32       = 2,    /* new Firmware: 32-bit Port Capabilities */
280 };
282 enum cc_pause {
283         PAUSE_RX      = 1 << 0,
284         PAUSE_TX      = 1 << 1,
285         PAUSE_AUTONEG = 1 << 2
286 };
288 enum cc_fec {
289         FEC_AUTO        = 1 << 0,  /* IEEE 802.3 "automatic" */
290         FEC_RS          = 1 << 1,  /* Reed-Solomon */
291         FEC_BASER_RS    = 1 << 2   /* BaseR/Reed-Solomon */
292 };
294 struct link_config {
295         fw_port_cap32_t pcaps;          /* link capabilities */
296         fw_port_cap32_t def_acaps;      /* default advertised capabilities */
297         fw_port_cap32_t acaps;          /* advertised capabilities */
298         fw_port_cap32_t lpacaps;        /* peer advertised capabilities */
300         fw_port_cap32_t speed_caps;     /* speed(s) user has requested */
301         unsigned int   speed;           /* actual link speed (Mb/s) */
303         enum cc_pause  requested_fc;    /* flow control user has requested */
304         enum cc_pause  fc;              /* actual link flow control */
306         enum cc_fec    requested_fec;   /* Forward Error Correction: */
307         enum cc_fec    fec;             /* requested and actual in use */
309         unsigned char  autoneg;         /* autonegotiating? */
311         unsigned char  link_ok;         /* link up? */
312         unsigned char  link_down_rc;    /* link down reason */
313 };
315 #define FW_LEN16(fw_struct) FW_CMD_LEN16_V(sizeof(fw_struct) / 16)
317 #define ADVERT_MASK (FW_PORT_CAP32_SPEED_V(FW_PORT_CAP32_SPEED_M) | \
318                      FW_PORT_CAP32_ANEG)
320 /* Enable or disable autonegotiation. */
321 #define AUTONEG_DISABLE 0x00
322 #define AUTONEG_ENABLE  0x01
324 struct csio_pport {
325         uint16_t        pcap;
326         uint16_t        acap;
327         uint8_t         portid;
328         uint8_t         link_status;
329         uint16_t        link_speed;
330         uint8_t         mac[6];
331         uint8_t         mod_type;
332         uint8_t         rsvd1;
333         uint8_t         rsvd2;
334         uint8_t         rsvd3;
335         struct link_config link_cfg;
336 };
338 /* fcoe resource information */
339 struct csio_fcoe_res_info {
340         uint16_t        e_d_tov;
341         uint16_t        r_a_tov_seq;
342         uint16_t        r_a_tov_els;
343         uint16_t        r_r_tov;
344         uint32_t        max_xchgs;
345         uint32_t        max_ssns;
346         uint32_t        used_xchgs;
347         uint32_t        used_ssns;
348         uint32_t        max_fcfs;
349         uint32_t        max_vnps;
350         uint32_t        used_fcfs;
351         uint32_t        used_vnps;
352 };
354 /* HW State machine Events */
355 enum csio_hw_ev {
356         CSIO_HWE_CFG = (uint32_t)1, /* Starts off the State machine */
357         CSIO_HWE_INIT,           /* Config done, start Init      */
358         CSIO_HWE_INIT_DONE,      /* Init Mailboxes sent, HW ready */
359         CSIO_HWE_FATAL,          /* Fatal error during initialization */
360         CSIO_HWE_PCIERR_DETECTED,/* PCI error recovery detetced */
361         CSIO_HWE_PCIERR_SLOT_RESET, /* Slot reset after PCI recoviery */
362         CSIO_HWE_PCIERR_RESUME,  /* Resume after PCI error recovery */
363         CSIO_HWE_QUIESCED,       /* HBA quiesced */
364         CSIO_HWE_HBA_RESET,      /* HBA reset requested */
365         CSIO_HWE_HBA_RESET_DONE, /* HBA reset completed */
366         CSIO_HWE_FW_DLOAD,       /* FW download requested */
367         CSIO_HWE_PCI_REMOVE,     /* PCI de-instantiation */
368         CSIO_HWE_SUSPEND,        /* HW suspend for Online(hot) replacement */
369         CSIO_HWE_RESUME,         /* HW resume for Online(hot) replacement */
370         CSIO_HWE_MAX,            /* Max HW event */
371 };
373 /* hw stats */
374 struct csio_hw_stats {
375         uint32_t        n_evt_activeq;  /* Number of event in active Q */
376         uint32_t        n_evt_freeq;    /* Number of event in free Q */
377         uint32_t        n_evt_drop;     /* Number of event droped */
378         uint32_t        n_evt_unexp;    /* Number of unexpected events */
379         uint32_t        n_pcich_offline;/* Number of pci channel offline */
380         uint32_t        n_lnlkup_miss;  /* Number of lnode lookup miss */
381         uint32_t        n_cpl_fw6_msg;  /* Number of cpl fw6 message*/
382         uint32_t        n_cpl_fw6_pld;  /* Number of cpl fw6 payload*/
383         uint32_t        n_cpl_unexp;    /* Number of unexpected cpl */
384         uint32_t        n_mbint_unexp;  /* Number of unexpected mbox */
385                                         /* interrupt */
386         uint32_t        n_plint_unexp;  /* Number of unexpected PL */
387                                         /* interrupt */
388         uint32_t        n_plint_cnt;    /* Number of PL interrupt */
389         uint32_t        n_int_stray;    /* Number of stray interrupt */
390         uint32_t        n_err;          /* Number of hw errors */
391         uint32_t        n_err_fatal;    /* Number of fatal errors */
392         uint32_t        n_err_nomem;    /* Number of memory alloc failure */
393         uint32_t        n_err_io;       /* Number of IO failure */
394         enum csio_hw_ev n_evt_sm[CSIO_HWE_MAX]; /* Number of sm events */
395         uint64_t        n_reset_start;  /* Start time after the reset */
396         uint32_t        rsvd1;
397 };
399 /* Defines for hw->flags */
400 #define CSIO_HWF_MASTER                 0x00000001      /* This is the Master
401                                                          * function for the
402                                                          * card.
403                                                          */
404 #define CSIO_HWF_HW_INTR_ENABLED        0x00000002      /* Are HW Interrupt
405                                                          * enable bit set?
406                                                          */
407 #define CSIO_HWF_FWEVT_PENDING          0x00000004      /* FW events pending */
408 #define CSIO_HWF_Q_MEM_ALLOCED          0x00000008      /* Queues have been
409                                                          * allocated memory.
410                                                          */
411 #define CSIO_HWF_Q_FW_ALLOCED           0x00000010      /* Queues have been
412                                                          * allocated in FW.
413                                                          */
414 #define CSIO_HWF_VPD_VALID              0x00000020      /* Valid VPD copied */
415 #define CSIO_HWF_DEVID_CACHED           0X00000040      /* PCI vendor & device
416                                                          * id cached */
417 #define CSIO_HWF_FWEVT_STOP             0x00000080      /* Stop processing
418                                                          * FW events
419                                                          */
420 #define CSIO_HWF_USING_SOFT_PARAMS      0x00000100      /* Using FW config
421                                                          * params
422                                                          */
423 #define CSIO_HWF_HOST_INTR_ENABLED      0x00000200      /* Are host interrupts
424                                                          * enabled?
425                                                          */
426 #define CSIO_HWF_ROOT_NO_RELAXED_ORDERING 0x00000400    /* Is PCIe relaxed
427                                                          * ordering enabled
428                                                          */
430 #define csio_is_hw_intr_enabled(__hw)   \
431                                 ((__hw)->flags & CSIO_HWF_HW_INTR_ENABLED)
432 #define csio_is_host_intr_enabled(__hw) \
433                                 ((__hw)->flags & CSIO_HWF_HOST_INTR_ENABLED)
434 #define csio_is_hw_master(__hw)         ((__hw)->flags & CSIO_HWF_MASTER)
435 #define csio_is_valid_vpd(__hw)         ((__hw)->flags & CSIO_HWF_VPD_VALID)
436 #define csio_is_dev_id_cached(__hw)     ((__hw)->flags & CSIO_HWF_DEVID_CACHED)
437 #define csio_valid_vpd_copied(__hw)     ((__hw)->flags |= CSIO_HWF_VPD_VALID)
438 #define csio_dev_id_cached(__hw)        ((__hw)->flags |= CSIO_HWF_DEVID_CACHED)
440 /* Defines for intr_mode */
441 enum csio_intr_mode {
442         CSIO_IM_NONE = 0,
443         CSIO_IM_INTX = 1,
444         CSIO_IM_MSI  = 2,
445         CSIO_IM_MSIX = 3,
446 };
448 /* Master HW structure: One per function */
449 struct csio_hw {
450         struct csio_sm          sm;                     /* State machine: should
451                                                          * be the 1st member.
452                                                          */
453         spinlock_t              lock;                   /* Lock for hw */
455         struct csio_scsim       scsim;                  /* SCSI module*/
456         struct csio_wrm         wrm;                    /* Work request module*/
457         struct pci_dev          *pdev;                  /* PCI device */
459         void __iomem            *regstart;              /* Virtual address of
460                                                          * register map
461                                                          */
462         /* SCSI queue sets */
463         uint32_t                num_sqsets;             /* Number of SCSI
464                                                          * queue sets */
465         uint32_t                num_scsi_msix_cpus;     /* Number of CPUs that
466                                                          * will be used
467                                                          * for ingress
468                                                          * processing.
469                                                          */
471         struct csio_scsi_qset   sqset[CSIO_MAX_PPORTS][CSIO_MAX_SCSI_CPU];
472         struct csio_scsi_cpu_info scsi_cpu_info[CSIO_MAX_PPORTS];
474         uint32_t                evtflag;                /* Event flag  */
475         uint32_t                flags;                  /* HW flags */
477         struct csio_mgmtm       mgmtm;                  /* management module */
478         struct csio_mbm         mbm;                    /* Mailbox module */
480         /* Lnodes */
481         uint32_t                num_lns;                /* Number of lnodes */
482         struct csio_lnode       *rln;                   /* Root lnode */
483         struct list_head        sln_head;               /* Sibling node list
484                                                          * list
485                                                          */
486         int                     intr_iq_idx;            /* Forward interrupt
487                                                          * queue.
488                                                          */
489         int                     fwevt_iq_idx;           /* FW evt queue */
490         struct work_struct      evtq_work;              /* Worker thread for
491                                                          * HW events.
492                                                          */
493         struct list_head        evt_free_q;             /* freelist of evt
494                                                          * elements
495                                                          */
496         struct list_head        evt_active_q;           /* active evt queue*/
498         /* board related info */
499         char                    name[32];
500         char                    hw_ver[16];
501         char                    model_desc[32];
502         char                    drv_version[32];
503         char                    fwrev_str[32];
504         uint32_t                optrom_ver;
505         uint32_t                fwrev;
506         uint32_t                tp_vers;
507         char                    chip_ver;
508         uint16_t                chip_id;                /* Tells T4/T5 chip */
509         enum csio_dev_state     fw_state;
510         struct csio_vpd         vpd;
512         uint8_t                 pfn;                    /* Physical Function
513                                                          * number
514                                                          */
515         uint32_t                port_vec;               /* Port vector */
516         uint8_t                 num_pports;             /* Number of physical
517                                                          * ports.
518                                                          */
519         uint8_t                 rst_retries;            /* Reset retries */
520         uint8_t                 cur_evt;                /* current s/m evt */
521         uint8_t                 prev_evt;               /* Previous s/m evt */
522         uint32_t                dev_num;                /* device number */
523         struct csio_pport       pport[CSIO_MAX_PPORTS]; /* Ports (XGMACs) */
524         struct csio_hw_params   params;                 /* Hw parameters */
526         struct dma_pool         *scsi_dma_pool;         /* DMA pool for SCSI */
527         mempool_t               *mb_mempool;            /* Mailbox memory pool*/
528         mempool_t               *rnode_mempool;         /* rnode memory pool */
530         /* Interrupt */
531         enum csio_intr_mode     intr_mode;              /* INTx, MSI, MSIX */
532         uint32_t                fwevt_intr_idx;         /* FW evt MSIX/interrupt
533                                                          * index
534                                                          */
535         uint32_t                nondata_intr_idx;       /* nondata MSIX/intr
536                                                          * idx
537                                                          */
539         uint8_t                 cfg_neq;                /* FW configured no of
540                                                          * egress queues
541                                                          */
542         uint8_t                 cfg_niq;                /* FW configured no of
543                                                          * iq queues.
544                                                          */
546         struct csio_fcoe_res_info  fres_info;           /* Fcoe resource info */
547         struct csio_hw_chip_ops *chip_ops;              /* T4/T5 Chip specific
548                                                          * Operations
549                                                          */
551         /* MSIX vectors */
552         struct csio_msix_entries msix_entries[CSIO_MAX_MSIX_VECS];
554         struct dentry           *debugfs_root;          /* Debug FS */
555         struct csio_hw_stats    stats;                  /* Hw statistics */
556 };
558 /* Register access macros */
559 #define csio_reg(_b, _r)                ((_b) + (_r))
561 #define csio_rd_reg8(_h, _r)            readb(csio_reg((_h)->regstart, (_r)))
562 #define csio_rd_reg16(_h, _r)           readw(csio_reg((_h)->regstart, (_r)))
563 #define csio_rd_reg32(_h, _r)           readl(csio_reg((_h)->regstart, (_r)))
564 #define csio_rd_reg64(_h, _r)           readq(csio_reg((_h)->regstart, (_r)))
566 #define csio_wr_reg8(_h, _v, _r)        writeb((_v), \
567                                                 csio_reg((_h)->regstart, (_r)))
568 #define csio_wr_reg16(_h, _v, _r)       writew((_v), \
569                                                 csio_reg((_h)->regstart, (_r)))
570 #define csio_wr_reg32(_h, _v, _r)       writel((_v), \
571                                                 csio_reg((_h)->regstart, (_r)))
572 #define csio_wr_reg64(_h, _v, _r)       writeq((_v), \
573                                                 csio_reg((_h)->regstart, (_r)))
575 void csio_set_reg_field(struct csio_hw *, uint32_t, uint32_t, uint32_t);
577 /* Core clocks <==> uSecs */
578 static inline uint32_t
579 csio_core_ticks_to_us(struct csio_hw *hw, uint32_t ticks)
581         /* add Core Clock / 2 to round ticks to nearest uS */
582         return (ticks * 1000 + hw->vpd.cclk/2) / hw->vpd.cclk;
585 static inline uint32_t
586 csio_us_to_core_ticks(struct csio_hw *hw, uint32_t us)
588         return (us * hw->vpd.cclk) / 1000;
591 /* Easy access macros */
592 #define csio_hw_to_wrm(hw)              ((struct csio_wrm *)(&(hw)->wrm))
593 #define csio_hw_to_mbm(hw)              ((struct csio_mbm *)(&(hw)->mbm))
594 #define csio_hw_to_scsim(hw)            ((struct csio_scsim *)(&(hw)->scsim))
595 #define csio_hw_to_mgmtm(hw)            ((struct csio_mgmtm *)(&(hw)->mgmtm))
597 #define CSIO_PCI_BUS(hw)                ((hw)->pdev->bus->number)
598 #define CSIO_PCI_DEV(hw)                (PCI_SLOT((hw)->pdev->devfn))
599 #define CSIO_PCI_FUNC(hw)               (PCI_FUNC((hw)->pdev->devfn))
601 #define csio_set_fwevt_intr_idx(_h, _i)         ((_h)->fwevt_intr_idx = (_i))
602 #define csio_get_fwevt_intr_idx(_h)             ((_h)->fwevt_intr_idx)
603 #define csio_set_nondata_intr_idx(_h, _i)       ((_h)->nondata_intr_idx = (_i))
604 #define csio_get_nondata_intr_idx(_h)           ((_h)->nondata_intr_idx)
606 /* Printing/logging */
607 #define CSIO_DEVID(__dev)               ((__dev)->dev_num)
608 #define CSIO_DEVID_LO(__dev)            (CSIO_DEVID((__dev)) & 0xFFFF)
609 #define CSIO_DEVID_HI(__dev)            ((CSIO_DEVID((__dev)) >> 16) & 0xFFFF)
611 #define csio_info(__hw, __fmt, ...)                                     \
612                         dev_info(&(__hw)->pdev->dev, __fmt, ##__VA_ARGS__)
614 #define csio_fatal(__hw, __fmt, ...)                                    \
615                         dev_crit(&(__hw)->pdev->dev, __fmt, ##__VA_ARGS__)
617 #define csio_err(__hw, __fmt, ...)                                      \
618                         dev_err(&(__hw)->pdev->dev, __fmt, ##__VA_ARGS__)
620 #define csio_warn(__hw, __fmt, ...)                                     \
621                         dev_warn(&(__hw)->pdev->dev, __fmt, ##__VA_ARGS__)
623 #ifdef __CSIO_DEBUG__
624 #define csio_dbg(__hw, __fmt, ...)                                      \
625                         csio_info((__hw), __fmt, ##__VA_ARGS__);
626 #else
627 #define csio_dbg(__hw, __fmt, ...)
628 #endif
630 int csio_hw_wait_op_done_val(struct csio_hw *, int, uint32_t, int,
631                              int, int, uint32_t *);
632 void csio_hw_tp_wr_bits_indirect(struct csio_hw *, unsigned int,
633                                  unsigned int, unsigned int);
634 int csio_mgmt_req_lookup(struct csio_mgmtm *, struct csio_ioreq *);
635 void csio_hw_intr_disable(struct csio_hw *);
636 int csio_hw_slow_intr_handler(struct csio_hw *);
637 int csio_handle_intr_status(struct csio_hw *, unsigned int,
638                             const struct intr_info *);
640 fw_port_cap32_t fwcap_to_fwspeed(fw_port_cap32_t acaps);
641 fw_port_cap32_t fwcaps16_to_caps32(fw_port_cap16_t caps16);
642 fw_port_cap16_t fwcaps32_to_caps16(fw_port_cap32_t caps32);
643 fw_port_cap32_t lstatus_to_fwcap(u32 lstatus);
645 int csio_hw_start(struct csio_hw *);
646 int csio_hw_stop(struct csio_hw *);
647 int csio_hw_reset(struct csio_hw *);
648 int csio_is_hw_ready(struct csio_hw *);
649 int csio_is_hw_removing(struct csio_hw *);
651 int csio_fwevtq_handler(struct csio_hw *);
652 void csio_evtq_worker(struct work_struct *);
653 int csio_enqueue_evt(struct csio_hw *, enum csio_evt, void *, uint16_t);
654 void csio_evtq_flush(struct csio_hw *hw);
656 int csio_request_irqs(struct csio_hw *);
657 void csio_intr_enable(struct csio_hw *);
658 void csio_intr_disable(struct csio_hw *, bool);
659 void csio_hw_fatal_err(struct csio_hw *);
661 struct csio_lnode *csio_lnode_alloc(struct csio_hw *);
662 int csio_config_queues(struct csio_hw *);
664 int csio_hw_init(struct csio_hw *);
665 void csio_hw_exit(struct csio_hw *);
666 #endif /* ifndef __CSIO_HW_H__ */