1 // SPDX-License-Identifier: GPL-2.0
2 /*
3 * Copyright (C) 1992 obz under the linux copyright
4 *
5 * Dynamic diacritical handling - aeb@cwi.nl - Dec 1993
6 * Dynamic keymap and string allocation - aeb@cwi.nl - May 1994
7 * Restrict VT switching via ioctl() - grif@cs.ucr.edu - Dec 1995
8 * Some code moved for less code duplication - Andi Kleen - Mar 1997
9 * Check put/get_user, cleanups - acme@conectiva.com.br - Jun 2001
10 */
12 #include <linux/types.h>
13 #include <linux/errno.h>
14 #include <linux/sched/signal.h>
15 #include <linux/tty.h>
16 #include <linux/timer.h>
17 #include <linux/kernel.h>
18 #include <linux/compat.h>
19 #include <linux/module.h>
20 #include <linux/kd.h>
21 #include <linux/vt.h>
22 #include <linux/string.h>
23 #include <linux/slab.h>
24 #include <linux/major.h>
25 #include <linux/fs.h>
26 #include <linux/console.h>
27 #include <linux/consolemap.h>
28 #include <linux/signal.h>
29 #include <linux/suspend.h>
30 #include <linux/timex.h>
32 #include <asm/io.h>
33 #include <linux/uaccess.h>
35 #include <linux/nospec.h>
37 #include <linux/kbd_kern.h>
38 #include <linux/vt_kern.h>
39 #include <linux/kbd_diacr.h>
40 #include <linux/selection.h>
42 char vt_dont_switch;
43 extern struct tty_driver *console_driver;
45 #define VT_IS_IN_USE(i) (console_driver->ttys[i] && console_driver->ttys[i]->count)
46 #define VT_BUSY(i) (VT_IS_IN_USE(i) || i == fg_console || vc_cons[i].d == sel_cons)
48 /*
49 * Console (vt and kd) routines, as defined by USL SVR4 manual, and by
50 * experimentation and study of X386 SYSV handling.
51 *
52 * One point of difference: SYSV vt's are /dev/vtX, which X >= 0, and
53 * /dev/console is a separate ttyp. Under Linux, /dev/tty0 is /dev/console,
54 * and the vc start at /dev/ttyX, X >= 1. We maintain that here, so we will
55 * always treat our set of vt as numbered 1..MAX_NR_CONSOLES (corresponding to
56 * ttys 0..MAX_NR_CONSOLES-1). Explicitly naming VT 0 is illegal, but using
57 * /dev/tty0 (fg_console) as a target is legal, since an implicit aliasing
58 * to the current console is done by the main ioctl code.
59 */
61 #ifdef CONFIG_X86
62 #include <asm/syscalls.h>
63 #endif
65 static void complete_change_console(struct vc_data *vc);
67 /*
68 * User space VT_EVENT handlers
69 */
71 struct vt_event_wait {
72 struct list_head list;
73 struct vt_event event;
74 int done;
75 };
77 static LIST_HEAD(vt_events);
78 static DEFINE_SPINLOCK(vt_event_lock);
79 static DECLARE_WAIT_QUEUE_HEAD(vt_event_waitqueue);
81 /**
82 * vt_event_post
83 * @event: the event that occurred
84 * @old: old console
85 * @new: new console
86 *
87 * Post an VT event to interested VT handlers
88 */
90 void vt_event_post(unsigned int event, unsigned int old, unsigned int new)
91 {
92 struct list_head *pos, *head;
93 unsigned long flags;
94 int wake = 0;
96 spin_lock_irqsave(&vt_event_lock, flags);
97 head = &vt_events;
99 list_for_each(pos, head) {
100 struct vt_event_wait *ve = list_entry(pos,
101 struct vt_event_wait, list);
102 if (!(ve->event.event & event))
103 continue;
104 ve->event.event = event;
105 /* kernel view is consoles 0..n-1, user space view is
106 console 1..n with 0 meaning current, so we must bias */
107 ve->event.oldev = old + 1;
108 ve->event.newev = new + 1;
109 wake = 1;
110 ve->done = 1;
111 }
112 spin_unlock_irqrestore(&vt_event_lock, flags);
113 if (wake)
114 wake_up_interruptible(&vt_event_waitqueue);
115 }
117 static void __vt_event_queue(struct vt_event_wait *vw)
118 {
119 unsigned long flags;
120 /* Prepare the event */
121 INIT_LIST_HEAD(&vw->list);
122 vw->done = 0;
123 /* Queue our event */
124 spin_lock_irqsave(&vt_event_lock, flags);
125 list_add(&vw->list, &vt_events);
126 spin_unlock_irqrestore(&vt_event_lock, flags);
127 }
129 static void __vt_event_wait(struct vt_event_wait *vw)
130 {
131 /* Wait for it to pass */
132 wait_event_interruptible(vt_event_waitqueue, vw->done);
133 }
135 static void __vt_event_dequeue(struct vt_event_wait *vw)
136 {
137 unsigned long flags;
139 /* Dequeue it */
140 spin_lock_irqsave(&vt_event_lock, flags);
141 list_del(&vw->list);
142 spin_unlock_irqrestore(&vt_event_lock, flags);
143 }
145 /**
146 * vt_event_wait - wait for an event
147 * @vw: our event
148 *
149 * Waits for an event to occur which completes our vt_event_wait
150 * structure. On return the structure has wv->done set to 1 for success
151 * or 0 if some event such as a signal ended the wait.
152 */
154 static void vt_event_wait(struct vt_event_wait *vw)
155 {
156 __vt_event_queue(vw);
157 __vt_event_wait(vw);
158 __vt_event_dequeue(vw);
159 }
161 /**
162 * vt_event_wait_ioctl - event ioctl handler
163 * @arg: argument to ioctl
164 *
165 * Implement the VT_WAITEVENT ioctl using the VT event interface
166 */
168 static int vt_event_wait_ioctl(struct vt_event __user *event)
169 {
170 struct vt_event_wait vw;
172 if (copy_from_user(&vw.event, event, sizeof(struct vt_event)))
173 return -EFAULT;
174 /* Highest supported event for now */
175 if (vw.event.event & ~VT_MAX_EVENT)
176 return -EINVAL;
178 vt_event_wait(&vw);
179 /* If it occurred report it */
180 if (vw.done) {
181 if (copy_to_user(event, &vw.event, sizeof(struct vt_event)))
182 return -EFAULT;
183 return 0;
184 }
185 return -EINTR;
186 }
188 /**
189 * vt_waitactive - active console wait
190 * @event: event code
191 * @n: new console
192 *
193 * Helper for event waits. Used to implement the legacy
194 * event waiting ioctls in terms of events
195 */
197 int vt_waitactive(int n)
198 {
199 struct vt_event_wait vw;
200 do {
201 vw.event.event = VT_EVENT_SWITCH;
202 __vt_event_queue(&vw);
203 if (n == fg_console + 1) {
204 __vt_event_dequeue(&vw);
205 break;
206 }
207 __vt_event_wait(&vw);
208 __vt_event_dequeue(&vw);
209 if (vw.done == 0)
210 return -EINTR;
211 } while (vw.event.newev != n);
212 return 0;
213 }
215 /*
216 * these are the valid i/o ports we're allowed to change. they map all the
217 * video ports
218 */
219 #define GPFIRST 0x3b4
220 #define GPLAST 0x3df
221 #define GPNUM (GPLAST - GPFIRST + 1)
225 static inline int
226 do_fontx_ioctl(int cmd, struct consolefontdesc __user *user_cfd, int perm, struct console_font_op *op)
227 {
228 struct consolefontdesc cfdarg;
229 int i;
231 if (copy_from_user(&cfdarg, user_cfd, sizeof(struct consolefontdesc)))
232 return -EFAULT;
234 switch (cmd) {
235 case PIO_FONTX:
236 if (!perm)
237 return -EPERM;
238 op->op = KD_FONT_OP_SET;
239 op->flags = KD_FONT_FLAG_OLD;
240 op->width = 8;
241 op->height = cfdarg.charheight;
242 op->charcount = cfdarg.charcount;
243 op->data = cfdarg.chardata;
244 return con_font_op(vc_cons[fg_console].d, op);
245 case GIO_FONTX: {
246 op->op = KD_FONT_OP_GET;
247 op->flags = KD_FONT_FLAG_OLD;
248 op->width = 8;
249 op->height = cfdarg.charheight;
250 op->charcount = cfdarg.charcount;
251 op->data = cfdarg.chardata;
252 i = con_font_op(vc_cons[fg_console].d, op);
253 if (i)
254 return i;
255 cfdarg.charheight = op->height;
256 cfdarg.charcount = op->charcount;
257 if (copy_to_user(user_cfd, &cfdarg, sizeof(struct consolefontdesc)))
258 return -EFAULT;
259 return 0;
260 }
261 }
262 return -EINVAL;
263 }
265 static inline int
266 do_unimap_ioctl(int cmd, struct unimapdesc __user *user_ud, int perm, struct vc_data *vc)
267 {
268 struct unimapdesc tmp;
270 if (copy_from_user(&tmp, user_ud, sizeof tmp))
271 return -EFAULT;
272 switch (cmd) {
273 case PIO_UNIMAP:
274 if (!perm)
275 return -EPERM;
276 return con_set_unimap(vc, tmp.entry_ct, tmp.entries);
277 case GIO_UNIMAP:
278 if (!perm && fg_console != vc->vc_num)
279 return -EPERM;
280 return con_get_unimap(vc, tmp.entry_ct, &(user_ud->entry_ct), tmp.entries);
281 }
282 return 0;
283 }
285 /* deallocate a single console, if possible (leave 0) */
286 static int vt_disallocate(unsigned int vc_num)
287 {
288 struct vc_data *vc = NULL;
289 int ret = 0;
291 console_lock();
292 if (VT_BUSY(vc_num))
293 ret = -EBUSY;
294 else if (vc_num)
295 vc = vc_deallocate(vc_num);
296 console_unlock();
298 if (vc && vc_num >= MIN_NR_CONSOLES) {
299 tty_port_destroy(&vc->port);
300 kfree(vc);
301 }
303 return ret;
304 }
306 /* deallocate all unused consoles, but leave 0 */
307 static void vt_disallocate_all(void)
308 {
309 struct vc_data *vc[MAX_NR_CONSOLES];
310 int i;
312 console_lock();
313 for (i = 1; i < MAX_NR_CONSOLES; i++)
314 if (!VT_BUSY(i))
315 vc[i] = vc_deallocate(i);
316 else
317 vc[i] = NULL;
318 console_unlock();
320 for (i = 1; i < MAX_NR_CONSOLES; i++) {
321 if (vc[i] && i >= MIN_NR_CONSOLES) {
322 tty_port_destroy(&vc[i]->port);
323 kfree(vc[i]);
324 }
325 }
326 }
329 /*
330 * We handle the console-specific ioctl's here. We allow the
331 * capability to modify any console, not just the fg_console.
332 */
333 int vt_ioctl(struct tty_struct *tty,
334 unsigned int cmd, unsigned long arg)
335 {
336 struct vc_data *vc = tty->driver_data;
337 struct console_font_op op; /* used in multiple places here */
338 unsigned int console;
339 unsigned char ucval;
340 unsigned int uival;
341 void __user *up = (void __user *)arg;
342 int i, perm;
343 int ret = 0;
345 console = vc->vc_num;
348 if (!vc_cons_allocated(console)) { /* impossible? */
349 ret = -ENOIOCTLCMD;
350 goto out;
351 }
354 /*
355 * To have permissions to do most of the vt ioctls, we either have
356 * to be the owner of the tty, or have CAP_SYS_TTY_CONFIG.
357 */
358 perm = 0;
359 if (current->signal->tty == tty || capable(CAP_SYS_TTY_CONFIG))
360 perm = 1;
362 switch (cmd) {
363 case TIOCLINUX:
364 ret = tioclinux(tty, arg);
365 break;
366 case KIOCSOUND:
367 if (!perm)
368 return -EPERM;
369 /*
370 * The use of PIT_TICK_RATE is historic, it used to be
371 * the platform-dependent CLOCK_TICK_RATE between 2.6.12
372 * and 2.6.36, which was a minor but unfortunate ABI
373 * change. kd_mksound is locked by the input layer.
374 */
375 if (arg)
376 arg = PIT_TICK_RATE / arg;
377 kd_mksound(arg, 0);
378 break;
380 case KDMKTONE:
381 if (!perm)
382 return -EPERM;
383 {
384 unsigned int ticks, count;
386 /*
387 * Generate the tone for the appropriate number of ticks.
388 * If the time is zero, turn off sound ourselves.
389 */
390 ticks = msecs_to_jiffies((arg >> 16) & 0xffff);
391 count = ticks ? (arg & 0xffff) : 0;
392 if (count)
393 count = PIT_TICK_RATE / count;
394 kd_mksound(count, ticks);
395 break;
396 }
398 case KDGKBTYPE:
399 /*
400 * this is naïve.
401 */
402 ucval = KB_101;
403 ret = put_user(ucval, (char __user *)arg);
404 break;
406 /*
407 * These cannot be implemented on any machine that implements
408 * ioperm() in user level (such as Alpha PCs) or not at all.
409 *
410 * XXX: you should never use these, just call ioperm directly..
411 */
412 #ifdef CONFIG_X86
413 case KDADDIO:
414 case KDDELIO:
415 /*
416 * KDADDIO and KDDELIO may be able to add ports beyond what
417 * we reject here, but to be safe...
418 *
419 * These are locked internally via sys_ioperm
420 */
421 if (arg < GPFIRST || arg > GPLAST) {
422 ret = -EINVAL;
423 break;
424 }
425 ret = ksys_ioperm(arg, 1, (cmd == KDADDIO)) ? -ENXIO : 0;
426 break;
428 case KDENABIO:
429 case KDDISABIO:
430 ret = ksys_ioperm(GPFIRST, GPNUM,
431 (cmd == KDENABIO)) ? -ENXIO : 0;
432 break;
433 #endif
435 /* Linux m68k/i386 interface for setting the keyboard delay/repeat rate */
437 case KDKBDREP:
438 {
439 struct kbd_repeat kbrep;
441 if (!capable(CAP_SYS_TTY_CONFIG))
442 return -EPERM;
444 if (copy_from_user(&kbrep, up, sizeof(struct kbd_repeat))) {
445 ret = -EFAULT;
446 break;
447 }
448 ret = kbd_rate(&kbrep);
449 if (ret)
450 break;
451 if (copy_to_user(up, &kbrep, sizeof(struct kbd_repeat)))
452 ret = -EFAULT;
453 break;
454 }
456 case KDSETMODE:
457 /*
458 * currently, setting the mode from KD_TEXT to KD_GRAPHICS
459 * doesn't do a whole lot. i'm not sure if it should do any
460 * restoration of modes or what...
461 *
462 * XXX It should at least call into the driver, fbdev's definitely
463 * need to restore their engine state. --BenH
464 */
465 if (!perm)
466 return -EPERM;
467 switch (arg) {
468 case KD_GRAPHICS:
469 break;
470 case KD_TEXT0:
471 case KD_TEXT1:
472 arg = KD_TEXT;
473 case KD_TEXT:
474 break;
475 default:
476 ret = -EINVAL;
477 goto out;
478 }
479 /* FIXME: this needs the console lock extending */
480 if (vc->vc_mode == (unsigned char) arg)
481 break;
482 vc->vc_mode = (unsigned char) arg;
483 if (console != fg_console)
484 break;
485 /*
486 * explicitly blank/unblank the screen if switching modes
487 */
488 console_lock();
489 if (arg == KD_TEXT)
490 do_unblank_screen(1);
491 else
492 do_blank_screen(1);
493 console_unlock();
494 break;
496 case KDGETMODE:
497 uival = vc->vc_mode;
498 goto setint;
500 case KDMAPDISP:
501 case KDUNMAPDISP:
502 /*
503 * these work like a combination of mmap and KDENABIO.
504 * this could be easily finished.
505 */
506 ret = -EINVAL;
507 break;
509 case KDSKBMODE:
510 if (!perm)
511 return -EPERM;
512 ret = vt_do_kdskbmode(console, arg);
513 if (ret == 0)
514 tty_ldisc_flush(tty);
515 break;
517 case KDGKBMODE:
518 uival = vt_do_kdgkbmode(console);
519 ret = put_user(uival, (int __user *)arg);
520 break;
522 /* this could be folded into KDSKBMODE, but for compatibility
523 reasons it is not so easy to fold KDGKBMETA into KDGKBMODE */
524 case KDSKBMETA:
525 ret = vt_do_kdskbmeta(console, arg);
526 break;
528 case KDGKBMETA:
529 /* FIXME: should review whether this is worth locking */
530 uival = vt_do_kdgkbmeta(console);
531 setint:
532 ret = put_user(uival, (int __user *)arg);
533 break;
535 case KDGETKEYCODE:
536 case KDSETKEYCODE:
537 if(!capable(CAP_SYS_TTY_CONFIG))
538 perm = 0;
539 ret = vt_do_kbkeycode_ioctl(cmd, up, perm);
540 break;
542 case KDGKBENT:
543 case KDSKBENT:
544 ret = vt_do_kdsk_ioctl(cmd, up, perm, console);
545 break;
547 case KDGKBSENT:
548 case KDSKBSENT:
549 ret = vt_do_kdgkb_ioctl(cmd, up, perm);
550 break;
552 /* Diacritical processing. Handled in keyboard.c as it has
553 to operate on the keyboard locks and structures */
554 case KDGKBDIACR:
555 case KDGKBDIACRUC:
556 case KDSKBDIACR:
557 case KDSKBDIACRUC:
558 ret = vt_do_diacrit(cmd, up, perm);
559 break;
561 /* the ioctls below read/set the flags usually shown in the leds */
562 /* don't use them - they will go away without warning */
563 case KDGKBLED:
564 case KDSKBLED:
565 case KDGETLED:
566 case KDSETLED:
567 ret = vt_do_kdskled(console, cmd, arg, perm);
568 break;
570 /*
571 * A process can indicate its willingness to accept signals
572 * generated by pressing an appropriate key combination.
573 * Thus, one can have a daemon that e.g. spawns a new console
574 * upon a keypress and then changes to it.
575 * See also the kbrequest field of inittab(5).
576 */
577 case KDSIGACCEPT:
578 {
579 if (!perm || !capable(CAP_KILL))
580 return -EPERM;
581 if (!valid_signal(arg) || arg < 1 || arg == SIGKILL)
582 ret = -EINVAL;
583 else {
584 spin_lock_irq(&vt_spawn_con.lock);
585 put_pid(vt_spawn_con.pid);
586 vt_spawn_con.pid = get_pid(task_pid(current));
587 vt_spawn_con.sig = arg;
588 spin_unlock_irq(&vt_spawn_con.lock);
589 }
590 break;
591 }
593 case VT_SETMODE:
594 {
595 struct vt_mode tmp;
597 if (!perm)
598 return -EPERM;
599 if (copy_from_user(&tmp, up, sizeof(struct vt_mode))) {
600 ret = -EFAULT;
601 goto out;
602 }
603 if (tmp.mode != VT_AUTO && tmp.mode != VT_PROCESS) {
604 ret = -EINVAL;
605 goto out;
606 }
607 console_lock();
608 vc->vt_mode = tmp;
609 /* the frsig is ignored, so we set it to 0 */
610 vc->vt_mode.frsig = 0;
611 put_pid(vc->vt_pid);
612 vc->vt_pid = get_pid(task_pid(current));
613 /* no switch is required -- saw@shade.msu.ru */
614 vc->vt_newvt = -1;
615 console_unlock();
616 break;
617 }
619 case VT_GETMODE:
620 {
621 struct vt_mode tmp;
622 int rc;
624 console_lock();
625 memcpy(&tmp, &vc->vt_mode, sizeof(struct vt_mode));
626 console_unlock();
628 rc = copy_to_user(up, &tmp, sizeof(struct vt_mode));
629 if (rc)
630 ret = -EFAULT;
631 break;
632 }
634 /*
635 * Returns global vt state. Note that VT 0 is always open, since
636 * it's an alias for the current VT, and people can't use it here.
637 * We cannot return state for more than 16 VTs, since v_state is short.
638 */
639 case VT_GETSTATE:
640 {
641 struct vt_stat __user *vtstat = up;
642 unsigned short state, mask;
644 /* Review: FIXME: Console lock ? */
645 if (put_user(fg_console + 1, &vtstat->v_active))
646 ret = -EFAULT;
647 else {
648 state = 1; /* /dev/tty0 is always open */
649 for (i = 0, mask = 2; i < MAX_NR_CONSOLES && mask;
650 ++i, mask <<= 1)
651 if (VT_IS_IN_USE(i))
652 state |= mask;
653 ret = put_user(state, &vtstat->v_state);
654 }
655 break;
656 }
658 /*
659 * Returns the first available (non-opened) console.
660 */
661 case VT_OPENQRY:
662 /* FIXME: locking ? - but then this is a stupid API */
663 for (i = 0; i < MAX_NR_CONSOLES; ++i)
664 if (! VT_IS_IN_USE(i))
665 break;
666 uival = i < MAX_NR_CONSOLES ? (i+1) : -1;
667 goto setint;
669 /*
670 * ioctl(fd, VT_ACTIVATE, num) will cause us to switch to vt # num,
671 * with num >= 1 (switches to vt 0, our console, are not allowed, just
672 * to preserve sanity).
673 */
674 case VT_ACTIVATE:
675 if (!perm)
676 return -EPERM;
677 if (arg == 0 || arg > MAX_NR_CONSOLES)
678 ret = -ENXIO;
679 else {
680 arg--;
681 console_lock();
682 ret = vc_allocate(arg);
683 console_unlock();
684 if (ret)
685 break;
686 set_console(arg);
687 }
688 break;
690 case VT_SETACTIVATE:
691 {
692 struct vt_setactivate vsa;
694 if (!perm)
695 return -EPERM;
697 if (copy_from_user(&vsa, (struct vt_setactivate __user *)arg,
698 sizeof(struct vt_setactivate))) {
699 ret = -EFAULT;
700 goto out;
701 }
702 if (vsa.console == 0 || vsa.console > MAX_NR_CONSOLES)
703 ret = -ENXIO;
704 else {
705 vsa.console = array_index_nospec(vsa.console,
706 MAX_NR_CONSOLES + 1);
707 vsa.console--;
708 console_lock();
709 ret = vc_allocate(vsa.console);
710 if (ret == 0) {
711 struct vc_data *nvc;
712 /* This is safe providing we don't drop the
713 console sem between vc_allocate and
714 finishing referencing nvc */
715 nvc = vc_cons[vsa.console].d;
716 nvc->vt_mode = vsa.mode;
717 nvc->vt_mode.frsig = 0;
718 put_pid(nvc->vt_pid);
719 nvc->vt_pid = get_pid(task_pid(current));
720 }
721 console_unlock();
722 if (ret)
723 break;
724 /* Commence switch and lock */
725 /* Review set_console locks */
726 set_console(vsa.console);
727 }
728 break;
729 }
731 /*
732 * wait until the specified VT has been activated
733 */
734 case VT_WAITACTIVE:
735 if (!perm)
736 return -EPERM;
737 if (arg == 0 || arg > MAX_NR_CONSOLES)
738 ret = -ENXIO;
739 else
740 ret = vt_waitactive(arg);
741 break;
743 /*
744 * If a vt is under process control, the kernel will not switch to it
745 * immediately, but postpone the operation until the process calls this
746 * ioctl, allowing the switch to complete.
747 *
748 * According to the X sources this is the behavior:
749 * 0: pending switch-from not OK
750 * 1: pending switch-from OK
751 * 2: completed switch-to OK
752 */
753 case VT_RELDISP:
754 if (!perm)
755 return -EPERM;
757 console_lock();
758 if (vc->vt_mode.mode != VT_PROCESS) {
759 console_unlock();
760 ret = -EINVAL;
761 break;
762 }
763 /*
764 * Switching-from response
765 */
766 if (vc->vt_newvt >= 0) {
767 if (arg == 0)
768 /*
769 * Switch disallowed, so forget we were trying
770 * to do it.
771 */
772 vc->vt_newvt = -1;
774 else {
775 /*
776 * The current vt has been released, so
777 * complete the switch.
778 */
779 int newvt;
780 newvt = vc->vt_newvt;
781 vc->vt_newvt = -1;
782 ret = vc_allocate(newvt);
783 if (ret) {
784 console_unlock();
785 break;
786 }
787 /*
788 * When we actually do the console switch,
789 * make sure we are atomic with respect to
790 * other console switches..
791 */
792 complete_change_console(vc_cons[newvt].d);
793 }
794 } else {
795 /*
796 * Switched-to response
797 */
798 /*
799 * If it's just an ACK, ignore it
800 */
801 if (arg != VT_ACKACQ)
802 ret = -EINVAL;
803 }
804 console_unlock();
805 break;
807 /*
808 * Disallocate memory associated to VT (but leave VT1)
809 */
810 case VT_DISALLOCATE:
811 if (arg > MAX_NR_CONSOLES) {
812 ret = -ENXIO;
813 break;
814 }
815 if (arg == 0)
816 vt_disallocate_all();
817 else
818 ret = vt_disallocate(--arg);
819 break;
821 case VT_RESIZE:
822 {
823 struct vt_sizes __user *vtsizes = up;
824 struct vc_data *vc;
826 ushort ll,cc;
827 if (!perm)
828 return -EPERM;
829 if (get_user(ll, &vtsizes->v_rows) ||
830 get_user(cc, &vtsizes->v_cols))
831 ret = -EFAULT;
832 else {
833 console_lock();
834 for (i = 0; i < MAX_NR_CONSOLES; i++) {
835 vc = vc_cons[i].d;
837 if (vc) {
838 vc->vc_resize_user = 1;
839 /* FIXME: review v tty lock */
840 vc_resize(vc_cons[i].d, cc, ll);
841 }
842 }
843 console_unlock();
844 }
845 break;
846 }
848 case VT_RESIZEX:
849 {
850 struct vt_consize v;
851 if (!perm)
852 return -EPERM;
853 if (copy_from_user(&v, up, sizeof(struct vt_consize)))
854 return -EFAULT;
855 /* FIXME: Should check the copies properly */
856 if (!v.v_vlin)
857 v.v_vlin = vc->vc_scan_lines;
858 if (v.v_clin) {
859 int rows = v.v_vlin/v.v_clin;
860 if (v.v_rows != rows) {
861 if (v.v_rows) /* Parameters don't add up */
862 return -EINVAL;
863 v.v_rows = rows;
864 }
865 }
866 if (v.v_vcol && v.v_ccol) {
867 int cols = v.v_vcol/v.v_ccol;
868 if (v.v_cols != cols) {
869 if (v.v_cols)
870 return -EINVAL;
871 v.v_cols = cols;
872 }
873 }
875 if (v.v_clin > 32)
876 return -EINVAL;
878 for (i = 0; i < MAX_NR_CONSOLES; i++) {
879 if (!vc_cons[i].d)
880 continue;
881 console_lock();
882 if (v.v_vlin)
883 vc_cons[i].d->vc_scan_lines = v.v_vlin;
884 if (v.v_clin)
885 vc_cons[i].d->vc_font.height = v.v_clin;
886 vc_cons[i].d->vc_resize_user = 1;
887 vc_resize(vc_cons[i].d, v.v_cols, v.v_rows);
888 console_unlock();
889 }
890 break;
891 }
893 case PIO_FONT: {
894 if (!perm)
895 return -EPERM;
896 op.op = KD_FONT_OP_SET;
897 op.flags = KD_FONT_FLAG_OLD | KD_FONT_FLAG_DONT_RECALC; /* Compatibility */
898 op.width = 8;
899 op.height = 0;
900 op.charcount = 256;
901 op.data = up;
902 ret = con_font_op(vc_cons[fg_console].d, &op);
903 break;
904 }
906 case GIO_FONT: {
907 op.op = KD_FONT_OP_GET;
908 op.flags = KD_FONT_FLAG_OLD;
909 op.width = 8;
910 op.height = 32;
911 op.charcount = 256;
912 op.data = up;
913 ret = con_font_op(vc_cons[fg_console].d, &op);
914 break;
915 }
917 case PIO_CMAP:
918 if (!perm)
919 ret = -EPERM;
920 else
921 ret = con_set_cmap(up);
922 break;
924 case GIO_CMAP:
925 ret = con_get_cmap(up);
926 break;
928 case PIO_FONTX:
929 case GIO_FONTX:
930 ret = do_fontx_ioctl(cmd, up, perm, &op);
931 break;
933 case PIO_FONTRESET:
934 {
935 if (!perm)
936 return -EPERM;
938 #ifdef BROKEN_GRAPHICS_PROGRAMS
939 /* With BROKEN_GRAPHICS_PROGRAMS defined, the default
940 font is not saved. */
941 ret = -ENOSYS;
942 break;
943 #else
944 {
945 op.op = KD_FONT_OP_SET_DEFAULT;
946 op.data = NULL;
947 ret = con_font_op(vc_cons[fg_console].d, &op);
948 if (ret)
949 break;
950 console_lock();
951 con_set_default_unimap(vc_cons[fg_console].d);
952 console_unlock();
953 break;
954 }
955 #endif
956 }
958 case KDFONTOP: {
959 if (copy_from_user(&op, up, sizeof(op))) {
960 ret = -EFAULT;
961 break;
962 }
963 if (!perm && op.op != KD_FONT_OP_GET)
964 return -EPERM;
965 ret = con_font_op(vc, &op);
966 if (ret)
967 break;
968 if (copy_to_user(up, &op, sizeof(op)))
969 ret = -EFAULT;
970 break;
971 }
973 case PIO_SCRNMAP:
974 if (!perm)
975 ret = -EPERM;
976 else
977 ret = con_set_trans_old(up);
978 break;
980 case GIO_SCRNMAP:
981 ret = con_get_trans_old(up);
982 break;
984 case PIO_UNISCRNMAP:
985 if (!perm)
986 ret = -EPERM;
987 else
988 ret = con_set_trans_new(up);
989 break;
991 case GIO_UNISCRNMAP:
992 ret = con_get_trans_new(up);
993 break;
995 case PIO_UNIMAPCLR:
996 if (!perm)
997 return -EPERM;
998 con_clear_unimap(vc);
999 break;
1001 case PIO_UNIMAP:
1002 case GIO_UNIMAP:
1003 ret = do_unimap_ioctl(cmd, up, perm, vc);
1004 break;
1006 case VT_LOCKSWITCH:
1007 if (!capable(CAP_SYS_TTY_CONFIG))
1008 return -EPERM;
1009 vt_dont_switch = 1;
1010 break;
1011 case VT_UNLOCKSWITCH:
1012 if (!capable(CAP_SYS_TTY_CONFIG))
1013 return -EPERM;
1014 vt_dont_switch = 0;
1015 break;
1016 case VT_GETHIFONTMASK:
1017 ret = put_user(vc->vc_hi_font_mask,
1018 (unsigned short __user *)arg);
1019 break;
1020 case VT_WAITEVENT:
1021 ret = vt_event_wait_ioctl((struct vt_event __user *)arg);
1022 break;
1023 default:
1024 ret = -ENOIOCTLCMD;
1025 }
1026 out:
1027 return ret;
1028 }
1030 void reset_vc(struct vc_data *vc)
1031 {
1032 vc->vc_mode = KD_TEXT;
1033 vt_reset_unicode(vc->vc_num);
1034 vc->vt_mode.mode = VT_AUTO;
1035 vc->vt_mode.waitv = 0;
1036 vc->vt_mode.relsig = 0;
1037 vc->vt_mode.acqsig = 0;
1038 vc->vt_mode.frsig = 0;
1039 put_pid(vc->vt_pid);
1040 vc->vt_pid = NULL;
1041 vc->vt_newvt = -1;
1042 if (!in_interrupt()) /* Via keyboard.c:SAK() - akpm */
1043 reset_palette(vc);
1044 }
1046 void vc_SAK(struct work_struct *work)
1047 {
1048 struct vc *vc_con =
1049 container_of(work, struct vc, SAK_work);
1050 struct vc_data *vc;
1051 struct tty_struct *tty;
1053 console_lock();
1054 vc = vc_con->d;
1055 if (vc) {
1056 /* FIXME: review tty ref counting */
1057 tty = vc->port.tty;
1058 /*
1059 * SAK should also work in all raw modes and reset
1060 * them properly.
1061 */
1062 if (tty)
1063 __do_SAK(tty);
1064 reset_vc(vc);
1065 }
1066 console_unlock();
1067 }
1069 #ifdef CONFIG_COMPAT
1071 struct compat_consolefontdesc {
1072 unsigned short charcount; /* characters in font (256 or 512) */
1073 unsigned short charheight; /* scan lines per character (1-32) */
1074 compat_caddr_t chardata; /* font data in expanded form */
1075 };
1077 static inline int
1078 compat_fontx_ioctl(int cmd, struct compat_consolefontdesc __user *user_cfd,
1079 int perm, struct console_font_op *op)
1080 {
1081 struct compat_consolefontdesc cfdarg;
1082 int i;
1084 if (copy_from_user(&cfdarg, user_cfd, sizeof(struct compat_consolefontdesc)))
1085 return -EFAULT;
1087 switch (cmd) {
1088 case PIO_FONTX:
1089 if (!perm)
1090 return -EPERM;
1091 op->op = KD_FONT_OP_SET;
1092 op->flags = KD_FONT_FLAG_OLD;
1093 op->width = 8;
1094 op->height = cfdarg.charheight;
1095 op->charcount = cfdarg.charcount;
1096 op->data = compat_ptr(cfdarg.chardata);
1097 return con_font_op(vc_cons[fg_console].d, op);
1098 case GIO_FONTX:
1099 op->op = KD_FONT_OP_GET;
1100 op->flags = KD_FONT_FLAG_OLD;
1101 op->width = 8;
1102 op->height = cfdarg.charheight;
1103 op->charcount = cfdarg.charcount;
1104 op->data = compat_ptr(cfdarg.chardata);
1105 i = con_font_op(vc_cons[fg_console].d, op);
1106 if (i)
1107 return i;
1108 cfdarg.charheight = op->height;
1109 cfdarg.charcount = op->charcount;
1110 if (copy_to_user(user_cfd, &cfdarg, sizeof(struct compat_consolefontdesc)))
1111 return -EFAULT;
1112 return 0;
1113 }
1114 return -EINVAL;
1115 }
1117 struct compat_console_font_op {
1118 compat_uint_t op; /* operation code KD_FONT_OP_* */
1119 compat_uint_t flags; /* KD_FONT_FLAG_* */
1120 compat_uint_t width, height; /* font size */
1121 compat_uint_t charcount;
1122 compat_caddr_t data; /* font data with height fixed to 32 */
1123 };
1125 static inline int
1126 compat_kdfontop_ioctl(struct compat_console_font_op __user *fontop,
1127 int perm, struct console_font_op *op, struct vc_data *vc)
1128 {
1129 int i;
1131 if (copy_from_user(op, fontop, sizeof(struct compat_console_font_op)))
1132 return -EFAULT;
1133 if (!perm && op->op != KD_FONT_OP_GET)
1134 return -EPERM;
1135 op->data = compat_ptr(((struct compat_console_font_op *)op)->data);
1136 i = con_font_op(vc, op);
1137 if (i)
1138 return i;
1139 ((struct compat_console_font_op *)op)->data = (unsigned long)op->data;
1140 if (copy_to_user(fontop, op, sizeof(struct compat_console_font_op)))
1141 return -EFAULT;
1142 return 0;
1143 }
1145 struct compat_unimapdesc {
1146 unsigned short entry_ct;
1147 compat_caddr_t entries;
1148 };
1150 static inline int
1151 compat_unimap_ioctl(unsigned int cmd, struct compat_unimapdesc __user *user_ud,
1152 int perm, struct vc_data *vc)
1153 {
1154 struct compat_unimapdesc tmp;
1155 struct unipair __user *tmp_entries;
1157 if (copy_from_user(&tmp, user_ud, sizeof tmp))
1158 return -EFAULT;
1159 tmp_entries = compat_ptr(tmp.entries);
1160 switch (cmd) {
1161 case PIO_UNIMAP:
1162 if (!perm)
1163 return -EPERM;
1164 return con_set_unimap(vc, tmp.entry_ct, tmp_entries);
1165 case GIO_UNIMAP:
1166 if (!perm && fg_console != vc->vc_num)
1167 return -EPERM;
1168 return con_get_unimap(vc, tmp.entry_ct, &(user_ud->entry_ct), tmp_entries);
1169 }
1170 return 0;
1171 }
1173 long vt_compat_ioctl(struct tty_struct *tty,
1174 unsigned int cmd, unsigned long arg)
1175 {
1176 struct vc_data *vc = tty->driver_data;
1177 struct console_font_op op; /* used in multiple places here */
1178 unsigned int console;
1179 void __user *up = (void __user *)arg;
1180 int perm;
1181 int ret = 0;
1183 console = vc->vc_num;
1185 if (!vc_cons_allocated(console)) { /* impossible? */
1186 ret = -ENOIOCTLCMD;
1187 goto out;
1188 }
1190 /*
1191 * To have permissions to do most of the vt ioctls, we either have
1192 * to be the owner of the tty, or have CAP_SYS_TTY_CONFIG.
1193 */
1194 perm = 0;
1195 if (current->signal->tty == tty || capable(CAP_SYS_TTY_CONFIG))
1196 perm = 1;
1198 switch (cmd) {
1199 /*
1200 * these need special handlers for incompatible data structures
1201 */
1202 case PIO_FONTX:
1203 case GIO_FONTX:
1204 ret = compat_fontx_ioctl(cmd, up, perm, &op);
1205 break;
1207 case KDFONTOP:
1208 ret = compat_kdfontop_ioctl(up, perm, &op, vc);
1209 break;
1211 case PIO_UNIMAP:
1212 case GIO_UNIMAP:
1213 ret = compat_unimap_ioctl(cmd, up, perm, vc);
1214 break;
1216 /*
1217 * all these treat 'arg' as an integer
1218 */
1219 case KIOCSOUND:
1220 case KDMKTONE:
1221 #ifdef CONFIG_X86
1222 case KDADDIO:
1223 case KDDELIO:
1224 #endif
1225 case KDSETMODE:
1226 case KDMAPDISP:
1227 case KDUNMAPDISP:
1228 case KDSKBMODE:
1229 case KDSKBMETA:
1230 case KDSKBLED:
1231 case KDSETLED:
1232 case KDSIGACCEPT:
1233 case VT_ACTIVATE:
1234 case VT_WAITACTIVE:
1235 case VT_RELDISP:
1236 case VT_DISALLOCATE:
1237 case VT_RESIZE:
1238 case VT_RESIZEX:
1239 goto fallback;
1241 /*
1242 * the rest has a compatible data structure behind arg,
1243 * but we have to convert it to a proper 64 bit pointer.
1244 */
1245 default:
1246 arg = (unsigned long)compat_ptr(arg);
1247 goto fallback;
1248 }
1249 out:
1250 return ret;
1252 fallback:
1253 return vt_ioctl(tty, cmd, arg);
1254 }
1257 #endif /* CONFIG_COMPAT */
1260 /*
1261 * Performs the back end of a vt switch. Called under the console
1262 * semaphore.
1263 */
1264 static void complete_change_console(struct vc_data *vc)
1265 {
1266 unsigned char old_vc_mode;
1267 int old = fg_console;
1269 last_console = fg_console;
1271 /*
1272 * If we're switching, we could be going from KD_GRAPHICS to
1273 * KD_TEXT mode or vice versa, which means we need to blank or
1274 * unblank the screen later.
1275 */
1276 old_vc_mode = vc_cons[fg_console].d->vc_mode;
1277 switch_screen(vc);
1279 /*
1280 * This can't appear below a successful kill_pid(). If it did,
1281 * then the *blank_screen operation could occur while X, having
1282 * received acqsig, is waking up on another processor. This
1283 * condition can lead to overlapping accesses to the VGA range
1284 * and the framebuffer (causing system lockups).
1285 *
1286 * To account for this we duplicate this code below only if the
1287 * controlling process is gone and we've called reset_vc.
1288 */
1289 if (old_vc_mode != vc->vc_mode) {
1290 if (vc->vc_mode == KD_TEXT)
1291 do_unblank_screen(1);
1292 else
1293 do_blank_screen(1);
1294 }
1296 /*
1297 * If this new console is under process control, send it a signal
1298 * telling it that it has acquired. Also check if it has died and
1299 * clean up (similar to logic employed in change_console())
1300 */
1301 if (vc->vt_mode.mode == VT_PROCESS) {
1302 /*
1303 * Send the signal as privileged - kill_pid() will
1304 * tell us if the process has gone or something else
1305 * is awry
1306 */
1307 if (kill_pid(vc->vt_pid, vc->vt_mode.acqsig, 1) != 0) {
1308 /*
1309 * The controlling process has died, so we revert back to
1310 * normal operation. In this case, we'll also change back
1311 * to KD_TEXT mode. I'm not sure if this is strictly correct
1312 * but it saves the agony when the X server dies and the screen
1313 * remains blanked due to KD_GRAPHICS! It would be nice to do
1314 * this outside of VT_PROCESS but there is no single process
1315 * to account for and tracking tty count may be undesirable.
1316 */
1317 reset_vc(vc);
1319 if (old_vc_mode != vc->vc_mode) {
1320 if (vc->vc_mode == KD_TEXT)
1321 do_unblank_screen(1);
1322 else
1323 do_blank_screen(1);
1324 }
1325 }
1326 }
1328 /*
1329 * Wake anyone waiting for their VT to activate
1330 */
1331 vt_event_post(VT_EVENT_SWITCH, old, vc->vc_num);
1332 return;
1333 }
1335 /*
1336 * Performs the front-end of a vt switch
1337 */
1338 void change_console(struct vc_data *new_vc)
1339 {
1340 struct vc_data *vc;
1342 if (!new_vc || new_vc->vc_num == fg_console || vt_dont_switch)
1343 return;
1345 /*
1346 * If this vt is in process mode, then we need to handshake with
1347 * that process before switching. Essentially, we store where that
1348 * vt wants to switch to and wait for it to tell us when it's done
1349 * (via VT_RELDISP ioctl).
1350 *
1351 * We also check to see if the controlling process still exists.
1352 * If it doesn't, we reset this vt to auto mode and continue.
1353 * This is a cheap way to track process control. The worst thing
1354 * that can happen is: we send a signal to a process, it dies, and
1355 * the switch gets "lost" waiting for a response; hopefully, the
1356 * user will try again, we'll detect the process is gone (unless
1357 * the user waits just the right amount of time :-) and revert the
1358 * vt to auto control.
1359 */
1360 vc = vc_cons[fg_console].d;
1361 if (vc->vt_mode.mode == VT_PROCESS) {
1362 /*
1363 * Send the signal as privileged - kill_pid() will
1364 * tell us if the process has gone or something else
1365 * is awry.
1366 *
1367 * We need to set vt_newvt *before* sending the signal or we
1368 * have a race.
1369 */
1370 vc->vt_newvt = new_vc->vc_num;
1371 if (kill_pid(vc->vt_pid, vc->vt_mode.relsig, 1) == 0) {
1372 /*
1373 * It worked. Mark the vt to switch to and
1374 * return. The process needs to send us a
1375 * VT_RELDISP ioctl to complete the switch.
1376 */
1377 return;
1378 }
1380 /*
1381 * The controlling process has died, so we revert back to
1382 * normal operation. In this case, we'll also change back
1383 * to KD_TEXT mode. I'm not sure if this is strictly correct
1384 * but it saves the agony when the X server dies and the screen
1385 * remains blanked due to KD_GRAPHICS! It would be nice to do
1386 * this outside of VT_PROCESS but there is no single process
1387 * to account for and tracking tty count may be undesirable.
1388 */
1389 reset_vc(vc);
1391 /*
1392 * Fall through to normal (VT_AUTO) handling of the switch...
1393 */
1394 }
1396 /*
1397 * Ignore all switches in KD_GRAPHICS+VT_AUTO mode
1398 */
1399 if (vc->vc_mode == KD_GRAPHICS)
1400 return;
1402 complete_change_console(new_vc);
1403 }
1405 /* Perform a kernel triggered VT switch for suspend/resume */
1407 static int disable_vt_switch;
1409 int vt_move_to_console(unsigned int vt, int alloc)
1410 {
1411 int prev;
1413 console_lock();
1414 /* Graphics mode - up to X */
1415 if (disable_vt_switch) {
1416 console_unlock();
1417 return 0;
1418 }
1419 prev = fg_console;
1421 if (alloc && vc_allocate(vt)) {
1422 /* we can't have a free VC for now. Too bad,
1423 * we don't want to mess the screen for now. */
1424 console_unlock();
1425 return -ENOSPC;
1426 }
1428 if (set_console(vt)) {
1429 /*
1430 * We're unable to switch to the SUSPEND_CONSOLE.
1431 * Let the calling function know so it can decide
1432 * what to do.
1433 */
1434 console_unlock();
1435 return -EIO;
1436 }
1437 console_unlock();
1438 if (vt_waitactive(vt + 1)) {
1439 pr_debug("Suspend: Can't switch VCs.");
1440 return -EINTR;
1441 }
1442 return prev;
1443 }
1445 /*
1446 * Normally during a suspend, we allocate a new console and switch to it.
1447 * When we resume, we switch back to the original console. This switch
1448 * can be slow, so on systems where the framebuffer can handle restoration
1449 * of video registers anyways, there's little point in doing the console
1450 * switch. This function allows you to disable it by passing it '0'.
1451 */
1452 void pm_set_vt_switch(int do_switch)
1453 {
1454 console_lock();
1455 disable_vt_switch = !do_switch;
1456 console_unlock();
1457 }
1458 EXPORT_SYMBOL(pm_set_vt_switch);