1 // SPDX-License-Identifier: GPL-2.0
2 /*
3 * USB Role Switch Support
4 *
5 * Copyright (C) 2018 Intel Corporation
6 * Author: Heikki Krogerus <heikki.krogerus@linux.intel.com>
7 * Hans de Goede <hdegoede@redhat.com>
8 */
10 #include <linux/usb/role.h>
11 #include <linux/device.h>
12 #include <linux/module.h>
13 #include <linux/mutex.h>
14 #include <linux/slab.h>
16 static struct class *role_class;
18 struct usb_role_switch {
19 struct device dev;
20 struct mutex lock; /* device lock*/
21 enum usb_role role;
23 /* From descriptor */
24 struct device *usb2_port;
25 struct device *usb3_port;
26 struct device *udc;
27 usb_role_switch_set_t set;
28 usb_role_switch_get_t get;
29 bool allow_userspace_control;
30 };
32 #define to_role_switch(d) container_of(d, struct usb_role_switch, dev)
34 /**
35 * usb_role_switch_set_role - Set USB role for a switch
36 * @sw: USB role switch
37 * @role: USB role to be switched to
38 *
39 * Set USB role @role for @sw.
40 */
41 int usb_role_switch_set_role(struct usb_role_switch *sw, enum usb_role role)
42 {
43 int ret;
45 if (IS_ERR_OR_NULL(sw))
46 return 0;
48 mutex_lock(&sw->lock);
50 ret = sw->set(sw->dev.parent, role);
51 if (!ret)
52 sw->role = role;
54 mutex_unlock(&sw->lock);
56 return ret;
57 }
58 EXPORT_SYMBOL_GPL(usb_role_switch_set_role);
60 /**
61 * usb_role_switch_get_role - Get the USB role for a switch
62 * @sw: USB role switch
63 *
64 * Depending on the role-switch-driver this function returns either a cached
65 * value of the last set role, or reads back the actual value from the hardware.
66 */
67 enum usb_role usb_role_switch_get_role(struct usb_role_switch *sw)
68 {
69 enum usb_role role;
71 if (IS_ERR_OR_NULL(sw))
72 return USB_ROLE_NONE;
74 mutex_lock(&sw->lock);
76 if (sw->get)
77 role = sw->get(sw->dev.parent);
78 else
79 role = sw->role;
81 mutex_unlock(&sw->lock);
83 return role;
84 }
85 EXPORT_SYMBOL_GPL(usb_role_switch_get_role);
87 static int __switch_match(struct device *dev, const void *name)
88 {
89 return !strcmp((const char *)name, dev_name(dev));
90 }
92 static void *usb_role_switch_match(struct device_connection *con, int ep,
93 void *data)
94 {
95 struct device *dev;
97 dev = class_find_device(role_class, NULL, con->endpoint[ep],
98 __switch_match);
100 return dev ? to_role_switch(dev) : ERR_PTR(-EPROBE_DEFER);
101 }
103 /**
104 * usb_role_switch_get - Find USB role switch linked with the caller
105 * @dev: The caller device
106 *
107 * Finds and returns role switch linked with @dev. The reference count for the
108 * found switch is incremented.
109 */
110 struct usb_role_switch *usb_role_switch_get(struct device *dev)
111 {
112 struct usb_role_switch *sw;
114 sw = device_connection_find_match(dev, "usb-role-switch", NULL,
115 usb_role_switch_match);
117 if (!IS_ERR_OR_NULL(sw))
118 WARN_ON(!try_module_get(sw->dev.parent->driver->owner));
120 return sw;
121 }
122 EXPORT_SYMBOL_GPL(usb_role_switch_get);
124 /**
125 * usb_role_switch_put - Release handle to a switch
126 * @sw: USB Role Switch
127 *
128 * Decrement reference count for @sw.
129 */
130 void usb_role_switch_put(struct usb_role_switch *sw)
131 {
132 if (!IS_ERR_OR_NULL(sw)) {
133 put_device(&sw->dev);
134 module_put(sw->dev.parent->driver->owner);
135 }
136 }
137 EXPORT_SYMBOL_GPL(usb_role_switch_put);
139 static umode_t
140 usb_role_switch_is_visible(struct kobject *kobj, struct attribute *attr, int n)
141 {
142 struct device *dev = container_of(kobj, typeof(*dev), kobj);
143 struct usb_role_switch *sw = to_role_switch(dev);
145 if (sw->allow_userspace_control)
146 return attr->mode;
148 return 0;
149 }
151 static const char * const usb_roles[] = {
152 [USB_ROLE_NONE] = "none",
153 [USB_ROLE_HOST] = "host",
154 [USB_ROLE_DEVICE] = "device",
155 };
157 static ssize_t
158 role_show(struct device *dev, struct device_attribute *attr, char *buf)
159 {
160 struct usb_role_switch *sw = to_role_switch(dev);
161 enum usb_role role = usb_role_switch_get_role(sw);
163 return sprintf(buf, "%s\n", usb_roles[role]);
164 }
166 static ssize_t role_store(struct device *dev, struct device_attribute *attr,
167 const char *buf, size_t size)
168 {
169 struct usb_role_switch *sw = to_role_switch(dev);
170 int ret;
172 ret = sysfs_match_string(usb_roles, buf);
173 if (ret < 0) {
174 bool res;
176 /* Extra check if the user wants to disable the switch */
177 ret = kstrtobool(buf, &res);
178 if (ret || res)
179 return -EINVAL;
180 }
182 ret = usb_role_switch_set_role(sw, ret);
183 if (ret)
184 return ret;
186 return size;
187 }
188 static DEVICE_ATTR_RW(role);
190 static struct attribute *usb_role_switch_attrs[] = {
191 &dev_attr_role.attr,
192 NULL,
193 };
195 static const struct attribute_group usb_role_switch_group = {
196 .is_visible = usb_role_switch_is_visible,
197 .attrs = usb_role_switch_attrs,
198 };
200 static const struct attribute_group *usb_role_switch_groups[] = {
201 &usb_role_switch_group,
202 NULL,
203 };
205 static int
206 usb_role_switch_uevent(struct device *dev, struct kobj_uevent_env *env)
207 {
208 int ret;
210 ret = add_uevent_var(env, "USB_ROLE_SWITCH=%s", dev_name(dev));
211 if (ret)
212 dev_err(dev, "failed to add uevent USB_ROLE_SWITCH\n");
214 return ret;
215 }
217 static void usb_role_switch_release(struct device *dev)
218 {
219 struct usb_role_switch *sw = to_role_switch(dev);
221 kfree(sw);
222 }
224 static const struct device_type usb_role_dev_type = {
225 .name = "usb_role_switch",
226 .groups = usb_role_switch_groups,
227 .uevent = usb_role_switch_uevent,
228 .release = usb_role_switch_release,
229 };
231 /**
232 * usb_role_switch_register - Register USB Role Switch
233 * @parent: Parent device for the switch
234 * @desc: Description of the switch
235 *
236 * USB Role Switch is a device capable or choosing the role for USB connector.
237 * On platforms where the USB controller is dual-role capable, the controller
238 * driver will need to register the switch. On platforms where the USB host and
239 * USB device controllers behind the connector are separate, there will be a
240 * mux, and the driver for that mux will need to register the switch.
241 *
242 * Returns handle to a new role switch or ERR_PTR. The content of @desc is
243 * copied.
244 */
245 struct usb_role_switch *
246 usb_role_switch_register(struct device *parent,
247 const struct usb_role_switch_desc *desc)
248 {
249 struct usb_role_switch *sw;
250 int ret;
252 if (!desc || !desc->set)
253 return ERR_PTR(-EINVAL);
255 sw = kzalloc(sizeof(*sw), GFP_KERNEL);
256 if (!sw)
257 return ERR_PTR(-ENOMEM);
259 mutex_init(&sw->lock);
261 sw->allow_userspace_control = desc->allow_userspace_control;
262 sw->usb2_port = desc->usb2_port;
263 sw->usb3_port = desc->usb3_port;
264 sw->udc = desc->udc;
265 sw->set = desc->set;
266 sw->get = desc->get;
268 sw->dev.parent = parent;
269 sw->dev.class = role_class;
270 sw->dev.type = &usb_role_dev_type;
271 dev_set_name(&sw->dev, "%s-role-switch", dev_name(parent));
273 ret = device_register(&sw->dev);
274 if (ret) {
275 put_device(&sw->dev);
276 return ERR_PTR(ret);
277 }
279 /* TODO: Symlinks for the host port and the device controller. */
281 return sw;
282 }
283 EXPORT_SYMBOL_GPL(usb_role_switch_register);
285 /**
286 * usb_role_switch_unregister - Unregsiter USB Role Switch
287 * @sw: USB Role Switch
288 *
289 * Unregister switch that was registered with usb_role_switch_register().
290 */
291 void usb_role_switch_unregister(struct usb_role_switch *sw)
292 {
293 if (!IS_ERR_OR_NULL(sw))
294 device_unregister(&sw->dev);
295 }
296 EXPORT_SYMBOL_GPL(usb_role_switch_unregister);
298 static int __init usb_roles_init(void)
299 {
300 role_class = class_create(THIS_MODULE, "usb_role");
301 return PTR_ERR_OR_ZERO(role_class);
302 }
303 subsys_initcall(usb_roles_init);
305 static void __exit usb_roles_exit(void)
306 {
307 class_destroy(role_class);
308 }
309 module_exit(usb_roles_exit);
311 MODULE_AUTHOR("Heikki Krogerus <heikki.krogerus@linux.intel.com>");
312 MODULE_AUTHOR("Hans de Goede <hdegoede@redhat.com>");
313 MODULE_LICENSE("GPL v2");
314 MODULE_DESCRIPTION("USB Role Class");