]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - drivers/video/fbdev/efifb.c
Merge tag 'kbuild-fixes-v4.19-2' of git://git.kernel.org/pub/scm/linux/kernel/git...
[rpmsg/rpmsg.git] / drivers / video / fbdev / efifb.c
1 // SPDX-License-Identifier: GPL-2.0
2 /*
3  * Framebuffer driver for EFI/UEFI based system
4  *
5  * (c) 2006 Edgar Hucek <gimli@dark-green.com>
6  * Original efi driver written by Gerd Knorr <kraxel@goldbach.in-berlin.de>
7  *
8  */
10 #include <linux/kernel.h>
11 #include <linux/efi.h>
12 #include <linux/efi-bgrt.h>
13 #include <linux/errno.h>
14 #include <linux/fb.h>
15 #include <linux/pci.h>
16 #include <linux/platform_device.h>
17 #include <linux/printk.h>
18 #include <linux/screen_info.h>
19 #include <video/vga.h>
20 #include <asm/efi.h>
21 #include <drm/drm_utils.h> /* For drm_get_panel_orientation_quirk */
22 #include <drm/drm_connector.h>  /* For DRM_MODE_PANEL_ORIENTATION_* */
24 struct bmp_file_header {
25         u16 id;
26         u32 file_size;
27         u32 reserved;
28         u32 bitmap_offset;
29 } __packed;
31 struct bmp_dib_header {
32         u32 dib_header_size;
33         s32 width;
34         s32 height;
35         u16 planes;
36         u16 bpp;
37         u32 compression;
38         u32 bitmap_size;
39         u32 horz_resolution;
40         u32 vert_resolution;
41         u32 colors_used;
42         u32 colors_important;
43 } __packed;
45 static bool use_bgrt = true;
46 static bool request_mem_succeeded = false;
47 static u64 mem_flags = EFI_MEMORY_WC | EFI_MEMORY_UC;
49 static struct fb_var_screeninfo efifb_defined = {
50         .activate               = FB_ACTIVATE_NOW,
51         .height                 = -1,
52         .width                  = -1,
53         .right_margin           = 32,
54         .upper_margin           = 16,
55         .lower_margin           = 4,
56         .vsync_len              = 4,
57         .vmode                  = FB_VMODE_NONINTERLACED,
58 };
60 static struct fb_fix_screeninfo efifb_fix = {
61         .id                     = "EFI VGA",
62         .type                   = FB_TYPE_PACKED_PIXELS,
63         .accel                  = FB_ACCEL_NONE,
64         .visual                 = FB_VISUAL_TRUECOLOR,
65 };
67 static int efifb_setcolreg(unsigned regno, unsigned red, unsigned green,
68                            unsigned blue, unsigned transp,
69                            struct fb_info *info)
70 {
71         /*
72          *  Set a single color register. The values supplied are
73          *  already rounded down to the hardware's capabilities
74          *  (according to the entries in the `var' structure). Return
75          *  != 0 for invalid regno.
76          */
78         if (regno >= info->cmap.len)
79                 return 1;
81         if (regno < 16) {
82                 red   >>= 16 - info->var.red.length;
83                 green >>= 16 - info->var.green.length;
84                 blue  >>= 16 - info->var.blue.length;
85                 ((u32 *)(info->pseudo_palette))[regno] =
86                         (red   << info->var.red.offset)   |
87                         (green << info->var.green.offset) |
88                         (blue  << info->var.blue.offset);
89         }
90         return 0;
91 }
93 /*
94  * If fbcon deffered console takeover is configured, the intent is for the
95  * framebuffer to show the boot graphics (e.g. vendor logo) until there is some
96  * (error) message to display. But the boot graphics may have been destroyed by
97  * e.g. option ROM output, detect this and restore the boot graphics.
98  */
99 #if defined CONFIG_FRAMEBUFFER_CONSOLE_DEFERRED_TAKEOVER && \
100     defined CONFIG_ACPI_BGRT
101 static void efifb_copy_bmp(u8 *src, u32 *dst, int width, struct screen_info *si)
103         u8 r, g, b;
105         while (width--) {
106                 b = *src++;
107                 g = *src++;
108                 r = *src++;
109                 *dst++ = (r << si->red_pos)   |
110                          (g << si->green_pos) |
111                          (b << si->blue_pos);
112         }
115 #ifdef CONFIG_X86
116 /*
117  * On x86 some firmwares use a low non native resolution for the display when
118  * they have shown some text messages. While keeping the bgrt filled with info
119  * for the native resolution. If the bgrt image intended for the native
120  * resolution still fits, it will be displayed very close to the right edge of
121  * the display looking quite bad. This function checks for this.
122  */
123 static bool efifb_bgrt_sanity_check(struct screen_info *si, u32 bmp_width)
125         static const int default_resolutions[][2] = {
126                 {  800,  600 },
127                 { 1024,  768 },
128                 { 1280, 1024 },
129         };
130         u32 i, right_margin;
132         for (i = 0; i < ARRAY_SIZE(default_resolutions); i++) {
133                 if (default_resolutions[i][0] == si->lfb_width &&
134                     default_resolutions[i][1] == si->lfb_height)
135                         break;
136         }
137         /* If not a default resolution used for textmode, this should be fine */
138         if (i >= ARRAY_SIZE(default_resolutions))
139                 return true;
141         /* If the right margin is 5 times smaller then the left one, reject */
142         right_margin = si->lfb_width - (bgrt_tab.image_offset_x + bmp_width);
143         if (right_margin < (bgrt_tab.image_offset_x / 5))
144                 return false;
146         return true;
148 #else
149 static bool efifb_bgrt_sanity_check(struct screen_info *si, u32 bmp_width)
151         return true;
153 #endif
155 static void efifb_show_boot_graphics(struct fb_info *info)
157         u32 bmp_width, bmp_height, bmp_pitch, screen_pitch, dst_x, y, src_y;
158         struct screen_info *si = &screen_info;
159         struct bmp_file_header *file_header;
160         struct bmp_dib_header *dib_header;
161         void *bgrt_image = NULL;
162         u8 *dst = info->screen_base;
164         if (!use_bgrt)
165                 return;
167         if (!bgrt_tab.image_address) {
168                 pr_info("efifb: No BGRT, not showing boot graphics\n");
169                 return;
170         }
172         /* Avoid flashing the logo if we're going to print std probe messages */
173         if (console_loglevel > CONSOLE_LOGLEVEL_QUIET)
174                 return;
176         /* bgrt_tab.status is unreliable, so we don't check it */
178         if (si->lfb_depth != 32) {
179                 pr_info("efifb: not 32 bits, not showing boot graphics\n");
180                 return;
181         }
183         bgrt_image = memremap(bgrt_tab.image_address, bgrt_image_size,
184                               MEMREMAP_WB);
185         if (!bgrt_image) {
186                 pr_warn("efifb: Ignoring BGRT: failed to map image memory\n");
187                 return;
188         }
190         if (bgrt_image_size < (sizeof(*file_header) + sizeof(*dib_header)))
191                 goto error;
193         file_header = bgrt_image;
194         if (file_header->id != 0x4d42 || file_header->reserved != 0)
195                 goto error;
197         dib_header = bgrt_image + sizeof(*file_header);
198         if (dib_header->dib_header_size != 40 || dib_header->width < 0 ||
199             dib_header->planes != 1 || dib_header->bpp != 24 ||
200             dib_header->compression != 0)
201                 goto error;
203         bmp_width = dib_header->width;
204         bmp_height = abs(dib_header->height);
205         bmp_pitch = round_up(3 * bmp_width, 4);
206         screen_pitch = si->lfb_linelength;
208         if ((file_header->bitmap_offset + bmp_pitch * bmp_height) >
209                                 bgrt_image_size)
210                 goto error;
212         if ((bgrt_tab.image_offset_x + bmp_width) > si->lfb_width ||
213             (bgrt_tab.image_offset_y + bmp_height) > si->lfb_height)
214                 goto error;
216         if (!efifb_bgrt_sanity_check(si, bmp_width))
217                 goto error;
219         pr_info("efifb: showing boot graphics\n");
221         for (y = 0; y < si->lfb_height; y++, dst += si->lfb_linelength) {
222                 /* Only background? */
223                 if (y < bgrt_tab.image_offset_y ||
224                     y >= (bgrt_tab.image_offset_y + bmp_height)) {
225                         memset(dst, 0, 4 * si->lfb_width);
226                         continue;
227                 }
229                 src_y = y - bgrt_tab.image_offset_y;
230                 /* Positive header height means upside down row order */
231                 if (dib_header->height > 0)
232                         src_y = (bmp_height - 1) - src_y;
234                 memset(dst, 0, bgrt_tab.image_offset_x * 4);
235                 dst_x = bgrt_tab.image_offset_x;
236                 efifb_copy_bmp(bgrt_image + file_header->bitmap_offset +
237                                             src_y * bmp_pitch,
238                                (u32 *)dst + dst_x, bmp_width, si);
239                 dst_x += bmp_width;
240                 memset((u32 *)dst + dst_x, 0, (si->lfb_width - dst_x) * 4);
241         }
243         memunmap(bgrt_image);
244         return;
246 error:
247         memunmap(bgrt_image);
248         pr_warn("efifb: Ignoring BGRT: unexpected or invalid BMP data\n");
250 #else
251 static inline void efifb_show_boot_graphics(struct fb_info *info) {}
252 #endif
254 static void efifb_destroy(struct fb_info *info)
256         if (info->screen_base) {
257                 if (mem_flags & (EFI_MEMORY_UC | EFI_MEMORY_WC))
258                         iounmap(info->screen_base);
259                 else
260                         memunmap(info->screen_base);
261         }
262         if (request_mem_succeeded)
263                 release_mem_region(info->apertures->ranges[0].base,
264                                    info->apertures->ranges[0].size);
265         fb_dealloc_cmap(&info->cmap);
268 static struct fb_ops efifb_ops = {
269         .owner          = THIS_MODULE,
270         .fb_destroy     = efifb_destroy,
271         .fb_setcolreg   = efifb_setcolreg,
272         .fb_fillrect    = cfb_fillrect,
273         .fb_copyarea    = cfb_copyarea,
274         .fb_imageblit   = cfb_imageblit,
275 };
277 static int efifb_setup(char *options)
279         char *this_opt;
281         if (options && *options) {
282                 while ((this_opt = strsep(&options, ",")) != NULL) {
283                         if (!*this_opt) continue;
285                         efifb_setup_from_dmi(&screen_info, this_opt);
287                         if (!strncmp(this_opt, "base:", 5))
288                                 screen_info.lfb_base = simple_strtoul(this_opt+5, NULL, 0);
289                         else if (!strncmp(this_opt, "stride:", 7))
290                                 screen_info.lfb_linelength = simple_strtoul(this_opt+7, NULL, 0) * 4;
291                         else if (!strncmp(this_opt, "height:", 7))
292                                 screen_info.lfb_height = simple_strtoul(this_opt+7, NULL, 0);
293                         else if (!strncmp(this_opt, "width:", 6))
294                                 screen_info.lfb_width = simple_strtoul(this_opt+6, NULL, 0);
295                         else if (!strcmp(this_opt, "nowc"))
296                                 mem_flags &= ~EFI_MEMORY_WC;
297                         else if (!strcmp(this_opt, "nobgrt"))
298                                 use_bgrt = false;
299                 }
300         }
302         return 0;
305 static inline bool fb_base_is_valid(void)
307         if (screen_info.lfb_base)
308                 return true;
310         if (!(screen_info.capabilities & VIDEO_CAPABILITY_64BIT_BASE))
311                 return false;
313         if (screen_info.ext_lfb_base)
314                 return true;
316         return false;
319 #define efifb_attr_decl(name, fmt)                                      \
320 static ssize_t name##_show(struct device *dev,                          \
321                            struct device_attribute *attr,               \
322                            char *buf)                                   \
323 {                                                                       \
324         return sprintf(buf, fmt "\n", (screen_info.lfb_##name));        \
325 }                                                                       \
326 static DEVICE_ATTR_RO(name)
328 efifb_attr_decl(base, "0x%x");
329 efifb_attr_decl(linelength, "%u");
330 efifb_attr_decl(height, "%u");
331 efifb_attr_decl(width, "%u");
332 efifb_attr_decl(depth, "%u");
334 static struct attribute *efifb_attrs[] = {
335         &dev_attr_base.attr,
336         &dev_attr_linelength.attr,
337         &dev_attr_width.attr,
338         &dev_attr_height.attr,
339         &dev_attr_depth.attr,
340         NULL
341 };
342 ATTRIBUTE_GROUPS(efifb);
344 static bool pci_dev_disabled;   /* FB base matches BAR of a disabled device */
346 static struct pci_dev *efifb_pci_dev;   /* dev with BAR covering the efifb */
347 static struct resource *bar_resource;
348 static u64 bar_offset;
350 static int efifb_probe(struct platform_device *dev)
352         struct fb_info *info;
353         int err, orientation;
354         unsigned int size_vmode;
355         unsigned int size_remap;
356         unsigned int size_total;
357         char *option = NULL;
358         efi_memory_desc_t md;
360         if (screen_info.orig_video_isVGA != VIDEO_TYPE_EFI || pci_dev_disabled)
361                 return -ENODEV;
363         if (fb_get_options("efifb", &option))
364                 return -ENODEV;
365         efifb_setup(option);
367         /* We don't get linelength from UGA Draw Protocol, only from
368          * EFI Graphics Protocol.  So if it's not in DMI, and it's not
369          * passed in from the user, we really can't use the framebuffer.
370          */
371         if (!screen_info.lfb_linelength)
372                 return -ENODEV;
374         if (!screen_info.lfb_depth)
375                 screen_info.lfb_depth = 32;
376         if (!screen_info.pages)
377                 screen_info.pages = 1;
378         if (!fb_base_is_valid()) {
379                 printk(KERN_DEBUG "efifb: invalid framebuffer address\n");
380                 return -ENODEV;
381         }
382         printk(KERN_INFO "efifb: probing for efifb\n");
384         /* just assume they're all unset if any are */
385         if (!screen_info.blue_size) {
386                 screen_info.blue_size = 8;
387                 screen_info.blue_pos = 0;
388                 screen_info.green_size = 8;
389                 screen_info.green_pos = 8;
390                 screen_info.red_size = 8;
391                 screen_info.red_pos = 16;
392                 screen_info.rsvd_size = 8;
393                 screen_info.rsvd_pos = 24;
394         }
396         efifb_fix.smem_start = screen_info.lfb_base;
398         if (screen_info.capabilities & VIDEO_CAPABILITY_64BIT_BASE) {
399                 u64 ext_lfb_base;
401                 ext_lfb_base = (u64)(unsigned long)screen_info.ext_lfb_base << 32;
402                 efifb_fix.smem_start |= ext_lfb_base;
403         }
405         if (bar_resource &&
406             bar_resource->start + bar_offset != efifb_fix.smem_start) {
407                 dev_info(&efifb_pci_dev->dev,
408                          "BAR has moved, updating efifb address\n");
409                 efifb_fix.smem_start = bar_resource->start + bar_offset;
410         }
412         efifb_defined.bits_per_pixel = screen_info.lfb_depth;
413         efifb_defined.xres = screen_info.lfb_width;
414         efifb_defined.yres = screen_info.lfb_height;
415         efifb_fix.line_length = screen_info.lfb_linelength;
417         /*   size_vmode -- that is the amount of memory needed for the
418          *                 used video mode, i.e. the minimum amount of
419          *                 memory we need. */
420         size_vmode = efifb_defined.yres * efifb_fix.line_length;
422         /*   size_total -- all video memory we have. Used for
423          *                 entries, ressource allocation and bounds
424          *                 checking. */
425         size_total = screen_info.lfb_size;
426         if (size_total < size_vmode)
427                 size_total = size_vmode;
429         /*   size_remap -- the amount of video memory we are going to
430          *                 use for efifb.  With modern cards it is no
431          *                 option to simply use size_total as that
432          *                 wastes plenty of kernel address space. */
433         size_remap  = size_vmode * 2;
434         if (size_remap > size_total)
435                 size_remap = size_total;
436         if (size_remap % PAGE_SIZE)
437                 size_remap += PAGE_SIZE - (size_remap % PAGE_SIZE);
438         efifb_fix.smem_len = size_remap;
440         if (request_mem_region(efifb_fix.smem_start, size_remap, "efifb")) {
441                 request_mem_succeeded = true;
442         } else {
443                 /* We cannot make this fatal. Sometimes this comes from magic
444                    spaces our resource handlers simply don't know about */
445                 pr_warn("efifb: cannot reserve video memory at 0x%lx\n",
446                         efifb_fix.smem_start);
447         }
449         info = framebuffer_alloc(sizeof(u32) * 16, &dev->dev);
450         if (!info) {
451                 pr_err("efifb: cannot allocate framebuffer\n");
452                 err = -ENOMEM;
453                 goto err_release_mem;
454         }
455         platform_set_drvdata(dev, info);
456         info->pseudo_palette = info->par;
457         info->par = NULL;
459         info->apertures = alloc_apertures(1);
460         if (!info->apertures) {
461                 err = -ENOMEM;
462                 goto err_release_fb;
463         }
464         info->apertures->ranges[0].base = efifb_fix.smem_start;
465         info->apertures->ranges[0].size = size_remap;
467         if (!efi_mem_desc_lookup(efifb_fix.smem_start, &md)) {
468                 if ((efifb_fix.smem_start + efifb_fix.smem_len) >
469                     (md.phys_addr + (md.num_pages << EFI_PAGE_SHIFT))) {
470                         pr_err("efifb: video memory @ 0x%lx spans multiple EFI memory regions\n",
471                                efifb_fix.smem_start);
472                         err = -EIO;
473                         goto err_release_fb;
474                 }
475                 /*
476                  * If the UEFI memory map covers the efifb region, we may only
477                  * remap it using the attributes the memory map prescribes.
478                  */
479                 mem_flags |= EFI_MEMORY_WT | EFI_MEMORY_WB;
480                 mem_flags &= md.attribute;
481         }
482         if (mem_flags & EFI_MEMORY_WC)
483                 info->screen_base = ioremap_wc(efifb_fix.smem_start,
484                                                efifb_fix.smem_len);
485         else if (mem_flags & EFI_MEMORY_UC)
486                 info->screen_base = ioremap(efifb_fix.smem_start,
487                                             efifb_fix.smem_len);
488         else if (mem_flags & EFI_MEMORY_WT)
489                 info->screen_base = memremap(efifb_fix.smem_start,
490                                              efifb_fix.smem_len, MEMREMAP_WT);
491         else if (mem_flags & EFI_MEMORY_WB)
492                 info->screen_base = memremap(efifb_fix.smem_start,
493                                              efifb_fix.smem_len, MEMREMAP_WB);
494         if (!info->screen_base) {
495                 pr_err("efifb: abort, cannot remap video memory 0x%x @ 0x%lx\n",
496                         efifb_fix.smem_len, efifb_fix.smem_start);
497                 err = -EIO;
498                 goto err_release_fb;
499         }
501         efifb_show_boot_graphics(info);
503         pr_info("efifb: framebuffer at 0x%lx, using %dk, total %dk\n",
504                efifb_fix.smem_start, size_remap/1024, size_total/1024);
505         pr_info("efifb: mode is %dx%dx%d, linelength=%d, pages=%d\n",
506                efifb_defined.xres, efifb_defined.yres,
507                efifb_defined.bits_per_pixel, efifb_fix.line_length,
508                screen_info.pages);
510         efifb_defined.xres_virtual = efifb_defined.xres;
511         efifb_defined.yres_virtual = efifb_fix.smem_len /
512                                         efifb_fix.line_length;
513         pr_info("efifb: scrolling: redraw\n");
514         efifb_defined.yres_virtual = efifb_defined.yres;
516         /* some dummy values for timing to make fbset happy */
517         efifb_defined.pixclock     = 10000000 / efifb_defined.xres *
518                                         1000 / efifb_defined.yres;
519         efifb_defined.left_margin  = (efifb_defined.xres / 8) & 0xf8;
520         efifb_defined.hsync_len    = (efifb_defined.xres / 8) & 0xf8;
522         efifb_defined.red.offset    = screen_info.red_pos;
523         efifb_defined.red.length    = screen_info.red_size;
524         efifb_defined.green.offset  = screen_info.green_pos;
525         efifb_defined.green.length  = screen_info.green_size;
526         efifb_defined.blue.offset   = screen_info.blue_pos;
527         efifb_defined.blue.length   = screen_info.blue_size;
528         efifb_defined.transp.offset = screen_info.rsvd_pos;
529         efifb_defined.transp.length = screen_info.rsvd_size;
531         pr_info("efifb: %s: "
532                "size=%d:%d:%d:%d, shift=%d:%d:%d:%d\n",
533                "Truecolor",
534                screen_info.rsvd_size,
535                screen_info.red_size,
536                screen_info.green_size,
537                screen_info.blue_size,
538                screen_info.rsvd_pos,
539                screen_info.red_pos,
540                screen_info.green_pos,
541                screen_info.blue_pos);
543         efifb_fix.ypanstep  = 0;
544         efifb_fix.ywrapstep = 0;
546         info->fbops = &efifb_ops;
547         info->var = efifb_defined;
548         info->fix = efifb_fix;
549         info->flags = FBINFO_FLAG_DEFAULT | FBINFO_MISC_FIRMWARE;
551         orientation = drm_get_panel_orientation_quirk(efifb_defined.xres,
552                                                       efifb_defined.yres);
553         switch (orientation) {
554         default:
555                 info->fbcon_rotate_hint = FB_ROTATE_UR;
556                 break;
557         case DRM_MODE_PANEL_ORIENTATION_BOTTOM_UP:
558                 info->fbcon_rotate_hint = FB_ROTATE_UD;
559                 break;
560         case DRM_MODE_PANEL_ORIENTATION_LEFT_UP:
561                 info->fbcon_rotate_hint = FB_ROTATE_CCW;
562                 break;
563         case DRM_MODE_PANEL_ORIENTATION_RIGHT_UP:
564                 info->fbcon_rotate_hint = FB_ROTATE_CW;
565                 break;
566         }
568         err = sysfs_create_groups(&dev->dev.kobj, efifb_groups);
569         if (err) {
570                 pr_err("efifb: cannot add sysfs attrs\n");
571                 goto err_unmap;
572         }
573         err = fb_alloc_cmap(&info->cmap, 256, 0);
574         if (err < 0) {
575                 pr_err("efifb: cannot allocate colormap\n");
576                 goto err_groups;
577         }
578         err = register_framebuffer(info);
579         if (err < 0) {
580                 pr_err("efifb: cannot register framebuffer\n");
581                 goto err_fb_dealoc;
582         }
583         fb_info(info, "%s frame buffer device\n", info->fix.id);
584         return 0;
586 err_fb_dealoc:
587         fb_dealloc_cmap(&info->cmap);
588 err_groups:
589         sysfs_remove_groups(&dev->dev.kobj, efifb_groups);
590 err_unmap:
591         if (mem_flags & (EFI_MEMORY_UC | EFI_MEMORY_WC))
592                 iounmap(info->screen_base);
593         else
594                 memunmap(info->screen_base);
595 err_release_fb:
596         framebuffer_release(info);
597 err_release_mem:
598         if (request_mem_succeeded)
599                 release_mem_region(efifb_fix.smem_start, size_total);
600         return err;
603 static int efifb_remove(struct platform_device *pdev)
605         struct fb_info *info = platform_get_drvdata(pdev);
607         unregister_framebuffer(info);
608         sysfs_remove_groups(&pdev->dev.kobj, efifb_groups);
609         framebuffer_release(info);
611         return 0;
614 static struct platform_driver efifb_driver = {
615         .driver = {
616                 .name = "efi-framebuffer",
617         },
618         .probe = efifb_probe,
619         .remove = efifb_remove,
620 };
622 builtin_platform_driver(efifb_driver);
624 #if defined(CONFIG_PCI)
626 static void record_efifb_bar_resource(struct pci_dev *dev, int idx, u64 offset)
628         u16 word;
630         efifb_pci_dev = dev;
632         pci_read_config_word(dev, PCI_COMMAND, &word);
633         if (!(word & PCI_COMMAND_MEMORY)) {
634                 pci_dev_disabled = true;
635                 dev_err(&dev->dev,
636                         "BAR %d: assigned to efifb but device is disabled!\n",
637                         idx);
638                 return;
639         }
641         bar_resource = &dev->resource[idx];
642         bar_offset = offset;
644         dev_info(&dev->dev, "BAR %d: assigned to efifb\n", idx);
647 static void efifb_fixup_resources(struct pci_dev *dev)
649         u64 base = screen_info.lfb_base;
650         u64 size = screen_info.lfb_size;
651         int i;
653         if (efifb_pci_dev || screen_info.orig_video_isVGA != VIDEO_TYPE_EFI)
654                 return;
656         if (screen_info.capabilities & VIDEO_CAPABILITY_64BIT_BASE)
657                 base |= (u64)screen_info.ext_lfb_base << 32;
659         if (!base)
660                 return;
662         for (i = 0; i <= PCI_STD_RESOURCE_END; i++) {
663                 struct resource *res = &dev->resource[i];
665                 if (!(res->flags & IORESOURCE_MEM))
666                         continue;
668                 if (res->start <= base && res->end >= base + size - 1) {
669                         record_efifb_bar_resource(dev, i, base - res->start);
670                         break;
671                 }
672         }
674 DECLARE_PCI_FIXUP_CLASS_HEADER(PCI_ANY_ID, PCI_ANY_ID, PCI_BASE_CLASS_DISPLAY,
675                                16, efifb_fixup_resources);
677 #endif