]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - fs/Kconfig
Revert "HACK: ARM: dts: dra7-ipu-common: Revert to CMA pools for IPU early boots"
[rpmsg/rpmsg.git] / fs / Kconfig
1 #
2 # File system configuration
3 #
5 menu "File systems"
7 # Use unaligned word dcache accesses
8 config DCACHE_WORD_ACCESS
9        bool
11 if BLOCK
13 config FS_IOMAP
14         bool
16 source "fs/ext2/Kconfig"
17 source "fs/ext4/Kconfig"
18 source "fs/jbd2/Kconfig"
20 config FS_MBCACHE
21 # Meta block cache for Extended Attributes (ext2/ext3/ext4)
22         tristate
23         default y if EXT2_FS=y && EXT2_FS_XATTR
24         default y if EXT4_FS=y
25         default m if EXT2_FS_XATTR || EXT4_FS
27 source "fs/reiserfs/Kconfig"
28 source "fs/jfs/Kconfig"
30 source "fs/xfs/Kconfig"
31 source "fs/gfs2/Kconfig"
32 source "fs/ocfs2/Kconfig"
33 source "fs/btrfs/Kconfig"
34 source "fs/nilfs2/Kconfig"
35 source "fs/f2fs/Kconfig"
37 config FS_DAX
38         bool "Direct Access (DAX) support"
39         depends on MMU
40         depends on !(ARM || MIPS || SPARC)
41         select DEV_PAGEMAP_OPS if (ZONE_DEVICE && !FS_DAX_LIMITED)
42         select FS_IOMAP
43         select DAX
44         help
45           Direct Access (DAX) can be used on memory-backed block devices.
46           If the block device supports DAX and the filesystem supports DAX,
47           then you can avoid using the pagecache to buffer I/Os.  Turning
48           on this option will compile in support for DAX; you will need to
49           mount the filesystem using the -o dax option.
51           If you do not have a block device that is capable of using this,
52           or if unsure, say N.  Saying Y will increase the size of the kernel
53           by about 5kB.
55 config FS_DAX_PMD
56         bool
57         default FS_DAX
58         depends on FS_DAX
59         depends on ZONE_DEVICE
60         depends on TRANSPARENT_HUGEPAGE
62 # Selected by DAX drivers that do not expect filesystem DAX to support
63 # get_user_pages() of DAX mappings. I.e. "limited" indicates no support
64 # for fork() of processes with MAP_SHARED mappings or support for
65 # direct-I/O to a DAX mapping.
66 config FS_DAX_LIMITED
67         bool
69 endif # BLOCK
71 # Posix ACL utility routines
72 #
73 # Note: Posix ACLs can be implemented without these helpers.  Never use
74 # this symbol for ifdefs in core code.
75 #
76 config FS_POSIX_ACL
77         def_bool n
79 config EXPORTFS
80         tristate
82 config EXPORTFS_BLOCK_OPS
83         bool "Enable filesystem export operations for block IO"
84         help
85           This option enables the export operations for a filesystem to support
86           external block IO.
88 config FILE_LOCKING
89         bool "Enable POSIX file locking API" if EXPERT
90         default y
91         help
92           This option enables standard file locking support, required
93           for filesystems like NFS and for the flock() system
94           call. Disabling this option saves about 11k.
96 config MANDATORY_FILE_LOCKING
97         bool "Enable Mandatory file locking"
98         depends on FILE_LOCKING
99         default y
100         help
101           This option enables files appropriately marked files on appropriely
102           mounted filesystems to support mandatory locking.
104           To the best of my knowledge this is dead code that no one cares about.
106 source "fs/crypto/Kconfig"
108 source "fs/notify/Kconfig"
110 source "fs/quota/Kconfig"
112 source "fs/autofs/Kconfig"
113 source "fs/fuse/Kconfig"
114 source "fs/overlayfs/Kconfig"
116 menu "Caches"
118 source "fs/fscache/Kconfig"
119 source "fs/cachefiles/Kconfig"
121 endmenu
123 if BLOCK
124 menu "CD-ROM/DVD Filesystems"
126 source "fs/isofs/Kconfig"
127 source "fs/udf/Kconfig"
129 endmenu
130 endif # BLOCK
132 if BLOCK
133 menu "DOS/FAT/NT Filesystems"
135 source "fs/fat/Kconfig"
136 source "fs/ntfs/Kconfig"
138 endmenu
139 endif # BLOCK
141 menu "Pseudo filesystems"
143 source "fs/proc/Kconfig"
144 source "fs/kernfs/Kconfig"
145 source "fs/sysfs/Kconfig"
147 config TMPFS
148         bool "Tmpfs virtual memory file system support (former shm fs)"
149         depends on SHMEM
150         help
151           Tmpfs is a file system which keeps all files in virtual memory.
153           Everything in tmpfs is temporary in the sense that no files will be
154           created on your hard drive. The files live in memory and swap
155           space. If you unmount a tmpfs instance, everything stored therein is
156           lost.
158           See <file:Documentation/filesystems/tmpfs.txt> for details.
160 config TMPFS_POSIX_ACL
161         bool "Tmpfs POSIX Access Control Lists"
162         depends on TMPFS
163         select TMPFS_XATTR
164         select FS_POSIX_ACL
165         help
166           POSIX Access Control Lists (ACLs) support additional access rights
167           for users and groups beyond the standard owner/group/world scheme,
168           and this option selects support for ACLs specifically for tmpfs
169           filesystems.
171           If you've selected TMPFS, it's possible that you'll also need
172           this option as there are a number of Linux distros that require
173           POSIX ACL support under /dev for certain features to work properly.
174           For example, some distros need this feature for ALSA-related /dev
175           files for sound to work properly.  In short, if you're not sure,
176           say Y.
178 config TMPFS_XATTR
179         bool "Tmpfs extended attributes"
180         depends on TMPFS
181         default n
182         help
183           Extended attributes are name:value pairs associated with inodes by
184           the kernel or by users (see the attr(5) manual page for details).
186           Currently this enables support for the trusted.* and
187           security.* namespaces.
189           You need this for POSIX ACL support on tmpfs.
191           If unsure, say N.
193 config HUGETLBFS
194         bool "HugeTLB file system support"
195         depends on X86 || IA64 || SPARC64 || (S390 && 64BIT) || \
196                    SYS_SUPPORTS_HUGETLBFS || BROKEN
197         help
198           hugetlbfs is a filesystem backing for HugeTLB pages, based on
199           ramfs. For architectures that support it, say Y here and read
200           <file:Documentation/admin-guide/mm/hugetlbpage.rst> for details.
202           If unsure, say N.
204 config HUGETLB_PAGE
205         def_bool HUGETLBFS
207 config MEMFD_CREATE
208         def_bool TMPFS || HUGETLBFS
210 config ARCH_HAS_GIGANTIC_PAGE
211         bool
213 source "fs/configfs/Kconfig"
214 source "fs/efivarfs/Kconfig"
216 endmenu
218 menuconfig MISC_FILESYSTEMS
219         bool "Miscellaneous filesystems"
220         default y
221         ---help---
222           Say Y here to get to see options for various miscellaneous
223           filesystems, such as filesystems that came from other
224           operating systems.
226           This option alone does not add any kernel code.
228           If you say N, all options in this submenu will be skipped and
229           disabled; if unsure, say Y here.
231 if MISC_FILESYSTEMS
233 source "fs/orangefs/Kconfig"
234 source "fs/adfs/Kconfig"
235 source "fs/affs/Kconfig"
236 source "fs/ecryptfs/Kconfig"
237 source "fs/hfs/Kconfig"
238 source "fs/hfsplus/Kconfig"
239 source "fs/befs/Kconfig"
240 source "fs/bfs/Kconfig"
241 source "fs/efs/Kconfig"
242 source "fs/jffs2/Kconfig"
243 # UBIFS File system configuration
244 source "fs/ubifs/Kconfig"
245 source "fs/cramfs/Kconfig"
246 source "fs/squashfs/Kconfig"
247 source "fs/freevxfs/Kconfig"
248 source "fs/minix/Kconfig"
249 source "fs/omfs/Kconfig"
250 source "fs/hpfs/Kconfig"
251 source "fs/qnx4/Kconfig"
252 source "fs/qnx6/Kconfig"
253 source "fs/romfs/Kconfig"
254 source "fs/pstore/Kconfig"
255 source "fs/sysv/Kconfig"
256 source "fs/ufs/Kconfig"
257 source "fs/exofs/Kconfig"
259 endif # MISC_FILESYSTEMS
261 source "fs/exofs/Kconfig.ore"
263 menuconfig NETWORK_FILESYSTEMS
264         bool "Network File Systems"
265         default y
266         depends on NET
267         ---help---
268           Say Y here to get to see options for network filesystems and
269           filesystem-related networking code, such as NFS daemon and
270           RPCSEC security modules.
272           This option alone does not add any kernel code.
274           If you say N, all options in this submenu will be skipped and
275           disabled; if unsure, say Y here.
277 if NETWORK_FILESYSTEMS
279 source "fs/nfs/Kconfig"
280 source "fs/nfsd/Kconfig"
282 config GRACE_PERIOD
283         tristate
285 config LOCKD
286         tristate
287         depends on FILE_LOCKING
288         select GRACE_PERIOD
290 config LOCKD_V4
291         bool
292         depends on NFSD_V3 || NFS_V3
293         depends on FILE_LOCKING
294         default y
296 config NFS_ACL_SUPPORT
297         tristate
298         select FS_POSIX_ACL
300 config NFS_COMMON
301         bool
302         depends on NFSD || NFS_FS || LOCKD
303         default y
305 source "net/sunrpc/Kconfig"
306 source "fs/ceph/Kconfig"
307 source "fs/cifs/Kconfig"
308 source "fs/coda/Kconfig"
309 source "fs/afs/Kconfig"
310 source "fs/9p/Kconfig"
312 endif # NETWORK_FILESYSTEMS
314 source "fs/nls/Kconfig"
315 source "fs/dlm/Kconfig"
317 endmenu