]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - fs/filesystems.c
Merge branch 'rpmsg-linux-4.19.y' of git://git.ti.com/rpmsg/rpmsg into rpmsg-ti-linux...
[rpmsg/rpmsg.git] / fs / filesystems.c
1 // SPDX-License-Identifier: GPL-2.0
2 /*
3  *  linux/fs/filesystems.c
4  *
5  *  Copyright (C) 1991, 1992  Linus Torvalds
6  *
7  *  table of configured filesystems
8  */
10 #include <linux/syscalls.h>
11 #include <linux/fs.h>
12 #include <linux/proc_fs.h>
13 #include <linux/seq_file.h>
14 #include <linux/kmod.h>
15 #include <linux/init.h>
16 #include <linux/module.h>
17 #include <linux/slab.h>
18 #include <linux/uaccess.h>
20 /*
21  * Handling of filesystem drivers list.
22  * Rules:
23  *      Inclusion to/removals from/scanning of list are protected by spinlock.
24  *      During the unload module must call unregister_filesystem().
25  *      We can access the fields of list element if:
26  *              1) spinlock is held or
27  *              2) we hold the reference to the module.
28  *      The latter can be guaranteed by call of try_module_get(); if it
29  *      returned 0 we must skip the element, otherwise we got the reference.
30  *      Once the reference is obtained we can drop the spinlock.
31  */
33 static struct file_system_type *file_systems;
34 static DEFINE_RWLOCK(file_systems_lock);
36 /* WARNING: This can be used only if we _already_ own a reference */
37 struct file_system_type *get_filesystem(struct file_system_type *fs)
38 {
39         __module_get(fs->owner);
40         return fs;
41 }
43 void put_filesystem(struct file_system_type *fs)
44 {
45         module_put(fs->owner);
46 }
48 static struct file_system_type **find_filesystem(const char *name, unsigned len)
49 {
50         struct file_system_type **p;
51         for (p = &file_systems; *p; p = &(*p)->next)
52                 if (strncmp((*p)->name, name, len) == 0 &&
53                     !(*p)->name[len])
54                         break;
55         return p;
56 }
58 /**
59  *      register_filesystem - register a new filesystem
60  *      @fs: the file system structure
61  *
62  *      Adds the file system passed to the list of file systems the kernel
63  *      is aware of for mount and other syscalls. Returns 0 on success,
64  *      or a negative errno code on an error.
65  *
66  *      The &struct file_system_type that is passed is linked into the kernel 
67  *      structures and must not be freed until the file system has been
68  *      unregistered.
69  */
70  
71 int register_filesystem(struct file_system_type * fs)
72 {
73         int res = 0;
74         struct file_system_type ** p;
76         BUG_ON(strchr(fs->name, '.'));
77         if (fs->next)
78                 return -EBUSY;
79         write_lock(&file_systems_lock);
80         p = find_filesystem(fs->name, strlen(fs->name));
81         if (*p)
82                 res = -EBUSY;
83         else
84                 *p = fs;
85         write_unlock(&file_systems_lock);
86         return res;
87 }
89 EXPORT_SYMBOL(register_filesystem);
91 /**
92  *      unregister_filesystem - unregister a file system
93  *      @fs: filesystem to unregister
94  *
95  *      Remove a file system that was previously successfully registered
96  *      with the kernel. An error is returned if the file system is not found.
97  *      Zero is returned on a success.
98  *      
99  *      Once this function has returned the &struct file_system_type structure
100  *      may be freed or reused.
101  */
102  
103 int unregister_filesystem(struct file_system_type * fs)
105         struct file_system_type ** tmp;
107         write_lock(&file_systems_lock);
108         tmp = &file_systems;
109         while (*tmp) {
110                 if (fs == *tmp) {
111                         *tmp = fs->next;
112                         fs->next = NULL;
113                         write_unlock(&file_systems_lock);
114                         synchronize_rcu();
115                         return 0;
116                 }
117                 tmp = &(*tmp)->next;
118         }
119         write_unlock(&file_systems_lock);
121         return -EINVAL;
124 EXPORT_SYMBOL(unregister_filesystem);
126 #ifdef CONFIG_SYSFS_SYSCALL
127 static int fs_index(const char __user * __name)
129         struct file_system_type * tmp;
130         struct filename *name;
131         int err, index;
133         name = getname(__name);
134         err = PTR_ERR(name);
135         if (IS_ERR(name))
136                 return err;
138         err = -EINVAL;
139         read_lock(&file_systems_lock);
140         for (tmp=file_systems, index=0 ; tmp ; tmp=tmp->next, index++) {
141                 if (strcmp(tmp->name, name->name) == 0) {
142                         err = index;
143                         break;
144                 }
145         }
146         read_unlock(&file_systems_lock);
147         putname(name);
148         return err;
151 static int fs_name(unsigned int index, char __user * buf)
153         struct file_system_type * tmp;
154         int len, res;
156         read_lock(&file_systems_lock);
157         for (tmp = file_systems; tmp; tmp = tmp->next, index--)
158                 if (index <= 0 && try_module_get(tmp->owner))
159                         break;
160         read_unlock(&file_systems_lock);
161         if (!tmp)
162                 return -EINVAL;
164         /* OK, we got the reference, so we can safely block */
165         len = strlen(tmp->name) + 1;
166         res = copy_to_user(buf, tmp->name, len) ? -EFAULT : 0;
167         put_filesystem(tmp);
168         return res;
171 static int fs_maxindex(void)
173         struct file_system_type * tmp;
174         int index;
176         read_lock(&file_systems_lock);
177         for (tmp = file_systems, index = 0 ; tmp ; tmp = tmp->next, index++)
178                 ;
179         read_unlock(&file_systems_lock);
180         return index;
183 /*
184  * Whee.. Weird sysv syscall. 
185  */
186 SYSCALL_DEFINE3(sysfs, int, option, unsigned long, arg1, unsigned long, arg2)
188         int retval = -EINVAL;
190         switch (option) {
191                 case 1:
192                         retval = fs_index((const char __user *) arg1);
193                         break;
195                 case 2:
196                         retval = fs_name(arg1, (char __user *) arg2);
197                         break;
199                 case 3:
200                         retval = fs_maxindex();
201                         break;
202         }
203         return retval;
205 #endif
207 int __init get_filesystem_list(char *buf)
209         int len = 0;
210         struct file_system_type * tmp;
212         read_lock(&file_systems_lock);
213         tmp = file_systems;
214         while (tmp && len < PAGE_SIZE - 80) {
215                 len += sprintf(buf+len, "%s\t%s\n",
216                         (tmp->fs_flags & FS_REQUIRES_DEV) ? "" : "nodev",
217                         tmp->name);
218                 tmp = tmp->next;
219         }
220         read_unlock(&file_systems_lock);
221         return len;
224 #ifdef CONFIG_PROC_FS
225 static int filesystems_proc_show(struct seq_file *m, void *v)
227         struct file_system_type * tmp;
229         read_lock(&file_systems_lock);
230         tmp = file_systems;
231         while (tmp) {
232                 seq_printf(m, "%s\t%s\n",
233                         (tmp->fs_flags & FS_REQUIRES_DEV) ? "" : "nodev",
234                         tmp->name);
235                 tmp = tmp->next;
236         }
237         read_unlock(&file_systems_lock);
238         return 0;
241 static int __init proc_filesystems_init(void)
243         proc_create_single("filesystems", 0, NULL, filesystems_proc_show);
244         return 0;
246 module_init(proc_filesystems_init);
247 #endif
249 static struct file_system_type *__get_fs_type(const char *name, int len)
251         struct file_system_type *fs;
253         read_lock(&file_systems_lock);
254         fs = *(find_filesystem(name, len));
255         if (fs && !try_module_get(fs->owner))
256                 fs = NULL;
257         read_unlock(&file_systems_lock);
258         return fs;
261 struct file_system_type *get_fs_type(const char *name)
263         struct file_system_type *fs;
264         const char *dot = strchr(name, '.');
265         int len = dot ? dot - name : strlen(name);
267         fs = __get_fs_type(name, len);
268         if (!fs && (request_module("fs-%.*s", len, name) == 0)) {
269                 fs = __get_fs_type(name, len);
270                 WARN_ONCE(!fs, "request_module fs-%.*s succeeded, but still no fs?\n", len, name);
271         }
273         if (dot && fs && !(fs->fs_flags & FS_HAS_SUBTYPE)) {
274                 put_filesystem(fs);
275                 fs = NULL;
276         }
277         return fs;
280 EXPORT_SYMBOL(get_fs_type);