1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3 * nilfs.h - NILFS local header file.
4 *
5 * Copyright (C) 2005-2008 Nippon Telegraph and Telephone Corporation.
6 *
7 * Written by Koji Sato and Ryusuke Konishi.
8 */
10 #ifndef _NILFS_H
11 #define _NILFS_H
13 #include <linux/kernel.h>
14 #include <linux/buffer_head.h>
15 #include <linux/spinlock.h>
16 #include <linux/blkdev.h>
17 #include <linux/nilfs2_api.h>
18 #include <linux/nilfs2_ondisk.h>
19 #include "the_nilfs.h"
20 #include "bmap.h"
22 /**
23 * struct nilfs_inode_info - nilfs inode data in memory
24 * @i_flags: inode flags
25 * @i_state: dynamic state flags
26 * @i_bmap: pointer on i_bmap_data
27 * @i_bmap_data: raw block mapping
28 * @i_xattr: <TODO>
29 * @i_dir_start_lookup: page index of last successful search
30 * @i_cno: checkpoint number for GC inode
31 * @i_btnode_cache: cached pages of b-tree nodes
32 * @i_dirty: list for connecting dirty files
33 * @xattr_sem: semaphore for extended attributes processing
34 * @i_bh: buffer contains disk inode
35 * @i_root: root object of the current filesystem tree
36 * @vfs_inode: VFS inode object
37 */
38 struct nilfs_inode_info {
39 __u32 i_flags;
40 unsigned long i_state; /* Dynamic state flags */
41 struct nilfs_bmap *i_bmap;
42 struct nilfs_bmap i_bmap_data;
43 __u64 i_xattr; /* sector_t ??? */
44 __u32 i_dir_start_lookup;
45 __u64 i_cno; /* check point number for GC inode */
46 struct address_space i_btnode_cache;
47 struct list_head i_dirty; /* List for connecting dirty files */
49 #ifdef CONFIG_NILFS_XATTR
50 /*
51 * Extended attributes can be read independently of the main file
52 * data. Taking i_sem even when reading would cause contention
53 * between readers of EAs and writers of regular file data, so
54 * instead we synchronize on xattr_sem when reading or changing
55 * EAs.
56 */
57 struct rw_semaphore xattr_sem;
58 #endif
59 struct buffer_head *i_bh; /*
60 * i_bh contains a new or dirty
61 * disk inode.
62 */
63 struct nilfs_root *i_root;
64 struct inode vfs_inode;
65 };
67 static inline struct nilfs_inode_info *NILFS_I(const struct inode *inode)
68 {
69 return container_of(inode, struct nilfs_inode_info, vfs_inode);
70 }
72 static inline struct nilfs_inode_info *
73 NILFS_BMAP_I(const struct nilfs_bmap *bmap)
74 {
75 return container_of(bmap, struct nilfs_inode_info, i_bmap_data);
76 }
78 static inline struct inode *NILFS_BTNC_I(struct address_space *btnc)
79 {
80 struct nilfs_inode_info *ii =
81 container_of(btnc, struct nilfs_inode_info, i_btnode_cache);
82 return &ii->vfs_inode;
83 }
85 /*
86 * Dynamic state flags of NILFS on-memory inode (i_state)
87 */
88 enum {
89 NILFS_I_NEW = 0, /* Inode is newly created */
90 NILFS_I_DIRTY, /* The file is dirty */
91 NILFS_I_QUEUED, /* inode is in dirty_files list */
92 NILFS_I_BUSY, /*
93 * Inode is grabbed by a segment
94 * constructor
95 */
96 NILFS_I_COLLECTED, /* All dirty blocks are collected */
97 NILFS_I_UPDATED, /* The file has been written back */
98 NILFS_I_INODE_SYNC, /* dsync is not allowed for inode */
99 NILFS_I_BMAP, /* has bmap and btnode_cache */
100 NILFS_I_GCINODE, /* inode for GC, on memory only */
101 };
103 /*
104 * commit flags for nilfs_commit_super and nilfs_sync_super
105 */
106 enum {
107 NILFS_SB_COMMIT = 0, /* Commit a super block alternately */
108 NILFS_SB_COMMIT_ALL /* Commit both super blocks */
109 };
111 /*
112 * Macros to check inode numbers
113 */
114 #define NILFS_MDT_INO_BITS \
115 (BIT(NILFS_DAT_INO) | BIT(NILFS_CPFILE_INO) | \
116 BIT(NILFS_SUFILE_INO) | BIT(NILFS_IFILE_INO) | \
117 BIT(NILFS_ATIME_INO) | BIT(NILFS_SKETCH_INO))
119 #define NILFS_SYS_INO_BITS (BIT(NILFS_ROOT_INO) | NILFS_MDT_INO_BITS)
121 #define NILFS_FIRST_INO(sb) (((struct the_nilfs *)sb->s_fs_info)->ns_first_ino)
123 #define NILFS_MDT_INODE(sb, ino) \
124 ((ino) < NILFS_FIRST_INO(sb) && (NILFS_MDT_INO_BITS & BIT(ino)))
125 #define NILFS_VALID_INODE(sb, ino) \
126 ((ino) >= NILFS_FIRST_INO(sb) || (NILFS_SYS_INO_BITS & BIT(ino)))
128 /**
129 * struct nilfs_transaction_info: context information for synchronization
130 * @ti_magic: Magic number
131 * @ti_save: Backup of journal_info field of task_struct
132 * @ti_flags: Flags
133 * @ti_count: Nest level
134 */
135 struct nilfs_transaction_info {
136 u32 ti_magic;
137 void *ti_save;
138 /*
139 * This should never be used. If it happens,
140 * one of other filesystems has a bug.
141 */
142 unsigned short ti_flags;
143 unsigned short ti_count;
144 };
146 /* ti_magic */
147 #define NILFS_TI_MAGIC 0xd9e392fb
149 /* ti_flags */
150 #define NILFS_TI_DYNAMIC_ALLOC 0x0001 /* Allocated from slab */
151 #define NILFS_TI_SYNC 0x0002 /*
152 * Force to construct segment at the
153 * end of transaction.
154 */
155 #define NILFS_TI_GC 0x0004 /* GC context */
156 #define NILFS_TI_COMMIT 0x0008 /* Change happened or not */
157 #define NILFS_TI_WRITER 0x0010 /* Constructor context */
160 int nilfs_transaction_begin(struct super_block *,
161 struct nilfs_transaction_info *, int);
162 int nilfs_transaction_commit(struct super_block *);
163 void nilfs_transaction_abort(struct super_block *);
165 static inline void nilfs_set_transaction_flag(unsigned int flag)
166 {
167 struct nilfs_transaction_info *ti = current->journal_info;
169 ti->ti_flags |= flag;
170 }
172 static inline int nilfs_test_transaction_flag(unsigned int flag)
173 {
174 struct nilfs_transaction_info *ti = current->journal_info;
176 if (ti == NULL || ti->ti_magic != NILFS_TI_MAGIC)
177 return 0;
178 return !!(ti->ti_flags & flag);
179 }
181 static inline int nilfs_doing_gc(void)
182 {
183 return nilfs_test_transaction_flag(NILFS_TI_GC);
184 }
186 static inline int nilfs_doing_construction(void)
187 {
188 return nilfs_test_transaction_flag(NILFS_TI_WRITER);
189 }
191 /*
192 * function prototype
193 */
194 #ifdef CONFIG_NILFS_POSIX_ACL
195 #error "NILFS: not yet supported POSIX ACL"
196 extern int nilfs_acl_chmod(struct inode *);
197 extern int nilfs_init_acl(struct inode *, struct inode *);
198 #else
199 static inline int nilfs_acl_chmod(struct inode *inode)
200 {
201 return 0;
202 }
204 static inline int nilfs_init_acl(struct inode *inode, struct inode *dir)
205 {
206 inode->i_mode &= ~current_umask();
207 return 0;
208 }
209 #endif
211 #define NILFS_ATIME_DISABLE
213 /* Flags that should be inherited by new inodes from their parent. */
214 #define NILFS_FL_INHERITED \
215 (FS_SECRM_FL | FS_UNRM_FL | FS_COMPR_FL | FS_SYNC_FL | \
216 FS_IMMUTABLE_FL | FS_APPEND_FL | FS_NODUMP_FL | FS_NOATIME_FL |\
217 FS_COMPRBLK_FL | FS_NOCOMP_FL | FS_NOTAIL_FL | FS_DIRSYNC_FL)
219 /* Mask out flags that are inappropriate for the given type of inode. */
220 static inline __u32 nilfs_mask_flags(umode_t mode, __u32 flags)
221 {
222 if (S_ISDIR(mode))
223 return flags;
224 else if (S_ISREG(mode))
225 return flags & ~(FS_DIRSYNC_FL | FS_TOPDIR_FL);
226 else
227 return flags & (FS_NODUMP_FL | FS_NOATIME_FL);
228 }
230 /* dir.c */
231 extern int nilfs_add_link(struct dentry *, struct inode *);
232 extern ino_t nilfs_inode_by_name(struct inode *, const struct qstr *);
233 extern int nilfs_make_empty(struct inode *, struct inode *);
234 extern struct nilfs_dir_entry *
235 nilfs_find_entry(struct inode *, const struct qstr *, struct page **);
236 extern int nilfs_delete_entry(struct nilfs_dir_entry *, struct page *);
237 extern int nilfs_empty_dir(struct inode *);
238 extern struct nilfs_dir_entry *nilfs_dotdot(struct inode *, struct page **);
239 extern void nilfs_set_link(struct inode *, struct nilfs_dir_entry *,
240 struct page *, struct inode *);
242 /* file.c */
243 extern int nilfs_sync_file(struct file *, loff_t, loff_t, int);
245 /* ioctl.c */
246 long nilfs_ioctl(struct file *, unsigned int, unsigned long);
247 long nilfs_compat_ioctl(struct file *file, unsigned int cmd, unsigned long arg);
248 int nilfs_ioctl_prepare_clean_segments(struct the_nilfs *, struct nilfs_argv *,
249 void **);
251 /* inode.c */
252 void nilfs_inode_add_blocks(struct inode *inode, int n);
253 void nilfs_inode_sub_blocks(struct inode *inode, int n);
254 extern struct inode *nilfs_new_inode(struct inode *, umode_t);
255 extern void nilfs_free_inode(struct inode *);
256 extern int nilfs_get_block(struct inode *, sector_t, struct buffer_head *, int);
257 extern void nilfs_set_inode_flags(struct inode *);
258 extern int nilfs_read_inode_common(struct inode *, struct nilfs_inode *);
259 extern void nilfs_write_inode_common(struct inode *, struct nilfs_inode *, int);
260 struct inode *nilfs_ilookup(struct super_block *sb, struct nilfs_root *root,
261 unsigned long ino);
262 struct inode *nilfs_iget_locked(struct super_block *sb, struct nilfs_root *root,
263 unsigned long ino);
264 struct inode *nilfs_iget(struct super_block *sb, struct nilfs_root *root,
265 unsigned long ino);
266 extern struct inode *nilfs_iget_for_gc(struct super_block *sb,
267 unsigned long ino, __u64 cno);
268 extern void nilfs_update_inode(struct inode *, struct buffer_head *, int);
269 extern void nilfs_truncate(struct inode *);
270 extern void nilfs_evict_inode(struct inode *);
271 extern int nilfs_setattr(struct dentry *, struct iattr *);
272 extern void nilfs_write_failed(struct address_space *mapping, loff_t to);
273 int nilfs_permission(struct inode *inode, int mask);
274 int nilfs_load_inode_block(struct inode *inode, struct buffer_head **pbh);
275 extern int nilfs_inode_dirty(struct inode *);
276 int nilfs_set_file_dirty(struct inode *inode, unsigned int nr_dirty);
277 extern int __nilfs_mark_inode_dirty(struct inode *, int);
278 extern void nilfs_dirty_inode(struct inode *, int flags);
279 int nilfs_fiemap(struct inode *inode, struct fiemap_extent_info *fieinfo,
280 __u64 start, __u64 len);
281 static inline int nilfs_mark_inode_dirty(struct inode *inode)
282 {
283 return __nilfs_mark_inode_dirty(inode, I_DIRTY);
284 }
285 static inline int nilfs_mark_inode_dirty_sync(struct inode *inode)
286 {
287 return __nilfs_mark_inode_dirty(inode, I_DIRTY_SYNC);
288 }
290 /* super.c */
291 extern struct inode *nilfs_alloc_inode(struct super_block *);
292 extern void nilfs_destroy_inode(struct inode *);
294 extern __printf(3, 4)
295 void __nilfs_msg(struct super_block *sb, const char *level,
296 const char *fmt, ...);
297 extern __printf(3, 4)
298 void __nilfs_error(struct super_block *sb, const char *function,
299 const char *fmt, ...);
301 #ifdef CONFIG_PRINTK
303 #define nilfs_msg(sb, level, fmt, ...) \
304 __nilfs_msg(sb, level, fmt, ##__VA_ARGS__)
305 #define nilfs_error(sb, fmt, ...) \
306 __nilfs_error(sb, __func__, fmt, ##__VA_ARGS__)
308 #else
310 #define nilfs_msg(sb, level, fmt, ...) \
311 do { \
312 no_printk(fmt, ##__VA_ARGS__); \
313 (void)(sb); \
314 } while (0)
315 #define nilfs_error(sb, fmt, ...) \
316 do { \
317 no_printk(fmt, ##__VA_ARGS__); \
318 __nilfs_error(sb, "", " "); \
319 } while (0)
321 #endif /* CONFIG_PRINTK */
323 extern struct nilfs_super_block *
324 nilfs_read_super_block(struct super_block *, u64, int, struct buffer_head **);
325 extern int nilfs_store_magic_and_option(struct super_block *,
326 struct nilfs_super_block *, char *);
327 extern int nilfs_check_feature_compatibility(struct super_block *,
328 struct nilfs_super_block *);
329 extern void nilfs_set_log_cursor(struct nilfs_super_block *,
330 struct the_nilfs *);
331 struct nilfs_super_block **nilfs_prepare_super(struct super_block *sb,
332 int flip);
333 int nilfs_commit_super(struct super_block *sb, int flag);
334 int nilfs_cleanup_super(struct super_block *sb);
335 int nilfs_resize_fs(struct super_block *sb, __u64 newsize);
336 int nilfs_attach_checkpoint(struct super_block *sb, __u64 cno, int curr_mnt,
337 struct nilfs_root **root);
338 int nilfs_checkpoint_is_mounted(struct super_block *sb, __u64 cno);
340 /* gcinode.c */
341 int nilfs_gccache_submit_read_data(struct inode *, sector_t, sector_t, __u64,
342 struct buffer_head **);
343 int nilfs_gccache_submit_read_node(struct inode *, sector_t, __u64,
344 struct buffer_head **);
345 int nilfs_gccache_wait_and_mark_dirty(struct buffer_head *);
346 int nilfs_init_gcinode(struct inode *inode);
347 void nilfs_remove_all_gcinodes(struct the_nilfs *nilfs);
349 /* sysfs.c */
350 int __init nilfs_sysfs_init(void);
351 void nilfs_sysfs_exit(void);
352 int nilfs_sysfs_create_device_group(struct super_block *);
353 void nilfs_sysfs_delete_device_group(struct the_nilfs *);
354 int nilfs_sysfs_create_snapshot_group(struct nilfs_root *);
355 void nilfs_sysfs_delete_snapshot_group(struct nilfs_root *);
357 /*
358 * Inodes and files operations
359 */
360 extern const struct file_operations nilfs_dir_operations;
361 extern const struct inode_operations nilfs_file_inode_operations;
362 extern const struct file_operations nilfs_file_operations;
363 extern const struct address_space_operations nilfs_aops;
364 extern const struct inode_operations nilfs_dir_inode_operations;
365 extern const struct inode_operations nilfs_special_inode_operations;
366 extern const struct inode_operations nilfs_symlink_inode_operations;
368 /*
369 * filesystem type
370 */
371 extern struct file_system_type nilfs_fs_type;
374 #endif /* _NILFS_H */