1 /* -*- mode: c; c-basic-offset: 8; -*-
2 * vim: noexpandtab sw=8 ts=8 sts=0:
3 *
4 * io.c
5 *
6 * Buffer cache handling
7 *
8 * Copyright (C) 2002, 2004 Oracle. All rights reserved.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public
12 * License as published by the Free Software Foundation; either
13 * version 2 of the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
18 * General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public
21 * License along with this program; if not, write to the
22 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
23 * Boston, MA 021110-1307, USA.
24 */
26 #include <linux/fs.h>
27 #include <linux/types.h>
28 #include <linux/highmem.h>
29 #include <linux/bio.h>
31 #include <cluster/masklog.h>
33 #include "ocfs2.h"
35 #include "alloc.h"
36 #include "inode.h"
37 #include "journal.h"
38 #include "uptodate.h"
39 #include "buffer_head_io.h"
40 #include "ocfs2_trace.h"
42 /*
43 * Bits on bh->b_state used by ocfs2.
44 *
45 * These MUST be after the JBD2 bits. Hence, we use BH_JBDPrivateStart.
46 */
47 enum ocfs2_state_bits {
48 BH_NeedsValidate = BH_JBDPrivateStart,
49 };
51 /* Expand the magic b_state functions */
52 BUFFER_FNS(NeedsValidate, needs_validate);
54 int ocfs2_write_block(struct ocfs2_super *osb, struct buffer_head *bh,
55 struct ocfs2_caching_info *ci)
56 {
57 int ret = 0;
59 trace_ocfs2_write_block((unsigned long long)bh->b_blocknr, ci);
61 BUG_ON(bh->b_blocknr < OCFS2_SUPER_BLOCK_BLKNO);
62 BUG_ON(buffer_jbd(bh));
64 /* No need to check for a soft readonly file system here. non
65 * journalled writes are only ever done on system files which
66 * can get modified during recovery even if read-only. */
67 if (ocfs2_is_hard_readonly(osb)) {
68 ret = -EROFS;
69 mlog_errno(ret);
70 goto out;
71 }
73 ocfs2_metadata_cache_io_lock(ci);
75 lock_buffer(bh);
76 set_buffer_uptodate(bh);
78 /* remove from dirty list before I/O. */
79 clear_buffer_dirty(bh);
81 get_bh(bh); /* for end_buffer_write_sync() */
82 bh->b_end_io = end_buffer_write_sync;
83 submit_bh(REQ_OP_WRITE, 0, bh);
85 wait_on_buffer(bh);
87 if (buffer_uptodate(bh)) {
88 ocfs2_set_buffer_uptodate(ci, bh);
89 } else {
90 /* We don't need to remove the clustered uptodate
91 * information for this bh as it's not marked locally
92 * uptodate. */
93 ret = -EIO;
94 mlog_errno(ret);
95 }
97 ocfs2_metadata_cache_io_unlock(ci);
98 out:
99 return ret;
100 }
102 int ocfs2_read_blocks_sync(struct ocfs2_super *osb, u64 block,
103 unsigned int nr, struct buffer_head *bhs[])
104 {
105 int status = 0;
106 unsigned int i;
107 struct buffer_head *bh;
109 trace_ocfs2_read_blocks_sync((unsigned long long)block, nr);
111 if (!nr)
112 goto bail;
114 for (i = 0 ; i < nr ; i++) {
115 if (bhs[i] == NULL) {
116 bhs[i] = sb_getblk(osb->sb, block++);
117 if (bhs[i] == NULL) {
118 status = -ENOMEM;
119 mlog_errno(status);
120 goto bail;
121 }
122 }
123 bh = bhs[i];
125 if (buffer_jbd(bh)) {
126 trace_ocfs2_read_blocks_sync_jbd(
127 (unsigned long long)bh->b_blocknr);
128 continue;
129 }
131 if (buffer_dirty(bh)) {
132 /* This should probably be a BUG, or
133 * at least return an error. */
134 mlog(ML_ERROR,
135 "trying to sync read a dirty "
136 "buffer! (blocknr = %llu), skipping\n",
137 (unsigned long long)bh->b_blocknr);
138 continue;
139 }
141 lock_buffer(bh);
142 if (buffer_jbd(bh)) {
143 #ifdef CATCH_BH_JBD_RACES
144 mlog(ML_ERROR,
145 "block %llu had the JBD bit set "
146 "while I was in lock_buffer!",
147 (unsigned long long)bh->b_blocknr);
148 BUG();
149 #else
150 unlock_buffer(bh);
151 continue;
152 #endif
153 }
155 clear_buffer_uptodate(bh);
156 get_bh(bh); /* for end_buffer_read_sync() */
157 bh->b_end_io = end_buffer_read_sync;
158 submit_bh(REQ_OP_READ, 0, bh);
159 }
161 for (i = nr; i > 0; i--) {
162 bh = bhs[i - 1];
164 /* No need to wait on the buffer if it's managed by JBD. */
165 if (!buffer_jbd(bh))
166 wait_on_buffer(bh);
168 if (!buffer_uptodate(bh)) {
169 /* Status won't be cleared from here on out,
170 * so we can safely record this and loop back
171 * to cleanup the other buffers. */
172 status = -EIO;
173 put_bh(bh);
174 bhs[i - 1] = NULL;
175 }
176 }
178 bail:
179 return status;
180 }
182 int ocfs2_read_blocks(struct ocfs2_caching_info *ci, u64 block, int nr,
183 struct buffer_head *bhs[], int flags,
184 int (*validate)(struct super_block *sb,
185 struct buffer_head *bh))
186 {
187 int status = 0;
188 int i, ignore_cache = 0;
189 struct buffer_head *bh;
190 struct super_block *sb = ocfs2_metadata_cache_get_super(ci);
192 trace_ocfs2_read_blocks_begin(ci, (unsigned long long)block, nr, flags);
194 BUG_ON(!ci);
195 BUG_ON((flags & OCFS2_BH_READAHEAD) &&
196 (flags & OCFS2_BH_IGNORE_CACHE));
198 if (bhs == NULL) {
199 status = -EINVAL;
200 mlog_errno(status);
201 goto bail;
202 }
204 if (nr < 0) {
205 mlog(ML_ERROR, "asked to read %d blocks!\n", nr);
206 status = -EINVAL;
207 mlog_errno(status);
208 goto bail;
209 }
211 if (nr == 0) {
212 status = 0;
213 goto bail;
214 }
216 ocfs2_metadata_cache_io_lock(ci);
217 for (i = 0 ; i < nr ; i++) {
218 if (bhs[i] == NULL) {
219 bhs[i] = sb_getblk(sb, block++);
220 if (bhs[i] == NULL) {
221 ocfs2_metadata_cache_io_unlock(ci);
222 status = -ENOMEM;
223 mlog_errno(status);
224 goto bail;
225 }
226 }
227 bh = bhs[i];
228 ignore_cache = (flags & OCFS2_BH_IGNORE_CACHE);
230 /* There are three read-ahead cases here which we need to
231 * be concerned with. All three assume a buffer has
232 * previously been submitted with OCFS2_BH_READAHEAD
233 * and it hasn't yet completed I/O.
234 *
235 * 1) The current request is sync to disk. This rarely
236 * happens these days, and never when performance
237 * matters - the code can just wait on the buffer
238 * lock and re-submit.
239 *
240 * 2) The current request is cached, but not
241 * readahead. ocfs2_buffer_uptodate() will return
242 * false anyway, so we'll wind up waiting on the
243 * buffer lock to do I/O. We re-check the request
244 * with after getting the lock to avoid a re-submit.
245 *
246 * 3) The current request is readahead (and so must
247 * also be a caching one). We short circuit if the
248 * buffer is locked (under I/O) and if it's in the
249 * uptodate cache. The re-check from #2 catches the
250 * case that the previous read-ahead completes just
251 * before our is-it-in-flight check.
252 */
254 if (!ignore_cache && !ocfs2_buffer_uptodate(ci, bh)) {
255 trace_ocfs2_read_blocks_from_disk(
256 (unsigned long long)bh->b_blocknr,
257 (unsigned long long)ocfs2_metadata_cache_owner(ci));
258 /* We're using ignore_cache here to say
259 * "go to disk" */
260 ignore_cache = 1;
261 }
263 trace_ocfs2_read_blocks_bh((unsigned long long)bh->b_blocknr,
264 ignore_cache, buffer_jbd(bh), buffer_dirty(bh));
266 if (buffer_jbd(bh)) {
267 continue;
268 }
270 if (ignore_cache) {
271 if (buffer_dirty(bh)) {
272 /* This should probably be a BUG, or
273 * at least return an error. */
274 continue;
275 }
277 /* A read-ahead request was made - if the
278 * buffer is already under read-ahead from a
279 * previously submitted request than we are
280 * done here. */
281 if ((flags & OCFS2_BH_READAHEAD)
282 && ocfs2_buffer_read_ahead(ci, bh))
283 continue;
285 lock_buffer(bh);
286 if (buffer_jbd(bh)) {
287 #ifdef CATCH_BH_JBD_RACES
288 mlog(ML_ERROR, "block %llu had the JBD bit set "
289 "while I was in lock_buffer!",
290 (unsigned long long)bh->b_blocknr);
291 BUG();
292 #else
293 unlock_buffer(bh);
294 continue;
295 #endif
296 }
298 /* Re-check ocfs2_buffer_uptodate() as a
299 * previously read-ahead buffer may have
300 * completed I/O while we were waiting for the
301 * buffer lock. */
302 if (!(flags & OCFS2_BH_IGNORE_CACHE)
303 && !(flags & OCFS2_BH_READAHEAD)
304 && ocfs2_buffer_uptodate(ci, bh)) {
305 unlock_buffer(bh);
306 continue;
307 }
309 clear_buffer_uptodate(bh);
310 get_bh(bh); /* for end_buffer_read_sync() */
311 if (validate)
312 set_buffer_needs_validate(bh);
313 bh->b_end_io = end_buffer_read_sync;
314 submit_bh(REQ_OP_READ, 0, bh);
315 continue;
316 }
317 }
319 status = 0;
321 for (i = (nr - 1); i >= 0; i--) {
322 bh = bhs[i];
324 if (!(flags & OCFS2_BH_READAHEAD)) {
325 if (status) {
326 /* Clear the rest of the buffers on error */
327 put_bh(bh);
328 bhs[i] = NULL;
329 continue;
330 }
331 /* We know this can't have changed as we hold the
332 * owner sem. Avoid doing any work on the bh if the
333 * journal has it. */
334 if (!buffer_jbd(bh))
335 wait_on_buffer(bh);
337 if (!buffer_uptodate(bh)) {
338 /* Status won't be cleared from here on out,
339 * so we can safely record this and loop back
340 * to cleanup the other buffers. Don't need to
341 * remove the clustered uptodate information
342 * for this bh as it's not marked locally
343 * uptodate. */
344 status = -EIO;
345 clear_buffer_needs_validate(bh);
346 put_bh(bh);
347 bhs[i] = NULL;
348 continue;
349 }
351 if (buffer_needs_validate(bh)) {
352 /* We never set NeedsValidate if the
353 * buffer was held by the journal, so
354 * that better not have changed */
355 BUG_ON(buffer_jbd(bh));
356 clear_buffer_needs_validate(bh);
357 status = validate(sb, bh);
358 if (status) {
359 put_bh(bh);
360 bhs[i] = NULL;
361 continue;
362 }
363 }
364 }
366 /* Always set the buffer in the cache, even if it was
367 * a forced read, or read-ahead which hasn't yet
368 * completed. */
369 ocfs2_set_buffer_uptodate(ci, bh);
370 }
371 ocfs2_metadata_cache_io_unlock(ci);
373 trace_ocfs2_read_blocks_end((unsigned long long)block, nr,
374 flags, ignore_cache);
376 bail:
378 return status;
379 }
381 /* Check whether the blkno is the super block or one of the backups. */
382 static void ocfs2_check_super_or_backup(struct super_block *sb,
383 sector_t blkno)
384 {
385 int i;
386 u64 backup_blkno;
388 if (blkno == OCFS2_SUPER_BLOCK_BLKNO)
389 return;
391 for (i = 0; i < OCFS2_MAX_BACKUP_SUPERBLOCKS; i++) {
392 backup_blkno = ocfs2_backup_super_blkno(sb, i);
393 if (backup_blkno == blkno)
394 return;
395 }
397 BUG();
398 }
400 /*
401 * Write super block and backups doesn't need to collaborate with journal,
402 * so we don't need to lock ip_io_mutex and ci doesn't need to bea passed
403 * into this function.
404 */
405 int ocfs2_write_super_or_backup(struct ocfs2_super *osb,
406 struct buffer_head *bh)
407 {
408 int ret = 0;
409 struct ocfs2_dinode *di = (struct ocfs2_dinode *)bh->b_data;
411 BUG_ON(buffer_jbd(bh));
412 ocfs2_check_super_or_backup(osb->sb, bh->b_blocknr);
414 if (ocfs2_is_hard_readonly(osb) || ocfs2_is_soft_readonly(osb)) {
415 ret = -EROFS;
416 mlog_errno(ret);
417 goto out;
418 }
420 lock_buffer(bh);
421 set_buffer_uptodate(bh);
423 /* remove from dirty list before I/O. */
424 clear_buffer_dirty(bh);
426 get_bh(bh); /* for end_buffer_write_sync() */
427 bh->b_end_io = end_buffer_write_sync;
428 ocfs2_compute_meta_ecc(osb->sb, bh->b_data, &di->i_check);
429 submit_bh(REQ_OP_WRITE, 0, bh);
431 wait_on_buffer(bh);
433 if (!buffer_uptodate(bh)) {
434 ret = -EIO;
435 mlog_errno(ret);
436 }
438 out:
439 return ret;
440 }