]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - kernel/panic.c
Revert "HACK: ARM: dts: dra7-ipu-common: Revert to CMA pools for IPU early boots"
[rpmsg/rpmsg.git] / kernel / panic.c
1 /*
2  *  linux/kernel/panic.c
3  *
4  *  Copyright (C) 1991, 1992  Linus Torvalds
5  */
7 /*
8  * This function is used through-out the kernel (including mm and fs)
9  * to indicate a major problem.
10  */
11 #include <linux/debug_locks.h>
12 #include <linux/sched/debug.h>
13 #include <linux/interrupt.h>
14 #include <linux/kmsg_dump.h>
15 #include <linux/kallsyms.h>
16 #include <linux/notifier.h>
17 #include <linux/module.h>
18 #include <linux/random.h>
19 #include <linux/ftrace.h>
20 #include <linux/reboot.h>
21 #include <linux/delay.h>
22 #include <linux/kexec.h>
23 #include <linux/sched.h>
24 #include <linux/sysrq.h>
25 #include <linux/init.h>
26 #include <linux/nmi.h>
27 #include <linux/console.h>
28 #include <linux/bug.h>
29 #include <linux/ratelimit.h>
30 #include <linux/debugfs.h>
31 #include <asm/sections.h>
33 #define PANIC_TIMER_STEP 100
34 #define PANIC_BLINK_SPD 18
36 int panic_on_oops = CONFIG_PANIC_ON_OOPS_VALUE;
37 static unsigned long tainted_mask =
38         IS_ENABLED(CONFIG_GCC_PLUGIN_RANDSTRUCT) ? (1 << TAINT_RANDSTRUCT) : 0;
39 static int pause_on_oops;
40 static int pause_on_oops_flag;
41 static DEFINE_SPINLOCK(pause_on_oops_lock);
42 bool crash_kexec_post_notifiers;
43 int panic_on_warn __read_mostly;
45 int panic_timeout = CONFIG_PANIC_TIMEOUT;
46 EXPORT_SYMBOL_GPL(panic_timeout);
48 ATOMIC_NOTIFIER_HEAD(panic_notifier_list);
50 EXPORT_SYMBOL(panic_notifier_list);
52 static long no_blink(int state)
53 {
54         return 0;
55 }
57 /* Returns how long it waited in ms */
58 long (*panic_blink)(int state);
59 EXPORT_SYMBOL(panic_blink);
61 /*
62  * Stop ourself in panic -- architecture code may override this
63  */
64 void __weak panic_smp_self_stop(void)
65 {
66         while (1)
67                 cpu_relax();
68 }
70 /*
71  * Stop ourselves in NMI context if another CPU has already panicked. Arch code
72  * may override this to prepare for crash dumping, e.g. save regs info.
73  */
74 void __weak nmi_panic_self_stop(struct pt_regs *regs)
75 {
76         panic_smp_self_stop();
77 }
79 /*
80  * Stop other CPUs in panic.  Architecture dependent code may override this
81  * with more suitable version.  For example, if the architecture supports
82  * crash dump, it should save registers of each stopped CPU and disable
83  * per-CPU features such as virtualization extensions.
84  */
85 void __weak crash_smp_send_stop(void)
86 {
87         static int cpus_stopped;
89         /*
90          * This function can be called twice in panic path, but obviously
91          * we execute this only once.
92          */
93         if (cpus_stopped)
94                 return;
96         /*
97          * Note smp_send_stop is the usual smp shutdown function, which
98          * unfortunately means it may not be hardened to work in a panic
99          * situation.
100          */
101         smp_send_stop();
102         cpus_stopped = 1;
105 atomic_t panic_cpu = ATOMIC_INIT(PANIC_CPU_INVALID);
107 /*
108  * A variant of panic() called from NMI context. We return if we've already
109  * panicked on this CPU. If another CPU already panicked, loop in
110  * nmi_panic_self_stop() which can provide architecture dependent code such
111  * as saving register state for crash dump.
112  */
113 void nmi_panic(struct pt_regs *regs, const char *msg)
115         int old_cpu, cpu;
117         cpu = raw_smp_processor_id();
118         old_cpu = atomic_cmpxchg(&panic_cpu, PANIC_CPU_INVALID, cpu);
120         if (old_cpu == PANIC_CPU_INVALID)
121                 panic("%s", msg);
122         else if (old_cpu != cpu)
123                 nmi_panic_self_stop(regs);
125 EXPORT_SYMBOL(nmi_panic);
127 /**
128  *      panic - halt the system
129  *      @fmt: The text string to print
130  *
131  *      Display a message, then perform cleanups.
132  *
133  *      This function never returns.
134  */
135 void panic(const char *fmt, ...)
137         static char buf[1024];
138         va_list args;
139         long i, i_next = 0;
140         int state = 0;
141         int old_cpu, this_cpu;
142         bool _crash_kexec_post_notifiers = crash_kexec_post_notifiers;
144         /*
145          * Disable local interrupts. This will prevent panic_smp_self_stop
146          * from deadlocking the first cpu that invokes the panic, since
147          * there is nothing to prevent an interrupt handler (that runs
148          * after setting panic_cpu) from invoking panic() again.
149          */
150         local_irq_disable();
152         /*
153          * It's possible to come here directly from a panic-assertion and
154          * not have preempt disabled. Some functions called from here want
155          * preempt to be disabled. No point enabling it later though...
156          *
157          * Only one CPU is allowed to execute the panic code from here. For
158          * multiple parallel invocations of panic, all other CPUs either
159          * stop themself or will wait until they are stopped by the 1st CPU
160          * with smp_send_stop().
161          *
162          * `old_cpu == PANIC_CPU_INVALID' means this is the 1st CPU which
163          * comes here, so go ahead.
164          * `old_cpu == this_cpu' means we came from nmi_panic() which sets
165          * panic_cpu to this CPU.  In this case, this is also the 1st CPU.
166          */
167         this_cpu = raw_smp_processor_id();
168         old_cpu  = atomic_cmpxchg(&panic_cpu, PANIC_CPU_INVALID, this_cpu);
170         if (old_cpu != PANIC_CPU_INVALID && old_cpu != this_cpu)
171                 panic_smp_self_stop();
173         console_verbose();
174         bust_spinlocks(1);
175         va_start(args, fmt);
176         vsnprintf(buf, sizeof(buf), fmt, args);
177         va_end(args);
178         pr_emerg("Kernel panic - not syncing: %s\n", buf);
179 #ifdef CONFIG_DEBUG_BUGVERBOSE
180         /*
181          * Avoid nested stack-dumping if a panic occurs during oops processing
182          */
183         if (!test_taint(TAINT_DIE) && oops_in_progress <= 1)
184                 dump_stack();
185 #endif
187         /*
188          * If we have crashed and we have a crash kernel loaded let it handle
189          * everything else.
190          * If we want to run this after calling panic_notifiers, pass
191          * the "crash_kexec_post_notifiers" option to the kernel.
192          *
193          * Bypass the panic_cpu check and call __crash_kexec directly.
194          */
195         if (!_crash_kexec_post_notifiers) {
196                 printk_safe_flush_on_panic();
197                 __crash_kexec(NULL);
199                 /*
200                  * Note smp_send_stop is the usual smp shutdown function, which
201                  * unfortunately means it may not be hardened to work in a
202                  * panic situation.
203                  */
204                 smp_send_stop();
205         } else {
206                 /*
207                  * If we want to do crash dump after notifier calls and
208                  * kmsg_dump, we will need architecture dependent extra
209                  * works in addition to stopping other CPUs.
210                  */
211                 crash_smp_send_stop();
212         }
214         /*
215          * Run any panic handlers, including those that might need to
216          * add information to the kmsg dump output.
217          */
218         atomic_notifier_call_chain(&panic_notifier_list, 0, buf);
220         /* Call flush even twice. It tries harder with a single online CPU */
221         printk_safe_flush_on_panic();
222         kmsg_dump(KMSG_DUMP_PANIC);
224         /*
225          * If you doubt kdump always works fine in any situation,
226          * "crash_kexec_post_notifiers" offers you a chance to run
227          * panic_notifiers and dumping kmsg before kdump.
228          * Note: since some panic_notifiers can make crashed kernel
229          * more unstable, it can increase risks of the kdump failure too.
230          *
231          * Bypass the panic_cpu check and call __crash_kexec directly.
232          */
233         if (_crash_kexec_post_notifiers)
234                 __crash_kexec(NULL);
236         bust_spinlocks(0);
238         /*
239          * We may have ended up stopping the CPU holding the lock (in
240          * smp_send_stop()) while still having some valuable data in the console
241          * buffer.  Try to acquire the lock then release it regardless of the
242          * result.  The release will also print the buffers out.  Locks debug
243          * should be disabled to avoid reporting bad unlock balance when
244          * panic() is not being callled from OOPS.
245          */
246         debug_locks_off();
247         console_flush_on_panic();
249         if (!panic_blink)
250                 panic_blink = no_blink;
252         if (panic_timeout > 0) {
253                 /*
254                  * Delay timeout seconds before rebooting the machine.
255                  * We can't use the "normal" timers since we just panicked.
256                  */
257                 pr_emerg("Rebooting in %d seconds..\n", panic_timeout);
259                 for (i = 0; i < panic_timeout * 1000; i += PANIC_TIMER_STEP) {
260                         touch_nmi_watchdog();
261                         if (i >= i_next) {
262                                 i += panic_blink(state ^= 1);
263                                 i_next = i + 3600 / PANIC_BLINK_SPD;
264                         }
265                         mdelay(PANIC_TIMER_STEP);
266                 }
267         }
268         if (panic_timeout != 0) {
269                 /*
270                  * This will not be a clean reboot, with everything
271                  * shutting down.  But if there is a chance of
272                  * rebooting the system it will be rebooted.
273                  */
274                 emergency_restart();
275         }
276 #ifdef __sparc__
277         {
278                 extern int stop_a_enabled;
279                 /* Make sure the user can actually press Stop-A (L1-A) */
280                 stop_a_enabled = 1;
281                 pr_emerg("Press Stop-A (L1-A) from sun keyboard or send break\n"
282                          "twice on console to return to the boot prom\n");
283         }
284 #endif
285 #if defined(CONFIG_S390)
286         {
287                 unsigned long caller;
289                 caller = (unsigned long)__builtin_return_address(0);
290                 disabled_wait(caller);
291         }
292 #endif
293         pr_emerg("---[ end Kernel panic - not syncing: %s ]---\n", buf);
294         local_irq_enable();
295         for (i = 0; ; i += PANIC_TIMER_STEP) {
296                 touch_softlockup_watchdog();
297                 if (i >= i_next) {
298                         i += panic_blink(state ^= 1);
299                         i_next = i + 3600 / PANIC_BLINK_SPD;
300                 }
301                 mdelay(PANIC_TIMER_STEP);
302         }
305 EXPORT_SYMBOL(panic);
307 /*
308  * TAINT_FORCED_RMMOD could be a per-module flag but the module
309  * is being removed anyway.
310  */
311 const struct taint_flag taint_flags[TAINT_FLAGS_COUNT] = {
312         [ TAINT_PROPRIETARY_MODULE ]    = { 'P', 'G', true },
313         [ TAINT_FORCED_MODULE ]         = { 'F', ' ', true },
314         [ TAINT_CPU_OUT_OF_SPEC ]       = { 'S', ' ', false },
315         [ TAINT_FORCED_RMMOD ]          = { 'R', ' ', false },
316         [ TAINT_MACHINE_CHECK ]         = { 'M', ' ', false },
317         [ TAINT_BAD_PAGE ]              = { 'B', ' ', false },
318         [ TAINT_USER ]                  = { 'U', ' ', false },
319         [ TAINT_DIE ]                   = { 'D', ' ', false },
320         [ TAINT_OVERRIDDEN_ACPI_TABLE ] = { 'A', ' ', false },
321         [ TAINT_WARN ]                  = { 'W', ' ', false },
322         [ TAINT_CRAP ]                  = { 'C', ' ', true },
323         [ TAINT_FIRMWARE_WORKAROUND ]   = { 'I', ' ', false },
324         [ TAINT_OOT_MODULE ]            = { 'O', ' ', true },
325         [ TAINT_UNSIGNED_MODULE ]       = { 'E', ' ', true },
326         [ TAINT_SOFTLOCKUP ]            = { 'L', ' ', false },
327         [ TAINT_LIVEPATCH ]             = { 'K', ' ', true },
328         [ TAINT_AUX ]                   = { 'X', ' ', true },
329         [ TAINT_RANDSTRUCT ]            = { 'T', ' ', true },
330 };
332 /**
333  * print_tainted - return a string to represent the kernel taint state.
334  *
335  * For individual taint flag meanings, see Documentation/sysctl/kernel.txt
336  *
337  * The string is overwritten by the next call to print_tainted(),
338  * but is always NULL terminated.
339  */
340 const char *print_tainted(void)
342         static char buf[TAINT_FLAGS_COUNT + sizeof("Tainted: ")];
344         BUILD_BUG_ON(ARRAY_SIZE(taint_flags) != TAINT_FLAGS_COUNT);
346         if (tainted_mask) {
347                 char *s;
348                 int i;
350                 s = buf + sprintf(buf, "Tainted: ");
351                 for (i = 0; i < TAINT_FLAGS_COUNT; i++) {
352                         const struct taint_flag *t = &taint_flags[i];
353                         *s++ = test_bit(i, &tainted_mask) ?
354                                         t->c_true : t->c_false;
355                 }
356                 *s = 0;
357         } else
358                 snprintf(buf, sizeof(buf), "Not tainted");
360         return buf;
363 int test_taint(unsigned flag)
365         return test_bit(flag, &tainted_mask);
367 EXPORT_SYMBOL(test_taint);
369 unsigned long get_taint(void)
371         return tainted_mask;
374 /**
375  * add_taint: add a taint flag if not already set.
376  * @flag: one of the TAINT_* constants.
377  * @lockdep_ok: whether lock debugging is still OK.
378  *
379  * If something bad has gone wrong, you'll want @lockdebug_ok = false, but for
380  * some notewortht-but-not-corrupting cases, it can be set to true.
381  */
382 void add_taint(unsigned flag, enum lockdep_ok lockdep_ok)
384         if (lockdep_ok == LOCKDEP_NOW_UNRELIABLE && __debug_locks_off())
385                 pr_warn("Disabling lock debugging due to kernel taint\n");
387         set_bit(flag, &tainted_mask);
389 EXPORT_SYMBOL(add_taint);
391 static void spin_msec(int msecs)
393         int i;
395         for (i = 0; i < msecs; i++) {
396                 touch_nmi_watchdog();
397                 mdelay(1);
398         }
401 /*
402  * It just happens that oops_enter() and oops_exit() are identically
403  * implemented...
404  */
405 static void do_oops_enter_exit(void)
407         unsigned long flags;
408         static int spin_counter;
410         if (!pause_on_oops)
411                 return;
413         spin_lock_irqsave(&pause_on_oops_lock, flags);
414         if (pause_on_oops_flag == 0) {
415                 /* This CPU may now print the oops message */
416                 pause_on_oops_flag = 1;
417         } else {
418                 /* We need to stall this CPU */
419                 if (!spin_counter) {
420                         /* This CPU gets to do the counting */
421                         spin_counter = pause_on_oops;
422                         do {
423                                 spin_unlock(&pause_on_oops_lock);
424                                 spin_msec(MSEC_PER_SEC);
425                                 spin_lock(&pause_on_oops_lock);
426                         } while (--spin_counter);
427                         pause_on_oops_flag = 0;
428                 } else {
429                         /* This CPU waits for a different one */
430                         while (spin_counter) {
431                                 spin_unlock(&pause_on_oops_lock);
432                                 spin_msec(1);
433                                 spin_lock(&pause_on_oops_lock);
434                         }
435                 }
436         }
437         spin_unlock_irqrestore(&pause_on_oops_lock, flags);
440 /*
441  * Return true if the calling CPU is allowed to print oops-related info.
442  * This is a bit racy..
443  */
444 int oops_may_print(void)
446         return pause_on_oops_flag == 0;
449 /*
450  * Called when the architecture enters its oops handler, before it prints
451  * anything.  If this is the first CPU to oops, and it's oopsing the first
452  * time then let it proceed.
453  *
454  * This is all enabled by the pause_on_oops kernel boot option.  We do all
455  * this to ensure that oopses don't scroll off the screen.  It has the
456  * side-effect of preventing later-oopsing CPUs from mucking up the display,
457  * too.
458  *
459  * It turns out that the CPU which is allowed to print ends up pausing for
460  * the right duration, whereas all the other CPUs pause for twice as long:
461  * once in oops_enter(), once in oops_exit().
462  */
463 void oops_enter(void)
465         tracing_off();
466         /* can't trust the integrity of the kernel anymore: */
467         debug_locks_off();
468         do_oops_enter_exit();
471 /*
472  * 64-bit random ID for oopses:
473  */
474 static u64 oops_id;
476 static int init_oops_id(void)
478         if (!oops_id)
479                 get_random_bytes(&oops_id, sizeof(oops_id));
480         else
481                 oops_id++;
483         return 0;
485 late_initcall(init_oops_id);
487 void print_oops_end_marker(void)
489         init_oops_id();
490         pr_warn("---[ end trace %016llx ]---\n", (unsigned long long)oops_id);
493 /*
494  * Called when the architecture exits its oops handler, after printing
495  * everything.
496  */
497 void oops_exit(void)
499         do_oops_enter_exit();
500         print_oops_end_marker();
501         kmsg_dump(KMSG_DUMP_OOPS);
504 struct warn_args {
505         const char *fmt;
506         va_list args;
507 };
509 void __warn(const char *file, int line, void *caller, unsigned taint,
510             struct pt_regs *regs, struct warn_args *args)
512         disable_trace_on_warning();
514         if (args)
515                 pr_warn(CUT_HERE);
517         if (file)
518                 pr_warn("WARNING: CPU: %d PID: %d at %s:%d %pS\n",
519                         raw_smp_processor_id(), current->pid, file, line,
520                         caller);
521         else
522                 pr_warn("WARNING: CPU: %d PID: %d at %pS\n",
523                         raw_smp_processor_id(), current->pid, caller);
525         if (args)
526                 vprintk(args->fmt, args->args);
528         if (panic_on_warn) {
529                 /*
530                  * This thread may hit another WARN() in the panic path.
531                  * Resetting this prevents additional WARN() from panicking the
532                  * system on this thread.  Other threads are blocked by the
533                  * panic_mutex in panic().
534                  */
535                 panic_on_warn = 0;
536                 panic("panic_on_warn set ...\n");
537         }
539         print_modules();
541         if (regs)
542                 show_regs(regs);
543         else
544                 dump_stack();
546         print_irqtrace_events(current);
548         print_oops_end_marker();
550         /* Just a warning, don't kill lockdep. */
551         add_taint(taint, LOCKDEP_STILL_OK);
554 #ifdef WANT_WARN_ON_SLOWPATH
555 void warn_slowpath_fmt(const char *file, int line, const char *fmt, ...)
557         struct warn_args args;
559         args.fmt = fmt;
560         va_start(args.args, fmt);
561         __warn(file, line, __builtin_return_address(0), TAINT_WARN, NULL,
562                &args);
563         va_end(args.args);
565 EXPORT_SYMBOL(warn_slowpath_fmt);
567 void warn_slowpath_fmt_taint(const char *file, int line,
568                              unsigned taint, const char *fmt, ...)
570         struct warn_args args;
572         args.fmt = fmt;
573         va_start(args.args, fmt);
574         __warn(file, line, __builtin_return_address(0), taint, NULL, &args);
575         va_end(args.args);
577 EXPORT_SYMBOL(warn_slowpath_fmt_taint);
579 void warn_slowpath_null(const char *file, int line)
581         pr_warn(CUT_HERE);
582         __warn(file, line, __builtin_return_address(0), TAINT_WARN, NULL, NULL);
584 EXPORT_SYMBOL(warn_slowpath_null);
585 #else
586 void __warn_printk(const char *fmt, ...)
588         va_list args;
590         pr_warn(CUT_HERE);
592         va_start(args, fmt);
593         vprintk(fmt, args);
594         va_end(args);
596 EXPORT_SYMBOL(__warn_printk);
597 #endif
599 #ifdef CONFIG_BUG
601 /* Support resetting WARN*_ONCE state */
603 static int clear_warn_once_set(void *data, u64 val)
605         generic_bug_clear_once();
606         memset(__start_once, 0, __end_once - __start_once);
607         return 0;
610 DEFINE_SIMPLE_ATTRIBUTE(clear_warn_once_fops,
611                         NULL,
612                         clear_warn_once_set,
613                         "%lld\n");
615 static __init int register_warn_debugfs(void)
617         /* Don't care about failure */
618         debugfs_create_file("clear_warn_once", 0200, NULL,
619                             NULL, &clear_warn_once_fops);
620         return 0;
623 device_initcall(register_warn_debugfs);
624 #endif
626 #ifdef CONFIG_STACKPROTECTOR
628 /*
629  * Called when gcc's -fstack-protector feature is used, and
630  * gcc detects corruption of the on-stack canary value
631  */
632 __visible void __stack_chk_fail(void)
634         panic("stack-protector: Kernel stack is corrupted in: %pB\n",
635                 __builtin_return_address(0));
637 EXPORT_SYMBOL(__stack_chk_fail);
639 #endif
641 #ifdef CONFIG_ARCH_HAS_REFCOUNT
642 void refcount_error_report(struct pt_regs *regs, const char *err)
644         WARN_RATELIMIT(1, "refcount_t %s at %pB in %s[%d], uid/euid: %u/%u\n",
645                 err, (void *)instruction_pointer(regs),
646                 current->comm, task_pid_nr(current),
647                 from_kuid_munged(&init_user_ns, current_uid()),
648                 from_kuid_munged(&init_user_ns, current_euid()));
650 #endif
652 core_param(panic, panic_timeout, int, 0644);
653 core_param(pause_on_oops, pause_on_oops, int, 0644);
654 core_param(panic_on_warn, panic_on_warn, int, 0644);
655 core_param(crash_kexec_post_notifiers, crash_kexec_post_notifiers, bool, 0644);
657 static int __init oops_setup(char *s)
659         if (!s)
660                 return -EINVAL;
661         if (!strcmp(s, "panic"))
662                 panic_on_oops = 1;
663         return 0;
665 early_param("oops", oops_setup);