]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - lib/Kconfig.kasan
Revert "HACK: ARM: dts: dra7-ipu-common: Revert to CMA pools for IPU early boots"
[rpmsg/rpmsg.git] / lib / Kconfig.kasan
1 config HAVE_ARCH_KASAN
2         bool
4 if HAVE_ARCH_KASAN
6 config KASAN
7         bool "KASan: runtime memory debugger"
8         depends on (SLUB && SYSFS) || (SLAB && !DEBUG_SLAB)
9         select SLUB_DEBUG if SLUB
10         select CONSTRUCTORS
11         select STACKDEPOT
12         help
13           Enables kernel address sanitizer - runtime memory debugger,
14           designed to find out-of-bounds accesses and use-after-free bugs.
15           This is strictly a debugging feature and it requires a gcc version
16           of 4.9.2 or later. Detection of out of bounds accesses to stack or
17           global variables requires gcc 5.0 or later.
18           This feature consumes about 1/8 of available memory and brings about
19           ~x3 performance slowdown.
20           For better error detection enable CONFIG_STACKTRACE.
21           Currently CONFIG_KASAN doesn't work with CONFIG_DEBUG_SLAB
22           (the resulting kernel does not boot).
24 config KASAN_EXTRA
25         bool "KAsan: extra checks"
26         depends on KASAN && DEBUG_KERNEL && !COMPILE_TEST
27         help
28           This enables further checks in the kernel address sanitizer, for now
29           it only includes the address-use-after-scope check that can lead
30           to excessive kernel stack usage, frame size warnings and longer
31           compile time.
32           https://gcc.gnu.org/bugzilla/show_bug.cgi?id=81715 has more
35 choice
36         prompt "Instrumentation type"
37         depends on KASAN
38         default KASAN_OUTLINE
40 config KASAN_OUTLINE
41         bool "Outline instrumentation"
42         help
43           Before every memory access compiler insert function call
44           __asan_load*/__asan_store*. These functions performs check
45           of shadow memory. This is slower than inline instrumentation,
46           however it doesn't bloat size of kernel's .text section so
47           much as inline does.
49 config KASAN_INLINE
50         bool "Inline instrumentation"
51         help
52           Compiler directly inserts code checking shadow memory before
53           memory accesses. This is faster than outline (in some workloads
54           it gives about x2 boost over outline instrumentation), but
55           make kernel's .text size much bigger.
56           This requires a gcc version of 5.0 or later.
58 endchoice
60 config TEST_KASAN
61         tristate "Module for testing kasan for bug detection"
62         depends on m && KASAN
63         help
64           This is a test module doing various nasty things like
65           out of bounds accesses, use after free. It is useful for testing
66           kernel debugging features like kernel address sanitizer.
68 endif