]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - lib/cmpdi2.c
Merge branch 'rpmsg-linux-4.19.y' of git://git.ti.com/rpmsg/rpmsg into rpmsg-ti-linux...
[rpmsg/rpmsg.git] / lib / cmpdi2.c
1 /*
2  * This program is free software; you can redistribute it and/or modify
3  * it under the terms of the GNU General Public License as published by
4  * the Free Software Foundation; either version 2 of the License, or
5  * (at your option) any later version.
6  *
7  * This program is distributed in the hope that it will be useful,
8  * but WITHOUT ANY WARRANTY; without even the implied warranty of
9  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
10  * GNU General Public License for more details.
11  *
12  * You should have received a copy of the GNU General Public License
13  * along with this program; if not, see the file COPYING, or write
14  * to the Free Software Foundation, Inc.
15  */
17 #include <linux/export.h>
19 #include <linux/libgcc.h>
21 word_type notrace __cmpdi2(long long a, long long b)
22 {
23         const DWunion au = {
24                 .ll = a
25         };
26         const DWunion bu = {
27                 .ll = b
28         };
30         if (au.s.high < bu.s.high)
31                 return 0;
32         else if (au.s.high > bu.s.high)
33                 return 2;
35         if ((unsigned int) au.s.low < (unsigned int) bu.s.low)
36                 return 0;
37         else if ((unsigned int) au.s.low > (unsigned int) bu.s.low)
38                 return 2;
40         return 1;
41 }
42 EXPORT_SYMBOL(__cmpdi2);