1 // SPDX-License-Identifier: GPL-2.0
2 /*
3 * Implement the default iomap interfaces
4 *
5 * (C) Copyright 2004 Linus Torvalds
6 */
7 #include <linux/pci.h>
8 #include <linux/io.h>
10 #include <linux/export.h>
12 /*
13 * Read/write from/to an (offsettable) iomem cookie. It might be a PIO
14 * access or a MMIO access, these functions don't care. The info is
15 * encoded in the hardware mapping set up by the mapping functions
16 * (or the cookie itself, depending on implementation and hw).
17 *
18 * The generic routines don't assume any hardware mappings, and just
19 * encode the PIO/MMIO as part of the cookie. They coldly assume that
20 * the MMIO IO mappings are not in the low address range.
21 *
22 * Architectures for which this is not true can't use this generic
23 * implementation and should do their own copy.
24 */
26 #ifndef HAVE_ARCH_PIO_SIZE
27 /*
28 * We encode the physical PIO addresses (0-0xffff) into the
29 * pointer by offsetting them with a constant (0x10000) and
30 * assuming that all the low addresses are always PIO. That means
31 * we can do some sanity checks on the low bits, and don't
32 * need to just take things for granted.
33 */
34 #define PIO_OFFSET 0x10000UL
35 #define PIO_MASK 0x0ffffUL
36 #define PIO_RESERVED 0x40000UL
37 #endif
39 static void bad_io_access(unsigned long port, const char *access)
40 {
41 static int count = 10;
42 if (count) {
43 count--;
44 WARN(1, KERN_ERR "Bad IO access at port %#lx (%s)\n", port, access);
45 }
46 }
48 /*
49 * Ugly macros are a way of life.
50 */
51 #define IO_COND(addr, is_pio, is_mmio) do { \
52 unsigned long port = (unsigned long __force)addr; \
53 if (port >= PIO_RESERVED) { \
54 is_mmio; \
55 } else if (port > PIO_OFFSET) { \
56 port &= PIO_MASK; \
57 is_pio; \
58 } else \
59 bad_io_access(port, #is_pio ); \
60 } while (0)
62 #ifndef pio_read16be
63 #define pio_read16be(port) swab16(inw(port))
64 #define pio_read32be(port) swab32(inl(port))
65 #endif
67 #ifndef mmio_read16be
68 #define mmio_read16be(addr) be16_to_cpu(__raw_readw(addr))
69 #define mmio_read32be(addr) be32_to_cpu(__raw_readl(addr))
70 #endif
72 unsigned int ioread8(void __iomem *addr)
73 {
74 IO_COND(addr, return inb(port), return readb(addr));
75 return 0xff;
76 }
77 unsigned int ioread16(void __iomem *addr)
78 {
79 IO_COND(addr, return inw(port), return readw(addr));
80 return 0xffff;
81 }
82 unsigned int ioread16be(void __iomem *addr)
83 {
84 IO_COND(addr, return pio_read16be(port), return mmio_read16be(addr));
85 return 0xffff;
86 }
87 unsigned int ioread32(void __iomem *addr)
88 {
89 IO_COND(addr, return inl(port), return readl(addr));
90 return 0xffffffff;
91 }
92 unsigned int ioread32be(void __iomem *addr)
93 {
94 IO_COND(addr, return pio_read32be(port), return mmio_read32be(addr));
95 return 0xffffffff;
96 }
97 EXPORT_SYMBOL(ioread8);
98 EXPORT_SYMBOL(ioread16);
99 EXPORT_SYMBOL(ioread16be);
100 EXPORT_SYMBOL(ioread32);
101 EXPORT_SYMBOL(ioread32be);
103 #ifndef pio_write16be
104 #define pio_write16be(val,port) outw(swab16(val),port)
105 #define pio_write32be(val,port) outl(swab32(val),port)
106 #endif
108 #ifndef mmio_write16be
109 #define mmio_write16be(val,port) __raw_writew(be16_to_cpu(val),port)
110 #define mmio_write32be(val,port) __raw_writel(be32_to_cpu(val),port)
111 #endif
113 void iowrite8(u8 val, void __iomem *addr)
114 {
115 IO_COND(addr, outb(val,port), writeb(val, addr));
116 }
117 void iowrite16(u16 val, void __iomem *addr)
118 {
119 IO_COND(addr, outw(val,port), writew(val, addr));
120 }
121 void iowrite16be(u16 val, void __iomem *addr)
122 {
123 IO_COND(addr, pio_write16be(val,port), mmio_write16be(val, addr));
124 }
125 void iowrite32(u32 val, void __iomem *addr)
126 {
127 IO_COND(addr, outl(val,port), writel(val, addr));
128 }
129 void iowrite32be(u32 val, void __iomem *addr)
130 {
131 IO_COND(addr, pio_write32be(val,port), mmio_write32be(val, addr));
132 }
133 EXPORT_SYMBOL(iowrite8);
134 EXPORT_SYMBOL(iowrite16);
135 EXPORT_SYMBOL(iowrite16be);
136 EXPORT_SYMBOL(iowrite32);
137 EXPORT_SYMBOL(iowrite32be);
139 /*
140 * These are the "repeat MMIO read/write" functions.
141 * Note the "__raw" accesses, since we don't want to
142 * convert to CPU byte order. We write in "IO byte
143 * order" (we also don't have IO barriers).
144 */
145 #ifndef mmio_insb
146 static inline void mmio_insb(void __iomem *addr, u8 *dst, int count)
147 {
148 while (--count >= 0) {
149 u8 data = __raw_readb(addr);
150 *dst = data;
151 dst++;
152 }
153 }
154 static inline void mmio_insw(void __iomem *addr, u16 *dst, int count)
155 {
156 while (--count >= 0) {
157 u16 data = __raw_readw(addr);
158 *dst = data;
159 dst++;
160 }
161 }
162 static inline void mmio_insl(void __iomem *addr, u32 *dst, int count)
163 {
164 while (--count >= 0) {
165 u32 data = __raw_readl(addr);
166 *dst = data;
167 dst++;
168 }
169 }
170 #endif
172 #ifndef mmio_outsb
173 static inline void mmio_outsb(void __iomem *addr, const u8 *src, int count)
174 {
175 while (--count >= 0) {
176 __raw_writeb(*src, addr);
177 src++;
178 }
179 }
180 static inline void mmio_outsw(void __iomem *addr, const u16 *src, int count)
181 {
182 while (--count >= 0) {
183 __raw_writew(*src, addr);
184 src++;
185 }
186 }
187 static inline void mmio_outsl(void __iomem *addr, const u32 *src, int count)
188 {
189 while (--count >= 0) {
190 __raw_writel(*src, addr);
191 src++;
192 }
193 }
194 #endif
196 void ioread8_rep(void __iomem *addr, void *dst, unsigned long count)
197 {
198 IO_COND(addr, insb(port,dst,count), mmio_insb(addr, dst, count));
199 }
200 void ioread16_rep(void __iomem *addr, void *dst, unsigned long count)
201 {
202 IO_COND(addr, insw(port,dst,count), mmio_insw(addr, dst, count));
203 }
204 void ioread32_rep(void __iomem *addr, void *dst, unsigned long count)
205 {
206 IO_COND(addr, insl(port,dst,count), mmio_insl(addr, dst, count));
207 }
208 EXPORT_SYMBOL(ioread8_rep);
209 EXPORT_SYMBOL(ioread16_rep);
210 EXPORT_SYMBOL(ioread32_rep);
212 void iowrite8_rep(void __iomem *addr, const void *src, unsigned long count)
213 {
214 IO_COND(addr, outsb(port, src, count), mmio_outsb(addr, src, count));
215 }
216 void iowrite16_rep(void __iomem *addr, const void *src, unsigned long count)
217 {
218 IO_COND(addr, outsw(port, src, count), mmio_outsw(addr, src, count));
219 }
220 void iowrite32_rep(void __iomem *addr, const void *src, unsigned long count)
221 {
222 IO_COND(addr, outsl(port, src,count), mmio_outsl(addr, src, count));
223 }
224 EXPORT_SYMBOL(iowrite8_rep);
225 EXPORT_SYMBOL(iowrite16_rep);
226 EXPORT_SYMBOL(iowrite32_rep);
228 #ifdef CONFIG_HAS_IOPORT_MAP
229 /* Create a virtual mapping cookie for an IO port range */
230 void __iomem *ioport_map(unsigned long port, unsigned int nr)
231 {
232 if (port > PIO_MASK)
233 return NULL;
234 return (void __iomem *) (unsigned long) (port + PIO_OFFSET);
235 }
237 void ioport_unmap(void __iomem *addr)
238 {
239 /* Nothing to do */
240 }
241 EXPORT_SYMBOL(ioport_map);
242 EXPORT_SYMBOL(ioport_unmap);
243 #endif /* CONFIG_HAS_IOPORT_MAP */
245 #ifdef CONFIG_PCI
246 /* Hide the details if this is a MMIO or PIO address space and just do what
247 * you expect in the correct way. */
248 void pci_iounmap(struct pci_dev *dev, void __iomem * addr)
249 {
250 IO_COND(addr, /* nothing */, iounmap(addr));
251 }
252 EXPORT_SYMBOL(pci_iounmap);
253 #endif /* CONFIG_PCI */