1 // SPDX-License-Identifier: GPL-2.0
2 /*
3 * Variant of atomic_t specialized for reference counts.
4 *
5 * The interface matches the atomic_t interface (to aid in porting) but only
6 * provides the few functions one should use for reference counting.
7 *
8 * It differs in that the counter saturates at UINT_MAX and will not move once
9 * there. This avoids wrapping the counter and causing 'spurious'
10 * use-after-free issues.
11 *
12 * Memory ordering rules are slightly relaxed wrt regular atomic_t functions
13 * and provide only what is strictly required for refcounts.
14 *
15 * The increments are fully relaxed; these will not provide ordering. The
16 * rationale is that whatever is used to obtain the object we're increasing the
17 * reference count on will provide the ordering. For locked data structures,
18 * its the lock acquire, for RCU/lockless data structures its the dependent
19 * load.
20 *
21 * Do note that inc_not_zero() provides a control dependency which will order
22 * future stores against the inc, this ensures we'll never modify the object
23 * if we did not in fact acquire a reference.
24 *
25 * The decrements will provide release order, such that all the prior loads and
26 * stores will be issued before, it also provides a control dependency, which
27 * will order us against the subsequent free().
28 *
29 * The control dependency is against the load of the cmpxchg (ll/sc) that
30 * succeeded. This means the stores aren't fully ordered, but this is fine
31 * because the 1->0 transition indicates no concurrency.
32 *
33 * Note that the allocator is responsible for ordering things between free()
34 * and alloc().
35 *
36 */
38 #include <linux/mutex.h>
39 #include <linux/refcount.h>
40 #include <linux/spinlock.h>
41 #include <linux/bug.h>
43 /**
44 * refcount_add_not_zero_checked - add a value to a refcount unless it is 0
45 * @i: the value to add to the refcount
46 * @r: the refcount
47 *
48 * Will saturate at UINT_MAX and WARN.
49 *
50 * Provides no memory ordering, it is assumed the caller has guaranteed the
51 * object memory to be stable (RCU, etc.). It does provide a control dependency
52 * and thereby orders future stores. See the comment on top.
53 *
54 * Use of this function is not recommended for the normal reference counting
55 * use case in which references are taken and released one at a time. In these
56 * cases, refcount_inc(), or one of its variants, should instead be used to
57 * increment a reference count.
58 *
59 * Return: false if the passed refcount is 0, true otherwise
60 */
61 bool refcount_add_not_zero_checked(unsigned int i, refcount_t *r)
62 {
63 unsigned int new, val = atomic_read(&r->refs);
65 do {
66 if (!val)
67 return false;
69 if (unlikely(val == UINT_MAX))
70 return true;
72 new = val + i;
73 if (new < val)
74 new = UINT_MAX;
76 } while (!atomic_try_cmpxchg_relaxed(&r->refs, &val, new));
78 WARN_ONCE(new == UINT_MAX, "refcount_t: saturated; leaking memory.\n");
80 return true;
81 }
82 EXPORT_SYMBOL(refcount_add_not_zero_checked);
84 /**
85 * refcount_add_checked - add a value to a refcount
86 * @i: the value to add to the refcount
87 * @r: the refcount
88 *
89 * Similar to atomic_add(), but will saturate at UINT_MAX and WARN.
90 *
91 * Provides no memory ordering, it is assumed the caller has guaranteed the
92 * object memory to be stable (RCU, etc.). It does provide a control dependency
93 * and thereby orders future stores. See the comment on top.
94 *
95 * Use of this function is not recommended for the normal reference counting
96 * use case in which references are taken and released one at a time. In these
97 * cases, refcount_inc(), or one of its variants, should instead be used to
98 * increment a reference count.
99 */
100 void refcount_add_checked(unsigned int i, refcount_t *r)
101 {
102 WARN_ONCE(!refcount_add_not_zero_checked(i, r), "refcount_t: addition on 0; use-after-free.\n");
103 }
104 EXPORT_SYMBOL(refcount_add_checked);
106 /**
107 * refcount_inc_not_zero_checked - increment a refcount unless it is 0
108 * @r: the refcount to increment
109 *
110 * Similar to atomic_inc_not_zero(), but will saturate at UINT_MAX and WARN.
111 *
112 * Provides no memory ordering, it is assumed the caller has guaranteed the
113 * object memory to be stable (RCU, etc.). It does provide a control dependency
114 * and thereby orders future stores. See the comment on top.
115 *
116 * Return: true if the increment was successful, false otherwise
117 */
118 bool refcount_inc_not_zero_checked(refcount_t *r)
119 {
120 unsigned int new, val = atomic_read(&r->refs);
122 do {
123 new = val + 1;
125 if (!val)
126 return false;
128 if (unlikely(!new))
129 return true;
131 } while (!atomic_try_cmpxchg_relaxed(&r->refs, &val, new));
133 WARN_ONCE(new == UINT_MAX, "refcount_t: saturated; leaking memory.\n");
135 return true;
136 }
137 EXPORT_SYMBOL(refcount_inc_not_zero_checked);
139 /**
140 * refcount_inc_checked - increment a refcount
141 * @r: the refcount to increment
142 *
143 * Similar to atomic_inc(), but will saturate at UINT_MAX and WARN.
144 *
145 * Provides no memory ordering, it is assumed the caller already has a
146 * reference on the object.
147 *
148 * Will WARN if the refcount is 0, as this represents a possible use-after-free
149 * condition.
150 */
151 void refcount_inc_checked(refcount_t *r)
152 {
153 WARN_ONCE(!refcount_inc_not_zero_checked(r), "refcount_t: increment on 0; use-after-free.\n");
154 }
155 EXPORT_SYMBOL(refcount_inc_checked);
157 /**
158 * refcount_sub_and_test_checked - subtract from a refcount and test if it is 0
159 * @i: amount to subtract from the refcount
160 * @r: the refcount
161 *
162 * Similar to atomic_dec_and_test(), but it will WARN, return false and
163 * ultimately leak on underflow and will fail to decrement when saturated
164 * at UINT_MAX.
165 *
166 * Provides release memory ordering, such that prior loads and stores are done
167 * before, and provides a control dependency such that free() must come after.
168 * See the comment on top.
169 *
170 * Use of this function is not recommended for the normal reference counting
171 * use case in which references are taken and released one at a time. In these
172 * cases, refcount_dec(), or one of its variants, should instead be used to
173 * decrement a reference count.
174 *
175 * Return: true if the resulting refcount is 0, false otherwise
176 */
177 bool refcount_sub_and_test_checked(unsigned int i, refcount_t *r)
178 {
179 unsigned int new, val = atomic_read(&r->refs);
181 do {
182 if (unlikely(val == UINT_MAX))
183 return false;
185 new = val - i;
186 if (new > val) {
187 WARN_ONCE(new > val, "refcount_t: underflow; use-after-free.\n");
188 return false;
189 }
191 } while (!atomic_try_cmpxchg_release(&r->refs, &val, new));
193 return !new;
194 }
195 EXPORT_SYMBOL(refcount_sub_and_test_checked);
197 /**
198 * refcount_dec_and_test_checked - decrement a refcount and test if it is 0
199 * @r: the refcount
200 *
201 * Similar to atomic_dec_and_test(), it will WARN on underflow and fail to
202 * decrement when saturated at UINT_MAX.
203 *
204 * Provides release memory ordering, such that prior loads and stores are done
205 * before, and provides a control dependency such that free() must come after.
206 * See the comment on top.
207 *
208 * Return: true if the resulting refcount is 0, false otherwise
209 */
210 bool refcount_dec_and_test_checked(refcount_t *r)
211 {
212 return refcount_sub_and_test_checked(1, r);
213 }
214 EXPORT_SYMBOL(refcount_dec_and_test_checked);
216 /**
217 * refcount_dec_checked - decrement a refcount
218 * @r: the refcount
219 *
220 * Similar to atomic_dec(), it will WARN on underflow and fail to decrement
221 * when saturated at UINT_MAX.
222 *
223 * Provides release memory ordering, such that prior loads and stores are done
224 * before.
225 */
226 void refcount_dec_checked(refcount_t *r)
227 {
228 WARN_ONCE(refcount_dec_and_test_checked(r), "refcount_t: decrement hit 0; leaking memory.\n");
229 }
230 EXPORT_SYMBOL(refcount_dec_checked);
232 /**
233 * refcount_dec_if_one - decrement a refcount if it is 1
234 * @r: the refcount
235 *
236 * No atomic_t counterpart, it attempts a 1 -> 0 transition and returns the
237 * success thereof.
238 *
239 * Like all decrement operations, it provides release memory order and provides
240 * a control dependency.
241 *
242 * It can be used like a try-delete operator; this explicit case is provided
243 * and not cmpxchg in generic, because that would allow implementing unsafe
244 * operations.
245 *
246 * Return: true if the resulting refcount is 0, false otherwise
247 */
248 bool refcount_dec_if_one(refcount_t *r)
249 {
250 int val = 1;
252 return atomic_try_cmpxchg_release(&r->refs, &val, 0);
253 }
254 EXPORT_SYMBOL(refcount_dec_if_one);
256 /**
257 * refcount_dec_not_one - decrement a refcount if it is not 1
258 * @r: the refcount
259 *
260 * No atomic_t counterpart, it decrements unless the value is 1, in which case
261 * it will return false.
262 *
263 * Was often done like: atomic_add_unless(&var, -1, 1)
264 *
265 * Return: true if the decrement operation was successful, false otherwise
266 */
267 bool refcount_dec_not_one(refcount_t *r)
268 {
269 unsigned int new, val = atomic_read(&r->refs);
271 do {
272 if (unlikely(val == UINT_MAX))
273 return true;
275 if (val == 1)
276 return false;
278 new = val - 1;
279 if (new > val) {
280 WARN_ONCE(new > val, "refcount_t: underflow; use-after-free.\n");
281 return true;
282 }
284 } while (!atomic_try_cmpxchg_release(&r->refs, &val, new));
286 return true;
287 }
288 EXPORT_SYMBOL(refcount_dec_not_one);
290 /**
291 * refcount_dec_and_mutex_lock - return holding mutex if able to decrement
292 * refcount to 0
293 * @r: the refcount
294 * @lock: the mutex to be locked
295 *
296 * Similar to atomic_dec_and_mutex_lock(), it will WARN on underflow and fail
297 * to decrement when saturated at UINT_MAX.
298 *
299 * Provides release memory ordering, such that prior loads and stores are done
300 * before, and provides a control dependency such that free() must come after.
301 * See the comment on top.
302 *
303 * Return: true and hold mutex if able to decrement refcount to 0, false
304 * otherwise
305 */
306 bool refcount_dec_and_mutex_lock(refcount_t *r, struct mutex *lock)
307 {
308 if (refcount_dec_not_one(r))
309 return false;
311 mutex_lock(lock);
312 if (!refcount_dec_and_test(r)) {
313 mutex_unlock(lock);
314 return false;
315 }
317 return true;
318 }
319 EXPORT_SYMBOL(refcount_dec_and_mutex_lock);
321 /**
322 * refcount_dec_and_lock - return holding spinlock if able to decrement
323 * refcount to 0
324 * @r: the refcount
325 * @lock: the spinlock to be locked
326 *
327 * Similar to atomic_dec_and_lock(), it will WARN on underflow and fail to
328 * decrement when saturated at UINT_MAX.
329 *
330 * Provides release memory ordering, such that prior loads and stores are done
331 * before, and provides a control dependency such that free() must come after.
332 * See the comment on top.
333 *
334 * Return: true and hold spinlock if able to decrement refcount to 0, false
335 * otherwise
336 */
337 bool refcount_dec_and_lock(refcount_t *r, spinlock_t *lock)
338 {
339 if (refcount_dec_not_one(r))
340 return false;
342 spin_lock(lock);
343 if (!refcount_dec_and_test(r)) {
344 spin_unlock(lock);
345 return false;
346 }
348 return true;
349 }
350 EXPORT_SYMBOL(refcount_dec_and_lock);
352 /**
353 * refcount_dec_and_lock_irqsave - return holding spinlock with disabled
354 * interrupts if able to decrement refcount to 0
355 * @r: the refcount
356 * @lock: the spinlock to be locked
357 * @flags: saved IRQ-flags if the is acquired
358 *
359 * Same as refcount_dec_and_lock() above except that the spinlock is acquired
360 * with disabled interupts.
361 *
362 * Return: true and hold spinlock if able to decrement refcount to 0, false
363 * otherwise
364 */
365 bool refcount_dec_and_lock_irqsave(refcount_t *r, spinlock_t *lock,
366 unsigned long *flags)
367 {
368 if (refcount_dec_not_one(r))
369 return false;
371 spin_lock_irqsave(lock, *flags);
372 if (!refcount_dec_and_test(r)) {
373 spin_unlock_irqrestore(lock, *flags);
374 return false;
375 }
377 return true;
378 }
379 EXPORT_SYMBOL(refcount_dec_and_lock_irqsave);