1 /*
2 * Copyright (C) 2007 Jens Axboe <jens.axboe@oracle.com>
3 *
4 * Scatterlist handling helpers.
5 *
6 * This source code is licensed under the GNU General Public License,
7 * Version 2. See the file COPYING for more details.
8 */
9 #include <linux/export.h>
10 #include <linux/slab.h>
11 #include <linux/scatterlist.h>
12 #include <linux/highmem.h>
13 #include <linux/kmemleak.h>
15 /**
16 * sg_next - return the next scatterlist entry in a list
17 * @sg: The current sg entry
18 *
19 * Description:
20 * Usually the next entry will be @sg@ + 1, but if this sg element is part
21 * of a chained scatterlist, it could jump to the start of a new
22 * scatterlist array.
23 *
24 **/
25 struct scatterlist *sg_next(struct scatterlist *sg)
26 {
27 if (sg_is_last(sg))
28 return NULL;
30 sg++;
31 if (unlikely(sg_is_chain(sg)))
32 sg = sg_chain_ptr(sg);
34 return sg;
35 }
36 EXPORT_SYMBOL(sg_next);
38 /**
39 * sg_nents - return total count of entries in scatterlist
40 * @sg: The scatterlist
41 *
42 * Description:
43 * Allows to know how many entries are in sg, taking into acount
44 * chaining as well
45 *
46 **/
47 int sg_nents(struct scatterlist *sg)
48 {
49 int nents;
50 for (nents = 0; sg; sg = sg_next(sg))
51 nents++;
52 return nents;
53 }
54 EXPORT_SYMBOL(sg_nents);
56 /**
57 * sg_nents_for_len - return total count of entries in scatterlist
58 * needed to satisfy the supplied length
59 * @sg: The scatterlist
60 * @len: The total required length
61 *
62 * Description:
63 * Determines the number of entries in sg that are required to meet
64 * the supplied length, taking into acount chaining as well
65 *
66 * Returns:
67 * the number of sg entries needed, negative error on failure
68 *
69 **/
70 int sg_nents_for_len(struct scatterlist *sg, u64 len)
71 {
72 int nents;
73 u64 total;
75 if (!len)
76 return 0;
78 for (nents = 0, total = 0; sg; sg = sg_next(sg)) {
79 nents++;
80 total += sg->length;
81 if (total >= len)
82 return nents;
83 }
85 return -EINVAL;
86 }
87 EXPORT_SYMBOL(sg_nents_for_len);
89 /**
90 * sg_last - return the last scatterlist entry in a list
91 * @sgl: First entry in the scatterlist
92 * @nents: Number of entries in the scatterlist
93 *
94 * Description:
95 * Should only be used casually, it (currently) scans the entire list
96 * to get the last entry.
97 *
98 * Note that the @sgl@ pointer passed in need not be the first one,
99 * the important bit is that @nents@ denotes the number of entries that
100 * exist from @sgl@.
101 *
102 **/
103 struct scatterlist *sg_last(struct scatterlist *sgl, unsigned int nents)
104 {
105 struct scatterlist *sg, *ret = NULL;
106 unsigned int i;
108 for_each_sg(sgl, sg, nents, i)
109 ret = sg;
111 BUG_ON(!sg_is_last(ret));
112 return ret;
113 }
114 EXPORT_SYMBOL(sg_last);
116 /**
117 * sg_init_table - Initialize SG table
118 * @sgl: The SG table
119 * @nents: Number of entries in table
120 *
121 * Notes:
122 * If this is part of a chained sg table, sg_mark_end() should be
123 * used only on the last table part.
124 *
125 **/
126 void sg_init_table(struct scatterlist *sgl, unsigned int nents)
127 {
128 memset(sgl, 0, sizeof(*sgl) * nents);
129 sg_init_marker(sgl, nents);
130 }
131 EXPORT_SYMBOL(sg_init_table);
133 /**
134 * sg_init_one - Initialize a single entry sg list
135 * @sg: SG entry
136 * @buf: Virtual address for IO
137 * @buflen: IO length
138 *
139 **/
140 void sg_init_one(struct scatterlist *sg, const void *buf, unsigned int buflen)
141 {
142 sg_init_table(sg, 1);
143 sg_set_buf(sg, buf, buflen);
144 }
145 EXPORT_SYMBOL(sg_init_one);
147 /*
148 * The default behaviour of sg_alloc_table() is to use these kmalloc/kfree
149 * helpers.
150 */
151 static struct scatterlist *sg_kmalloc(unsigned int nents, gfp_t gfp_mask)
152 {
153 if (nents == SG_MAX_SINGLE_ALLOC) {
154 /*
155 * Kmemleak doesn't track page allocations as they are not
156 * commonly used (in a raw form) for kernel data structures.
157 * As we chain together a list of pages and then a normal
158 * kmalloc (tracked by kmemleak), in order to for that last
159 * allocation not to become decoupled (and thus a
160 * false-positive) we need to inform kmemleak of all the
161 * intermediate allocations.
162 */
163 void *ptr = (void *) __get_free_page(gfp_mask);
164 kmemleak_alloc(ptr, PAGE_SIZE, 1, gfp_mask);
165 return ptr;
166 } else
167 return kmalloc_array(nents, sizeof(struct scatterlist),
168 gfp_mask);
169 }
171 static void sg_kfree(struct scatterlist *sg, unsigned int nents)
172 {
173 if (nents == SG_MAX_SINGLE_ALLOC) {
174 kmemleak_free(sg);
175 free_page((unsigned long) sg);
176 } else
177 kfree(sg);
178 }
180 /**
181 * __sg_free_table - Free a previously mapped sg table
182 * @table: The sg table header to use
183 * @max_ents: The maximum number of entries per single scatterlist
184 * @skip_first_chunk: don't free the (preallocated) first scatterlist chunk
185 * @free_fn: Free function
186 *
187 * Description:
188 * Free an sg table previously allocated and setup with
189 * __sg_alloc_table(). The @max_ents value must be identical to
190 * that previously used with __sg_alloc_table().
191 *
192 **/
193 void __sg_free_table(struct sg_table *table, unsigned int max_ents,
194 bool skip_first_chunk, sg_free_fn *free_fn)
195 {
196 struct scatterlist *sgl, *next;
198 if (unlikely(!table->sgl))
199 return;
201 sgl = table->sgl;
202 while (table->orig_nents) {
203 unsigned int alloc_size = table->orig_nents;
204 unsigned int sg_size;
206 /*
207 * If we have more than max_ents segments left,
208 * then assign 'next' to the sg table after the current one.
209 * sg_size is then one less than alloc size, since the last
210 * element is the chain pointer.
211 */
212 if (alloc_size > max_ents) {
213 next = sg_chain_ptr(&sgl[max_ents - 1]);
214 alloc_size = max_ents;
215 sg_size = alloc_size - 1;
216 } else {
217 sg_size = alloc_size;
218 next = NULL;
219 }
221 table->orig_nents -= sg_size;
222 if (skip_first_chunk)
223 skip_first_chunk = false;
224 else
225 free_fn(sgl, alloc_size);
226 sgl = next;
227 }
229 table->sgl = NULL;
230 }
231 EXPORT_SYMBOL(__sg_free_table);
233 /**
234 * sg_free_table - Free a previously allocated sg table
235 * @table: The mapped sg table header
236 *
237 **/
238 void sg_free_table(struct sg_table *table)
239 {
240 __sg_free_table(table, SG_MAX_SINGLE_ALLOC, false, sg_kfree);
241 }
242 EXPORT_SYMBOL(sg_free_table);
244 /**
245 * __sg_alloc_table - Allocate and initialize an sg table with given allocator
246 * @table: The sg table header to use
247 * @nents: Number of entries in sg list
248 * @max_ents: The maximum number of entries the allocator returns per call
249 * @gfp_mask: GFP allocation mask
250 * @alloc_fn: Allocator to use
251 *
252 * Description:
253 * This function returns a @table @nents long. The allocator is
254 * defined to return scatterlist chunks of maximum size @max_ents.
255 * Thus if @nents is bigger than @max_ents, the scatterlists will be
256 * chained in units of @max_ents.
257 *
258 * Notes:
259 * If this function returns non-0 (eg failure), the caller must call
260 * __sg_free_table() to cleanup any leftover allocations.
261 *
262 **/
263 int __sg_alloc_table(struct sg_table *table, unsigned int nents,
264 unsigned int max_ents, struct scatterlist *first_chunk,
265 gfp_t gfp_mask, sg_alloc_fn *alloc_fn)
266 {
267 struct scatterlist *sg, *prv;
268 unsigned int left;
270 memset(table, 0, sizeof(*table));
272 if (nents == 0)
273 return -EINVAL;
274 #ifndef CONFIG_ARCH_HAS_SG_CHAIN
275 if (WARN_ON_ONCE(nents > max_ents))
276 return -EINVAL;
277 #endif
279 left = nents;
280 prv = NULL;
281 do {
282 unsigned int sg_size, alloc_size = left;
284 if (alloc_size > max_ents) {
285 alloc_size = max_ents;
286 sg_size = alloc_size - 1;
287 } else
288 sg_size = alloc_size;
290 left -= sg_size;
292 if (first_chunk) {
293 sg = first_chunk;
294 first_chunk = NULL;
295 } else {
296 sg = alloc_fn(alloc_size, gfp_mask);
297 }
298 if (unlikely(!sg)) {
299 /*
300 * Adjust entry count to reflect that the last
301 * entry of the previous table won't be used for
302 * linkage. Without this, sg_kfree() may get
303 * confused.
304 */
305 if (prv)
306 table->nents = ++table->orig_nents;
308 return -ENOMEM;
309 }
311 sg_init_table(sg, alloc_size);
312 table->nents = table->orig_nents += sg_size;
314 /*
315 * If this is the first mapping, assign the sg table header.
316 * If this is not the first mapping, chain previous part.
317 */
318 if (prv)
319 sg_chain(prv, max_ents, sg);
320 else
321 table->sgl = sg;
323 /*
324 * If no more entries after this one, mark the end
325 */
326 if (!left)
327 sg_mark_end(&sg[sg_size - 1]);
329 prv = sg;
330 } while (left);
332 return 0;
333 }
334 EXPORT_SYMBOL(__sg_alloc_table);
336 /**
337 * sg_alloc_table - Allocate and initialize an sg table
338 * @table: The sg table header to use
339 * @nents: Number of entries in sg list
340 * @gfp_mask: GFP allocation mask
341 *
342 * Description:
343 * Allocate and initialize an sg table. If @nents@ is larger than
344 * SG_MAX_SINGLE_ALLOC a chained sg table will be setup.
345 *
346 **/
347 int sg_alloc_table(struct sg_table *table, unsigned int nents, gfp_t gfp_mask)
348 {
349 int ret;
351 ret = __sg_alloc_table(table, nents, SG_MAX_SINGLE_ALLOC,
352 NULL, gfp_mask, sg_kmalloc);
353 if (unlikely(ret))
354 __sg_free_table(table, SG_MAX_SINGLE_ALLOC, false, sg_kfree);
356 return ret;
357 }
358 EXPORT_SYMBOL(sg_alloc_table);
360 /**
361 * __sg_alloc_table_from_pages - Allocate and initialize an sg table from
362 * an array of pages
363 * @sgt: The sg table header to use
364 * @pages: Pointer to an array of page pointers
365 * @n_pages: Number of pages in the pages array
366 * @offset: Offset from start of the first page to the start of a buffer
367 * @size: Number of valid bytes in the buffer (after offset)
368 * @max_segment: Maximum size of a scatterlist node in bytes (page aligned)
369 * @gfp_mask: GFP allocation mask
370 *
371 * Description:
372 * Allocate and initialize an sg table from a list of pages. Contiguous
373 * ranges of the pages are squashed into a single scatterlist node up to the
374 * maximum size specified in @max_segment. An user may provide an offset at a
375 * start and a size of valid data in a buffer specified by the page array.
376 * The returned sg table is released by sg_free_table.
377 *
378 * Returns:
379 * 0 on success, negative error on failure
380 */
381 int __sg_alloc_table_from_pages(struct sg_table *sgt, struct page **pages,
382 unsigned int n_pages, unsigned int offset,
383 unsigned long size, unsigned int max_segment,
384 gfp_t gfp_mask)
385 {
386 unsigned int chunks, cur_page, seg_len, i;
387 int ret;
388 struct scatterlist *s;
390 if (WARN_ON(!max_segment || offset_in_page(max_segment)))
391 return -EINVAL;
393 /* compute number of contiguous chunks */
394 chunks = 1;
395 seg_len = 0;
396 for (i = 1; i < n_pages; i++) {
397 seg_len += PAGE_SIZE;
398 if (seg_len >= max_segment ||
399 page_to_pfn(pages[i]) != page_to_pfn(pages[i - 1]) + 1) {
400 chunks++;
401 seg_len = 0;
402 }
403 }
405 ret = sg_alloc_table(sgt, chunks, gfp_mask);
406 if (unlikely(ret))
407 return ret;
409 /* merging chunks and putting them into the scatterlist */
410 cur_page = 0;
411 for_each_sg(sgt->sgl, s, sgt->orig_nents, i) {
412 unsigned int j, chunk_size;
414 /* look for the end of the current chunk */
415 seg_len = 0;
416 for (j = cur_page + 1; j < n_pages; j++) {
417 seg_len += PAGE_SIZE;
418 if (seg_len >= max_segment ||
419 page_to_pfn(pages[j]) !=
420 page_to_pfn(pages[j - 1]) + 1)
421 break;
422 }
424 chunk_size = ((j - cur_page) << PAGE_SHIFT) - offset;
425 sg_set_page(s, pages[cur_page],
426 min_t(unsigned long, size, chunk_size), offset);
427 size -= chunk_size;
428 offset = 0;
429 cur_page = j;
430 }
432 return 0;
433 }
434 EXPORT_SYMBOL(__sg_alloc_table_from_pages);
436 /**
437 * sg_alloc_table_from_pages - Allocate and initialize an sg table from
438 * an array of pages
439 * @sgt: The sg table header to use
440 * @pages: Pointer to an array of page pointers
441 * @n_pages: Number of pages in the pages array
442 * @offset: Offset from start of the first page to the start of a buffer
443 * @size: Number of valid bytes in the buffer (after offset)
444 * @gfp_mask: GFP allocation mask
445 *
446 * Description:
447 * Allocate and initialize an sg table from a list of pages. Contiguous
448 * ranges of the pages are squashed into a single scatterlist node. A user
449 * may provide an offset at a start and a size of valid data in a buffer
450 * specified by the page array. The returned sg table is released by
451 * sg_free_table.
452 *
453 * Returns:
454 * 0 on success, negative error on failure
455 */
456 int sg_alloc_table_from_pages(struct sg_table *sgt, struct page **pages,
457 unsigned int n_pages, unsigned int offset,
458 unsigned long size, gfp_t gfp_mask)
459 {
460 return __sg_alloc_table_from_pages(sgt, pages, n_pages, offset, size,
461 SCATTERLIST_MAX_SEGMENT, gfp_mask);
462 }
463 EXPORT_SYMBOL(sg_alloc_table_from_pages);
465 #ifdef CONFIG_SGL_ALLOC
467 /**
468 * sgl_alloc_order - allocate a scatterlist and its pages
469 * @length: Length in bytes of the scatterlist. Must be at least one
470 * @order: Second argument for alloc_pages()
471 * @chainable: Whether or not to allocate an extra element in the scatterlist
472 * for scatterlist chaining purposes
473 * @gfp: Memory allocation flags
474 * @nent_p: [out] Number of entries in the scatterlist that have pages
475 *
476 * Returns: A pointer to an initialized scatterlist or %NULL upon failure.
477 */
478 struct scatterlist *sgl_alloc_order(unsigned long long length,
479 unsigned int order, bool chainable,
480 gfp_t gfp, unsigned int *nent_p)
481 {
482 struct scatterlist *sgl, *sg;
483 struct page *page;
484 unsigned int nent, nalloc;
485 u32 elem_len;
487 nent = round_up(length, PAGE_SIZE << order) >> (PAGE_SHIFT + order);
488 /* Check for integer overflow */
489 if (length > (nent << (PAGE_SHIFT + order)))
490 return NULL;
491 nalloc = nent;
492 if (chainable) {
493 /* Check for integer overflow */
494 if (nalloc + 1 < nalloc)
495 return NULL;
496 nalloc++;
497 }
498 sgl = kmalloc_array(nalloc, sizeof(struct scatterlist),
499 (gfp & ~GFP_DMA) | __GFP_ZERO);
500 if (!sgl)
501 return NULL;
503 sg_init_table(sgl, nalloc);
504 sg = sgl;
505 while (length) {
506 elem_len = min_t(u64, length, PAGE_SIZE << order);
507 page = alloc_pages(gfp, order);
508 if (!page) {
509 sgl_free(sgl);
510 return NULL;
511 }
513 sg_set_page(sg, page, elem_len, 0);
514 length -= elem_len;
515 sg = sg_next(sg);
516 }
517 WARN_ONCE(length, "length = %lld\n", length);
518 if (nent_p)
519 *nent_p = nent;
520 return sgl;
521 }
522 EXPORT_SYMBOL(sgl_alloc_order);
524 /**
525 * sgl_alloc - allocate a scatterlist and its pages
526 * @length: Length in bytes of the scatterlist
527 * @gfp: Memory allocation flags
528 * @nent_p: [out] Number of entries in the scatterlist
529 *
530 * Returns: A pointer to an initialized scatterlist or %NULL upon failure.
531 */
532 struct scatterlist *sgl_alloc(unsigned long long length, gfp_t gfp,
533 unsigned int *nent_p)
534 {
535 return sgl_alloc_order(length, 0, false, gfp, nent_p);
536 }
537 EXPORT_SYMBOL(sgl_alloc);
539 /**
540 * sgl_free_n_order - free a scatterlist and its pages
541 * @sgl: Scatterlist with one or more elements
542 * @nents: Maximum number of elements to free
543 * @order: Second argument for __free_pages()
544 *
545 * Notes:
546 * - If several scatterlists have been chained and each chain element is
547 * freed separately then it's essential to set nents correctly to avoid that a
548 * page would get freed twice.
549 * - All pages in a chained scatterlist can be freed at once by setting @nents
550 * to a high number.
551 */
552 void sgl_free_n_order(struct scatterlist *sgl, int nents, int order)
553 {
554 struct scatterlist *sg;
555 struct page *page;
556 int i;
558 for_each_sg(sgl, sg, nents, i) {
559 if (!sg)
560 break;
561 page = sg_page(sg);
562 if (page)
563 __free_pages(page, order);
564 }
565 kfree(sgl);
566 }
567 EXPORT_SYMBOL(sgl_free_n_order);
569 /**
570 * sgl_free_order - free a scatterlist and its pages
571 * @sgl: Scatterlist with one or more elements
572 * @order: Second argument for __free_pages()
573 */
574 void sgl_free_order(struct scatterlist *sgl, int order)
575 {
576 sgl_free_n_order(sgl, INT_MAX, order);
577 }
578 EXPORT_SYMBOL(sgl_free_order);
580 /**
581 * sgl_free - free a scatterlist and its pages
582 * @sgl: Scatterlist with one or more elements
583 */
584 void sgl_free(struct scatterlist *sgl)
585 {
586 sgl_free_order(sgl, 0);
587 }
588 EXPORT_SYMBOL(sgl_free);
590 #endif /* CONFIG_SGL_ALLOC */
592 void __sg_page_iter_start(struct sg_page_iter *piter,
593 struct scatterlist *sglist, unsigned int nents,
594 unsigned long pgoffset)
595 {
596 piter->__pg_advance = 0;
597 piter->__nents = nents;
599 piter->sg = sglist;
600 piter->sg_pgoffset = pgoffset;
601 }
602 EXPORT_SYMBOL(__sg_page_iter_start);
604 static int sg_page_count(struct scatterlist *sg)
605 {
606 return PAGE_ALIGN(sg->offset + sg->length) >> PAGE_SHIFT;
607 }
609 bool __sg_page_iter_next(struct sg_page_iter *piter)
610 {
611 if (!piter->__nents || !piter->sg)
612 return false;
614 piter->sg_pgoffset += piter->__pg_advance;
615 piter->__pg_advance = 1;
617 while (piter->sg_pgoffset >= sg_page_count(piter->sg)) {
618 piter->sg_pgoffset -= sg_page_count(piter->sg);
619 piter->sg = sg_next(piter->sg);
620 if (!--piter->__nents || !piter->sg)
621 return false;
622 }
624 return true;
625 }
626 EXPORT_SYMBOL(__sg_page_iter_next);
628 /**
629 * sg_miter_start - start mapping iteration over a sg list
630 * @miter: sg mapping iter to be started
631 * @sgl: sg list to iterate over
632 * @nents: number of sg entries
633 *
634 * Description:
635 * Starts mapping iterator @miter.
636 *
637 * Context:
638 * Don't care.
639 */
640 void sg_miter_start(struct sg_mapping_iter *miter, struct scatterlist *sgl,
641 unsigned int nents, unsigned int flags)
642 {
643 memset(miter, 0, sizeof(struct sg_mapping_iter));
645 __sg_page_iter_start(&miter->piter, sgl, nents, 0);
646 WARN_ON(!(flags & (SG_MITER_TO_SG | SG_MITER_FROM_SG)));
647 miter->__flags = flags;
648 }
649 EXPORT_SYMBOL(sg_miter_start);
651 static bool sg_miter_get_next_page(struct sg_mapping_iter *miter)
652 {
653 if (!miter->__remaining) {
654 struct scatterlist *sg;
655 unsigned long pgoffset;
657 if (!__sg_page_iter_next(&miter->piter))
658 return false;
660 sg = miter->piter.sg;
661 pgoffset = miter->piter.sg_pgoffset;
663 miter->__offset = pgoffset ? 0 : sg->offset;
664 miter->__remaining = sg->offset + sg->length -
665 (pgoffset << PAGE_SHIFT) - miter->__offset;
666 miter->__remaining = min_t(unsigned long, miter->__remaining,
667 PAGE_SIZE - miter->__offset);
668 }
670 return true;
671 }
673 /**
674 * sg_miter_skip - reposition mapping iterator
675 * @miter: sg mapping iter to be skipped
676 * @offset: number of bytes to plus the current location
677 *
678 * Description:
679 * Sets the offset of @miter to its current location plus @offset bytes.
680 * If mapping iterator @miter has been proceeded by sg_miter_next(), this
681 * stops @miter.
682 *
683 * Context:
684 * Don't care if @miter is stopped, or not proceeded yet.
685 * Otherwise, preemption disabled if the SG_MITER_ATOMIC is set.
686 *
687 * Returns:
688 * true if @miter contains the valid mapping. false if end of sg
689 * list is reached.
690 */
691 bool sg_miter_skip(struct sg_mapping_iter *miter, off_t offset)
692 {
693 sg_miter_stop(miter);
695 while (offset) {
696 off_t consumed;
698 if (!sg_miter_get_next_page(miter))
699 return false;
701 consumed = min_t(off_t, offset, miter->__remaining);
702 miter->__offset += consumed;
703 miter->__remaining -= consumed;
704 offset -= consumed;
705 }
707 return true;
708 }
709 EXPORT_SYMBOL(sg_miter_skip);
711 /**
712 * sg_miter_next - proceed mapping iterator to the next mapping
713 * @miter: sg mapping iter to proceed
714 *
715 * Description:
716 * Proceeds @miter to the next mapping. @miter should have been started
717 * using sg_miter_start(). On successful return, @miter->page,
718 * @miter->addr and @miter->length point to the current mapping.
719 *
720 * Context:
721 * Preemption disabled if SG_MITER_ATOMIC. Preemption must stay disabled
722 * till @miter is stopped. May sleep if !SG_MITER_ATOMIC.
723 *
724 * Returns:
725 * true if @miter contains the next mapping. false if end of sg
726 * list is reached.
727 */
728 bool sg_miter_next(struct sg_mapping_iter *miter)
729 {
730 sg_miter_stop(miter);
732 /*
733 * Get to the next page if necessary.
734 * __remaining, __offset is adjusted by sg_miter_stop
735 */
736 if (!sg_miter_get_next_page(miter))
737 return false;
739 miter->page = sg_page_iter_page(&miter->piter);
740 miter->consumed = miter->length = miter->__remaining;
742 if (miter->__flags & SG_MITER_ATOMIC)
743 miter->addr = kmap_atomic(miter->page) + miter->__offset;
744 else
745 miter->addr = kmap(miter->page) + miter->__offset;
747 return true;
748 }
749 EXPORT_SYMBOL(sg_miter_next);
751 /**
752 * sg_miter_stop - stop mapping iteration
753 * @miter: sg mapping iter to be stopped
754 *
755 * Description:
756 * Stops mapping iterator @miter. @miter should have been started
757 * using sg_miter_start(). A stopped iteration can be resumed by
758 * calling sg_miter_next() on it. This is useful when resources (kmap)
759 * need to be released during iteration.
760 *
761 * Context:
762 * Preemption disabled if the SG_MITER_ATOMIC is set. Don't care
763 * otherwise.
764 */
765 void sg_miter_stop(struct sg_mapping_iter *miter)
766 {
767 WARN_ON(miter->consumed > miter->length);
769 /* drop resources from the last iteration */
770 if (miter->addr) {
771 miter->__offset += miter->consumed;
772 miter->__remaining -= miter->consumed;
774 if ((miter->__flags & SG_MITER_TO_SG) &&
775 !PageSlab(miter->page))
776 flush_kernel_dcache_page(miter->page);
778 if (miter->__flags & SG_MITER_ATOMIC) {
779 WARN_ON_ONCE(preemptible());
780 kunmap_atomic(miter->addr);
781 } else
782 kunmap(miter->page);
784 miter->page = NULL;
785 miter->addr = NULL;
786 miter->length = 0;
787 miter->consumed = 0;
788 }
789 }
790 EXPORT_SYMBOL(sg_miter_stop);
792 /**
793 * sg_copy_buffer - Copy data between a linear buffer and an SG list
794 * @sgl: The SG list
795 * @nents: Number of SG entries
796 * @buf: Where to copy from
797 * @buflen: The number of bytes to copy
798 * @skip: Number of bytes to skip before copying
799 * @to_buffer: transfer direction (true == from an sg list to a
800 * buffer, false == from a buffer to an sg list
801 *
802 * Returns the number of copied bytes.
803 *
804 **/
805 size_t sg_copy_buffer(struct scatterlist *sgl, unsigned int nents, void *buf,
806 size_t buflen, off_t skip, bool to_buffer)
807 {
808 unsigned int offset = 0;
809 struct sg_mapping_iter miter;
810 unsigned int sg_flags = SG_MITER_ATOMIC;
812 if (to_buffer)
813 sg_flags |= SG_MITER_FROM_SG;
814 else
815 sg_flags |= SG_MITER_TO_SG;
817 sg_miter_start(&miter, sgl, nents, sg_flags);
819 if (!sg_miter_skip(&miter, skip))
820 return false;
822 while ((offset < buflen) && sg_miter_next(&miter)) {
823 unsigned int len;
825 len = min(miter.length, buflen - offset);
827 if (to_buffer)
828 memcpy(buf + offset, miter.addr, len);
829 else
830 memcpy(miter.addr, buf + offset, len);
832 offset += len;
833 }
835 sg_miter_stop(&miter);
837 return offset;
838 }
839 EXPORT_SYMBOL(sg_copy_buffer);
841 /**
842 * sg_copy_from_buffer - Copy from a linear buffer to an SG list
843 * @sgl: The SG list
844 * @nents: Number of SG entries
845 * @buf: Where to copy from
846 * @buflen: The number of bytes to copy
847 *
848 * Returns the number of copied bytes.
849 *
850 **/
851 size_t sg_copy_from_buffer(struct scatterlist *sgl, unsigned int nents,
852 const void *buf, size_t buflen)
853 {
854 return sg_copy_buffer(sgl, nents, (void *)buf, buflen, 0, false);
855 }
856 EXPORT_SYMBOL(sg_copy_from_buffer);
858 /**
859 * sg_copy_to_buffer - Copy from an SG list to a linear buffer
860 * @sgl: The SG list
861 * @nents: Number of SG entries
862 * @buf: Where to copy to
863 * @buflen: The number of bytes to copy
864 *
865 * Returns the number of copied bytes.
866 *
867 **/
868 size_t sg_copy_to_buffer(struct scatterlist *sgl, unsigned int nents,
869 void *buf, size_t buflen)
870 {
871 return sg_copy_buffer(sgl, nents, buf, buflen, 0, true);
872 }
873 EXPORT_SYMBOL(sg_copy_to_buffer);
875 /**
876 * sg_pcopy_from_buffer - Copy from a linear buffer to an SG list
877 * @sgl: The SG list
878 * @nents: Number of SG entries
879 * @buf: Where to copy from
880 * @buflen: The number of bytes to copy
881 * @skip: Number of bytes to skip before copying
882 *
883 * Returns the number of copied bytes.
884 *
885 **/
886 size_t sg_pcopy_from_buffer(struct scatterlist *sgl, unsigned int nents,
887 const void *buf, size_t buflen, off_t skip)
888 {
889 return sg_copy_buffer(sgl, nents, (void *)buf, buflen, skip, false);
890 }
891 EXPORT_SYMBOL(sg_pcopy_from_buffer);
893 /**
894 * sg_pcopy_to_buffer - Copy from an SG list to a linear buffer
895 * @sgl: The SG list
896 * @nents: Number of SG entries
897 * @buf: Where to copy to
898 * @buflen: The number of bytes to copy
899 * @skip: Number of bytes to skip before copying
900 *
901 * Returns the number of copied bytes.
902 *
903 **/
904 size_t sg_pcopy_to_buffer(struct scatterlist *sgl, unsigned int nents,
905 void *buf, size_t buflen, off_t skip)
906 {
907 return sg_copy_buffer(sgl, nents, buf, buflen, skip, true);
908 }
909 EXPORT_SYMBOL(sg_pcopy_to_buffer);
911 /**
912 * sg_zero_buffer - Zero-out a part of a SG list
913 * @sgl: The SG list
914 * @nents: Number of SG entries
915 * @buflen: The number of bytes to zero out
916 * @skip: Number of bytes to skip before zeroing
917 *
918 * Returns the number of bytes zeroed.
919 **/
920 size_t sg_zero_buffer(struct scatterlist *sgl, unsigned int nents,
921 size_t buflen, off_t skip)
922 {
923 unsigned int offset = 0;
924 struct sg_mapping_iter miter;
925 unsigned int sg_flags = SG_MITER_ATOMIC | SG_MITER_TO_SG;
927 sg_miter_start(&miter, sgl, nents, sg_flags);
929 if (!sg_miter_skip(&miter, skip))
930 return false;
932 while (offset < buflen && sg_miter_next(&miter)) {
933 unsigned int len;
935 len = min(miter.length, buflen - offset);
936 memset(miter.addr, 0, len);
938 offset += len;
939 }
941 sg_miter_stop(&miter);
942 return offset;
943 }
944 EXPORT_SYMBOL(sg_zero_buffer);