1 /*
2 * Generic stack depot for storing stack traces.
3 *
4 * Some debugging tools need to save stack traces of certain events which can
5 * be later presented to the user. For example, KASAN needs to safe alloc and
6 * free stacks for each object, but storing two stack traces per object
7 * requires too much memory (e.g. SLUB_DEBUG needs 256 bytes per object for
8 * that).
9 *
10 * Instead, stack depot maintains a hashtable of unique stacktraces. Since alloc
11 * and free stacks repeat a lot, we save about 100x space.
12 * Stacks are never removed from depot, so we store them contiguously one after
13 * another in a contiguos memory allocation.
14 *
15 * Author: Alexander Potapenko <glider@google.com>
16 * Copyright (C) 2016 Google, Inc.
17 *
18 * Based on code by Dmitry Chernenkov.
19 *
20 * This program is free software; you can redistribute it and/or
21 * modify it under the terms of the GNU General Public License
22 * version 2 as published by the Free Software Foundation.
23 *
24 * This program is distributed in the hope that it will be useful, but
25 * WITHOUT ANY WARRANTY; without even the implied warranty of
26 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
27 * General Public License for more details.
28 *
29 */
31 #include <linux/gfp.h>
32 #include <linux/jhash.h>
33 #include <linux/kernel.h>
34 #include <linux/mm.h>
35 #include <linux/percpu.h>
36 #include <linux/printk.h>
37 #include <linux/slab.h>
38 #include <linux/stacktrace.h>
39 #include <linux/stackdepot.h>
40 #include <linux/string.h>
41 #include <linux/types.h>
43 #define DEPOT_STACK_BITS (sizeof(depot_stack_handle_t) * 8)
45 #define STACK_ALLOC_NULL_PROTECTION_BITS 1
46 #define STACK_ALLOC_ORDER 2 /* 'Slab' size order for stack depot, 4 pages */
47 #define STACK_ALLOC_SIZE (1LL << (PAGE_SHIFT + STACK_ALLOC_ORDER))
48 #define STACK_ALLOC_ALIGN 4
49 #define STACK_ALLOC_OFFSET_BITS (STACK_ALLOC_ORDER + PAGE_SHIFT - \
50 STACK_ALLOC_ALIGN)
51 #define STACK_ALLOC_INDEX_BITS (DEPOT_STACK_BITS - \
52 STACK_ALLOC_NULL_PROTECTION_BITS - STACK_ALLOC_OFFSET_BITS)
53 #define STACK_ALLOC_SLABS_CAP 8192
54 #define STACK_ALLOC_MAX_SLABS \
55 (((1LL << (STACK_ALLOC_INDEX_BITS)) < STACK_ALLOC_SLABS_CAP) ? \
56 (1LL << (STACK_ALLOC_INDEX_BITS)) : STACK_ALLOC_SLABS_CAP)
58 /* The compact structure to store the reference to stacks. */
59 union handle_parts {
60 depot_stack_handle_t handle;
61 struct {
62 u32 slabindex : STACK_ALLOC_INDEX_BITS;
63 u32 offset : STACK_ALLOC_OFFSET_BITS;
64 u32 valid : STACK_ALLOC_NULL_PROTECTION_BITS;
65 };
66 };
68 struct stack_record {
69 struct stack_record *next; /* Link in the hashtable */
70 u32 hash; /* Hash in the hastable */
71 u32 size; /* Number of frames in the stack */
72 union handle_parts handle;
73 unsigned long entries[1]; /* Variable-sized array of entries. */
74 };
76 static void *stack_slabs[STACK_ALLOC_MAX_SLABS];
78 static int depot_index;
79 static int next_slab_inited;
80 static size_t depot_offset;
81 static DEFINE_SPINLOCK(depot_lock);
83 static bool init_stack_slab(void **prealloc)
84 {
85 if (!*prealloc)
86 return false;
87 /*
88 * This smp_load_acquire() pairs with smp_store_release() to
89 * |next_slab_inited| below and in depot_alloc_stack().
90 */
91 if (smp_load_acquire(&next_slab_inited))
92 return true;
93 if (stack_slabs[depot_index] == NULL) {
94 stack_slabs[depot_index] = *prealloc;
95 } else {
96 stack_slabs[depot_index + 1] = *prealloc;
97 /*
98 * This smp_store_release pairs with smp_load_acquire() from
99 * |next_slab_inited| above and in depot_save_stack().
100 */
101 smp_store_release(&next_slab_inited, 1);
102 }
103 *prealloc = NULL;
104 return true;
105 }
107 /* Allocation of a new stack in raw storage */
108 static struct stack_record *depot_alloc_stack(unsigned long *entries, int size,
109 u32 hash, void **prealloc, gfp_t alloc_flags)
110 {
111 int required_size = offsetof(struct stack_record, entries) +
112 sizeof(unsigned long) * size;
113 struct stack_record *stack;
115 required_size = ALIGN(required_size, 1 << STACK_ALLOC_ALIGN);
117 if (unlikely(depot_offset + required_size > STACK_ALLOC_SIZE)) {
118 if (unlikely(depot_index + 1 >= STACK_ALLOC_MAX_SLABS)) {
119 WARN_ONCE(1, "Stack depot reached limit capacity");
120 return NULL;
121 }
122 depot_index++;
123 depot_offset = 0;
124 /*
125 * smp_store_release() here pairs with smp_load_acquire() from
126 * |next_slab_inited| in depot_save_stack() and
127 * init_stack_slab().
128 */
129 if (depot_index + 1 < STACK_ALLOC_MAX_SLABS)
130 smp_store_release(&next_slab_inited, 0);
131 }
132 init_stack_slab(prealloc);
133 if (stack_slabs[depot_index] == NULL)
134 return NULL;
136 stack = stack_slabs[depot_index] + depot_offset;
138 stack->hash = hash;
139 stack->size = size;
140 stack->handle.slabindex = depot_index;
141 stack->handle.offset = depot_offset >> STACK_ALLOC_ALIGN;
142 stack->handle.valid = 1;
143 memcpy(stack->entries, entries, size * sizeof(unsigned long));
144 depot_offset += required_size;
146 return stack;
147 }
149 #define STACK_HASH_ORDER 20
150 #define STACK_HASH_SIZE (1L << STACK_HASH_ORDER)
151 #define STACK_HASH_MASK (STACK_HASH_SIZE - 1)
152 #define STACK_HASH_SEED 0x9747b28c
154 static struct stack_record *stack_table[STACK_HASH_SIZE] = {
155 [0 ... STACK_HASH_SIZE - 1] = NULL
156 };
158 /* Calculate hash for a stack */
159 static inline u32 hash_stack(unsigned long *entries, unsigned int size)
160 {
161 return jhash2((u32 *)entries,
162 size * sizeof(unsigned long) / sizeof(u32),
163 STACK_HASH_SEED);
164 }
166 /* Use our own, non-instrumented version of memcmp().
167 *
168 * We actually don't care about the order, just the equality.
169 */
170 static inline
171 int stackdepot_memcmp(const unsigned long *u1, const unsigned long *u2,
172 unsigned int n)
173 {
174 for ( ; n-- ; u1++, u2++) {
175 if (*u1 != *u2)
176 return 1;
177 }
178 return 0;
179 }
181 /* Find a stack that is equal to the one stored in entries in the hash */
182 static inline struct stack_record *find_stack(struct stack_record *bucket,
183 unsigned long *entries, int size,
184 u32 hash)
185 {
186 struct stack_record *found;
188 for (found = bucket; found; found = found->next) {
189 if (found->hash == hash &&
190 found->size == size &&
191 !stackdepot_memcmp(entries, found->entries, size))
192 return found;
193 }
194 return NULL;
195 }
197 void depot_fetch_stack(depot_stack_handle_t handle, struct stack_trace *trace)
198 {
199 union handle_parts parts = { .handle = handle };
200 void *slab = stack_slabs[parts.slabindex];
201 size_t offset = parts.offset << STACK_ALLOC_ALIGN;
202 struct stack_record *stack = slab + offset;
204 trace->nr_entries = trace->max_entries = stack->size;
205 trace->entries = stack->entries;
206 trace->skip = 0;
207 }
208 EXPORT_SYMBOL_GPL(depot_fetch_stack);
210 /**
211 * depot_save_stack - save stack in a stack depot.
212 * @trace - the stacktrace to save.
213 * @alloc_flags - flags for allocating additional memory if required.
214 *
215 * Returns the handle of the stack struct stored in depot.
216 */
217 depot_stack_handle_t depot_save_stack(struct stack_trace *trace,
218 gfp_t alloc_flags)
219 {
220 u32 hash;
221 depot_stack_handle_t retval = 0;
222 struct stack_record *found = NULL, **bucket;
223 unsigned long flags;
224 struct page *page = NULL;
225 void *prealloc = NULL;
227 if (unlikely(trace->nr_entries == 0))
228 goto fast_exit;
230 hash = hash_stack(trace->entries, trace->nr_entries);
231 bucket = &stack_table[hash & STACK_HASH_MASK];
233 /*
234 * Fast path: look the stack trace up without locking.
235 * The smp_load_acquire() here pairs with smp_store_release() to
236 * |bucket| below.
237 */
238 found = find_stack(smp_load_acquire(bucket), trace->entries,
239 trace->nr_entries, hash);
240 if (found)
241 goto exit;
243 /*
244 * Check if the current or the next stack slab need to be initialized.
245 * If so, allocate the memory - we won't be able to do that under the
246 * lock.
247 *
248 * The smp_load_acquire() here pairs with smp_store_release() to
249 * |next_slab_inited| in depot_alloc_stack() and init_stack_slab().
250 */
251 if (unlikely(!smp_load_acquire(&next_slab_inited))) {
252 /*
253 * Zero out zone modifiers, as we don't have specific zone
254 * requirements. Keep the flags related to allocation in atomic
255 * contexts and I/O.
256 */
257 alloc_flags &= ~GFP_ZONEMASK;
258 alloc_flags &= (GFP_ATOMIC | GFP_KERNEL);
259 alloc_flags |= __GFP_NOWARN;
260 page = alloc_pages(alloc_flags, STACK_ALLOC_ORDER);
261 if (page)
262 prealloc = page_address(page);
263 }
265 spin_lock_irqsave(&depot_lock, flags);
267 found = find_stack(*bucket, trace->entries, trace->nr_entries, hash);
268 if (!found) {
269 struct stack_record *new =
270 depot_alloc_stack(trace->entries, trace->nr_entries,
271 hash, &prealloc, alloc_flags);
272 if (new) {
273 new->next = *bucket;
274 /*
275 * This smp_store_release() pairs with
276 * smp_load_acquire() from |bucket| above.
277 */
278 smp_store_release(bucket, new);
279 found = new;
280 }
281 } else if (prealloc) {
282 /*
283 * We didn't need to store this stack trace, but let's keep
284 * the preallocated memory for the future.
285 */
286 WARN_ON(!init_stack_slab(&prealloc));
287 }
289 spin_unlock_irqrestore(&depot_lock, flags);
290 exit:
291 if (prealloc) {
292 /* Nobody used this memory, ok to free it. */
293 free_pages((unsigned long)prealloc, STACK_ALLOC_ORDER);
294 }
295 if (found)
296 retval = found->handle.handle;
297 fast_exit:
298 return retval;
299 }
300 EXPORT_SYMBOL_GPL(depot_save_stack);