]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - mm/readahead.c
Merge tag 'alloc-args-v4.19-rc8' of https://git.kernel.org/pub/scm/linux/kernel/git...
[rpmsg/rpmsg.git] / mm / readahead.c
1 /*
2  * mm/readahead.c - address_space-level file readahead.
3  *
4  * Copyright (C) 2002, Linus Torvalds
5  *
6  * 09Apr2002    Andrew Morton
7  *              Initial version.
8  */
10 #include <linux/kernel.h>
11 #include <linux/dax.h>
12 #include <linux/gfp.h>
13 #include <linux/export.h>
14 #include <linux/blkdev.h>
15 #include <linux/backing-dev.h>
16 #include <linux/task_io_accounting_ops.h>
17 #include <linux/pagevec.h>
18 #include <linux/pagemap.h>
19 #include <linux/syscalls.h>
20 #include <linux/file.h>
21 #include <linux/mm_inline.h>
22 #include <linux/blk-cgroup.h>
23 #include <linux/fadvise.h>
25 #include "internal.h"
27 /*
28  * Initialise a struct file's readahead state.  Assumes that the caller has
29  * memset *ra to zero.
30  */
31 void
32 file_ra_state_init(struct file_ra_state *ra, struct address_space *mapping)
33 {
34         ra->ra_pages = inode_to_bdi(mapping->host)->ra_pages;
35         ra->prev_pos = -1;
36 }
37 EXPORT_SYMBOL_GPL(file_ra_state_init);
39 /*
40  * see if a page needs releasing upon read_cache_pages() failure
41  * - the caller of read_cache_pages() may have set PG_private or PG_fscache
42  *   before calling, such as the NFS fs marking pages that are cached locally
43  *   on disk, thus we need to give the fs a chance to clean up in the event of
44  *   an error
45  */
46 static void read_cache_pages_invalidate_page(struct address_space *mapping,
47                                              struct page *page)
48 {
49         if (page_has_private(page)) {
50                 if (!trylock_page(page))
51                         BUG();
52                 page->mapping = mapping;
53                 do_invalidatepage(page, 0, PAGE_SIZE);
54                 page->mapping = NULL;
55                 unlock_page(page);
56         }
57         put_page(page);
58 }
60 /*
61  * release a list of pages, invalidating them first if need be
62  */
63 static void read_cache_pages_invalidate_pages(struct address_space *mapping,
64                                               struct list_head *pages)
65 {
66         struct page *victim;
68         while (!list_empty(pages)) {
69                 victim = lru_to_page(pages);
70                 list_del(&victim->lru);
71                 read_cache_pages_invalidate_page(mapping, victim);
72         }
73 }
75 /**
76  * read_cache_pages - populate an address space with some pages & start reads against them
77  * @mapping: the address_space
78  * @pages: The address of a list_head which contains the target pages.  These
79  *   pages have their ->index populated and are otherwise uninitialised.
80  * @filler: callback routine for filling a single page.
81  * @data: private data for the callback routine.
82  *
83  * Hides the details of the LRU cache etc from the filesystems.
84  */
85 int read_cache_pages(struct address_space *mapping, struct list_head *pages,
86                         int (*filler)(void *, struct page *), void *data)
87 {
88         struct page *page;
89         int ret = 0;
91         while (!list_empty(pages)) {
92                 page = lru_to_page(pages);
93                 list_del(&page->lru);
94                 if (add_to_page_cache_lru(page, mapping, page->index,
95                                 readahead_gfp_mask(mapping))) {
96                         read_cache_pages_invalidate_page(mapping, page);
97                         continue;
98                 }
99                 put_page(page);
101                 ret = filler(data, page);
102                 if (unlikely(ret)) {
103                         read_cache_pages_invalidate_pages(mapping, pages);
104                         break;
105                 }
106                 task_io_account_read(PAGE_SIZE);
107         }
108         return ret;
111 EXPORT_SYMBOL(read_cache_pages);
113 static int read_pages(struct address_space *mapping, struct file *filp,
114                 struct list_head *pages, unsigned int nr_pages, gfp_t gfp)
116         struct blk_plug plug;
117         unsigned page_idx;
118         int ret;
120         blk_start_plug(&plug);
122         if (mapping->a_ops->readpages) {
123                 ret = mapping->a_ops->readpages(filp, mapping, pages, nr_pages);
124                 /* Clean up the remaining pages */
125                 put_pages_list(pages);
126                 goto out;
127         }
129         for (page_idx = 0; page_idx < nr_pages; page_idx++) {
130                 struct page *page = lru_to_page(pages);
131                 list_del(&page->lru);
132                 if (!add_to_page_cache_lru(page, mapping, page->index, gfp))
133                         mapping->a_ops->readpage(filp, page);
134                 put_page(page);
135         }
136         ret = 0;
138 out:
139         blk_finish_plug(&plug);
141         return ret;
144 /*
145  * __do_page_cache_readahead() actually reads a chunk of disk.  It allocates
146  * the pages first, then submits them for I/O. This avoids the very bad
147  * behaviour which would occur if page allocations are causing VM writeback.
148  * We really don't want to intermingle reads and writes like that.
149  *
150  * Returns the number of pages requested, or the maximum amount of I/O allowed.
151  */
152 unsigned int __do_page_cache_readahead(struct address_space *mapping,
153                 struct file *filp, pgoff_t offset, unsigned long nr_to_read,
154                 unsigned long lookahead_size)
156         struct inode *inode = mapping->host;
157         struct page *page;
158         unsigned long end_index;        /* The last page we want to read */
159         LIST_HEAD(page_pool);
160         int page_idx;
161         unsigned int nr_pages = 0;
162         loff_t isize = i_size_read(inode);
163         gfp_t gfp_mask = readahead_gfp_mask(mapping);
165         if (isize == 0)
166                 goto out;
168         end_index = ((isize - 1) >> PAGE_SHIFT);
170         /*
171          * Preallocate as many pages as we will need.
172          */
173         for (page_idx = 0; page_idx < nr_to_read; page_idx++) {
174                 pgoff_t page_offset = offset + page_idx;
176                 if (page_offset > end_index)
177                         break;
179                 rcu_read_lock();
180                 page = radix_tree_lookup(&mapping->i_pages, page_offset);
181                 rcu_read_unlock();
182                 if (page && !radix_tree_exceptional_entry(page)) {
183                         /*
184                          * Page already present?  Kick off the current batch of
185                          * contiguous pages before continuing with the next
186                          * batch.
187                          */
188                         if (nr_pages)
189                                 read_pages(mapping, filp, &page_pool, nr_pages,
190                                                 gfp_mask);
191                         nr_pages = 0;
192                         continue;
193                 }
195                 page = __page_cache_alloc(gfp_mask);
196                 if (!page)
197                         break;
198                 page->index = page_offset;
199                 list_add(&page->lru, &page_pool);
200                 if (page_idx == nr_to_read - lookahead_size)
201                         SetPageReadahead(page);
202                 nr_pages++;
203         }
205         /*
206          * Now start the IO.  We ignore I/O errors - if the page is not
207          * uptodate then the caller will launch readpage again, and
208          * will then handle the error.
209          */
210         if (nr_pages)
211                 read_pages(mapping, filp, &page_pool, nr_pages, gfp_mask);
212         BUG_ON(!list_empty(&page_pool));
213 out:
214         return nr_pages;
217 /*
218  * Chunk the readahead into 2 megabyte units, so that we don't pin too much
219  * memory at once.
220  */
221 int force_page_cache_readahead(struct address_space *mapping, struct file *filp,
222                                pgoff_t offset, unsigned long nr_to_read)
224         struct backing_dev_info *bdi = inode_to_bdi(mapping->host);
225         struct file_ra_state *ra = &filp->f_ra;
226         unsigned long max_pages;
228         if (unlikely(!mapping->a_ops->readpage && !mapping->a_ops->readpages))
229                 return -EINVAL;
231         /*
232          * If the request exceeds the readahead window, allow the read to
233          * be up to the optimal hardware IO size
234          */
235         max_pages = max_t(unsigned long, bdi->io_pages, ra->ra_pages);
236         nr_to_read = min(nr_to_read, max_pages);
237         while (nr_to_read) {
238                 unsigned long this_chunk = (2 * 1024 * 1024) / PAGE_SIZE;
240                 if (this_chunk > nr_to_read)
241                         this_chunk = nr_to_read;
242                 __do_page_cache_readahead(mapping, filp, offset, this_chunk, 0);
244                 offset += this_chunk;
245                 nr_to_read -= this_chunk;
246         }
247         return 0;
250 /*
251  * Set the initial window size, round to next power of 2 and square
252  * for small size, x 4 for medium, and x 2 for large
253  * for 128k (32 page) max ra
254  * 1-8 page = 32k initial, > 8 page = 128k initial
255  */
256 static unsigned long get_init_ra_size(unsigned long size, unsigned long max)
258         unsigned long newsize = roundup_pow_of_two(size);
260         if (newsize <= max / 32)
261                 newsize = newsize * 4;
262         else if (newsize <= max / 4)
263                 newsize = newsize * 2;
264         else
265                 newsize = max;
267         return newsize;
270 /*
271  *  Get the previous window size, ramp it up, and
272  *  return it as the new window size.
273  */
274 static unsigned long get_next_ra_size(struct file_ra_state *ra,
275                                                 unsigned long max)
277         unsigned long cur = ra->size;
278         unsigned long newsize;
280         if (cur < max / 16)
281                 newsize = 4 * cur;
282         else
283                 newsize = 2 * cur;
285         return min(newsize, max);
288 /*
289  * On-demand readahead design.
290  *
291  * The fields in struct file_ra_state represent the most-recently-executed
292  * readahead attempt:
293  *
294  *                        |<----- async_size ---------|
295  *     |------------------- size -------------------->|
296  *     |==================#===========================|
297  *     ^start             ^page marked with PG_readahead
298  *
299  * To overlap application thinking time and disk I/O time, we do
300  * `readahead pipelining': Do not wait until the application consumed all
301  * readahead pages and stalled on the missing page at readahead_index;
302  * Instead, submit an asynchronous readahead I/O as soon as there are
303  * only async_size pages left in the readahead window. Normally async_size
304  * will be equal to size, for maximum pipelining.
305  *
306  * In interleaved sequential reads, concurrent streams on the same fd can
307  * be invalidating each other's readahead state. So we flag the new readahead
308  * page at (start+size-async_size) with PG_readahead, and use it as readahead
309  * indicator. The flag won't be set on already cached pages, to avoid the
310  * readahead-for-nothing fuss, saving pointless page cache lookups.
311  *
312  * prev_pos tracks the last visited byte in the _previous_ read request.
313  * It should be maintained by the caller, and will be used for detecting
314  * small random reads. Note that the readahead algorithm checks loosely
315  * for sequential patterns. Hence interleaved reads might be served as
316  * sequential ones.
317  *
318  * There is a special-case: if the first page which the application tries to
319  * read happens to be the first page of the file, it is assumed that a linear
320  * read is about to happen and the window is immediately set to the initial size
321  * based on I/O request size and the max_readahead.
322  *
323  * The code ramps up the readahead size aggressively at first, but slow down as
324  * it approaches max_readhead.
325  */
327 /*
328  * Count contiguously cached pages from @offset-1 to @offset-@max,
329  * this count is a conservative estimation of
330  *      - length of the sequential read sequence, or
331  *      - thrashing threshold in memory tight systems
332  */
333 static pgoff_t count_history_pages(struct address_space *mapping,
334                                    pgoff_t offset, unsigned long max)
336         pgoff_t head;
338         rcu_read_lock();
339         head = page_cache_prev_hole(mapping, offset - 1, max);
340         rcu_read_unlock();
342         return offset - 1 - head;
345 /*
346  * page cache context based read-ahead
347  */
348 static int try_context_readahead(struct address_space *mapping,
349                                  struct file_ra_state *ra,
350                                  pgoff_t offset,
351                                  unsigned long req_size,
352                                  unsigned long max)
354         pgoff_t size;
356         size = count_history_pages(mapping, offset, max);
358         /*
359          * not enough history pages:
360          * it could be a random read
361          */
362         if (size <= req_size)
363                 return 0;
365         /*
366          * starts from beginning of file:
367          * it is a strong indication of long-run stream (or whole-file-read)
368          */
369         if (size >= offset)
370                 size *= 2;
372         ra->start = offset;
373         ra->size = min(size + req_size, max);
374         ra->async_size = 1;
376         return 1;
379 /*
380  * A minimal readahead algorithm for trivial sequential/random reads.
381  */
382 static unsigned long
383 ondemand_readahead(struct address_space *mapping,
384                    struct file_ra_state *ra, struct file *filp,
385                    bool hit_readahead_marker, pgoff_t offset,
386                    unsigned long req_size)
388         struct backing_dev_info *bdi = inode_to_bdi(mapping->host);
389         unsigned long max_pages = ra->ra_pages;
390         unsigned long add_pages;
391         pgoff_t prev_offset;
393         /*
394          * If the request exceeds the readahead window, allow the read to
395          * be up to the optimal hardware IO size
396          */
397         if (req_size > max_pages && bdi->io_pages > max_pages)
398                 max_pages = min(req_size, bdi->io_pages);
400         /*
401          * start of file
402          */
403         if (!offset)
404                 goto initial_readahead;
406         /*
407          * It's the expected callback offset, assume sequential access.
408          * Ramp up sizes, and push forward the readahead window.
409          */
410         if ((offset == (ra->start + ra->size - ra->async_size) ||
411              offset == (ra->start + ra->size))) {
412                 ra->start += ra->size;
413                 ra->size = get_next_ra_size(ra, max_pages);
414                 ra->async_size = ra->size;
415                 goto readit;
416         }
418         /*
419          * Hit a marked page without valid readahead state.
420          * E.g. interleaved reads.
421          * Query the pagecache for async_size, which normally equals to
422          * readahead size. Ramp it up and use it as the new readahead size.
423          */
424         if (hit_readahead_marker) {
425                 pgoff_t start;
427                 rcu_read_lock();
428                 start = page_cache_next_hole(mapping, offset + 1, max_pages);
429                 rcu_read_unlock();
431                 if (!start || start - offset > max_pages)
432                         return 0;
434                 ra->start = start;
435                 ra->size = start - offset;      /* old async_size */
436                 ra->size += req_size;
437                 ra->size = get_next_ra_size(ra, max_pages);
438                 ra->async_size = ra->size;
439                 goto readit;
440         }
442         /*
443          * oversize read
444          */
445         if (req_size > max_pages)
446                 goto initial_readahead;
448         /*
449          * sequential cache miss
450          * trivial case: (offset - prev_offset) == 1
451          * unaligned reads: (offset - prev_offset) == 0
452          */
453         prev_offset = (unsigned long long)ra->prev_pos >> PAGE_SHIFT;
454         if (offset - prev_offset <= 1UL)
455                 goto initial_readahead;
457         /*
458          * Query the page cache and look for the traces(cached history pages)
459          * that a sequential stream would leave behind.
460          */
461         if (try_context_readahead(mapping, ra, offset, req_size, max_pages))
462                 goto readit;
464         /*
465          * standalone, small random read
466          * Read as is, and do not pollute the readahead state.
467          */
468         return __do_page_cache_readahead(mapping, filp, offset, req_size, 0);
470 initial_readahead:
471         ra->start = offset;
472         ra->size = get_init_ra_size(req_size, max_pages);
473         ra->async_size = ra->size > req_size ? ra->size - req_size : ra->size;
475 readit:
476         /*
477          * Will this read hit the readahead marker made by itself?
478          * If so, trigger the readahead marker hit now, and merge
479          * the resulted next readahead window into the current one.
480          * Take care of maximum IO pages as above.
481          */
482         if (offset == ra->start && ra->size == ra->async_size) {
483                 add_pages = get_next_ra_size(ra, max_pages);
484                 if (ra->size + add_pages <= max_pages) {
485                         ra->async_size = add_pages;
486                         ra->size += add_pages;
487                 } else {
488                         ra->size = max_pages;
489                         ra->async_size = max_pages >> 1;
490                 }
491         }
493         return ra_submit(ra, mapping, filp);
496 /**
497  * page_cache_sync_readahead - generic file readahead
498  * @mapping: address_space which holds the pagecache and I/O vectors
499  * @ra: file_ra_state which holds the readahead state
500  * @filp: passed on to ->readpage() and ->readpages()
501  * @offset: start offset into @mapping, in pagecache page-sized units
502  * @req_size: hint: total size of the read which the caller is performing in
503  *            pagecache pages
504  *
505  * page_cache_sync_readahead() should be called when a cache miss happened:
506  * it will submit the read.  The readahead logic may decide to piggyback more
507  * pages onto the read request if access patterns suggest it will improve
508  * performance.
509  */
510 void page_cache_sync_readahead(struct address_space *mapping,
511                                struct file_ra_state *ra, struct file *filp,
512                                pgoff_t offset, unsigned long req_size)
514         /* no read-ahead */
515         if (!ra->ra_pages)
516                 return;
518         if (blk_cgroup_congested())
519                 return;
521         /* be dumb */
522         if (filp && (filp->f_mode & FMODE_RANDOM)) {
523                 force_page_cache_readahead(mapping, filp, offset, req_size);
524                 return;
525         }
527         /* do read-ahead */
528         ondemand_readahead(mapping, ra, filp, false, offset, req_size);
530 EXPORT_SYMBOL_GPL(page_cache_sync_readahead);
532 /**
533  * page_cache_async_readahead - file readahead for marked pages
534  * @mapping: address_space which holds the pagecache and I/O vectors
535  * @ra: file_ra_state which holds the readahead state
536  * @filp: passed on to ->readpage() and ->readpages()
537  * @page: the page at @offset which has the PG_readahead flag set
538  * @offset: start offset into @mapping, in pagecache page-sized units
539  * @req_size: hint: total size of the read which the caller is performing in
540  *            pagecache pages
541  *
542  * page_cache_async_readahead() should be called when a page is used which
543  * has the PG_readahead flag; this is a marker to suggest that the application
544  * has used up enough of the readahead window that we should start pulling in
545  * more pages.
546  */
547 void
548 page_cache_async_readahead(struct address_space *mapping,
549                            struct file_ra_state *ra, struct file *filp,
550                            struct page *page, pgoff_t offset,
551                            unsigned long req_size)
553         /* no read-ahead */
554         if (!ra->ra_pages)
555                 return;
557         /*
558          * Same bit is used for PG_readahead and PG_reclaim.
559          */
560         if (PageWriteback(page))
561                 return;
563         ClearPageReadahead(page);
565         /*
566          * Defer asynchronous read-ahead on IO congestion.
567          */
568         if (inode_read_congested(mapping->host))
569                 return;
571         if (blk_cgroup_congested())
572                 return;
574         /* do read-ahead */
575         ondemand_readahead(mapping, ra, filp, true, offset, req_size);
577 EXPORT_SYMBOL_GPL(page_cache_async_readahead);
579 ssize_t ksys_readahead(int fd, loff_t offset, size_t count)
581         ssize_t ret;
582         struct fd f;
584         ret = -EBADF;
585         f = fdget(fd);
586         if (!f.file || !(f.file->f_mode & FMODE_READ))
587                 goto out;
589         /*
590          * The readahead() syscall is intended to run only on files
591          * that can execute readahead. If readahead is not possible
592          * on this file, then we must return -EINVAL.
593          */
594         ret = -EINVAL;
595         if (!f.file->f_mapping || !f.file->f_mapping->a_ops ||
596             !S_ISREG(file_inode(f.file)->i_mode))
597                 goto out;
599         ret = vfs_fadvise(f.file, offset, count, POSIX_FADV_WILLNEED);
600 out:
601         fdput(f);
602         return ret;
605 SYSCALL_DEFINE3(readahead, int, fd, loff_t, offset, size_t, count)
607         return ksys_readahead(fd, offset, count);