]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - net/Kconfig
Revert "HACK: ARM: dts: dra7-ipu-common: Revert to CMA pools for IPU early boots"
[rpmsg/rpmsg.git] / net / Kconfig
1 #
2 # Network configuration
3 #
5 menuconfig NET
6         bool "Networking support"
7         select NLATTR
8         select GENERIC_NET_UTILS
9         select BPF
10         ---help---
11           Unless you really know what you are doing, you should say Y here.
12           The reason is that some programs need kernel networking support even
13           when running on a stand-alone machine that isn't connected to any
14           other computer.
16           If you are upgrading from an older kernel, you
17           should consider updating your networking tools too because changes
18           in the kernel and the tools often go hand in hand. The tools are
19           contained in the package net-tools, the location and version number
20           of which are given in <file:Documentation/Changes>.
22           For a general introduction to Linux networking, it is highly
23           recommended to read the NET-HOWTO, available from
24           <http://www.tldp.org/docs.html#howto>.
26 if NET
28 config WANT_COMPAT_NETLINK_MESSAGES
29         bool
30         help
31           This option can be selected by other options that need compat
32           netlink messages.
34 config COMPAT_NETLINK_MESSAGES
35         def_bool y
36         depends on COMPAT
37         depends on WEXT_CORE || WANT_COMPAT_NETLINK_MESSAGES
38         help
39           This option makes it possible to send different netlink messages
40           to tasks depending on whether the task is a compat task or not. To
41           achieve this, you need to set skb_shinfo(skb)->frag_list to the
42           compat skb before sending the skb, the netlink code will sort out
43           which message to actually pass to the task.
45           Newly written code should NEVER need this option but do
46           compat-independent messages instead!
48 config NET_INGRESS
49         bool
51 config NET_EGRESS
52         bool
54 menu "Networking options"
56 source "net/packet/Kconfig"
57 source "net/unix/Kconfig"
58 source "net/tls/Kconfig"
59 source "net/xfrm/Kconfig"
60 source "net/iucv/Kconfig"
61 source "net/smc/Kconfig"
62 source "net/xdp/Kconfig"
64 config INET
65         bool "TCP/IP networking"
66         select CRYPTO
67         select CRYPTO_AES
68         ---help---
69           These are the protocols used on the Internet and on most local
70           Ethernets. It is highly recommended to say Y here (this will enlarge
71           your kernel by about 400 KB), since some programs (e.g. the X window
72           system) use TCP/IP even if your machine is not connected to any
73           other computer. You will get the so-called loopback device which
74           allows you to ping yourself (great fun, that!).
76           For an excellent introduction to Linux networking, please read the
77           Linux Networking HOWTO, available from
78           <http://www.tldp.org/docs.html#howto>.
80           If you say Y here and also to "/proc file system support" and
81           "Sysctl support" below, you can change various aspects of the
82           behavior of the TCP/IP code by writing to the (virtual) files in
83           /proc/sys/net/ipv4/*; the options are explained in the file
84           <file:Documentation/networking/ip-sysctl.txt>.
86           Short answer: say Y.
88 if INET
89 source "net/ipv4/Kconfig"
90 source "net/ipv6/Kconfig"
91 source "net/netlabel/Kconfig"
93 endif # if INET
95 config NETWORK_SECMARK
96         bool "Security Marking"
97         help
98           This enables security marking of network packets, similar
99           to nfmark, but designated for security purposes.
100           If you are unsure how to answer this question, answer N.
102 config NET_PTP_CLASSIFY
103         def_bool n
105 config NETWORK_PHY_TIMESTAMPING
106         bool "Timestamping in PHY devices"
107         select NET_PTP_CLASSIFY
108         help
109           This allows timestamping of network packets by PHYs with
110           hardware timestamping capabilities. This option adds some
111           overhead in the transmit and receive paths.
113           If you are unsure how to answer this question, answer N.
115 menuconfig NETFILTER
116         bool "Network packet filtering framework (Netfilter)"
117         ---help---
118           Netfilter is a framework for filtering and mangling network packets
119           that pass through your Linux box.
121           The most common use of packet filtering is to run your Linux box as
122           a firewall protecting a local network from the Internet. The type of
123           firewall provided by this kernel support is called a "packet
124           filter", which means that it can reject individual network packets
125           based on type, source, destination etc. The other kind of firewall,
126           a "proxy-based" one, is more secure but more intrusive and more
127           bothersome to set up; it inspects the network traffic much more
128           closely, modifies it and has knowledge about the higher level
129           protocols, which a packet filter lacks. Moreover, proxy-based
130           firewalls often require changes to the programs running on the local
131           clients. Proxy-based firewalls don't need support by the kernel, but
132           they are often combined with a packet filter, which only works if
133           you say Y here.
135           You should also say Y here if you intend to use your Linux box as
136           the gateway to the Internet for a local network of machines without
137           globally valid IP addresses. This is called "masquerading": if one
138           of the computers on your local network wants to send something to
139           the outside, your box can "masquerade" as that computer, i.e. it
140           forwards the traffic to the intended outside destination, but
141           modifies the packets to make it look like they came from the
142           firewall box itself. It works both ways: if the outside host
143           replies, the Linux box will silently forward the traffic to the
144           correct local computer. This way, the computers on your local net
145           are completely invisible to the outside world, even though they can
146           reach the outside and can receive replies. It is even possible to
147           run globally visible servers from within a masqueraded local network
148           using a mechanism called portforwarding. Masquerading is also often
149           called NAT (Network Address Translation).
151           Another use of Netfilter is in transparent proxying: if a machine on
152           the local network tries to connect to an outside host, your Linux
153           box can transparently forward the traffic to a local server,
154           typically a caching proxy server.
156           Yet another use of Netfilter is building a bridging firewall. Using
157           a bridge with Network packet filtering enabled makes iptables "see"
158           the bridged traffic. For filtering on the lower network and Ethernet
159           protocols over the bridge, use ebtables (under bridge netfilter
160           configuration).
162           Various modules exist for netfilter which replace the previous
163           masquerading (ipmasqadm), packet filtering (ipchains), transparent
164           proxying, and portforwarding mechanisms. Please see
165           <file:Documentation/Changes> under "iptables" for the location of
166           these packages.
168 if NETFILTER
170 config NETFILTER_ADVANCED
171         bool "Advanced netfilter configuration"
172         depends on NETFILTER
173         default y
174         help
175           If you say Y here you can select between all the netfilter modules.
176           If you say N the more unusual ones will not be shown and the
177           basic ones needed by most people will default to 'M'.
179           If unsure, say Y.
181 config BRIDGE_NETFILTER
182         tristate "Bridged IP/ARP packets filtering"
183         depends on BRIDGE
184         depends on NETFILTER && INET
185         depends on NETFILTER_ADVANCED
186         select NETFILTER_FAMILY_BRIDGE
187         default m
188         ---help---
189           Enabling this option will let arptables resp. iptables see bridged
190           ARP resp. IP traffic. If you want a bridging firewall, you probably
191           want this option enabled.
192           Enabling or disabling this option doesn't enable or disable
193           ebtables.
195           If unsure, say N.
197 source "net/netfilter/Kconfig"
198 source "net/ipv4/netfilter/Kconfig"
199 source "net/ipv6/netfilter/Kconfig"
200 source "net/decnet/netfilter/Kconfig"
201 source "net/bridge/netfilter/Kconfig"
203 endif
205 source "net/bpfilter/Kconfig"
207 source "net/dccp/Kconfig"
208 source "net/sctp/Kconfig"
209 source "net/rds/Kconfig"
210 source "net/tipc/Kconfig"
211 source "net/atm/Kconfig"
212 source "net/l2tp/Kconfig"
213 source "net/802/Kconfig"
214 source "net/bridge/Kconfig"
215 source "net/dsa/Kconfig"
216 source "net/8021q/Kconfig"
217 source "net/decnet/Kconfig"
218 source "net/llc/Kconfig"
219 source "drivers/net/appletalk/Kconfig"
220 source "net/x25/Kconfig"
221 source "net/lapb/Kconfig"
222 source "net/phonet/Kconfig"
223 source "net/6lowpan/Kconfig"
224 source "net/ieee802154/Kconfig"
225 source "net/mac802154/Kconfig"
226 source "net/sched/Kconfig"
227 source "net/dcb/Kconfig"
228 source "net/dns_resolver/Kconfig"
229 source "net/batman-adv/Kconfig"
230 source "net/openvswitch/Kconfig"
231 source "net/vmw_vsock/Kconfig"
232 source "net/netlink/Kconfig"
233 source "net/mpls/Kconfig"
234 source "net/nsh/Kconfig"
235 source "net/hsr/Kconfig"
236 source "net/switchdev/Kconfig"
237 source "net/l3mdev/Kconfig"
238 source "net/qrtr/Kconfig"
239 source "net/ncsi/Kconfig"
241 config RPS
242         bool
243         depends on SMP && SYSFS
244         default y
246 config RFS_ACCEL
247         bool
248         depends on RPS
249         select CPU_RMAP
250         default y
252 config XPS
253         bool
254         depends on SMP
255         default y
257 config HWBM
258        bool
260 config CGROUP_NET_PRIO
261         bool "Network priority cgroup"
262         depends on CGROUPS
263         select SOCK_CGROUP_DATA
264         ---help---
265           Cgroup subsystem for use in assigning processes to network priorities on
266           a per-interface basis.
268 config CGROUP_NET_CLASSID
269         bool "Network classid cgroup"
270         depends on CGROUPS
271         select SOCK_CGROUP_DATA
272         ---help---
273           Cgroup subsystem for use as general purpose socket classid marker that is
274           being used in cls_cgroup and for netfilter matching.
276 config NET_RX_BUSY_POLL
277         bool
278         default y
280 config BQL
281         bool
282         depends on SYSFS
283         select DQL
284         default y
286 config BPF_JIT
287         bool "enable BPF Just In Time compiler"
288         depends on HAVE_CBPF_JIT || HAVE_EBPF_JIT
289         depends on MODULES
290         ---help---
291           Berkeley Packet Filter filtering capabilities are normally handled
292           by an interpreter. This option allows kernel to generate a native
293           code when filter is loaded in memory. This should speedup
294           packet sniffing (libpcap/tcpdump).
296           Note, admin should enable this feature changing:
297           /proc/sys/net/core/bpf_jit_enable
298           /proc/sys/net/core/bpf_jit_harden   (optional)
299           /proc/sys/net/core/bpf_jit_kallsyms (optional)
301 config BPF_STREAM_PARSER
302         bool "enable BPF STREAM_PARSER"
303         depends on BPF_SYSCALL
304         select STREAM_PARSER
305         ---help---
306          Enabling this allows a stream parser to be used with
307          BPF_MAP_TYPE_SOCKMAP.
309          BPF_MAP_TYPE_SOCKMAP provides a map type to use with network sockets.
310          It can be used to enforce socket policy, implement socket redirects,
311          etc.
313 config NET_FLOW_LIMIT
314         bool
315         depends on RPS
316         default y
317         ---help---
318           The network stack has to drop packets when a receive processing CPU's
319           backlog reaches netdev_max_backlog. If a few out of many active flows
320           generate the vast majority of load, drop their traffic earlier to
321           maintain capacity for the other flows. This feature provides servers
322           with many clients some protection against DoS by a single (spoofed)
323           flow that greatly exceeds average workload.
325 menu "Network testing"
327 config NET_PKTGEN
328         tristate "Packet Generator (USE WITH CAUTION)"
329         depends on INET && PROC_FS
330         ---help---
331           This module will inject preconfigured packets, at a configurable
332           rate, out of a given interface.  It is used for network interface
333           stress testing and performance analysis.  If you don't understand
334           what was just said, you don't need it: say N.
336           Documentation on how to use the packet generator can be found
337           at <file:Documentation/networking/pktgen.txt>.
339           To compile this code as a module, choose M here: the
340           module will be called pktgen.
342 config NET_DROP_MONITOR
343         tristate "Network packet drop alerting service"
344         depends on INET && TRACEPOINTS
345         ---help---
346         This feature provides an alerting service to userspace in the
347         event that packets are discarded in the network stack.  Alerts
348         are broadcast via netlink socket to any listening user space
349         process.  If you don't need network drop alerts, or if you are ok
350         just checking the various proc files and other utilities for
351         drop statistics, say N here.
353 endmenu
355 endmenu
357 source "net/ax25/Kconfig"
358 source "net/can/Kconfig"
359 source "net/bluetooth/Kconfig"
360 source "net/rxrpc/Kconfig"
361 source "net/kcm/Kconfig"
362 source "net/strparser/Kconfig"
364 config FIB_RULES
365         bool
367 menuconfig WIRELESS
368         bool "Wireless"
369         depends on !S390
370         default y
372 if WIRELESS
374 source "net/wireless/Kconfig"
375 source "net/mac80211/Kconfig"
377 endif # WIRELESS
379 source "net/wimax/Kconfig"
381 source "net/rfkill/Kconfig"
382 source "net/9p/Kconfig"
383 source "net/caif/Kconfig"
384 source "net/ceph/Kconfig"
385 source "net/nfc/Kconfig"
386 source "net/psample/Kconfig"
387 source "net/ife/Kconfig"
389 config LWTUNNEL
390         bool "Network light weight tunnels"
391         ---help---
392           This feature provides an infrastructure to support light weight
393           tunnels like mpls. There is no netdevice associated with a light
394           weight tunnel endpoint. Tunnel encapsulation parameters are stored
395           with light weight tunnel state associated with fib routes.
397 config LWTUNNEL_BPF
398         bool "Execute BPF program as route nexthop action"
399         depends on LWTUNNEL
400         default y if LWTUNNEL=y
401         ---help---
402           Allows to run BPF programs as a nexthop action following a route
403           lookup for incoming and outgoing packets.
405 config DST_CACHE
406         bool
407         default n
409 config GRO_CELLS
410         bool
411         default n
413 config SOCK_VALIDATE_XMIT
414         bool
416 config NET_DEVLINK
417         tristate "Network physical/parent device Netlink interface"
418         help
419           Network physical/parent device Netlink interface provides
420           infrastructure to support access to physical chip-wide config and
421           monitoring.
423 config MAY_USE_DEVLINK
424         tristate
425         default m if NET_DEVLINK=m
426         default y if NET_DEVLINK=y || NET_DEVLINK=n
427         help
428           Drivers using the devlink infrastructure should have a dependency
429           on MAY_USE_DEVLINK to ensure they do not cause link errors when
430           devlink is a loadable module and the driver using it is built-in.
432 config PAGE_POOL
433        bool
435 config FAILOVER
436         tristate "Generic failover module"
437         help
438           The failover module provides a generic interface for paravirtual
439           drivers to register a netdev and a set of ops with a failover
440           instance. The ops are used as event handlers that get called to
441           handle netdev register/unregister/link change/name change events
442           on slave pci ethernet devices with the same mac address as the
443           failover netdev. This enables paravirtual drivers to use a
444           VF as an accelerated low latency datapath. It also allows live
445           migration of VMs with direct attached VFs by failing over to the
446           paravirtual datapath when the VF is unplugged.
448 endif   # if NET
450 # Used by archs to tell that they support BPF JIT compiler plus which flavour.
451 # Only one of the two can be selected for a specific arch since eBPF JIT supersedes
452 # the cBPF JIT.
454 # Classic BPF JIT (cBPF)
455 config HAVE_CBPF_JIT
456         bool
458 # Extended BPF JIT (eBPF)
459 config HAVE_EBPF_JIT
460         bool