1 #
2 # Network configuration
3 #
5 menuconfig NET
6 bool "Networking support"
7 select NLATTR
8 select GENERIC_NET_UTILS
9 select BPF
10 ---help---
11 Unless you really know what you are doing, you should say Y here.
12 The reason is that some programs need kernel networking support even
13 when running on a stand-alone machine that isn't connected to any
14 other computer.
16 If you are upgrading from an older kernel, you
17 should consider updating your networking tools too because changes
18 in the kernel and the tools often go hand in hand. The tools are
19 contained in the package net-tools, the location and version number
20 of which are given in <file:Documentation/Changes>.
22 For a general introduction to Linux networking, it is highly
23 recommended to read the NET-HOWTO, available from
24 <http://www.tldp.org/docs.html#howto>.
26 if NET
28 config WANT_COMPAT_NETLINK_MESSAGES
29 bool
30 help
31 This option can be selected by other options that need compat
32 netlink messages.
34 config COMPAT_NETLINK_MESSAGES
35 def_bool y
36 depends on COMPAT
37 depends on WEXT_CORE || WANT_COMPAT_NETLINK_MESSAGES
38 help
39 This option makes it possible to send different netlink messages
40 to tasks depending on whether the task is a compat task or not. To
41 achieve this, you need to set skb_shinfo(skb)->frag_list to the
42 compat skb before sending the skb, the netlink code will sort out
43 which message to actually pass to the task.
45 Newly written code should NEVER need this option but do
46 compat-independent messages instead!
48 config NET_INGRESS
49 bool
51 config NET_EGRESS
52 bool
54 menu "Networking options"
56 source "net/packet/Kconfig"
57 source "net/unix/Kconfig"
58 source "net/tls/Kconfig"
59 source "net/xfrm/Kconfig"
60 source "net/iucv/Kconfig"
61 source "net/smc/Kconfig"
62 source "net/xdp/Kconfig"
64 config INET
65 bool "TCP/IP networking"
66 select CRYPTO
67 select CRYPTO_AES
68 ---help---
69 These are the protocols used on the Internet and on most local
70 Ethernets. It is highly recommended to say Y here (this will enlarge
71 your kernel by about 400 KB), since some programs (e.g. the X window
72 system) use TCP/IP even if your machine is not connected to any
73 other computer. You will get the so-called loopback device which
74 allows you to ping yourself (great fun, that!).
76 For an excellent introduction to Linux networking, please read the
77 Linux Networking HOWTO, available from
78 <http://www.tldp.org/docs.html#howto>.
80 If you say Y here and also to "/proc file system support" and
81 "Sysctl support" below, you can change various aspects of the
82 behavior of the TCP/IP code by writing to the (virtual) files in
83 /proc/sys/net/ipv4/*; the options are explained in the file
84 <file:Documentation/networking/ip-sysctl.txt>.
86 Short answer: say Y.
88 if INET
89 source "net/ipv4/Kconfig"
90 source "net/ipv6/Kconfig"
91 source "net/netlabel/Kconfig"
93 endif # if INET
95 config NETWORK_SECMARK
96 bool "Security Marking"
97 help
98 This enables security marking of network packets, similar
99 to nfmark, but designated for security purposes.
100 If you are unsure how to answer this question, answer N.
102 config NET_PTP_CLASSIFY
103 def_bool n
105 config NETWORK_PHY_TIMESTAMPING
106 bool "Timestamping in PHY devices"
107 select NET_PTP_CLASSIFY
108 help
109 This allows timestamping of network packets by PHYs with
110 hardware timestamping capabilities. This option adds some
111 overhead in the transmit and receive paths.
113 If you are unsure how to answer this question, answer N.
115 menuconfig NETFILTER
116 bool "Network packet filtering framework (Netfilter)"
117 ---help---
118 Netfilter is a framework for filtering and mangling network packets
119 that pass through your Linux box.
121 The most common use of packet filtering is to run your Linux box as
122 a firewall protecting a local network from the Internet. The type of
123 firewall provided by this kernel support is called a "packet
124 filter", which means that it can reject individual network packets
125 based on type, source, destination etc. The other kind of firewall,
126 a "proxy-based" one, is more secure but more intrusive and more
127 bothersome to set up; it inspects the network traffic much more
128 closely, modifies it and has knowledge about the higher level
129 protocols, which a packet filter lacks. Moreover, proxy-based
130 firewalls often require changes to the programs running on the local
131 clients. Proxy-based firewalls don't need support by the kernel, but
132 they are often combined with a packet filter, which only works if
133 you say Y here.
135 You should also say Y here if you intend to use your Linux box as
136 the gateway to the Internet for a local network of machines without
137 globally valid IP addresses. This is called "masquerading": if one
138 of the computers on your local network wants to send something to
139 the outside, your box can "masquerade" as that computer, i.e. it
140 forwards the traffic to the intended outside destination, but
141 modifies the packets to make it look like they came from the
142 firewall box itself. It works both ways: if the outside host
143 replies, the Linux box will silently forward the traffic to the
144 correct local computer. This way, the computers on your local net
145 are completely invisible to the outside world, even though they can
146 reach the outside and can receive replies. It is even possible to
147 run globally visible servers from within a masqueraded local network
148 using a mechanism called portforwarding. Masquerading is also often
149 called NAT (Network Address Translation).
151 Another use of Netfilter is in transparent proxying: if a machine on
152 the local network tries to connect to an outside host, your Linux
153 box can transparently forward the traffic to a local server,
154 typically a caching proxy server.
156 Yet another use of Netfilter is building a bridging firewall. Using
157 a bridge with Network packet filtering enabled makes iptables "see"
158 the bridged traffic. For filtering on the lower network and Ethernet
159 protocols over the bridge, use ebtables (under bridge netfilter
160 configuration).
162 Various modules exist for netfilter which replace the previous
163 masquerading (ipmasqadm), packet filtering (ipchains), transparent
164 proxying, and portforwarding mechanisms. Please see
165 <file:Documentation/Changes> under "iptables" for the location of
166 these packages.
168 if NETFILTER
170 config NETFILTER_ADVANCED
171 bool "Advanced netfilter configuration"
172 depends on NETFILTER
173 default y
174 help
175 If you say Y here you can select between all the netfilter modules.
176 If you say N the more unusual ones will not be shown and the
177 basic ones needed by most people will default to 'M'.
179 If unsure, say Y.
181 config BRIDGE_NETFILTER
182 tristate "Bridged IP/ARP packets filtering"
183 depends on BRIDGE
184 depends on NETFILTER && INET
185 depends on NETFILTER_ADVANCED
186 select NETFILTER_FAMILY_BRIDGE
187 default m
188 ---help---
189 Enabling this option will let arptables resp. iptables see bridged
190 ARP resp. IP traffic. If you want a bridging firewall, you probably
191 want this option enabled.
192 Enabling or disabling this option doesn't enable or disable
193 ebtables.
195 If unsure, say N.
197 source "net/netfilter/Kconfig"
198 source "net/ipv4/netfilter/Kconfig"
199 source "net/ipv6/netfilter/Kconfig"
200 source "net/decnet/netfilter/Kconfig"
201 source "net/bridge/netfilter/Kconfig"
203 endif
205 source "net/bpfilter/Kconfig"
207 source "net/dccp/Kconfig"
208 source "net/sctp/Kconfig"
209 source "net/rds/Kconfig"
210 source "net/tipc/Kconfig"
211 source "net/atm/Kconfig"
212 source "net/l2tp/Kconfig"
213 source "net/802/Kconfig"
214 source "net/bridge/Kconfig"
215 source "net/dsa/Kconfig"
216 source "net/8021q/Kconfig"
217 source "net/decnet/Kconfig"
218 source "net/llc/Kconfig"
219 source "drivers/net/appletalk/Kconfig"
220 source "net/x25/Kconfig"
221 source "net/lapb/Kconfig"
222 source "net/phonet/Kconfig"
223 source "net/6lowpan/Kconfig"
224 source "net/ieee802154/Kconfig"
225 source "net/mac802154/Kconfig"
226 source "net/sched/Kconfig"
227 source "net/dcb/Kconfig"
228 source "net/dns_resolver/Kconfig"
229 source "net/batman-adv/Kconfig"
230 source "net/openvswitch/Kconfig"
231 source "net/vmw_vsock/Kconfig"
232 source "net/netlink/Kconfig"
233 source "net/mpls/Kconfig"
234 source "net/nsh/Kconfig"
235 source "net/hsr/Kconfig"
236 source "net/switchdev/Kconfig"
237 source "net/l3mdev/Kconfig"
238 source "net/qrtr/Kconfig"
239 source "net/ncsi/Kconfig"
241 config RPS
242 bool
243 depends on SMP && SYSFS
244 default y
246 config RFS_ACCEL
247 bool
248 depends on RPS
249 select CPU_RMAP
250 default y
252 config XPS
253 bool
254 depends on SMP
255 default y
257 config HWBM
258 bool
260 config CGROUP_NET_PRIO
261 bool "Network priority cgroup"
262 depends on CGROUPS
263 select SOCK_CGROUP_DATA
264 ---help---
265 Cgroup subsystem for use in assigning processes to network priorities on
266 a per-interface basis.
268 config CGROUP_NET_CLASSID
269 bool "Network classid cgroup"
270 depends on CGROUPS
271 select SOCK_CGROUP_DATA
272 ---help---
273 Cgroup subsystem for use as general purpose socket classid marker that is
274 being used in cls_cgroup and for netfilter matching.
276 config NET_RX_BUSY_POLL
277 bool
278 default y
280 config BQL
281 bool
282 depends on SYSFS
283 select DQL
284 default y
286 config BPF_JIT
287 bool "enable BPF Just In Time compiler"
288 depends on HAVE_CBPF_JIT || HAVE_EBPF_JIT
289 depends on MODULES
290 ---help---
291 Berkeley Packet Filter filtering capabilities are normally handled
292 by an interpreter. This option allows kernel to generate a native
293 code when filter is loaded in memory. This should speedup
294 packet sniffing (libpcap/tcpdump).
296 Note, admin should enable this feature changing:
297 /proc/sys/net/core/bpf_jit_enable
298 /proc/sys/net/core/bpf_jit_harden (optional)
299 /proc/sys/net/core/bpf_jit_kallsyms (optional)
301 config BPF_STREAM_PARSER
302 bool "enable BPF STREAM_PARSER"
303 depends on BPF_SYSCALL
304 select STREAM_PARSER
305 ---help---
306 Enabling this allows a stream parser to be used with
307 BPF_MAP_TYPE_SOCKMAP.
309 BPF_MAP_TYPE_SOCKMAP provides a map type to use with network sockets.
310 It can be used to enforce socket policy, implement socket redirects,
311 etc.
313 config NET_FLOW_LIMIT
314 bool
315 depends on RPS
316 default y
317 ---help---
318 The network stack has to drop packets when a receive processing CPU's
319 backlog reaches netdev_max_backlog. If a few out of many active flows
320 generate the vast majority of load, drop their traffic earlier to
321 maintain capacity for the other flows. This feature provides servers
322 with many clients some protection against DoS by a single (spoofed)
323 flow that greatly exceeds average workload.
325 menu "Network testing"
327 config NET_PKTGEN
328 tristate "Packet Generator (USE WITH CAUTION)"
329 depends on INET && PROC_FS
330 ---help---
331 This module will inject preconfigured packets, at a configurable
332 rate, out of a given interface. It is used for network interface
333 stress testing and performance analysis. If you don't understand
334 what was just said, you don't need it: say N.
336 Documentation on how to use the packet generator can be found
337 at <file:Documentation/networking/pktgen.txt>.
339 To compile this code as a module, choose M here: the
340 module will be called pktgen.
342 config NET_DROP_MONITOR
343 tristate "Network packet drop alerting service"
344 depends on INET && TRACEPOINTS
345 ---help---
346 This feature provides an alerting service to userspace in the
347 event that packets are discarded in the network stack. Alerts
348 are broadcast via netlink socket to any listening user space
349 process. If you don't need network drop alerts, or if you are ok
350 just checking the various proc files and other utilities for
351 drop statistics, say N here.
353 endmenu
355 endmenu
357 source "net/ax25/Kconfig"
358 source "net/can/Kconfig"
359 source "net/bluetooth/Kconfig"
360 source "net/rxrpc/Kconfig"
361 source "net/kcm/Kconfig"
362 source "net/strparser/Kconfig"
364 config FIB_RULES
365 bool
367 menuconfig WIRELESS
368 bool "Wireless"
369 depends on !S390
370 default y
372 if WIRELESS
374 source "net/wireless/Kconfig"
375 source "net/mac80211/Kconfig"
377 endif # WIRELESS
379 source "net/wimax/Kconfig"
381 source "net/rfkill/Kconfig"
382 source "net/9p/Kconfig"
383 source "net/caif/Kconfig"
384 source "net/rpmsg/Kconfig"
385 source "net/ceph/Kconfig"
386 source "net/nfc/Kconfig"
387 source "net/psample/Kconfig"
388 source "net/ife/Kconfig"
390 config LWTUNNEL
391 bool "Network light weight tunnels"
392 ---help---
393 This feature provides an infrastructure to support light weight
394 tunnels like mpls. There is no netdevice associated with a light
395 weight tunnel endpoint. Tunnel encapsulation parameters are stored
396 with light weight tunnel state associated with fib routes.
398 config LWTUNNEL_BPF
399 bool "Execute BPF program as route nexthop action"
400 depends on LWTUNNEL
401 default y if LWTUNNEL=y
402 ---help---
403 Allows to run BPF programs as a nexthop action following a route
404 lookup for incoming and outgoing packets.
406 config DST_CACHE
407 bool
408 default n
410 config GRO_CELLS
411 bool
412 default n
414 config SOCK_VALIDATE_XMIT
415 bool
417 config NET_DEVLINK
418 tristate "Network physical/parent device Netlink interface"
419 help
420 Network physical/parent device Netlink interface provides
421 infrastructure to support access to physical chip-wide config and
422 monitoring.
424 config MAY_USE_DEVLINK
425 tristate
426 default m if NET_DEVLINK=m
427 default y if NET_DEVLINK=y || NET_DEVLINK=n
428 help
429 Drivers using the devlink infrastructure should have a dependency
430 on MAY_USE_DEVLINK to ensure they do not cause link errors when
431 devlink is a loadable module and the driver using it is built-in.
433 config PAGE_POOL
434 bool
436 config FAILOVER
437 tristate "Generic failover module"
438 help
439 The failover module provides a generic interface for paravirtual
440 drivers to register a netdev and a set of ops with a failover
441 instance. The ops are used as event handlers that get called to
442 handle netdev register/unregister/link change/name change events
443 on slave pci ethernet devices with the same mac address as the
444 failover netdev. This enables paravirtual drivers to use a
445 VF as an accelerated low latency datapath. It also allows live
446 migration of VMs with direct attached VFs by failing over to the
447 paravirtual datapath when the VF is unplugged.
449 endif # if NET
451 # Used by archs to tell that they support BPF JIT compiler plus which flavour.
452 # Only one of the two can be selected for a specific arch since eBPF JIT supersedes
453 # the cBPF JIT.
455 # Classic BPF JIT (cBPF)
456 config HAVE_CBPF_JIT
457 bool
459 # Extended BPF JIT (eBPF)
460 config HAVE_EBPF_JIT
461 bool