1 /*
2 * NetLabel Unlabeled Support
3 *
4 * This file defines functions for dealing with unlabeled packets for the
5 * NetLabel system. The NetLabel system manages static and dynamic label
6 * mappings for network protocols such as CIPSO and RIPSO.
7 *
8 * Author: Paul Moore <paul@paul-moore.com>
9 *
10 */
12 /*
13 * (c) Copyright Hewlett-Packard Development Company, L.P., 2006 - 2008
14 *
15 * This program is free software; you can redistribute it and/or modify
16 * it under the terms of the GNU General Public License as published by
17 * the Free Software Foundation; either version 2 of the License, or
18 * (at your option) any later version.
19 *
20 * This program is distributed in the hope that it will be useful,
21 * but WITHOUT ANY WARRANTY; without even the implied warranty of
22 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See
23 * the GNU General Public License for more details.
24 *
25 * You should have received a copy of the GNU General Public License
26 * along with this program; if not, see <http://www.gnu.org/licenses/>.
27 *
28 */
30 #include <linux/types.h>
31 #include <linux/rcupdate.h>
32 #include <linux/list.h>
33 #include <linux/spinlock.h>
34 #include <linux/socket.h>
35 #include <linux/string.h>
36 #include <linux/skbuff.h>
37 #include <linux/audit.h>
38 #include <linux/in.h>
39 #include <linux/in6.h>
40 #include <linux/ip.h>
41 #include <linux/ipv6.h>
42 #include <linux/notifier.h>
43 #include <linux/netdevice.h>
44 #include <linux/security.h>
45 #include <linux/slab.h>
46 #include <net/sock.h>
47 #include <net/netlink.h>
48 #include <net/genetlink.h>
49 #include <net/ip.h>
50 #include <net/ipv6.h>
51 #include <net/net_namespace.h>
52 #include <net/netlabel.h>
53 #include <asm/bug.h>
54 #include <linux/atomic.h>
56 #include "netlabel_user.h"
57 #include "netlabel_addrlist.h"
58 #include "netlabel_domainhash.h"
59 #include "netlabel_unlabeled.h"
60 #include "netlabel_mgmt.h"
62 /* NOTE: at present we always use init's network namespace since we don't
63 * presently support different namespaces even though the majority of
64 * the functions in this file are "namespace safe" */
66 /* The unlabeled connection hash table which we use to map network interfaces
67 * and addresses of unlabeled packets to a user specified secid value for the
68 * LSM. The hash table is used to lookup the network interface entry
69 * (struct netlbl_unlhsh_iface) and then the interface entry is used to
70 * lookup an IP address match from an ordered list. If a network interface
71 * match can not be found in the hash table then the default entry
72 * (netlbl_unlhsh_def) is used. The IP address entry list
73 * (struct netlbl_unlhsh_addr) is ordered such that the entries with a
74 * larger netmask come first.
75 */
76 struct netlbl_unlhsh_tbl {
77 struct list_head *tbl;
78 u32 size;
79 };
80 #define netlbl_unlhsh_addr4_entry(iter) \
81 container_of(iter, struct netlbl_unlhsh_addr4, list)
82 struct netlbl_unlhsh_addr4 {
83 u32 secid;
85 struct netlbl_af4list list;
86 struct rcu_head rcu;
87 };
88 #define netlbl_unlhsh_addr6_entry(iter) \
89 container_of(iter, struct netlbl_unlhsh_addr6, list)
90 struct netlbl_unlhsh_addr6 {
91 u32 secid;
93 struct netlbl_af6list list;
94 struct rcu_head rcu;
95 };
96 struct netlbl_unlhsh_iface {
97 int ifindex;
98 struct list_head addr4_list;
99 struct list_head addr6_list;
101 u32 valid;
102 struct list_head list;
103 struct rcu_head rcu;
104 };
106 /* Argument struct for netlbl_unlhsh_walk() */
107 struct netlbl_unlhsh_walk_arg {
108 struct netlink_callback *nl_cb;
109 struct sk_buff *skb;
110 u32 seq;
111 };
113 /* Unlabeled connection hash table */
114 /* updates should be so rare that having one spinlock for the entire
115 * hash table should be okay */
116 static DEFINE_SPINLOCK(netlbl_unlhsh_lock);
117 #define netlbl_unlhsh_rcu_deref(p) \
118 rcu_dereference_check(p, lockdep_is_held(&netlbl_unlhsh_lock))
119 static struct netlbl_unlhsh_tbl __rcu *netlbl_unlhsh;
120 static struct netlbl_unlhsh_iface __rcu *netlbl_unlhsh_def;
122 /* Accept unlabeled packets flag */
123 static u8 netlabel_unlabel_acceptflg;
125 /* NetLabel Generic NETLINK unlabeled family */
126 static struct genl_family netlbl_unlabel_gnl_family;
128 /* NetLabel Netlink attribute policy */
129 static const struct nla_policy netlbl_unlabel_genl_policy[NLBL_UNLABEL_A_MAX + 1] = {
130 [NLBL_UNLABEL_A_ACPTFLG] = { .type = NLA_U8 },
131 [NLBL_UNLABEL_A_IPV6ADDR] = { .type = NLA_BINARY,
132 .len = sizeof(struct in6_addr) },
133 [NLBL_UNLABEL_A_IPV6MASK] = { .type = NLA_BINARY,
134 .len = sizeof(struct in6_addr) },
135 [NLBL_UNLABEL_A_IPV4ADDR] = { .type = NLA_BINARY,
136 .len = sizeof(struct in_addr) },
137 [NLBL_UNLABEL_A_IPV4MASK] = { .type = NLA_BINARY,
138 .len = sizeof(struct in_addr) },
139 [NLBL_UNLABEL_A_IFACE] = { .type = NLA_NUL_STRING,
140 .len = IFNAMSIZ - 1 },
141 [NLBL_UNLABEL_A_SECCTX] = { .type = NLA_BINARY }
142 };
144 /*
145 * Unlabeled Connection Hash Table Functions
146 */
148 /**
149 * netlbl_unlhsh_free_iface - Frees an interface entry from the hash table
150 * @entry: the entry's RCU field
151 *
152 * Description:
153 * This function is designed to be used as a callback to the call_rcu()
154 * function so that memory allocated to a hash table interface entry can be
155 * released safely. It is important to note that this function does not free
156 * the IPv4 and IPv6 address lists contained as part of an interface entry. It
157 * is up to the rest of the code to make sure an interface entry is only freed
158 * once it's address lists are empty.
159 *
160 */
161 static void netlbl_unlhsh_free_iface(struct rcu_head *entry)
162 {
163 struct netlbl_unlhsh_iface *iface;
164 struct netlbl_af4list *iter4;
165 struct netlbl_af4list *tmp4;
166 #if IS_ENABLED(CONFIG_IPV6)
167 struct netlbl_af6list *iter6;
168 struct netlbl_af6list *tmp6;
169 #endif /* IPv6 */
171 iface = container_of(entry, struct netlbl_unlhsh_iface, rcu);
173 /* no need for locks here since we are the only one with access to this
174 * structure */
176 netlbl_af4list_foreach_safe(iter4, tmp4, &iface->addr4_list) {
177 netlbl_af4list_remove_entry(iter4);
178 kfree(netlbl_unlhsh_addr4_entry(iter4));
179 }
180 #if IS_ENABLED(CONFIG_IPV6)
181 netlbl_af6list_foreach_safe(iter6, tmp6, &iface->addr6_list) {
182 netlbl_af6list_remove_entry(iter6);
183 kfree(netlbl_unlhsh_addr6_entry(iter6));
184 }
185 #endif /* IPv6 */
186 kfree(iface);
187 }
189 /**
190 * netlbl_unlhsh_hash - Hashing function for the hash table
191 * @ifindex: the network interface/device to hash
192 *
193 * Description:
194 * This is the hashing function for the unlabeled hash table, it returns the
195 * bucket number for the given device/interface. The caller is responsible for
196 * ensuring that the hash table is protected with either a RCU read lock or
197 * the hash table lock.
198 *
199 */
200 static u32 netlbl_unlhsh_hash(int ifindex)
201 {
202 return ifindex & (netlbl_unlhsh_rcu_deref(netlbl_unlhsh)->size - 1);
203 }
205 /**
206 * netlbl_unlhsh_search_iface - Search for a matching interface entry
207 * @ifindex: the network interface
208 *
209 * Description:
210 * Searches the unlabeled connection hash table and returns a pointer to the
211 * interface entry which matches @ifindex, otherwise NULL is returned. The
212 * caller is responsible for ensuring that the hash table is protected with
213 * either a RCU read lock or the hash table lock.
214 *
215 */
216 static struct netlbl_unlhsh_iface *netlbl_unlhsh_search_iface(int ifindex)
217 {
218 u32 bkt;
219 struct list_head *bkt_list;
220 struct netlbl_unlhsh_iface *iter;
222 bkt = netlbl_unlhsh_hash(ifindex);
223 bkt_list = &netlbl_unlhsh_rcu_deref(netlbl_unlhsh)->tbl[bkt];
224 list_for_each_entry_rcu(iter, bkt_list, list)
225 if (iter->valid && iter->ifindex == ifindex)
226 return iter;
228 return NULL;
229 }
231 /**
232 * netlbl_unlhsh_add_addr4 - Add a new IPv4 address entry to the hash table
233 * @iface: the associated interface entry
234 * @addr: IPv4 address in network byte order
235 * @mask: IPv4 address mask in network byte order
236 * @secid: LSM secid value for entry
237 *
238 * Description:
239 * Add a new address entry into the unlabeled connection hash table using the
240 * interface entry specified by @iface. On success zero is returned, otherwise
241 * a negative value is returned.
242 *
243 */
244 static int netlbl_unlhsh_add_addr4(struct netlbl_unlhsh_iface *iface,
245 const struct in_addr *addr,
246 const struct in_addr *mask,
247 u32 secid)
248 {
249 int ret_val;
250 struct netlbl_unlhsh_addr4 *entry;
252 entry = kzalloc(sizeof(*entry), GFP_ATOMIC);
253 if (entry == NULL)
254 return -ENOMEM;
256 entry->list.addr = addr->s_addr & mask->s_addr;
257 entry->list.mask = mask->s_addr;
258 entry->list.valid = 1;
259 entry->secid = secid;
261 spin_lock(&netlbl_unlhsh_lock);
262 ret_val = netlbl_af4list_add(&entry->list, &iface->addr4_list);
263 spin_unlock(&netlbl_unlhsh_lock);
265 if (ret_val != 0)
266 kfree(entry);
267 return ret_val;
268 }
270 #if IS_ENABLED(CONFIG_IPV6)
271 /**
272 * netlbl_unlhsh_add_addr6 - Add a new IPv6 address entry to the hash table
273 * @iface: the associated interface entry
274 * @addr: IPv6 address in network byte order
275 * @mask: IPv6 address mask in network byte order
276 * @secid: LSM secid value for entry
277 *
278 * Description:
279 * Add a new address entry into the unlabeled connection hash table using the
280 * interface entry specified by @iface. On success zero is returned, otherwise
281 * a negative value is returned.
282 *
283 */
284 static int netlbl_unlhsh_add_addr6(struct netlbl_unlhsh_iface *iface,
285 const struct in6_addr *addr,
286 const struct in6_addr *mask,
287 u32 secid)
288 {
289 int ret_val;
290 struct netlbl_unlhsh_addr6 *entry;
292 entry = kzalloc(sizeof(*entry), GFP_ATOMIC);
293 if (entry == NULL)
294 return -ENOMEM;
296 entry->list.addr = *addr;
297 entry->list.addr.s6_addr32[0] &= mask->s6_addr32[0];
298 entry->list.addr.s6_addr32[1] &= mask->s6_addr32[1];
299 entry->list.addr.s6_addr32[2] &= mask->s6_addr32[2];
300 entry->list.addr.s6_addr32[3] &= mask->s6_addr32[3];
301 entry->list.mask = *mask;
302 entry->list.valid = 1;
303 entry->secid = secid;
305 spin_lock(&netlbl_unlhsh_lock);
306 ret_val = netlbl_af6list_add(&entry->list, &iface->addr6_list);
307 spin_unlock(&netlbl_unlhsh_lock);
309 if (ret_val != 0)
310 kfree(entry);
311 return 0;
312 }
313 #endif /* IPv6 */
315 /**
316 * netlbl_unlhsh_add_iface - Adds a new interface entry to the hash table
317 * @ifindex: network interface
318 *
319 * Description:
320 * Add a new, empty, interface entry into the unlabeled connection hash table.
321 * On success a pointer to the new interface entry is returned, on failure NULL
322 * is returned.
323 *
324 */
325 static struct netlbl_unlhsh_iface *netlbl_unlhsh_add_iface(int ifindex)
326 {
327 u32 bkt;
328 struct netlbl_unlhsh_iface *iface;
330 iface = kzalloc(sizeof(*iface), GFP_ATOMIC);
331 if (iface == NULL)
332 return NULL;
334 iface->ifindex = ifindex;
335 INIT_LIST_HEAD(&iface->addr4_list);
336 INIT_LIST_HEAD(&iface->addr6_list);
337 iface->valid = 1;
339 spin_lock(&netlbl_unlhsh_lock);
340 if (ifindex > 0) {
341 bkt = netlbl_unlhsh_hash(ifindex);
342 if (netlbl_unlhsh_search_iface(ifindex) != NULL)
343 goto add_iface_failure;
344 list_add_tail_rcu(&iface->list,
345 &netlbl_unlhsh_rcu_deref(netlbl_unlhsh)->tbl[bkt]);
346 } else {
347 INIT_LIST_HEAD(&iface->list);
348 if (netlbl_unlhsh_rcu_deref(netlbl_unlhsh_def) != NULL)
349 goto add_iface_failure;
350 rcu_assign_pointer(netlbl_unlhsh_def, iface);
351 }
352 spin_unlock(&netlbl_unlhsh_lock);
354 return iface;
356 add_iface_failure:
357 spin_unlock(&netlbl_unlhsh_lock);
358 kfree(iface);
359 return NULL;
360 }
362 /**
363 * netlbl_unlhsh_add - Adds a new entry to the unlabeled connection hash table
364 * @net: network namespace
365 * @dev_name: interface name
366 * @addr: IP address in network byte order
367 * @mask: address mask in network byte order
368 * @addr_len: length of address/mask (4 for IPv4, 16 for IPv6)
369 * @secid: LSM secid value for the entry
370 * @audit_info: NetLabel audit information
371 *
372 * Description:
373 * Adds a new entry to the unlabeled connection hash table. Returns zero on
374 * success, negative values on failure.
375 *
376 */
377 int netlbl_unlhsh_add(struct net *net,
378 const char *dev_name,
379 const void *addr,
380 const void *mask,
381 u32 addr_len,
382 u32 secid,
383 struct netlbl_audit *audit_info)
384 {
385 int ret_val;
386 int ifindex;
387 struct net_device *dev;
388 struct netlbl_unlhsh_iface *iface;
389 struct audit_buffer *audit_buf = NULL;
390 char *secctx = NULL;
391 u32 secctx_len;
393 if (addr_len != sizeof(struct in_addr) &&
394 addr_len != sizeof(struct in6_addr))
395 return -EINVAL;
397 rcu_read_lock();
398 if (dev_name != NULL) {
399 dev = dev_get_by_name_rcu(net, dev_name);
400 if (dev == NULL) {
401 ret_val = -ENODEV;
402 goto unlhsh_add_return;
403 }
404 ifindex = dev->ifindex;
405 iface = netlbl_unlhsh_search_iface(ifindex);
406 } else {
407 ifindex = 0;
408 iface = rcu_dereference(netlbl_unlhsh_def);
409 }
410 if (iface == NULL) {
411 iface = netlbl_unlhsh_add_iface(ifindex);
412 if (iface == NULL) {
413 ret_val = -ENOMEM;
414 goto unlhsh_add_return;
415 }
416 }
417 audit_buf = netlbl_audit_start_common(AUDIT_MAC_UNLBL_STCADD,
418 audit_info);
419 switch (addr_len) {
420 case sizeof(struct in_addr): {
421 const struct in_addr *addr4 = addr;
422 const struct in_addr *mask4 = mask;
424 ret_val = netlbl_unlhsh_add_addr4(iface, addr4, mask4, secid);
425 if (audit_buf != NULL)
426 netlbl_af4list_audit_addr(audit_buf, 1,
427 dev_name,
428 addr4->s_addr,
429 mask4->s_addr);
430 break;
431 }
432 #if IS_ENABLED(CONFIG_IPV6)
433 case sizeof(struct in6_addr): {
434 const struct in6_addr *addr6 = addr;
435 const struct in6_addr *mask6 = mask;
437 ret_val = netlbl_unlhsh_add_addr6(iface, addr6, mask6, secid);
438 if (audit_buf != NULL)
439 netlbl_af6list_audit_addr(audit_buf, 1,
440 dev_name,
441 addr6, mask6);
442 break;
443 }
444 #endif /* IPv6 */
445 default:
446 ret_val = -EINVAL;
447 }
448 if (ret_val == 0)
449 atomic_inc(&netlabel_mgmt_protocount);
451 unlhsh_add_return:
452 rcu_read_unlock();
453 if (audit_buf != NULL) {
454 if (security_secid_to_secctx(secid,
455 &secctx,
456 &secctx_len) == 0) {
457 audit_log_format(audit_buf, " sec_obj=%s", secctx);
458 security_release_secctx(secctx, secctx_len);
459 }
460 audit_log_format(audit_buf, " res=%u", ret_val == 0 ? 1 : 0);
461 audit_log_end(audit_buf);
462 }
463 return ret_val;
464 }
466 /**
467 * netlbl_unlhsh_remove_addr4 - Remove an IPv4 address entry
468 * @net: network namespace
469 * @iface: interface entry
470 * @addr: IP address
471 * @mask: IP address mask
472 * @audit_info: NetLabel audit information
473 *
474 * Description:
475 * Remove an IP address entry from the unlabeled connection hash table.
476 * Returns zero on success, negative values on failure.
477 *
478 */
479 static int netlbl_unlhsh_remove_addr4(struct net *net,
480 struct netlbl_unlhsh_iface *iface,
481 const struct in_addr *addr,
482 const struct in_addr *mask,
483 struct netlbl_audit *audit_info)
484 {
485 struct netlbl_af4list *list_entry;
486 struct netlbl_unlhsh_addr4 *entry;
487 struct audit_buffer *audit_buf;
488 struct net_device *dev;
489 char *secctx;
490 u32 secctx_len;
492 spin_lock(&netlbl_unlhsh_lock);
493 list_entry = netlbl_af4list_remove(addr->s_addr, mask->s_addr,
494 &iface->addr4_list);
495 spin_unlock(&netlbl_unlhsh_lock);
496 if (list_entry != NULL)
497 entry = netlbl_unlhsh_addr4_entry(list_entry);
498 else
499 entry = NULL;
501 audit_buf = netlbl_audit_start_common(AUDIT_MAC_UNLBL_STCDEL,
502 audit_info);
503 if (audit_buf != NULL) {
504 dev = dev_get_by_index(net, iface->ifindex);
505 netlbl_af4list_audit_addr(audit_buf, 1,
506 (dev != NULL ? dev->name : NULL),
507 addr->s_addr, mask->s_addr);
508 if (dev != NULL)
509 dev_put(dev);
510 if (entry != NULL &&
511 security_secid_to_secctx(entry->secid,
512 &secctx, &secctx_len) == 0) {
513 audit_log_format(audit_buf, " sec_obj=%s", secctx);
514 security_release_secctx(secctx, secctx_len);
515 }
516 audit_log_format(audit_buf, " res=%u", entry != NULL ? 1 : 0);
517 audit_log_end(audit_buf);
518 }
520 if (entry == NULL)
521 return -ENOENT;
523 kfree_rcu(entry, rcu);
524 return 0;
525 }
527 #if IS_ENABLED(CONFIG_IPV6)
528 /**
529 * netlbl_unlhsh_remove_addr6 - Remove an IPv6 address entry
530 * @net: network namespace
531 * @iface: interface entry
532 * @addr: IP address
533 * @mask: IP address mask
534 * @audit_info: NetLabel audit information
535 *
536 * Description:
537 * Remove an IP address entry from the unlabeled connection hash table.
538 * Returns zero on success, negative values on failure.
539 *
540 */
541 static int netlbl_unlhsh_remove_addr6(struct net *net,
542 struct netlbl_unlhsh_iface *iface,
543 const struct in6_addr *addr,
544 const struct in6_addr *mask,
545 struct netlbl_audit *audit_info)
546 {
547 struct netlbl_af6list *list_entry;
548 struct netlbl_unlhsh_addr6 *entry;
549 struct audit_buffer *audit_buf;
550 struct net_device *dev;
551 char *secctx;
552 u32 secctx_len;
554 spin_lock(&netlbl_unlhsh_lock);
555 list_entry = netlbl_af6list_remove(addr, mask, &iface->addr6_list);
556 spin_unlock(&netlbl_unlhsh_lock);
557 if (list_entry != NULL)
558 entry = netlbl_unlhsh_addr6_entry(list_entry);
559 else
560 entry = NULL;
562 audit_buf = netlbl_audit_start_common(AUDIT_MAC_UNLBL_STCDEL,
563 audit_info);
564 if (audit_buf != NULL) {
565 dev = dev_get_by_index(net, iface->ifindex);
566 netlbl_af6list_audit_addr(audit_buf, 1,
567 (dev != NULL ? dev->name : NULL),
568 addr, mask);
569 if (dev != NULL)
570 dev_put(dev);
571 if (entry != NULL &&
572 security_secid_to_secctx(entry->secid,
573 &secctx, &secctx_len) == 0) {
574 audit_log_format(audit_buf, " sec_obj=%s", secctx);
575 security_release_secctx(secctx, secctx_len);
576 }
577 audit_log_format(audit_buf, " res=%u", entry != NULL ? 1 : 0);
578 audit_log_end(audit_buf);
579 }
581 if (entry == NULL)
582 return -ENOENT;
584 kfree_rcu(entry, rcu);
585 return 0;
586 }
587 #endif /* IPv6 */
589 /**
590 * netlbl_unlhsh_condremove_iface - Remove an interface entry
591 * @iface: the interface entry
592 *
593 * Description:
594 * Remove an interface entry from the unlabeled connection hash table if it is
595 * empty. An interface entry is considered to be empty if there are no
596 * address entries assigned to it.
597 *
598 */
599 static void netlbl_unlhsh_condremove_iface(struct netlbl_unlhsh_iface *iface)
600 {
601 struct netlbl_af4list *iter4;
602 #if IS_ENABLED(CONFIG_IPV6)
603 struct netlbl_af6list *iter6;
604 #endif /* IPv6 */
606 spin_lock(&netlbl_unlhsh_lock);
607 netlbl_af4list_foreach_rcu(iter4, &iface->addr4_list)
608 goto unlhsh_condremove_failure;
609 #if IS_ENABLED(CONFIG_IPV6)
610 netlbl_af6list_foreach_rcu(iter6, &iface->addr6_list)
611 goto unlhsh_condremove_failure;
612 #endif /* IPv6 */
613 iface->valid = 0;
614 if (iface->ifindex > 0)
615 list_del_rcu(&iface->list);
616 else
617 RCU_INIT_POINTER(netlbl_unlhsh_def, NULL);
618 spin_unlock(&netlbl_unlhsh_lock);
620 call_rcu(&iface->rcu, netlbl_unlhsh_free_iface);
621 return;
623 unlhsh_condremove_failure:
624 spin_unlock(&netlbl_unlhsh_lock);
625 }
627 /**
628 * netlbl_unlhsh_remove - Remove an entry from the unlabeled hash table
629 * @net: network namespace
630 * @dev_name: interface name
631 * @addr: IP address in network byte order
632 * @mask: address mask in network byte order
633 * @addr_len: length of address/mask (4 for IPv4, 16 for IPv6)
634 * @audit_info: NetLabel audit information
635 *
636 * Description:
637 * Removes and existing entry from the unlabeled connection hash table.
638 * Returns zero on success, negative values on failure.
639 *
640 */
641 int netlbl_unlhsh_remove(struct net *net,
642 const char *dev_name,
643 const void *addr,
644 const void *mask,
645 u32 addr_len,
646 struct netlbl_audit *audit_info)
647 {
648 int ret_val;
649 struct net_device *dev;
650 struct netlbl_unlhsh_iface *iface;
652 if (addr_len != sizeof(struct in_addr) &&
653 addr_len != sizeof(struct in6_addr))
654 return -EINVAL;
656 rcu_read_lock();
657 if (dev_name != NULL) {
658 dev = dev_get_by_name_rcu(net, dev_name);
659 if (dev == NULL) {
660 ret_val = -ENODEV;
661 goto unlhsh_remove_return;
662 }
663 iface = netlbl_unlhsh_search_iface(dev->ifindex);
664 } else
665 iface = rcu_dereference(netlbl_unlhsh_def);
666 if (iface == NULL) {
667 ret_val = -ENOENT;
668 goto unlhsh_remove_return;
669 }
670 switch (addr_len) {
671 case sizeof(struct in_addr):
672 ret_val = netlbl_unlhsh_remove_addr4(net,
673 iface, addr, mask,
674 audit_info);
675 break;
676 #if IS_ENABLED(CONFIG_IPV6)
677 case sizeof(struct in6_addr):
678 ret_val = netlbl_unlhsh_remove_addr6(net,
679 iface, addr, mask,
680 audit_info);
681 break;
682 #endif /* IPv6 */
683 default:
684 ret_val = -EINVAL;
685 }
686 if (ret_val == 0) {
687 netlbl_unlhsh_condremove_iface(iface);
688 atomic_dec(&netlabel_mgmt_protocount);
689 }
691 unlhsh_remove_return:
692 rcu_read_unlock();
693 return ret_val;
694 }
696 /*
697 * General Helper Functions
698 */
700 /**
701 * netlbl_unlhsh_netdev_handler - Network device notification handler
702 * @this: notifier block
703 * @event: the event
704 * @ptr: the netdevice notifier info (cast to void)
705 *
706 * Description:
707 * Handle network device events, although at present all we care about is a
708 * network device going away. In the case of a device going away we clear any
709 * related entries from the unlabeled connection hash table.
710 *
711 */
712 static int netlbl_unlhsh_netdev_handler(struct notifier_block *this,
713 unsigned long event, void *ptr)
714 {
715 struct net_device *dev = netdev_notifier_info_to_dev(ptr);
716 struct netlbl_unlhsh_iface *iface = NULL;
718 if (!net_eq(dev_net(dev), &init_net))
719 return NOTIFY_DONE;
721 /* XXX - should this be a check for NETDEV_DOWN or _UNREGISTER? */
722 if (event == NETDEV_DOWN) {
723 spin_lock(&netlbl_unlhsh_lock);
724 iface = netlbl_unlhsh_search_iface(dev->ifindex);
725 if (iface != NULL && iface->valid) {
726 iface->valid = 0;
727 list_del_rcu(&iface->list);
728 } else
729 iface = NULL;
730 spin_unlock(&netlbl_unlhsh_lock);
731 }
733 if (iface != NULL)
734 call_rcu(&iface->rcu, netlbl_unlhsh_free_iface);
736 return NOTIFY_DONE;
737 }
739 /**
740 * netlbl_unlabel_acceptflg_set - Set the unlabeled accept flag
741 * @value: desired value
742 * @audit_info: NetLabel audit information
743 *
744 * Description:
745 * Set the value of the unlabeled accept flag to @value.
746 *
747 */
748 static void netlbl_unlabel_acceptflg_set(u8 value,
749 struct netlbl_audit *audit_info)
750 {
751 struct audit_buffer *audit_buf;
752 u8 old_val;
754 old_val = netlabel_unlabel_acceptflg;
755 netlabel_unlabel_acceptflg = value;
756 audit_buf = netlbl_audit_start_common(AUDIT_MAC_UNLBL_ALLOW,
757 audit_info);
758 if (audit_buf != NULL) {
759 audit_log_format(audit_buf,
760 " unlbl_accept=%u old=%u", value, old_val);
761 audit_log_end(audit_buf);
762 }
763 }
765 /**
766 * netlbl_unlabel_addrinfo_get - Get the IPv4/6 address information
767 * @info: the Generic NETLINK info block
768 * @addr: the IP address
769 * @mask: the IP address mask
770 * @len: the address length
771 *
772 * Description:
773 * Examine the Generic NETLINK message and extract the IP address information.
774 * Returns zero on success, negative values on failure.
775 *
776 */
777 static int netlbl_unlabel_addrinfo_get(struct genl_info *info,
778 void **addr,
779 void **mask,
780 u32 *len)
781 {
782 u32 addr_len;
784 if (info->attrs[NLBL_UNLABEL_A_IPV4ADDR] &&
785 info->attrs[NLBL_UNLABEL_A_IPV4MASK]) {
786 addr_len = nla_len(info->attrs[NLBL_UNLABEL_A_IPV4ADDR]);
787 if (addr_len != sizeof(struct in_addr) &&
788 addr_len != nla_len(info->attrs[NLBL_UNLABEL_A_IPV4MASK]))
789 return -EINVAL;
790 *len = addr_len;
791 *addr = nla_data(info->attrs[NLBL_UNLABEL_A_IPV4ADDR]);
792 *mask = nla_data(info->attrs[NLBL_UNLABEL_A_IPV4MASK]);
793 return 0;
794 } else if (info->attrs[NLBL_UNLABEL_A_IPV6ADDR]) {
795 addr_len = nla_len(info->attrs[NLBL_UNLABEL_A_IPV6ADDR]);
796 if (addr_len != sizeof(struct in6_addr) &&
797 addr_len != nla_len(info->attrs[NLBL_UNLABEL_A_IPV6MASK]))
798 return -EINVAL;
799 *len = addr_len;
800 *addr = nla_data(info->attrs[NLBL_UNLABEL_A_IPV6ADDR]);
801 *mask = nla_data(info->attrs[NLBL_UNLABEL_A_IPV6MASK]);
802 return 0;
803 }
805 return -EINVAL;
806 }
808 /*
809 * NetLabel Command Handlers
810 */
812 /**
813 * netlbl_unlabel_accept - Handle an ACCEPT message
814 * @skb: the NETLINK buffer
815 * @info: the Generic NETLINK info block
816 *
817 * Description:
818 * Process a user generated ACCEPT message and set the accept flag accordingly.
819 * Returns zero on success, negative values on failure.
820 *
821 */
822 static int netlbl_unlabel_accept(struct sk_buff *skb, struct genl_info *info)
823 {
824 u8 value;
825 struct netlbl_audit audit_info;
827 if (info->attrs[NLBL_UNLABEL_A_ACPTFLG]) {
828 value = nla_get_u8(info->attrs[NLBL_UNLABEL_A_ACPTFLG]);
829 if (value == 1 || value == 0) {
830 netlbl_netlink_auditinfo(skb, &audit_info);
831 netlbl_unlabel_acceptflg_set(value, &audit_info);
832 return 0;
833 }
834 }
836 return -EINVAL;
837 }
839 /**
840 * netlbl_unlabel_list - Handle a LIST message
841 * @skb: the NETLINK buffer
842 * @info: the Generic NETLINK info block
843 *
844 * Description:
845 * Process a user generated LIST message and respond with the current status.
846 * Returns zero on success, negative values on failure.
847 *
848 */
849 static int netlbl_unlabel_list(struct sk_buff *skb, struct genl_info *info)
850 {
851 int ret_val = -EINVAL;
852 struct sk_buff *ans_skb;
853 void *data;
855 ans_skb = nlmsg_new(NLMSG_DEFAULT_SIZE, GFP_KERNEL);
856 if (ans_skb == NULL)
857 goto list_failure;
858 data = genlmsg_put_reply(ans_skb, info, &netlbl_unlabel_gnl_family,
859 0, NLBL_UNLABEL_C_LIST);
860 if (data == NULL) {
861 ret_val = -ENOMEM;
862 goto list_failure;
863 }
865 ret_val = nla_put_u8(ans_skb,
866 NLBL_UNLABEL_A_ACPTFLG,
867 netlabel_unlabel_acceptflg);
868 if (ret_val != 0)
869 goto list_failure;
871 genlmsg_end(ans_skb, data);
872 return genlmsg_reply(ans_skb, info);
874 list_failure:
875 kfree_skb(ans_skb);
876 return ret_val;
877 }
879 /**
880 * netlbl_unlabel_staticadd - Handle a STATICADD message
881 * @skb: the NETLINK buffer
882 * @info: the Generic NETLINK info block
883 *
884 * Description:
885 * Process a user generated STATICADD message and add a new unlabeled
886 * connection entry to the hash table. Returns zero on success, negative
887 * values on failure.
888 *
889 */
890 static int netlbl_unlabel_staticadd(struct sk_buff *skb,
891 struct genl_info *info)
892 {
893 int ret_val;
894 char *dev_name;
895 void *addr;
896 void *mask;
897 u32 addr_len;
898 u32 secid;
899 struct netlbl_audit audit_info;
901 /* Don't allow users to add both IPv4 and IPv6 addresses for a
902 * single entry. However, allow users to create two entries, one each
903 * for IPv4 and IPv4, with the same LSM security context which should
904 * achieve the same result. */
905 if (!info->attrs[NLBL_UNLABEL_A_SECCTX] ||
906 !info->attrs[NLBL_UNLABEL_A_IFACE] ||
907 !((!info->attrs[NLBL_UNLABEL_A_IPV4ADDR] ||
908 !info->attrs[NLBL_UNLABEL_A_IPV4MASK]) ^
909 (!info->attrs[NLBL_UNLABEL_A_IPV6ADDR] ||
910 !info->attrs[NLBL_UNLABEL_A_IPV6MASK])))
911 return -EINVAL;
913 netlbl_netlink_auditinfo(skb, &audit_info);
915 ret_val = netlbl_unlabel_addrinfo_get(info, &addr, &mask, &addr_len);
916 if (ret_val != 0)
917 return ret_val;
918 dev_name = nla_data(info->attrs[NLBL_UNLABEL_A_IFACE]);
919 ret_val = security_secctx_to_secid(
920 nla_data(info->attrs[NLBL_UNLABEL_A_SECCTX]),
921 nla_len(info->attrs[NLBL_UNLABEL_A_SECCTX]),
922 &secid);
923 if (ret_val != 0)
924 return ret_val;
926 return netlbl_unlhsh_add(&init_net,
927 dev_name, addr, mask, addr_len, secid,
928 &audit_info);
929 }
931 /**
932 * netlbl_unlabel_staticadddef - Handle a STATICADDDEF message
933 * @skb: the NETLINK buffer
934 * @info: the Generic NETLINK info block
935 *
936 * Description:
937 * Process a user generated STATICADDDEF message and add a new default
938 * unlabeled connection entry. Returns zero on success, negative values on
939 * failure.
940 *
941 */
942 static int netlbl_unlabel_staticadddef(struct sk_buff *skb,
943 struct genl_info *info)
944 {
945 int ret_val;
946 void *addr;
947 void *mask;
948 u32 addr_len;
949 u32 secid;
950 struct netlbl_audit audit_info;
952 /* Don't allow users to add both IPv4 and IPv6 addresses for a
953 * single entry. However, allow users to create two entries, one each
954 * for IPv4 and IPv6, with the same LSM security context which should
955 * achieve the same result. */
956 if (!info->attrs[NLBL_UNLABEL_A_SECCTX] ||
957 !((!info->attrs[NLBL_UNLABEL_A_IPV4ADDR] ||
958 !info->attrs[NLBL_UNLABEL_A_IPV4MASK]) ^
959 (!info->attrs[NLBL_UNLABEL_A_IPV6ADDR] ||
960 !info->attrs[NLBL_UNLABEL_A_IPV6MASK])))
961 return -EINVAL;
963 netlbl_netlink_auditinfo(skb, &audit_info);
965 ret_val = netlbl_unlabel_addrinfo_get(info, &addr, &mask, &addr_len);
966 if (ret_val != 0)
967 return ret_val;
968 ret_val = security_secctx_to_secid(
969 nla_data(info->attrs[NLBL_UNLABEL_A_SECCTX]),
970 nla_len(info->attrs[NLBL_UNLABEL_A_SECCTX]),
971 &secid);
972 if (ret_val != 0)
973 return ret_val;
975 return netlbl_unlhsh_add(&init_net,
976 NULL, addr, mask, addr_len, secid,
977 &audit_info);
978 }
980 /**
981 * netlbl_unlabel_staticremove - Handle a STATICREMOVE message
982 * @skb: the NETLINK buffer
983 * @info: the Generic NETLINK info block
984 *
985 * Description:
986 * Process a user generated STATICREMOVE message and remove the specified
987 * unlabeled connection entry. Returns zero on success, negative values on
988 * failure.
989 *
990 */
991 static int netlbl_unlabel_staticremove(struct sk_buff *skb,
992 struct genl_info *info)
993 {
994 int ret_val;
995 char *dev_name;
996 void *addr;
997 void *mask;
998 u32 addr_len;
999 struct netlbl_audit audit_info;
1001 /* See the note in netlbl_unlabel_staticadd() about not allowing both
1002 * IPv4 and IPv6 in the same entry. */
1003 if (!info->attrs[NLBL_UNLABEL_A_IFACE] ||
1004 !((!info->attrs[NLBL_UNLABEL_A_IPV4ADDR] ||
1005 !info->attrs[NLBL_UNLABEL_A_IPV4MASK]) ^
1006 (!info->attrs[NLBL_UNLABEL_A_IPV6ADDR] ||
1007 !info->attrs[NLBL_UNLABEL_A_IPV6MASK])))
1008 return -EINVAL;
1010 netlbl_netlink_auditinfo(skb, &audit_info);
1012 ret_val = netlbl_unlabel_addrinfo_get(info, &addr, &mask, &addr_len);
1013 if (ret_val != 0)
1014 return ret_val;
1015 dev_name = nla_data(info->attrs[NLBL_UNLABEL_A_IFACE]);
1017 return netlbl_unlhsh_remove(&init_net,
1018 dev_name, addr, mask, addr_len,
1019 &audit_info);
1020 }
1022 /**
1023 * netlbl_unlabel_staticremovedef - Handle a STATICREMOVEDEF message
1024 * @skb: the NETLINK buffer
1025 * @info: the Generic NETLINK info block
1026 *
1027 * Description:
1028 * Process a user generated STATICREMOVEDEF message and remove the default
1029 * unlabeled connection entry. Returns zero on success, negative values on
1030 * failure.
1031 *
1032 */
1033 static int netlbl_unlabel_staticremovedef(struct sk_buff *skb,
1034 struct genl_info *info)
1035 {
1036 int ret_val;
1037 void *addr;
1038 void *mask;
1039 u32 addr_len;
1040 struct netlbl_audit audit_info;
1042 /* See the note in netlbl_unlabel_staticadd() about not allowing both
1043 * IPv4 and IPv6 in the same entry. */
1044 if (!((!info->attrs[NLBL_UNLABEL_A_IPV4ADDR] ||
1045 !info->attrs[NLBL_UNLABEL_A_IPV4MASK]) ^
1046 (!info->attrs[NLBL_UNLABEL_A_IPV6ADDR] ||
1047 !info->attrs[NLBL_UNLABEL_A_IPV6MASK])))
1048 return -EINVAL;
1050 netlbl_netlink_auditinfo(skb, &audit_info);
1052 ret_val = netlbl_unlabel_addrinfo_get(info, &addr, &mask, &addr_len);
1053 if (ret_val != 0)
1054 return ret_val;
1056 return netlbl_unlhsh_remove(&init_net,
1057 NULL, addr, mask, addr_len,
1058 &audit_info);
1059 }
1062 /**
1063 * netlbl_unlabel_staticlist_gen - Generate messages for STATICLIST[DEF]
1064 * @cmd: command/message
1065 * @iface: the interface entry
1066 * @addr4: the IPv4 address entry
1067 * @addr6: the IPv6 address entry
1068 * @arg: the netlbl_unlhsh_walk_arg structure
1069 *
1070 * Description:
1071 * This function is designed to be used to generate a response for a
1072 * STATICLIST or STATICLISTDEF message. When called either @addr4 or @addr6
1073 * can be specified, not both, the other unspecified entry should be set to
1074 * NULL by the caller. Returns the size of the message on success, negative
1075 * values on failure.
1076 *
1077 */
1078 static int netlbl_unlabel_staticlist_gen(u32 cmd,
1079 const struct netlbl_unlhsh_iface *iface,
1080 const struct netlbl_unlhsh_addr4 *addr4,
1081 const struct netlbl_unlhsh_addr6 *addr6,
1082 void *arg)
1083 {
1084 int ret_val = -ENOMEM;
1085 struct netlbl_unlhsh_walk_arg *cb_arg = arg;
1086 struct net_device *dev;
1087 void *data;
1088 u32 secid;
1089 char *secctx;
1090 u32 secctx_len;
1092 data = genlmsg_put(cb_arg->skb, NETLINK_CB(cb_arg->nl_cb->skb).portid,
1093 cb_arg->seq, &netlbl_unlabel_gnl_family,
1094 NLM_F_MULTI, cmd);
1095 if (data == NULL)
1096 goto list_cb_failure;
1098 if (iface->ifindex > 0) {
1099 dev = dev_get_by_index(&init_net, iface->ifindex);
1100 if (!dev) {
1101 ret_val = -ENODEV;
1102 goto list_cb_failure;
1103 }
1104 ret_val = nla_put_string(cb_arg->skb,
1105 NLBL_UNLABEL_A_IFACE, dev->name);
1106 dev_put(dev);
1107 if (ret_val != 0)
1108 goto list_cb_failure;
1109 }
1111 if (addr4) {
1112 struct in_addr addr_struct;
1114 addr_struct.s_addr = addr4->list.addr;
1115 ret_val = nla_put_in_addr(cb_arg->skb,
1116 NLBL_UNLABEL_A_IPV4ADDR,
1117 addr_struct.s_addr);
1118 if (ret_val != 0)
1119 goto list_cb_failure;
1121 addr_struct.s_addr = addr4->list.mask;
1122 ret_val = nla_put_in_addr(cb_arg->skb,
1123 NLBL_UNLABEL_A_IPV4MASK,
1124 addr_struct.s_addr);
1125 if (ret_val != 0)
1126 goto list_cb_failure;
1128 secid = addr4->secid;
1129 } else {
1130 ret_val = nla_put_in6_addr(cb_arg->skb,
1131 NLBL_UNLABEL_A_IPV6ADDR,
1132 &addr6->list.addr);
1133 if (ret_val != 0)
1134 goto list_cb_failure;
1136 ret_val = nla_put_in6_addr(cb_arg->skb,
1137 NLBL_UNLABEL_A_IPV6MASK,
1138 &addr6->list.mask);
1139 if (ret_val != 0)
1140 goto list_cb_failure;
1142 secid = addr6->secid;
1143 }
1145 ret_val = security_secid_to_secctx(secid, &secctx, &secctx_len);
1146 if (ret_val != 0)
1147 goto list_cb_failure;
1148 ret_val = nla_put(cb_arg->skb,
1149 NLBL_UNLABEL_A_SECCTX,
1150 secctx_len,
1151 secctx);
1152 security_release_secctx(secctx, secctx_len);
1153 if (ret_val != 0)
1154 goto list_cb_failure;
1156 cb_arg->seq++;
1157 genlmsg_end(cb_arg->skb, data);
1158 return 0;
1160 list_cb_failure:
1161 genlmsg_cancel(cb_arg->skb, data);
1162 return ret_val;
1163 }
1165 /**
1166 * netlbl_unlabel_staticlist - Handle a STATICLIST message
1167 * @skb: the NETLINK buffer
1168 * @cb: the NETLINK callback
1169 *
1170 * Description:
1171 * Process a user generated STATICLIST message and dump the unlabeled
1172 * connection hash table in a form suitable for use in a kernel generated
1173 * STATICLIST message. Returns the length of @skb.
1174 *
1175 */
1176 static int netlbl_unlabel_staticlist(struct sk_buff *skb,
1177 struct netlink_callback *cb)
1178 {
1179 struct netlbl_unlhsh_walk_arg cb_arg;
1180 u32 skip_bkt = cb->args[0];
1181 u32 skip_chain = cb->args[1];
1182 u32 iter_bkt;
1183 u32 iter_chain = 0, iter_addr4 = 0, iter_addr6 = 0;
1184 struct netlbl_unlhsh_iface *iface;
1185 struct list_head *iter_list;
1186 struct netlbl_af4list *addr4;
1187 #if IS_ENABLED(CONFIG_IPV6)
1188 struct netlbl_af6list *addr6;
1189 #endif
1191 cb_arg.nl_cb = cb;
1192 cb_arg.skb = skb;
1193 cb_arg.seq = cb->nlh->nlmsg_seq;
1195 rcu_read_lock();
1196 for (iter_bkt = skip_bkt;
1197 iter_bkt < rcu_dereference(netlbl_unlhsh)->size;
1198 iter_bkt++, iter_chain = 0, iter_addr4 = 0, iter_addr6 = 0) {
1199 iter_list = &rcu_dereference(netlbl_unlhsh)->tbl[iter_bkt];
1200 list_for_each_entry_rcu(iface, iter_list, list) {
1201 if (!iface->valid ||
1202 iter_chain++ < skip_chain)
1203 continue;
1204 netlbl_af4list_foreach_rcu(addr4,
1205 &iface->addr4_list) {
1206 if (iter_addr4++ < cb->args[2])
1207 continue;
1208 if (netlbl_unlabel_staticlist_gen(
1209 NLBL_UNLABEL_C_STATICLIST,
1210 iface,
1211 netlbl_unlhsh_addr4_entry(addr4),
1212 NULL,
1213 &cb_arg) < 0) {
1214 iter_addr4--;
1215 iter_chain--;
1216 goto unlabel_staticlist_return;
1217 }
1218 }
1219 #if IS_ENABLED(CONFIG_IPV6)
1220 netlbl_af6list_foreach_rcu(addr6,
1221 &iface->addr6_list) {
1222 if (iter_addr6++ < cb->args[3])
1223 continue;
1224 if (netlbl_unlabel_staticlist_gen(
1225 NLBL_UNLABEL_C_STATICLIST,
1226 iface,
1227 NULL,
1228 netlbl_unlhsh_addr6_entry(addr6),
1229 &cb_arg) < 0) {
1230 iter_addr6--;
1231 iter_chain--;
1232 goto unlabel_staticlist_return;
1233 }
1234 }
1235 #endif /* IPv6 */
1236 }
1237 }
1239 unlabel_staticlist_return:
1240 rcu_read_unlock();
1241 cb->args[0] = iter_bkt;
1242 cb->args[1] = iter_chain;
1243 cb->args[2] = iter_addr4;
1244 cb->args[3] = iter_addr6;
1245 return skb->len;
1246 }
1248 /**
1249 * netlbl_unlabel_staticlistdef - Handle a STATICLISTDEF message
1250 * @skb: the NETLINK buffer
1251 * @cb: the NETLINK callback
1252 *
1253 * Description:
1254 * Process a user generated STATICLISTDEF message and dump the default
1255 * unlabeled connection entry in a form suitable for use in a kernel generated
1256 * STATICLISTDEF message. Returns the length of @skb.
1257 *
1258 */
1259 static int netlbl_unlabel_staticlistdef(struct sk_buff *skb,
1260 struct netlink_callback *cb)
1261 {
1262 struct netlbl_unlhsh_walk_arg cb_arg;
1263 struct netlbl_unlhsh_iface *iface;
1264 u32 iter_addr4 = 0, iter_addr6 = 0;
1265 struct netlbl_af4list *addr4;
1266 #if IS_ENABLED(CONFIG_IPV6)
1267 struct netlbl_af6list *addr6;
1268 #endif
1270 cb_arg.nl_cb = cb;
1271 cb_arg.skb = skb;
1272 cb_arg.seq = cb->nlh->nlmsg_seq;
1274 rcu_read_lock();
1275 iface = rcu_dereference(netlbl_unlhsh_def);
1276 if (iface == NULL || !iface->valid)
1277 goto unlabel_staticlistdef_return;
1279 netlbl_af4list_foreach_rcu(addr4, &iface->addr4_list) {
1280 if (iter_addr4++ < cb->args[0])
1281 continue;
1282 if (netlbl_unlabel_staticlist_gen(NLBL_UNLABEL_C_STATICLISTDEF,
1283 iface,
1284 netlbl_unlhsh_addr4_entry(addr4),
1285 NULL,
1286 &cb_arg) < 0) {
1287 iter_addr4--;
1288 goto unlabel_staticlistdef_return;
1289 }
1290 }
1291 #if IS_ENABLED(CONFIG_IPV6)
1292 netlbl_af6list_foreach_rcu(addr6, &iface->addr6_list) {
1293 if (iter_addr6++ < cb->args[1])
1294 continue;
1295 if (netlbl_unlabel_staticlist_gen(NLBL_UNLABEL_C_STATICLISTDEF,
1296 iface,
1297 NULL,
1298 netlbl_unlhsh_addr6_entry(addr6),
1299 &cb_arg) < 0) {
1300 iter_addr6--;
1301 goto unlabel_staticlistdef_return;
1302 }
1303 }
1304 #endif /* IPv6 */
1306 unlabel_staticlistdef_return:
1307 rcu_read_unlock();
1308 cb->args[0] = iter_addr4;
1309 cb->args[1] = iter_addr6;
1310 return skb->len;
1311 }
1313 /*
1314 * NetLabel Generic NETLINK Command Definitions
1315 */
1317 static const struct genl_ops netlbl_unlabel_genl_ops[] = {
1318 {
1319 .cmd = NLBL_UNLABEL_C_STATICADD,
1320 .flags = GENL_ADMIN_PERM,
1321 .policy = netlbl_unlabel_genl_policy,
1322 .doit = netlbl_unlabel_staticadd,
1323 .dumpit = NULL,
1324 },
1325 {
1326 .cmd = NLBL_UNLABEL_C_STATICREMOVE,
1327 .flags = GENL_ADMIN_PERM,
1328 .policy = netlbl_unlabel_genl_policy,
1329 .doit = netlbl_unlabel_staticremove,
1330 .dumpit = NULL,
1331 },
1332 {
1333 .cmd = NLBL_UNLABEL_C_STATICLIST,
1334 .flags = 0,
1335 .policy = netlbl_unlabel_genl_policy,
1336 .doit = NULL,
1337 .dumpit = netlbl_unlabel_staticlist,
1338 },
1339 {
1340 .cmd = NLBL_UNLABEL_C_STATICADDDEF,
1341 .flags = GENL_ADMIN_PERM,
1342 .policy = netlbl_unlabel_genl_policy,
1343 .doit = netlbl_unlabel_staticadddef,
1344 .dumpit = NULL,
1345 },
1346 {
1347 .cmd = NLBL_UNLABEL_C_STATICREMOVEDEF,
1348 .flags = GENL_ADMIN_PERM,
1349 .policy = netlbl_unlabel_genl_policy,
1350 .doit = netlbl_unlabel_staticremovedef,
1351 .dumpit = NULL,
1352 },
1353 {
1354 .cmd = NLBL_UNLABEL_C_STATICLISTDEF,
1355 .flags = 0,
1356 .policy = netlbl_unlabel_genl_policy,
1357 .doit = NULL,
1358 .dumpit = netlbl_unlabel_staticlistdef,
1359 },
1360 {
1361 .cmd = NLBL_UNLABEL_C_ACCEPT,
1362 .flags = GENL_ADMIN_PERM,
1363 .policy = netlbl_unlabel_genl_policy,
1364 .doit = netlbl_unlabel_accept,
1365 .dumpit = NULL,
1366 },
1367 {
1368 .cmd = NLBL_UNLABEL_C_LIST,
1369 .flags = 0,
1370 .policy = netlbl_unlabel_genl_policy,
1371 .doit = netlbl_unlabel_list,
1372 .dumpit = NULL,
1373 },
1374 };
1376 static struct genl_family netlbl_unlabel_gnl_family __ro_after_init = {
1377 .hdrsize = 0,
1378 .name = NETLBL_NLTYPE_UNLABELED_NAME,
1379 .version = NETLBL_PROTO_VERSION,
1380 .maxattr = NLBL_UNLABEL_A_MAX,
1381 .module = THIS_MODULE,
1382 .ops = netlbl_unlabel_genl_ops,
1383 .n_ops = ARRAY_SIZE(netlbl_unlabel_genl_ops),
1384 };
1386 /*
1387 * NetLabel Generic NETLINK Protocol Functions
1388 */
1390 /**
1391 * netlbl_unlabel_genl_init - Register the Unlabeled NetLabel component
1392 *
1393 * Description:
1394 * Register the unlabeled packet NetLabel component with the Generic NETLINK
1395 * mechanism. Returns zero on success, negative values on failure.
1396 *
1397 */
1398 int __init netlbl_unlabel_genl_init(void)
1399 {
1400 return genl_register_family(&netlbl_unlabel_gnl_family);
1401 }
1403 /*
1404 * NetLabel KAPI Hooks
1405 */
1407 static struct notifier_block netlbl_unlhsh_netdev_notifier = {
1408 .notifier_call = netlbl_unlhsh_netdev_handler,
1409 };
1411 /**
1412 * netlbl_unlabel_init - Initialize the unlabeled connection hash table
1413 * @size: the number of bits to use for the hash buckets
1414 *
1415 * Description:
1416 * Initializes the unlabeled connection hash table and registers a network
1417 * device notification handler. This function should only be called by the
1418 * NetLabel subsystem itself during initialization. Returns zero on success,
1419 * non-zero values on error.
1420 *
1421 */
1422 int __init netlbl_unlabel_init(u32 size)
1423 {
1424 u32 iter;
1425 struct netlbl_unlhsh_tbl *hsh_tbl;
1427 if (size == 0)
1428 return -EINVAL;
1430 hsh_tbl = kmalloc(sizeof(*hsh_tbl), GFP_KERNEL);
1431 if (hsh_tbl == NULL)
1432 return -ENOMEM;
1433 hsh_tbl->size = 1 << size;
1434 hsh_tbl->tbl = kcalloc(hsh_tbl->size,
1435 sizeof(struct list_head),
1436 GFP_KERNEL);
1437 if (hsh_tbl->tbl == NULL) {
1438 kfree(hsh_tbl);
1439 return -ENOMEM;
1440 }
1441 for (iter = 0; iter < hsh_tbl->size; iter++)
1442 INIT_LIST_HEAD(&hsh_tbl->tbl[iter]);
1444 spin_lock(&netlbl_unlhsh_lock);
1445 rcu_assign_pointer(netlbl_unlhsh, hsh_tbl);
1446 spin_unlock(&netlbl_unlhsh_lock);
1448 register_netdevice_notifier(&netlbl_unlhsh_netdev_notifier);
1450 return 0;
1451 }
1453 /**
1454 * netlbl_unlabel_getattr - Get the security attributes for an unlabled packet
1455 * @skb: the packet
1456 * @family: protocol family
1457 * @secattr: the security attributes
1458 *
1459 * Description:
1460 * Determine the security attributes, if any, for an unlabled packet and return
1461 * them in @secattr. Returns zero on success and negative values on failure.
1462 *
1463 */
1464 int netlbl_unlabel_getattr(const struct sk_buff *skb,
1465 u16 family,
1466 struct netlbl_lsm_secattr *secattr)
1467 {
1468 struct netlbl_unlhsh_iface *iface;
1470 rcu_read_lock();
1471 iface = netlbl_unlhsh_search_iface(skb->skb_iif);
1472 if (iface == NULL)
1473 iface = rcu_dereference(netlbl_unlhsh_def);
1474 if (iface == NULL || !iface->valid)
1475 goto unlabel_getattr_nolabel;
1477 #if IS_ENABLED(CONFIG_IPV6)
1478 /* When resolving a fallback label, check the sk_buff version as
1479 * it is possible (e.g. SCTP) to have family = PF_INET6 while
1480 * receiving ip_hdr(skb)->version = 4.
1481 */
1482 if (family == PF_INET6 && ip_hdr(skb)->version == 4)
1483 family = PF_INET;
1484 #endif /* IPv6 */
1486 switch (family) {
1487 case PF_INET: {
1488 struct iphdr *hdr4;
1489 struct netlbl_af4list *addr4;
1491 hdr4 = ip_hdr(skb);
1492 addr4 = netlbl_af4list_search(hdr4->saddr,
1493 &iface->addr4_list);
1494 if (addr4 == NULL)
1495 goto unlabel_getattr_nolabel;
1496 secattr->attr.secid = netlbl_unlhsh_addr4_entry(addr4)->secid;
1497 break;
1498 }
1499 #if IS_ENABLED(CONFIG_IPV6)
1500 case PF_INET6: {
1501 struct ipv6hdr *hdr6;
1502 struct netlbl_af6list *addr6;
1504 hdr6 = ipv6_hdr(skb);
1505 addr6 = netlbl_af6list_search(&hdr6->saddr,
1506 &iface->addr6_list);
1507 if (addr6 == NULL)
1508 goto unlabel_getattr_nolabel;
1509 secattr->attr.secid = netlbl_unlhsh_addr6_entry(addr6)->secid;
1510 break;
1511 }
1512 #endif /* IPv6 */
1513 default:
1514 goto unlabel_getattr_nolabel;
1515 }
1516 rcu_read_unlock();
1518 secattr->flags |= NETLBL_SECATTR_SECID;
1519 secattr->type = NETLBL_NLTYPE_UNLABELED;
1520 return 0;
1522 unlabel_getattr_nolabel:
1523 rcu_read_unlock();
1524 if (netlabel_unlabel_acceptflg == 0)
1525 return -ENOMSG;
1526 secattr->type = NETLBL_NLTYPE_UNLABELED;
1527 return 0;
1528 }
1530 /**
1531 * netlbl_unlabel_defconf - Set the default config to allow unlabeled packets
1532 *
1533 * Description:
1534 * Set the default NetLabel configuration to allow incoming unlabeled packets
1535 * and to send unlabeled network traffic by default.
1536 *
1537 */
1538 int __init netlbl_unlabel_defconf(void)
1539 {
1540 int ret_val;
1541 struct netlbl_dom_map *entry;
1542 struct netlbl_audit audit_info;
1544 /* Only the kernel is allowed to call this function and the only time
1545 * it is called is at bootup before the audit subsystem is reporting
1546 * messages so don't worry to much about these values. */
1547 security_task_getsecid(current, &audit_info.secid);
1548 audit_info.loginuid = GLOBAL_ROOT_UID;
1549 audit_info.sessionid = 0;
1551 entry = kzalloc(sizeof(*entry), GFP_KERNEL);
1552 if (entry == NULL)
1553 return -ENOMEM;
1554 entry->family = AF_UNSPEC;
1555 entry->def.type = NETLBL_NLTYPE_UNLABELED;
1556 ret_val = netlbl_domhsh_add_default(entry, &audit_info);
1557 if (ret_val != 0)
1558 return ret_val;
1560 netlbl_unlabel_acceptflg_set(1, &audit_info);
1562 return 0;
1563 }