samples/rpmsg: Introduce a module parameter for message count
[rpmsg/rpmsg.git] / samples / rpmsg / rpmsg_client_sample.c
1 /*
2  * Remote processor messaging - sample client driver
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  * Copyright (C) 2011 Google, Inc.
6  *
7  * Ohad Ben-Cohen <ohad@wizery.com>
8  * Brian Swetland <swetland@google.com>
9  *
10  * This software is licensed under the terms of the GNU General Public
11  * License version 2, as published by the Free Software Foundation, and
12  * may be copied, distributed, and modified under those terms.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  */
20 #include <linux/kernel.h>
21 #include <linux/module.h>
22 #include <linux/rpmsg.h>
24 #define MSG             "hello world!"
26 static int count = 100;
27 module_param(count, int, 0644);
29 struct instance_data {
30         int rx_count;
31 };
33 static int rpmsg_sample_cb(struct rpmsg_device *rpdev, void *data, int len,
34                                                 void *priv, u32 src)
35 {
36         int ret;
37         struct instance_data *idata = dev_get_drvdata(&rpdev->dev);
39         dev_info(&rpdev->dev, "incoming msg %d (src: 0x%x)\n",
40                  ++idata->rx_count, src);
42         print_hex_dump(KERN_DEBUG, __func__, DUMP_PREFIX_NONE, 16, 1,
43                        data, len,  true);
45         /* samples should not live forever */
46         if (idata->rx_count >= count) {
47                 dev_info(&rpdev->dev, "goodbye!\n");
48                 return 0;
49         }
51         /* send a new message now */
52         ret = rpmsg_send(rpdev->ept, MSG, strlen(MSG));
53         if (ret)
54                 dev_err(&rpdev->dev, "rpmsg_send failed: %d\n", ret);
56         return 0;
57 }
59 static int rpmsg_sample_probe(struct rpmsg_device *rpdev)
60 {
61         int ret;
62         struct instance_data *idata;
64         dev_info(&rpdev->dev, "new channel: 0x%x -> 0x%x!\n",
65                                         rpdev->src, rpdev->dst);
67         idata = devm_kzalloc(&rpdev->dev, sizeof(*idata), GFP_KERNEL);
68         if (!idata)
69                 return -ENOMEM;
71         dev_set_drvdata(&rpdev->dev, idata);
73         /* send a message to our remote processor */
74         ret = rpmsg_send(rpdev->ept, MSG, strlen(MSG));
75         if (ret) {
76                 dev_err(&rpdev->dev, "rpmsg_send failed: %d\n", ret);
77                 return ret;
78         }
80         return 0;
81 }
83 static void rpmsg_sample_remove(struct rpmsg_device *rpdev)
84 {
85         dev_info(&rpdev->dev, "rpmsg sample client driver is removed\n");
86 }
88 static struct rpmsg_device_id rpmsg_driver_sample_id_table[] = {
89         { .name = "rpmsg-client-sample" },
90         { },
91 };
92 MODULE_DEVICE_TABLE(rpmsg, rpmsg_driver_sample_id_table);
94 static struct rpmsg_driver rpmsg_sample_client = {
95         .drv.name       = KBUILD_MODNAME,
96         .id_table       = rpmsg_driver_sample_id_table,
97         .probe          = rpmsg_sample_probe,
98         .callback       = rpmsg_sample_cb,
99         .remove         = rpmsg_sample_remove,
100 };
101 module_rpmsg_driver(rpmsg_sample_client);
103 MODULE_DESCRIPTION("Remote processor messaging sample client driver");
104 MODULE_LICENSE("GPL v2");