1 #!/bin/sh
3 # Script to create/update include/generated/autoksyms.h and dependency files
4 #
5 # Copyright: (C) 2016 Linaro Limited
6 # Created by: Nicolas Pitre, January 2016
7 #
8 # This program is free software; you can redistribute it and/or modify
9 # it under the terms of the GNU General Public License version 2 as
10 # published by the Free Software Foundation.
12 # Create/update the include/generated/autoksyms.h file from the list
13 # of all module's needed symbols as recorded on the third line of
14 # .tmp_versions/*.mod files.
15 #
16 # For each symbol being added or removed, the corresponding dependency
17 # file's timestamp is updated to force a rebuild of the affected source
18 # file. All arguments passed to this script are assumed to be a command
19 # to be exec'd to trigger a rebuild of those files.
21 set -e
23 cur_ksyms_file="include/generated/autoksyms.h"
24 new_ksyms_file="include/generated/autoksyms.h.tmpnew"
26 info() {
27 if [ "$quiet" != "silent_" ]; then
28 printf " %-7s %s\n" "$1" "$2"
29 fi
30 }
32 info "CHK" "$cur_ksyms_file"
34 # Use "make V=1" to debug this script.
35 case "$KBUILD_VERBOSE" in
36 *1*)
37 set -x
38 ;;
39 esac
41 # We need access to CONFIG_ symbols
42 case "${KCONFIG_CONFIG}" in
43 */*)
44 . "${KCONFIG_CONFIG}"
45 ;;
46 *)
47 # Force using a file from the current directory
48 . "./${KCONFIG_CONFIG}"
49 esac
51 # Generate a new ksym list file with symbols needed by the current
52 # set of modules.
53 cat > "$new_ksyms_file" << EOT
54 /*
55 * Automatically generated file; DO NOT EDIT.
56 */
58 EOT
59 [ "$(ls -A "$MODVERDIR")" ] &&
60 for mod in "$MODVERDIR"/*.mod; do
61 sed -n -e '3{s/ /\n/g;/^$/!p;}' "$mod"
62 done | sort -u |
63 while read sym; do
64 echo "#define __KSYM_${sym} 1"
65 done >> "$new_ksyms_file"
67 # Special case for modversions (see modpost.c)
68 if [ -n "$CONFIG_MODVERSIONS" ]; then
69 echo "#define __KSYM_module_layout 1" >> "$new_ksyms_file"
70 fi
72 # Extract changes between old and new list and touch corresponding
73 # dependency files.
74 changed=$(
75 count=0
76 sort "$cur_ksyms_file" "$new_ksyms_file" | uniq -u |
77 sed -n 's/^#define __KSYM_\(.*\) 1/\1/p' | tr "A-Z_" "a-z/" |
78 while read sympath; do
79 if [ -z "$sympath" ]; then continue; fi
80 depfile="include/ksym/${sympath}.h"
81 mkdir -p "$(dirname "$depfile")"
82 touch "$depfile"
83 # Filesystems with coarse time precision may create timestamps
84 # equal to the one from a file that was very recently built and that
85 # needs to be rebuild. Let's guard against that by making sure our
86 # dep files are always newer than the first file we created here.
87 while [ ! "$depfile" -nt "$new_ksyms_file" ]; do
88 touch "$depfile"
89 done
90 echo $((count += 1))
91 done | tail -1 )
92 changed=${changed:-0}
94 if [ $changed -gt 0 ]; then
95 # Replace the old list with tne new one
96 old=$(grep -c "^#define __KSYM_" "$cur_ksyms_file" || true)
97 new=$(grep -c "^#define __KSYM_" "$new_ksyms_file" || true)
98 info "KSYMS" "symbols: before=$old, after=$new, changed=$changed"
99 info "UPD" "$cur_ksyms_file"
100 mv -f "$new_ksyms_file" "$cur_ksyms_file"
101 # Then trigger a rebuild of affected source files
102 exec $@
103 else
104 rm -f "$new_ksyms_file"
105 fi