]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - usr/Kconfig
Merge branch 'linux-4.15' of git://github.com/skeggsb/linux into drm-fixes
[rpmsg/rpmsg.git] / usr / Kconfig
1 # SPDX-License-Identifier: GPL-2.0
2 #
3 # Configuration for initramfs
4 #
6 config INITRAMFS_SOURCE
7         string "Initramfs source file(s)"
8         default ""
9         help
10           This can be either a single cpio archive with a .cpio suffix or a
11           space-separated list of directories and files for building the
12           initramfs image.  A cpio archive should contain a filesystem archive
13           to be used as an initramfs image.  Directories should contain a
14           filesystem layout to be included in the initramfs image.  Files
15           should contain entries according to the format described by the
16           "usr/gen_init_cpio" program in the kernel tree.
18           When multiple directories and files are specified then the
19           initramfs image will be the aggregate of all of them.
21           See <file:Documentation/early-userspace/README> for more details.
23           If you are not sure, leave it blank.
25 config INITRAMFS_FORCE
26         bool "Ignore the initramfs passed by the bootloader"
27         depends on CMDLINE_EXTEND || CMDLINE_FORCE
28         help
29           This option causes the kernel to ignore the initramfs image
30           (or initrd image) passed to it by the bootloader. This is
31           analogous to CMDLINE_FORCE, which is found on some architectures,
32           and is useful if you cannot or don't want to change the image
33           your bootloader passes to the kernel.
35 config INITRAMFS_ROOT_UID
36         int "User ID to map to 0 (user root)"
37         depends on INITRAMFS_SOURCE!=""
38         default "0"
39         help
40           If INITRAMFS_SOURCE points to a directory, files owned by this UID
41           (-1 = current user) will be owned by root in the resulting image.
43           If you are not sure, leave it set to "0".
45 config INITRAMFS_ROOT_GID
46         int "Group ID to map to 0 (group root)"
47         depends on INITRAMFS_SOURCE!=""
48         default "0"
49         help
50           If INITRAMFS_SOURCE points to a directory, files owned by this GID
51           (-1 = current group) will be owned by root in the resulting image.
53           If you are not sure, leave it set to "0".
55 config RD_GZIP
56         bool "Support initial ramdisk/ramfs compressed using gzip"
57         depends on BLK_DEV_INITRD
58         default y
59         select DECOMPRESS_GZIP
60         help
61           Support loading of a gzip encoded initial ramdisk or cpio buffer.
62           If unsure, say Y.
64 config RD_BZIP2
65         bool "Support initial ramdisk/ramfs compressed using bzip2"
66         default y
67         depends on BLK_DEV_INITRD
68         select DECOMPRESS_BZIP2
69         help
70           Support loading of a bzip2 encoded initial ramdisk or cpio buffer
71           If unsure, say N.
73 config RD_LZMA
74         bool "Support initial ramdisk/ramfs compressed using LZMA"
75         default y
76         depends on BLK_DEV_INITRD
77         select DECOMPRESS_LZMA
78         help
79           Support loading of a LZMA encoded initial ramdisk or cpio buffer
80           If unsure, say N.
82 config RD_XZ
83         bool "Support initial ramdisk/ramfs compressed using XZ"
84         depends on BLK_DEV_INITRD
85         default y
86         select DECOMPRESS_XZ
87         help
88           Support loading of a XZ encoded initial ramdisk or cpio buffer.
89           If unsure, say N.
91 config RD_LZO
92         bool "Support initial ramdisk/ramfs compressed using LZO"
93         default y
94         depends on BLK_DEV_INITRD
95         select DECOMPRESS_LZO
96         help
97           Support loading of a LZO encoded initial ramdisk or cpio buffer
98           If unsure, say N.
100 config RD_LZ4
101         bool "Support initial ramdisk/ramfs compressed using LZ4"
102         default y
103         depends on BLK_DEV_INITRD
104         select DECOMPRESS_LZ4
105         help
106           Support loading of a LZ4 encoded initial ramdisk or cpio buffer
107           If unsure, say N.
109 choice
110         prompt "Built-in initramfs compression mode"
111         depends on INITRAMFS_SOURCE!=""
112         optional
113         help
114           This option allows you to decide by which algorithm the builtin
115           initramfs will be compressed.  Several compression algorithms are
116           available, which differ in efficiency, compression and
117           decompression speed.  Compression speed is only relevant
118           when building a kernel.  Decompression speed is relevant at
119           each boot. Also the memory usage during decompression may become
120           relevant on memory constrained systems. This is usually based on the
121           dictionary size of the algorithm with algorithms like XZ and LZMA
122           featuring large dictionary sizes.
124           High compression options are mostly useful for users who are
125           low on RAM, since it reduces the memory consumption during
126           boot.
128           Keep in mind that your build system needs to provide the appropriate
129           compression tool to compress the generated initram cpio file for
130           embedding.
132           If in doubt, select 'None'
134 config INITRAMFS_COMPRESSION_NONE
135         bool "None"
136         help
137           Do not compress the built-in initramfs at all. This may sound wasteful
138           in space, but, you should be aware that the built-in initramfs will be
139           compressed at a later stage anyways along with the rest of the kernel,
140           on those architectures that support this. However, not compressing the
141           initramfs may lead to slightly higher memory consumption during a
142           short time at boot, while both the cpio image and the unpacked
143           filesystem image will be present in memory simultaneously
145 config INITRAMFS_COMPRESSION_GZIP
146         bool "Gzip"
147         depends on RD_GZIP
148         help
149           Use the old and well tested gzip compression algorithm. Gzip provides
150           a good balance between compression ratio and decompression speed and
151           has a reasonable compression speed. It is also more likely to be
152           supported by your build system as the gzip tool is present by default
153           on most distros.
155 config INITRAMFS_COMPRESSION_BZIP2
156         bool "Bzip2"
157         depends on RD_BZIP2
158         help
159           It's compression ratio and speed is intermediate. Decompression speed
160           is slowest among the choices. The initramfs size is about 10% smaller
161           with bzip2, in comparison to gzip. Bzip2 uses a large amount of
162           memory. For modern kernels you will need at least 8MB RAM or more for
163           booting.
165           If you choose this, keep in mind that you need to have the bzip2 tool
166           available to be able to compress the initram.
168 config INITRAMFS_COMPRESSION_LZMA
169         bool "LZMA"
170         depends on RD_LZMA
171         help
172           This algorithm's compression ratio is best but has a large dictionary
173           size which might cause issues in memory constrained systems.
174           Decompression speed is between the other choices. Compression is
175           slowest. The initramfs size is about 33% smaller with LZMA in
176           comparison to gzip.
178           If you choose this, keep in mind that you may need to install the xz
179           or lzma tools to be able to compress the initram.
181 config INITRAMFS_COMPRESSION_XZ
182         bool "XZ"
183         depends on RD_XZ
184         help
185           XZ uses the LZMA2 algorithm and has a large dictionary which may cause
186           problems on memory constrained systems. The initramfs size is about
187           30% smaller with XZ in comparison to gzip. Decompression speed is
188           better than that of bzip2 but worse than gzip and LZO. Compression is
189           slow.
191           If you choose this, keep in mind that you may need to install the xz
192           tool to be able to compress the initram.
194 config INITRAMFS_COMPRESSION_LZO
195         bool "LZO"
196         depends on RD_LZO
197         help
198           It's compression ratio is the second poorest amongst the choices. The
199           kernel size is about 10% bigger than gzip. Despite that, it's
200           decompression speed is the second fastest and it's compression speed
201           is quite fast too.
203           If you choose this, keep in mind that you may need to install the lzop
204           tool to be able to compress the initram.
206 config INITRAMFS_COMPRESSION_LZ4
207         bool "LZ4"
208         depends on RD_LZ4
209         help
210           It's compression ratio is the poorest amongst the choices. The kernel
211           size is about 15% bigger than gzip; however its decompression speed
212           is the fastest.
214           If you choose this, keep in mind that most distros don't provide lz4
215           by default which could cause a build failure.
217 endchoice
219 config INITRAMFS_COMPRESSION
220         depends on INITRAMFS_SOURCE!=""
221         string
222         default ""      if INITRAMFS_COMPRESSION_NONE
223         default ".gz"   if INITRAMFS_COMPRESSION_GZIP
224         default ".bz2"  if INITRAMFS_COMPRESSION_BZIP2
225         default ".lzma" if INITRAMFS_COMPRESSION_LZMA
226         default ".xz"   if INITRAMFS_COMPRESSION_XZ
227         default ".lzo"  if INITRAMFS_COMPRESSION_LZO
228         default ".lz4"  if INITRAMFS_COMPRESSION_LZ4
229         default ".gz"   if RD_GZIP
230         default ".lz4"  if RD_LZ4
231         default ".lzo"  if RD_LZO
232         default ".xz"   if RD_XZ
233         default ".lzma" if RD_LZMA
234         default ".bz2"  if RD_BZIP2
235         default ""