1 /*
2 * kvm asynchronous fault support
3 *
4 * Copyright 2010 Red Hat, Inc.
5 *
6 * Author:
7 * Gleb Natapov <gleb@redhat.com>
8 *
9 * This file is free software; you can redistribute it and/or modify
10 * it under the terms of version 2 of the GNU General Public License
11 * as published by the Free Software Foundation.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software Foundation,
20 * Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301, USA.
21 */
23 #ifndef __KVM_ASYNC_PF_H__
24 #define __KVM_ASYNC_PF_H__
26 #ifdef CONFIG_KVM_ASYNC_PF
27 int kvm_async_pf_init(void);
28 void kvm_async_pf_deinit(void);
29 void kvm_async_pf_vcpu_init(struct kvm_vcpu *vcpu);
30 #else
31 #define kvm_async_pf_init() (0)
32 #define kvm_async_pf_deinit() do {} while (0)
33 #define kvm_async_pf_vcpu_init(C) do {} while (0)
34 #endif
36 #endif