]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - virt/kvm/async_pf.h
Merge branch 'drm-armada-fixes' of git://ftp.arm.linux.org.uk/~rmk/linux-arm into...
[rpmsg/rpmsg.git] / virt / kvm / async_pf.h
1 /*
2  * kvm asynchronous fault support
3  *
4  * Copyright 2010 Red Hat, Inc.
5  *
6  * Author:
7  *      Gleb Natapov <gleb@redhat.com>
8  *
9  * This file is free software; you can redistribute it and/or modify
10  * it under the terms of version 2 of the GNU General Public License
11  * as published by the Free Software Foundation.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software Foundation,
20  * Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301, USA.
21  */
23 #ifndef __KVM_ASYNC_PF_H__
24 #define __KVM_ASYNC_PF_H__
26 #ifdef CONFIG_KVM_ASYNC_PF
27 int kvm_async_pf_init(void);
28 void kvm_async_pf_deinit(void);
29 void kvm_async_pf_vcpu_init(struct kvm_vcpu *vcpu);
30 #else
31 #define kvm_async_pf_init() (0)
32 #define kvm_async_pf_deinit() do {} while (0)
33 #define kvm_async_pf_vcpu_init(C) do {} while (0)
34 #endif
36 #endif