// SPDX-License-Identifier: GPL-2.0 /* * ioctl32.c: Conversion between 32bit and 64bit native ioctls. * * Copyright (C) 1997-2000 Jakub Jelinek (jakub@redhat.com) * Copyright (C) 1998 Eddie C. Dost (ecd@skynet.be) * Copyright (C) 2001,2002 Andi Kleen, SuSE Labs * Copyright (C) 2003 Pavel Machek (pavel@ucw.cz) * * These routines maintain argument size conversion between 32bit and 64bit * ioctls. */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "internal.h" #include #include #include #include #include #ifdef CONFIG_BLOCK #include #include #include #include #include #endif #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #define __DVB_CORE__ #include #include #include #include #include #ifdef CONFIG_SPARC #include #endif #define convert_in_user(srcptr, dstptr) \ ({ \ typeof(*srcptr) val; \ \ get_user(val, srcptr) || put_user(val, dstptr); \ }) static int do_ioctl(struct file *file, unsigned int cmd, unsigned long arg) { int err; err = security_file_ioctl(file, cmd, arg); if (err) return err; return vfs_ioctl(file, cmd, arg); } struct compat_video_event { int32_t type; compat_time_t timestamp; union { video_size_t size; unsigned int frame_rate; } u; }; static int do_video_get_event(struct file *file, unsigned int cmd, struct compat_video_event __user *up) { struct video_event __user *kevent = compat_alloc_user_space(sizeof(*kevent)); int err; if (kevent == NULL) return -EFAULT; err = do_ioctl(file, cmd, (unsigned long)kevent); if (!err) { err = convert_in_user(&kevent->type, &up->type); err |= convert_in_user(&kevent->timestamp, &up->timestamp); err |= convert_in_user(&kevent->u.size.w, &up->u.size.w); err |= convert_in_user(&kevent->u.size.h, &up->u.size.h); err |= convert_in_user(&kevent->u.size.aspect_ratio, &up->u.size.aspect_ratio); if (err) err = -EFAULT; } return err; } struct compat_video_still_picture { compat_uptr_t iFrame; int32_t size; }; static int do_video_stillpicture(struct file *file, unsigned int cmd, struct compat_video_still_picture __user *up) { struct video_still_picture __user *up_native; compat_uptr_t fp; int32_t size; int err; err = get_user(fp, &up->iFrame); err |= get_user(size, &up->size); if (err) return -EFAULT; up_native = compat_alloc_user_space(sizeof(struct video_still_picture)); err = put_user(compat_ptr(fp), &up_native->iFrame); err |= put_user(size, &up_native->size); if (err) return -EFAULT; err = do_ioctl(file, cmd, (unsigned long) up_native); return err; } #ifdef CONFIG_BLOCK typedef struct sg_io_hdr32 { compat_int_t interface_id; /* [i] 'S' for SCSI generic (required) */ compat_int_t dxfer_direction; /* [i] data transfer direction */ unsigned char cmd_len; /* [i] SCSI command length ( <= 16 bytes) */ unsigned char mx_sb_len; /* [i] max length to write to sbp */ unsigned short iovec_count; /* [i] 0 implies no scatter gather */ compat_uint_t dxfer_len; /* [i] byte count of data transfer */ compat_uint_t dxferp; /* [i], [*io] points to data transfer memory or scatter gather list */ compat_uptr_t cmdp; /* [i], [*i] points to command to perform */ compat_uptr_t sbp; /* [i], [*o] points to sense_buffer memory */ compat_uint_t timeout; /* [i] MAX_UINT->no timeout (unit: millisec) */ compat_uint_t flags; /* [i] 0 -> default, see SG_FLAG... */ compat_int_t pack_id; /* [i->o] unused internally (normally) */ compat_uptr_t usr_ptr; /* [i->o] unused internally */ unsigned char status; /* [o] scsi status */ unsigned char masked_status; /* [o] shifted, masked scsi status */ unsigned char msg_status; /* [o] messaging level data (optional) */ unsigned char sb_len_wr; /* [o] byte count actually written to sbp */ unsigned short host_status; /* [o] errors from host adapter */ unsigned short driver_status; /* [o] errors from software driver */ compat_int_t resid; /* [o] dxfer_len - actual_transferred */ compat_uint_t duration; /* [o] time taken by cmd (unit: millisec) */ compat_uint_t info; /* [o] auxiliary information */ } sg_io_hdr32_t; /* 64 bytes long (on sparc32) */ typedef struct sg_iovec32 { compat_uint_t iov_base; compat_uint_t iov_len; } sg_iovec32_t; static int sg_build_iovec(sg_io_hdr_t __user *sgio, void __user *dxferp, u16 iovec_count) { sg_iovec_t __user *iov = (sg_iovec_t __user *) (sgio + 1); sg_iovec32_t __user *iov32 = dxferp; int i; for (i = 0; i < iovec_count; i++) { u32 base, len; if (get_user(base, &iov32[i].iov_base) || get_user(len, &iov32[i].iov_len) || put_user(compat_ptr(base), &iov[i].iov_base) || put_user(len, &iov[i].iov_len)) return -EFAULT; } if (put_user(iov, &sgio->dxferp)) return -EFAULT; return 0; } static int sg_ioctl_trans(struct file *file, unsigned int cmd, sg_io_hdr32_t __user *sgio32) { sg_io_hdr_t __user *sgio; u16 iovec_count; u32 data; void __user *dxferp; int err; int interface_id; if (get_user(interface_id, &sgio32->interface_id)) return -EFAULT; if (interface_id != 'S') return do_ioctl(file, cmd, (unsigned long)sgio32); if (get_user(iovec_count, &sgio32->iovec_count)) return -EFAULT; { void __user *top = compat_alloc_user_space(0); void __user *new = compat_alloc_user_space(sizeof(sg_io_hdr_t) + (iovec_count * sizeof(sg_iovec_t))); if (new > top) return -EINVAL; sgio = new; } /* Ok, now construct. */ if (copy_in_user(&sgio->interface_id, &sgio32->interface_id, (2 * sizeof(int)) + (2 * sizeof(unsigned char)) + (1 * sizeof(unsigned short)) + (1 * sizeof(unsigned int)))) return -EFAULT; if (get_user(data, &sgio32->dxferp)) return -EFAULT; dxferp = compat_ptr(data); if (iovec_count) { if (sg_build_iovec(sgio, dxferp, iovec_count)) return -EFAULT; } else { if (put_user(dxferp, &sgio->dxferp)) return -EFAULT; } { unsigned char __user *cmdp; unsigned char __user *sbp; if (get_user(data, &sgio32->cmdp)) return -EFAULT; cmdp = compat_ptr(data); if (get_user(data, &sgio32->sbp)) return -EFAULT; sbp = compat_ptr(data); if (put_user(cmdp, &sgio->cmdp) || put_user(sbp, &sgio->sbp)) return -EFAULT; } if (copy_in_user(&sgio->timeout, &sgio32->timeout, 3 * sizeof(int))) return -EFAULT; if (get_user(data, &sgio32->usr_ptr)) return -EFAULT; if (put_user(compat_ptr(data), &sgio->usr_ptr)) return -EFAULT; err = do_ioctl(file, cmd, (unsigned long) sgio); if (err >= 0) { void __user *datap; if (copy_in_user(&sgio32->pack_id, &sgio->pack_id, sizeof(int)) || get_user(datap, &sgio->usr_ptr) || put_user((u32)(unsigned long)datap, &sgio32->usr_ptr) || copy_in_user(&sgio32->status, &sgio->status, (4 * sizeof(unsigned char)) + (2 * sizeof(unsigned short)) + (3 * sizeof(int)))) err = -EFAULT; } return err; } struct compat_sg_req_info { /* used by SG_GET_REQUEST_TABLE ioctl() */ char req_state; char orphan; char sg_io_owned; char problem; int pack_id; compat_uptr_t usr_ptr; unsigned int duration; int unused; }; static int sg_grt_trans(struct file *file, unsigned int cmd, struct compat_sg_req_info __user *o) { int err, i; sg_req_info_t __user *r; r = compat_alloc_user_space(sizeof(sg_req_info_t)*SG_MAX_QUEUE); err = do_ioctl(file, cmd, (unsigned long)r); if (err < 0) return err; for (i = 0; i < SG_MAX_QUEUE; i++) { void __user *ptr; int d; if (copy_in_user(o + i, r + i, offsetof(sg_req_info_t, usr_ptr)) || get_user(ptr, &r[i].usr_ptr) || get_user(d, &r[i].duration) || put_user((u32)(unsigned long)(ptr), &o[i].usr_ptr) || put_user(d, &o[i].duration)) return -EFAULT; } return err; } #endif /* CONFIG_BLOCK */ struct sock_fprog32 { unsigned short len; compat_caddr_t filter; }; #define PPPIOCSPASS32 _IOW('t', 71, struct sock_fprog32) #define PPPIOCSACTIVE32 _IOW('t', 70, struct sock_fprog32) static int ppp_sock_fprog_ioctl_trans(struct file *file, unsigned int cmd, struct sock_fprog32 __user *u_fprog32) { struct sock_fprog __user *u_fprog64 = compat_alloc_user_space(sizeof(struct sock_fprog)); void __user *fptr64; u32 fptr32; u16 flen; if (get_user(flen, &u_fprog32->len) || get_user(fptr32, &u_fprog32->filter)) return -EFAULT; fptr64 = compat_ptr(fptr32); if (put_user(flen, &u_fprog64->len) || put_user(fptr64, &u_fprog64->filter)) return -EFAULT; if (cmd == PPPIOCSPASS32) cmd = PPPIOCSPASS; else cmd = PPPIOCSACTIVE; return do_ioctl(file, cmd, (unsigned long) u_fprog64); } struct ppp_option_data32 { compat_caddr_t ptr; u32 length; compat_int_t transmit; }; #define PPPIOCSCOMPRESS32 _IOW('t', 77, struct ppp_option_data32) struct ppp_idle32 { compat_time_t xmit_idle; compat_time_t recv_idle; }; #define PPPIOCGIDLE32 _IOR('t', 63, struct ppp_idle32) static int ppp_gidle(struct file *file, unsigned int cmd, struct ppp_idle32 __user *idle32) { struct ppp_idle __user *idle; __kernel_time_t xmit, recv; int err; idle = compat_alloc_user_space(sizeof(*idle)); err = do_ioctl(file, PPPIOCGIDLE, (unsigned long) idle); if (!err) { if (get_user(xmit, &idle->xmit_idle) || get_user(recv, &idle->recv_idle) || put_user(xmit, &idle32->xmit_idle) || put_user(recv, &idle32->recv_idle)) err = -EFAULT; } return err; } static int ppp_scompress(struct file *file, unsigned int cmd, struct ppp_option_data32 __user *odata32) { struct ppp_option_data __user *odata; __u32 data; void __user *datap; odata = compat_alloc_user_space(sizeof(*odata)); if (get_user(data, &odata32->ptr)) return -EFAULT; datap = compat_ptr(data); if (put_user(datap, &odata->ptr)) return -EFAULT; if (copy_in_user(&odata->length, &odata32->length, sizeof(__u32) + sizeof(int))) return -EFAULT; return do_ioctl(file, PPPIOCSCOMPRESS, (unsigned long) odata); } #ifdef CONFIG_BLOCK struct mtget32 { compat_long_t mt_type; compat_long_t mt_resid; compat_long_t mt_dsreg; compat_long_t mt_gstat; compat_long_t mt_erreg; compat_daddr_t mt_fileno; compat_daddr_t mt_blkno; }; #define MTIOCGET32 _IOR('m', 2, struct mtget32) struct mtpos32 { compat_long_t mt_blkno; }; #define MTIOCPOS32 _IOR('m', 3, struct mtpos32) static int mt_ioctl_trans(struct file *file, unsigned int cmd, void __user *argp) { /* NULL initialization to make gcc shut up */ struct mtget __user *get = NULL; struct mtget32 __user *umget32; struct mtpos __user *pos = NULL; struct mtpos32 __user *upos32; unsigned long kcmd; void *karg; int err = 0; switch(cmd) { case MTIOCPOS32: kcmd = MTIOCPOS; pos = compat_alloc_user_space(sizeof(*pos)); karg = pos; break; default: /* MTIOCGET32 */ kcmd = MTIOCGET; get = compat_alloc_user_space(sizeof(*get)); karg = get; break; } if (karg == NULL) return -EFAULT; err = do_ioctl(file, kcmd, (unsigned long)karg); if (err) return err; switch (cmd) { case MTIOCPOS32: upos32 = argp; err = convert_in_user(&pos->mt_blkno, &upos32->mt_blkno); break; case MTIOCGET32: umget32 = argp; err = convert_in_user(&get->mt_type, &umget32->mt_type); err |= convert_in_user(&get->mt_resid, &umget32->mt_resid); err |= convert_in_user(&get->mt_dsreg, &umget32->mt_dsreg); err |= convert_in_user(&get->mt_gstat, &umget32->mt_gstat); err |= convert_in_user(&get->mt_erreg, &umget32->mt_erreg); err |= convert_in_user(&get->mt_fileno, &umget32->mt_fileno); err |= convert_in_user(&get->mt_blkno, &umget32->mt_blkno); break; } return err ? -EFAULT: 0; } #endif /* CONFIG_BLOCK */ /* Bluetooth ioctls */ #define HCIUARTSETPROTO _IOW('U', 200, int) #define HCIUARTGETPROTO _IOR('U', 201, int) #define HCIUARTGETDEVICE _IOR('U', 202, int) #define HCIUARTSETFLAGS _IOW('U', 203, int) #define HCIUARTGETFLAGS _IOR('U', 204, int) #define BNEPCONNADD _IOW('B', 200, int) #define BNEPCONNDEL _IOW('B', 201, int) #define BNEPGETCONNLIST _IOR('B', 210, int) #define BNEPGETCONNINFO _IOR('B', 211, int) #define BNEPGETSUPPFEAT _IOR('B', 212, int) #define CMTPCONNADD _IOW('C', 200, int) #define CMTPCONNDEL _IOW('C', 201, int) #define CMTPGETCONNLIST _IOR('C', 210, int) #define CMTPGETCONNINFO _IOR('C', 211, int) #define HIDPCONNADD _IOW('H', 200, int) #define HIDPCONNDEL _IOW('H', 201, int) #define HIDPGETCONNLIST _IOR('H', 210, int) #define HIDPGETCONNINFO _IOR('H', 211, int) struct serial_struct32 { compat_int_t type; compat_int_t line; compat_uint_t port; compat_int_t irq; compat_int_t flags; compat_int_t xmit_fifo_size; compat_int_t custom_divisor; compat_int_t baud_base; unsigned short close_delay; char io_type; char reserved_char[1]; compat_int_t hub6; unsigned short closing_wait; /* time to wait before closing */ unsigned short closing_wait2; /* no longer used... */ compat_uint_t iomem_base; unsigned short iomem_reg_shift; unsigned int port_high; /* compat_ulong_t iomap_base FIXME */ compat_int_t reserved[1]; }; static int serial_struct_ioctl(struct file *file, unsigned cmd, struct serial_struct32 __user *ss32) { typedef struct serial_struct32 SS32; int err; struct serial_struct __user *ss = compat_alloc_user_space(sizeof(*ss)); __u32 udata; unsigned int base; unsigned char *iomem_base; if (ss == NULL) return -EFAULT; if (cmd == TIOCSSERIAL) { if (copy_in_user(ss, ss32, offsetof(SS32, iomem_base)) || get_user(udata, &ss32->iomem_base)) return -EFAULT; iomem_base = compat_ptr(udata); if (put_user(iomem_base, &ss->iomem_base) || convert_in_user(&ss32->iomem_reg_shift, &ss->iomem_reg_shift) || convert_in_user(&ss32->port_high, &ss->port_high) || put_user(0UL, &ss->iomap_base)) return -EFAULT; } err = do_ioctl(file, cmd, (unsigned long)ss); if (cmd == TIOCGSERIAL && err >= 0) { if (copy_in_user(ss32, ss, offsetof(SS32, iomem_base)) || get_user(iomem_base, &ss->iomem_base)) return -EFAULT; base = (unsigned long)iomem_base >> 32 ? 0xffffffff : (unsigned)(unsigned long)iomem_base; if (put_user(base, &ss32->iomem_base) || convert_in_user(&ss->iomem_reg_shift, &ss32->iomem_reg_shift) || convert_in_user(&ss->port_high, &ss32->port_high)) return -EFAULT; } return err; } #define RTC_IRQP_READ32 _IOR('p', 0x0b, compat_ulong_t) #define RTC_IRQP_SET32 _IOW('p', 0x0c, compat_ulong_t) #define RTC_EPOCH_READ32 _IOR('p', 0x0d, compat_ulong_t) #define RTC_EPOCH_SET32 _IOW('p', 0x0e, compat_ulong_t) static int rtc_ioctl(struct file *file, unsigned cmd, void __user *argp) { unsigned long __user *valp = compat_alloc_user_space(sizeof(*valp)); int ret; if (valp == NULL) return -EFAULT; switch (cmd) { case RTC_IRQP_READ32: case RTC_EPOCH_READ32: ret = do_ioctl(file, (cmd == RTC_IRQP_READ32) ? RTC_IRQP_READ : RTC_EPOCH_READ, (unsigned long)valp); if (ret) return ret; return convert_in_user(valp, (unsigned int __user *)argp); case RTC_IRQP_SET32: return do_ioctl(file, RTC_IRQP_SET, (unsigned long)argp); case RTC_EPOCH_SET32: return do_ioctl(file, RTC_EPOCH_SET, (unsigned long)argp); } return -ENOIOCTLCMD; } /* on ia32 l_start is on a 32-bit boundary */ #if defined(CONFIG_IA64) || defined(CONFIG_X86_64) struct space_resv_32 { __s16 l_type; __s16 l_whence; __s64 l_start __attribute__((packed)); /* len == 0 means until end of file */ __s64 l_len __attribute__((packed)); __s32 l_sysid; __u32 l_pid; __s32 l_pad[4]; /* reserve area */ }; #define FS_IOC_RESVSP_32 _IOW ('X', 40, struct space_resv_32) #define FS_IOC_RESVSP64_32 _IOW ('X', 42, struct space_resv_32) /* just account for different alignment */ static int compat_ioctl_preallocate(struct file *file, struct space_resv_32 __user *p32) { struct space_resv __user *p = compat_alloc_user_space(sizeof(*p)); if (copy_in_user(&p->l_type, &p32->l_type, sizeof(s16)) || copy_in_user(&p->l_whence, &p32->l_whence, sizeof(s16)) || copy_in_user(&p->l_start, &p32->l_start, sizeof(s64)) || copy_in_user(&p->l_len, &p32->l_len, sizeof(s64)) || copy_in_user(&p->l_sysid, &p32->l_sysid, sizeof(s32)) || copy_in_user(&p->l_pid, &p32->l_pid, sizeof(u32)) || copy_in_user(&p->l_pad, &p32->l_pad, 4*sizeof(u32))) return -EFAULT; return ioctl_preallocate(file, p); } #endif /* * simple reversible transform to make our table more evenly * distributed after sorting. */ #define XFORM(i) (((i) ^ ((i) << 27) ^ ((i) << 17)) & 0xffffffff) #define COMPATIBLE_IOCTL(cmd) XFORM((u32)cmd), /* ioctl should not be warned about even if it's not implemented. Valid reasons to use this: - It is implemented with ->compat_ioctl on some device, but programs call it on others too. - The ioctl is not implemented in the native kernel, but programs call it commonly anyways. Most other reasons are not valid. */ #define IGNORE_IOCTL(cmd) COMPATIBLE_IOCTL(cmd) static unsigned int ioctl_pointer[] = { /* compatible ioctls first */ COMPATIBLE_IOCTL(0x4B50) /* KDGHWCLK - not in the kernel, but don't complain */ COMPATIBLE_IOCTL(0x4B51) /* KDSHWCLK - not in the kernel, but don't complain */ /* Big T */ COMPATIBLE_IOCTL(TCGETA) COMPATIBLE_IOCTL(TCSETA) COMPATIBLE_IOCTL(TCSETAW) COMPATIBLE_IOCTL(TCSETAF) COMPATIBLE_IOCTL(TCSBRK) COMPATIBLE_IOCTL(TCXONC) COMPATIBLE_IOCTL(TCFLSH) COMPATIBLE_IOCTL(TCGETS) COMPATIBLE_IOCTL(TCSETS) COMPATIBLE_IOCTL(TCSETSW) COMPATIBLE_IOCTL(TCSETSF) COMPATIBLE_IOCTL(TIOCLINUX) COMPATIBLE_IOCTL(TIOCSBRK) COMPATIBLE_IOCTL(TIOCGDEV) COMPATIBLE_IOCTL(TIOCCBRK) COMPATIBLE_IOCTL(TIOCGSID) COMPATIBLE_IOCTL(TIOCGICOUNT) COMPATIBLE_IOCTL(TIOCGEXCL) /* Little t */ COMPATIBLE_IOCTL(TIOCGETD) COMPATIBLE_IOCTL(TIOCSETD) COMPATIBLE_IOCTL(TIOCEXCL) COMPATIBLE_IOCTL(TIOCNXCL) COMPATIBLE_IOCTL(TIOCCONS) COMPATIBLE_IOCTL(TIOCGSOFTCAR) COMPATIBLE_IOCTL(TIOCSSOFTCAR) COMPATIBLE_IOCTL(TIOCSWINSZ) COMPATIBLE_IOCTL(TIOCGWINSZ) COMPATIBLE_IOCTL(TIOCMGET) COMPATIBLE_IOCTL(TIOCMBIC) COMPATIBLE_IOCTL(TIOCMBIS) COMPATIBLE_IOCTL(TIOCMSET) COMPATIBLE_IOCTL(TIOCNOTTY) COMPATIBLE_IOCTL(TIOCSTI) COMPATIBLE_IOCTL(TIOCOUTQ) COMPATIBLE_IOCTL(TIOCSPGRP) COMPATIBLE_IOCTL(TIOCGPGRP) COMPATIBLE_IOCTL(TIOCSERGETLSR) #ifdef TIOCSRS485 COMPATIBLE_IOCTL(TIOCSRS485) #endif #ifdef TIOCGRS485 COMPATIBLE_IOCTL(TIOCGRS485) #endif #ifdef TCGETS2 COMPATIBLE_IOCTL(TCGETS2) COMPATIBLE_IOCTL(TCSETS2) COMPATIBLE_IOCTL(TCSETSW2) COMPATIBLE_IOCTL(TCSETSF2) #endif /* Little f */ COMPATIBLE_IOCTL(FIOCLEX) COMPATIBLE_IOCTL(FIONCLEX) COMPATIBLE_IOCTL(FIOASYNC) COMPATIBLE_IOCTL(FIONBIO) COMPATIBLE_IOCTL(FIONREAD) /* This is also TIOCINQ */ COMPATIBLE_IOCTL(FS_IOC_FIEMAP) /* 0x00 */ COMPATIBLE_IOCTL(FIBMAP) COMPATIBLE_IOCTL(FIGETBSZ) /* 'X' - originally XFS but some now in the VFS */ COMPATIBLE_IOCTL(FIFREEZE) COMPATIBLE_IOCTL(FITHAW) COMPATIBLE_IOCTL(FITRIM) COMPATIBLE_IOCTL(KDGETKEYCODE) COMPATIBLE_IOCTL(KDSETKEYCODE) COMPATIBLE_IOCTL(KDGKBTYPE) COMPATIBLE_IOCTL(KDGETMODE) COMPATIBLE_IOCTL(KDGKBMODE) COMPATIBLE_IOCTL(KDGKBMETA) COMPATIBLE_IOCTL(KDGKBENT) COMPATIBLE_IOCTL(KDSKBENT) COMPATIBLE_IOCTL(KDGKBSENT) COMPATIBLE_IOCTL(KDSKBSENT) COMPATIBLE_IOCTL(KDGKBDIACR) COMPATIBLE_IOCTL(KDSKBDIACR) COMPATIBLE_IOCTL(KDGKBDIACRUC) COMPATIBLE_IOCTL(KDSKBDIACRUC) COMPATIBLE_IOCTL(KDKBDREP) COMPATIBLE_IOCTL(KDGKBLED) COMPATIBLE_IOCTL(KDGETLED) #ifdef CONFIG_BLOCK /* Big S */ COMPATIBLE_IOCTL(SCSI_IOCTL_GET_IDLUN) COMPATIBLE_IOCTL(SCSI_IOCTL_DOORLOCK) COMPATIBLE_IOCTL(SCSI_IOCTL_DOORUNLOCK) COMPATIBLE_IOCTL(SCSI_IOCTL_TEST_UNIT_READY) COMPATIBLE_IOCTL(SCSI_IOCTL_GET_BUS_NUMBER) COMPATIBLE_IOCTL(SCSI_IOCTL_SEND_COMMAND) COMPATIBLE_IOCTL(SCSI_IOCTL_PROBE_HOST) COMPATIBLE_IOCTL(SCSI_IOCTL_GET_PCI) #endif /* Big V (don't complain on serial console) */ IGNORE_IOCTL(VT_OPENQRY) IGNORE_IOCTL(VT_GETMODE) /* Little p (/dev/rtc, /dev/envctrl, etc.) */ COMPATIBLE_IOCTL(RTC_AIE_ON) COMPATIBLE_IOCTL(RTC_AIE_OFF) COMPATIBLE_IOCTL(RTC_UIE_ON) COMPATIBLE_IOCTL(RTC_UIE_OFF) COMPATIBLE_IOCTL(RTC_PIE_ON) COMPATIBLE_IOCTL(RTC_PIE_OFF) COMPATIBLE_IOCTL(RTC_WIE_ON) COMPATIBLE_IOCTL(RTC_WIE_OFF) COMPATIBLE_IOCTL(RTC_ALM_SET) COMPATIBLE_IOCTL(RTC_ALM_READ) COMPATIBLE_IOCTL(RTC_RD_TIME) COMPATIBLE_IOCTL(RTC_SET_TIME) COMPATIBLE_IOCTL(RTC_WKALM_SET) COMPATIBLE_IOCTL(RTC_WKALM_RD) /* * These two are only for the sbus rtc driver, but * hwclock tries them on every rtc device first when * running on sparc. On other architectures the entries * are useless but harmless. */ COMPATIBLE_IOCTL(_IOR('p', 20, int[7])) /* RTCGET */ COMPATIBLE_IOCTL(_IOW('p', 21, int[7])) /* RTCSET */ /* Little m */ COMPATIBLE_IOCTL(MTIOCTOP) /* Socket level stuff */ COMPATIBLE_IOCTL(FIOQSIZE) #ifdef CONFIG_BLOCK /* md calls this on random blockdevs */ IGNORE_IOCTL(RAID_VERSION) /* qemu/qemu-img might call these two on plain files for probing */ IGNORE_IOCTL(CDROM_DRIVE_STATUS) IGNORE_IOCTL(FDGETPRM32) /* SG stuff */ COMPATIBLE_IOCTL(SG_SET_TIMEOUT) COMPATIBLE_IOCTL(SG_GET_TIMEOUT) COMPATIBLE_IOCTL(SG_EMULATED_HOST) COMPATIBLE_IOCTL(SG_GET_TRANSFORM) COMPATIBLE_IOCTL(SG_SET_RESERVED_SIZE) COMPATIBLE_IOCTL(SG_GET_RESERVED_SIZE) COMPATIBLE_IOCTL(SG_GET_SCSI_ID) COMPATIBLE_IOCTL(SG_SET_FORCE_LOW_DMA) COMPATIBLE_IOCTL(SG_GET_LOW_DMA) COMPATIBLE_IOCTL(SG_SET_FORCE_PACK_ID) COMPATIBLE_IOCTL(SG_GET_PACK_ID) COMPATIBLE_IOCTL(SG_GET_NUM_WAITING) COMPATIBLE_IOCTL(SG_SET_DEBUG) COMPATIBLE_IOCTL(SG_GET_SG_TABLESIZE) COMPATIBLE_IOCTL(SG_GET_COMMAND_Q) COMPATIBLE_IOCTL(SG_SET_COMMAND_Q) COMPATIBLE_IOCTL(SG_GET_VERSION_NUM) COMPATIBLE_IOCTL(SG_NEXT_CMD_LEN) COMPATIBLE_IOCTL(SG_SCSI_RESET) COMPATIBLE_IOCTL(SG_GET_REQUEST_TABLE) COMPATIBLE_IOCTL(SG_SET_KEEP_ORPHAN) COMPATIBLE_IOCTL(SG_GET_KEEP_ORPHAN) #endif /* PPP stuff */ COMPATIBLE_IOCTL(PPPIOCGFLAGS) COMPATIBLE_IOCTL(PPPIOCSFLAGS) COMPATIBLE_IOCTL(PPPIOCGASYNCMAP) COMPATIBLE_IOCTL(PPPIOCSASYNCMAP) COMPATIBLE_IOCTL(PPPIOCGUNIT) COMPATIBLE_IOCTL(PPPIOCGRASYNCMAP) COMPATIBLE_IOCTL(PPPIOCSRASYNCMAP) COMPATIBLE_IOCTL(PPPIOCGMRU) COMPATIBLE_IOCTL(PPPIOCSMRU) COMPATIBLE_IOCTL(PPPIOCSMAXCID) COMPATIBLE_IOCTL(PPPIOCGXASYNCMAP) COMPATIBLE_IOCTL(PPPIOCSXASYNCMAP) COMPATIBLE_IOCTL(PPPIOCXFERUNIT) /* PPPIOCSCOMPRESS is translated */ COMPATIBLE_IOCTL(PPPIOCGNPMODE) COMPATIBLE_IOCTL(PPPIOCSNPMODE) COMPATIBLE_IOCTL(PPPIOCGDEBUG) COMPATIBLE_IOCTL(PPPIOCSDEBUG) /* PPPIOCSPASS is translated */ /* PPPIOCSACTIVE is translated */ /* PPPIOCGIDLE is translated */ COMPATIBLE_IOCTL(PPPIOCNEWUNIT) COMPATIBLE_IOCTL(PPPIOCATTACH) COMPATIBLE_IOCTL(PPPIOCDETACH) COMPATIBLE_IOCTL(PPPIOCSMRRU) COMPATIBLE_IOCTL(PPPIOCCONNECT) COMPATIBLE_IOCTL(PPPIOCDISCONN) COMPATIBLE_IOCTL(PPPIOCATTCHAN) COMPATIBLE_IOCTL(PPPIOCGCHAN) COMPATIBLE_IOCTL(PPPIOCGL2TPSTATS) /* PPPOX */ COMPATIBLE_IOCTL(PPPOEIOCSFWD) COMPATIBLE_IOCTL(PPPOEIOCDFWD) /* Big A */ /* sparc only */ /* Big Q for sound/OSS */ COMPATIBLE_IOCTL(SNDCTL_SEQ_RESET) COMPATIBLE_IOCTL(SNDCTL_SEQ_SYNC) COMPATIBLE_IOCTL(SNDCTL_SYNTH_INFO) COMPATIBLE_IOCTL(SNDCTL_SEQ_CTRLRATE) COMPATIBLE_IOCTL(SNDCTL_SEQ_GETOUTCOUNT) COMPATIBLE_IOCTL(SNDCTL_SEQ_GETINCOUNT) COMPATIBLE_IOCTL(SNDCTL_SEQ_PERCMODE) COMPATIBLE_IOCTL(SNDCTL_FM_LOAD_INSTR) COMPATIBLE_IOCTL(SNDCTL_SEQ_TESTMIDI) COMPATIBLE_IOCTL(SNDCTL_SEQ_RESETSAMPLES) COMPATIBLE_IOCTL(SNDCTL_SEQ_NRSYNTHS) COMPATIBLE_IOCTL(SNDCTL_SEQ_NRMIDIS) COMPATIBLE_IOCTL(SNDCTL_MIDI_INFO) COMPATIBLE_IOCTL(SNDCTL_SEQ_THRESHOLD) COMPATIBLE_IOCTL(SNDCTL_SYNTH_MEMAVL) COMPATIBLE_IOCTL(SNDCTL_FM_4OP_ENABLE) COMPATIBLE_IOCTL(SNDCTL_SEQ_PANIC) COMPATIBLE_IOCTL(SNDCTL_SEQ_OUTOFBAND) COMPATIBLE_IOCTL(SNDCTL_SEQ_GETTIME) COMPATIBLE_IOCTL(SNDCTL_SYNTH_ID) COMPATIBLE_IOCTL(SNDCTL_SYNTH_CONTROL) COMPATIBLE_IOCTL(SNDCTL_SYNTH_REMOVESAMPLE) /* Big T for sound/OSS */ COMPATIBLE_IOCTL(SNDCTL_TMR_TIMEBASE) COMPATIBLE_IOCTL(SNDCTL_TMR_START) COMPATIBLE_IOCTL(SNDCTL_TMR_STOP) COMPATIBLE_IOCTL(SNDCTL_TMR_CONTINUE) COMPATIBLE_IOCTL(SNDCTL_TMR_TEMPO) COMPATIBLE_IOCTL(SNDCTL_TMR_SOURCE) COMPATIBLE_IOCTL(SNDCTL_TMR_METRONOME) COMPATIBLE_IOCTL(SNDCTL_TMR_SELECT) /* Little m for sound/OSS */ COMPATIBLE_IOCTL(SNDCTL_MIDI_PRETIME) COMPATIBLE_IOCTL(SNDCTL_MIDI_MPUMODE) COMPATIBLE_IOCTL(SNDCTL_MIDI_MPUCMD) /* Big P for sound/OSS */ COMPATIBLE_IOCTL(SNDCTL_DSP_RESET) COMPATIBLE_IOCTL(SNDCTL_DSP_SYNC) COMPATIBLE_IOCTL(SNDCTL_DSP_SPEED) COMPATIBLE_IOCTL(SNDCTL_DSP_STEREO) COMPATIBLE_IOCTL(SNDCTL_DSP_GETBLKSIZE) COMPATIBLE_IOCTL(SNDCTL_DSP_CHANNELS) COMPATIBLE_IOCTL(SOUND_PCM_WRITE_FILTER) COMPATIBLE_IOCTL(SNDCTL_DSP_POST) COMPATIBLE_IOCTL(SNDCTL_DSP_SUBDIVIDE) COMPATIBLE_IOCTL(SNDCTL_DSP_SETFRAGMENT) COMPATIBLE_IOCTL(SNDCTL_DSP_GETFMTS) COMPATIBLE_IOCTL(SNDCTL_DSP_SETFMT) COMPATIBLE_IOCTL(SNDCTL_DSP_GETOSPACE) COMPATIBLE_IOCTL(SNDCTL_DSP_GETISPACE) COMPATIBLE_IOCTL(SNDCTL_DSP_NONBLOCK) COMPATIBLE_IOCTL(SNDCTL_DSP_GETCAPS) COMPATIBLE_IOCTL(SNDCTL_DSP_GETTRIGGER) COMPATIBLE_IOCTL(SNDCTL_DSP_SETTRIGGER) COMPATIBLE_IOCTL(SNDCTL_DSP_GETIPTR) COMPATIBLE_IOCTL(SNDCTL_DSP_GETOPTR) /* SNDCTL_DSP_MAPINBUF, XXX needs translation */ /* SNDCTL_DSP_MAPOUTBUF, XXX needs translation */ COMPATIBLE_IOCTL(SNDCTL_DSP_SETSYNCRO) COMPATIBLE_IOCTL(SNDCTL_DSP_SETDUPLEX) COMPATIBLE_IOCTL(SNDCTL_DSP_GETODELAY) COMPATIBLE_IOCTL(SNDCTL_DSP_PROFILE) COMPATIBLE_IOCTL(SOUND_PCM_READ_RATE) COMPATIBLE_IOCTL(SOUND_PCM_READ_CHANNELS) COMPATIBLE_IOCTL(SOUND_PCM_READ_BITS) COMPATIBLE_IOCTL(SOUND_PCM_READ_FILTER) /* Big C for sound/OSS */ COMPATIBLE_IOCTL(SNDCTL_COPR_RESET) COMPATIBLE_IOCTL(SNDCTL_COPR_LOAD) COMPATIBLE_IOCTL(SNDCTL_COPR_RDATA) COMPATIBLE_IOCTL(SNDCTL_COPR_RCODE) COMPATIBLE_IOCTL(SNDCTL_COPR_WDATA) COMPATIBLE_IOCTL(SNDCTL_COPR_WCODE) COMPATIBLE_IOCTL(SNDCTL_COPR_RUN) COMPATIBLE_IOCTL(SNDCTL_COPR_HALT) COMPATIBLE_IOCTL(SNDCTL_COPR_SENDMSG) COMPATIBLE_IOCTL(SNDCTL_COPR_RCVMSG) /* Big M for sound/OSS */ COMPATIBLE_IOCTL(SOUND_MIXER_READ_VOLUME) COMPATIBLE_IOCTL(SOUND_MIXER_READ_BASS) COMPATIBLE_IOCTL(SOUND_MIXER_READ_TREBLE) COMPATIBLE_IOCTL(SOUND_MIXER_READ_SYNTH) COMPATIBLE_IOCTL(SOUND_MIXER_READ_PCM) COMPATIBLE_IOCTL(SOUND_MIXER_READ_SPEAKER) COMPATIBLE_IOCTL(SOUND_MIXER_READ_LINE) COMPATIBLE_IOCTL(SOUND_MIXER_READ_MIC) COMPATIBLE_IOCTL(SOUND_MIXER_READ_CD) COMPATIBLE_IOCTL(SOUND_MIXER_READ_IMIX) COMPATIBLE_IOCTL(SOUND_MIXER_READ_ALTPCM) COMPATIBLE_IOCTL(SOUND_MIXER_READ_RECLEV) COMPATIBLE_IOCTL(SOUND_MIXER_READ_IGAIN) COMPATIBLE_IOCTL(SOUND_MIXER_READ_OGAIN) COMPATIBLE_IOCTL(SOUND_MIXER_READ_LINE1) COMPATIBLE_IOCTL(SOUND_MIXER_READ_LINE2) COMPATIBLE_IOCTL(SOUND_MIXER_READ_LINE3) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_DIGITAL1)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_DIGITAL2)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_DIGITAL3)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_PHONEIN)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_PHONEOUT)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_VIDEO)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_RADIO)) COMPATIBLE_IOCTL(MIXER_READ(SOUND_MIXER_MONITOR)) COMPATIBLE_IOCTL(SOUND_MIXER_READ_MUTE) /* SOUND_MIXER_READ_ENHANCE, same value as READ_MUTE */ /* SOUND_MIXER_READ_LOUD, same value as READ_MUTE */ COMPATIBLE_IOCTL(SOUND_MIXER_READ_RECSRC) COMPATIBLE_IOCTL(SOUND_MIXER_READ_DEVMASK) COMPATIBLE_IOCTL(SOUND_MIXER_READ_RECMASK) COMPATIBLE_IOCTL(SOUND_MIXER_READ_STEREODEVS) COMPATIBLE_IOCTL(SOUND_MIXER_READ_CAPS) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_VOLUME) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_BASS) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_TREBLE) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_SYNTH) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_PCM) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_SPEAKER) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_LINE) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_MIC) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_CD) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_IMIX) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_ALTPCM) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_RECLEV) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_IGAIN) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_OGAIN) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_LINE1) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_LINE2) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_LINE3) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_DIGITAL1)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_DIGITAL2)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_DIGITAL3)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_PHONEIN)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_PHONEOUT)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_VIDEO)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_RADIO)) COMPATIBLE_IOCTL(MIXER_WRITE(SOUND_MIXER_MONITOR)) COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_MUTE) /* SOUND_MIXER_WRITE_ENHANCE, same value as WRITE_MUTE */ /* SOUND_MIXER_WRITE_LOUD, same value as WRITE_MUTE */ COMPATIBLE_IOCTL(SOUND_MIXER_WRITE_RECSRC) COMPATIBLE_IOCTL(SOUND_MIXER_INFO) COMPATIBLE_IOCTL(SOUND_OLD_MIXER_INFO) COMPATIBLE_IOCTL(SOUND_MIXER_ACCESS) COMPATIBLE_IOCTL(SOUND_MIXER_AGC) COMPATIBLE_IOCTL(SOUND_MIXER_3DSE) COMPATIBLE_IOCTL(SOUND_MIXER_PRIVATE1) COMPATIBLE_IOCTL(SOUND_MIXER_PRIVATE2) COMPATIBLE_IOCTL(SOUND_MIXER_PRIVATE3) COMPATIBLE_IOCTL(SOUND_MIXER_PRIVATE4) COMPATIBLE_IOCTL(SOUND_MIXER_PRIVATE5) COMPATIBLE_IOCTL(SOUND_MIXER_GETLEVELS) COMPATIBLE_IOCTL(SOUND_MIXER_SETLEVELS) COMPATIBLE_IOCTL(OSS_GETVERSION) /* Raw devices */ COMPATIBLE_IOCTL(RAW_SETBIND) COMPATIBLE_IOCTL(RAW_GETBIND) /* Watchdog */ COMPATIBLE_IOCTL(WDIOC_GETSUPPORT) COMPATIBLE_IOCTL(WDIOC_GETSTATUS) COMPATIBLE_IOCTL(WDIOC_GETBOOTSTATUS) COMPATIBLE_IOCTL(WDIOC_GETTEMP) COMPATIBLE_IOCTL(WDIOC_SETOPTIONS) COMPATIBLE_IOCTL(WDIOC_KEEPALIVE) COMPATIBLE_IOCTL(WDIOC_SETTIMEOUT) COMPATIBLE_IOCTL(WDIOC_GETTIMEOUT) COMPATIBLE_IOCTL(WDIOC_SETPRETIMEOUT) COMPATIBLE_IOCTL(WDIOC_GETPRETIMEOUT) /* Big R */ COMPATIBLE_IOCTL(RNDGETENTCNT) COMPATIBLE_IOCTL(RNDADDTOENTCNT) COMPATIBLE_IOCTL(RNDGETPOOL) COMPATIBLE_IOCTL(RNDADDENTROPY) COMPATIBLE_IOCTL(RNDZAPENTCNT) COMPATIBLE_IOCTL(RNDCLEARPOOL) /* Bluetooth */ COMPATIBLE_IOCTL(HCIDEVUP) COMPATIBLE_IOCTL(HCIDEVDOWN) COMPATIBLE_IOCTL(HCIDEVRESET) COMPATIBLE_IOCTL(HCIDEVRESTAT) COMPATIBLE_IOCTL(HCIGETDEVLIST) COMPATIBLE_IOCTL(HCIGETDEVINFO) COMPATIBLE_IOCTL(HCIGETCONNLIST) COMPATIBLE_IOCTL(HCIGETCONNINFO) COMPATIBLE_IOCTL(HCIGETAUTHINFO) COMPATIBLE_IOCTL(HCISETRAW) COMPATIBLE_IOCTL(HCISETSCAN) COMPATIBLE_IOCTL(HCISETAUTH) COMPATIBLE_IOCTL(HCISETENCRYPT) COMPATIBLE_IOCTL(HCISETPTYPE) COMPATIBLE_IOCTL(HCISETLINKPOL) COMPATIBLE_IOCTL(HCISETLINKMODE) COMPATIBLE_IOCTL(HCISETACLMTU) COMPATIBLE_IOCTL(HCISETSCOMTU) COMPATIBLE_IOCTL(HCIBLOCKADDR) COMPATIBLE_IOCTL(HCIUNBLOCKADDR) COMPATIBLE_IOCTL(HCIINQUIRY) COMPATIBLE_IOCTL(HCIUARTSETPROTO) COMPATIBLE_IOCTL(HCIUARTGETPROTO) COMPATIBLE_IOCTL(HCIUARTGETDEVICE) COMPATIBLE_IOCTL(HCIUARTSETFLAGS) COMPATIBLE_IOCTL(HCIUARTGETFLAGS) COMPATIBLE_IOCTL(RFCOMMCREATEDEV) COMPATIBLE_IOCTL(RFCOMMRELEASEDEV) COMPATIBLE_IOCTL(RFCOMMGETDEVLIST) COMPATIBLE_IOCTL(RFCOMMGETDEVINFO) COMPATIBLE_IOCTL(RFCOMMSTEALDLC) COMPATIBLE_IOCTL(BNEPCONNADD) COMPATIBLE_IOCTL(BNEPCONNDEL) COMPATIBLE_IOCTL(BNEPGETCONNLIST) COMPATIBLE_IOCTL(BNEPGETCONNINFO) COMPATIBLE_IOCTL(BNEPGETSUPPFEAT) COMPATIBLE_IOCTL(CMTPCONNADD) COMPATIBLE_IOCTL(CMTPCONNDEL) COMPATIBLE_IOCTL(CMTPGETCONNLIST) COMPATIBLE_IOCTL(CMTPGETCONNINFO) COMPATIBLE_IOCTL(HIDPCONNADD) COMPATIBLE_IOCTL(HIDPCONNDEL) COMPATIBLE_IOCTL(HIDPGETCONNLIST) COMPATIBLE_IOCTL(HIDPGETCONNINFO) /* CAPI */ COMPATIBLE_IOCTL(CAPI_REGISTER) COMPATIBLE_IOCTL(CAPI_GET_MANUFACTURER) COMPATIBLE_IOCTL(CAPI_GET_VERSION) COMPATIBLE_IOCTL(CAPI_GET_SERIAL) COMPATIBLE_IOCTL(CAPI_GET_PROFILE) COMPATIBLE_IOCTL(CAPI_MANUFACTURER_CMD) COMPATIBLE_IOCTL(CAPI_GET_ERRCODE) COMPATIBLE_IOCTL(CAPI_INSTALLED) COMPATIBLE_IOCTL(CAPI_GET_FLAGS) COMPATIBLE_IOCTL(CAPI_SET_FLAGS) COMPATIBLE_IOCTL(CAPI_CLR_FLAGS) COMPATIBLE_IOCTL(CAPI_NCCI_OPENCOUNT) COMPATIBLE_IOCTL(CAPI_NCCI_GETUNIT) /* Siemens Gigaset */ COMPATIBLE_IOCTL(GIGASET_REDIR) COMPATIBLE_IOCTL(GIGASET_CONFIG) COMPATIBLE_IOCTL(GIGASET_BRKCHARS) COMPATIBLE_IOCTL(GIGASET_VERSION) /* Misc. */ COMPATIBLE_IOCTL(0x41545900) /* ATYIO_CLKR */ COMPATIBLE_IOCTL(0x41545901) /* ATYIO_CLKW */ COMPATIBLE_IOCTL(PCIIOC_CONTROLLER) COMPATIBLE_IOCTL(PCIIOC_MMAP_IS_IO) COMPATIBLE_IOCTL(PCIIOC_MMAP_IS_MEM) COMPATIBLE_IOCTL(PCIIOC_WRITE_COMBINE) /* hiddev */ COMPATIBLE_IOCTL(HIDIOCGVERSION) COMPATIBLE_IOCTL(HIDIOCAPPLICATION) COMPATIBLE_IOCTL(HIDIOCGDEVINFO) COMPATIBLE_IOCTL(HIDIOCGSTRING) COMPATIBLE_IOCTL(HIDIOCINITREPORT) COMPATIBLE_IOCTL(HIDIOCGREPORT) COMPATIBLE_IOCTL(HIDIOCSREPORT) COMPATIBLE_IOCTL(HIDIOCGREPORTINFO) COMPATIBLE_IOCTL(HIDIOCGFIELDINFO) COMPATIBLE_IOCTL(HIDIOCGUSAGE) COMPATIBLE_IOCTL(HIDIOCSUSAGE) COMPATIBLE_IOCTL(HIDIOCGUCODE) COMPATIBLE_IOCTL(HIDIOCGFLAG) COMPATIBLE_IOCTL(HIDIOCSFLAG) COMPATIBLE_IOCTL(HIDIOCGCOLLECTIONINDEX) COMPATIBLE_IOCTL(HIDIOCGCOLLECTIONINFO) /* dvb */ COMPATIBLE_IOCTL(AUDIO_STOP) COMPATIBLE_IOCTL(AUDIO_PLAY) COMPATIBLE_IOCTL(AUDIO_PAUSE) COMPATIBLE_IOCTL(AUDIO_CONTINUE) COMPATIBLE_IOCTL(AUDIO_SELECT_SOURCE) COMPATIBLE_IOCTL(AUDIO_SET_MUTE) COMPATIBLE_IOCTL(AUDIO_SET_AV_SYNC) COMPATIBLE_IOCTL(AUDIO_SET_BYPASS_MODE) COMPATIBLE_IOCTL(AUDIO_CHANNEL_SELECT) COMPATIBLE_IOCTL(AUDIO_GET_STATUS) COMPATIBLE_IOCTL(AUDIO_GET_CAPABILITIES) COMPATIBLE_IOCTL(AUDIO_CLEAR_BUFFER) COMPATIBLE_IOCTL(AUDIO_SET_ID) COMPATIBLE_IOCTL(AUDIO_SET_MIXER) COMPATIBLE_IOCTL(AUDIO_SET_STREAMTYPE) COMPATIBLE_IOCTL(DMX_START) COMPATIBLE_IOCTL(DMX_STOP) COMPATIBLE_IOCTL(DMX_SET_FILTER) COMPATIBLE_IOCTL(DMX_SET_PES_FILTER) COMPATIBLE_IOCTL(DMX_SET_BUFFER_SIZE) COMPATIBLE_IOCTL(DMX_GET_PES_PIDS) COMPATIBLE_IOCTL(DMX_GET_STC) COMPATIBLE_IOCTL(DMX_REQBUFS) COMPATIBLE_IOCTL(DMX_QUERYBUF) COMPATIBLE_IOCTL(DMX_EXPBUF) COMPATIBLE_IOCTL(DMX_QBUF) COMPATIBLE_IOCTL(DMX_DQBUF) COMPATIBLE_IOCTL(VIDEO_STOP) COMPATIBLE_IOCTL(VIDEO_PLAY) COMPATIBLE_IOCTL(VIDEO_FREEZE) COMPATIBLE_IOCTL(VIDEO_CONTINUE) COMPATIBLE_IOCTL(VIDEO_SELECT_SOURCE) COMPATIBLE_IOCTL(VIDEO_SET_BLANK) COMPATIBLE_IOCTL(VIDEO_GET_STATUS) COMPATIBLE_IOCTL(VIDEO_SET_DISPLAY_FORMAT) COMPATIBLE_IOCTL(VIDEO_FAST_FORWARD) COMPATIBLE_IOCTL(VIDEO_SLOWMOTION) COMPATIBLE_IOCTL(VIDEO_GET_CAPABILITIES) COMPATIBLE_IOCTL(VIDEO_CLEAR_BUFFER) COMPATIBLE_IOCTL(VIDEO_SET_STREAMTYPE) COMPATIBLE_IOCTL(VIDEO_SET_FORMAT) COMPATIBLE_IOCTL(VIDEO_GET_SIZE) /* cec */ COMPATIBLE_IOCTL(CEC_ADAP_G_CAPS) COMPATIBLE_IOCTL(CEC_ADAP_G_LOG_ADDRS) COMPATIBLE_IOCTL(CEC_ADAP_S_LOG_ADDRS) COMPATIBLE_IOCTL(CEC_ADAP_G_PHYS_ADDR) COMPATIBLE_IOCTL(CEC_ADAP_S_PHYS_ADDR) COMPATIBLE_IOCTL(CEC_G_MODE) COMPATIBLE_IOCTL(CEC_S_MODE) COMPATIBLE_IOCTL(CEC_TRANSMIT) COMPATIBLE_IOCTL(CEC_RECEIVE) COMPATIBLE_IOCTL(CEC_DQEVENT) /* joystick */ COMPATIBLE_IOCTL(JSIOCGVERSION) COMPATIBLE_IOCTL(JSIOCGAXES) COMPATIBLE_IOCTL(JSIOCGBUTTONS) COMPATIBLE_IOCTL(JSIOCGNAME(0)) #ifdef TIOCGLTC COMPATIBLE_IOCTL(TIOCGLTC) COMPATIBLE_IOCTL(TIOCSLTC) #endif #ifdef TIOCSTART /* * For these two we have definitions in ioctls.h and/or termios.h on * some architectures but no actual implemention. Some applications * like bash call them if they are defined in the headers, so we provide * entries here to avoid syslog message spew. */ COMPATIBLE_IOCTL(TIOCSTART) COMPATIBLE_IOCTL(TIOCSTOP) #endif /* fat 'r' ioctls. These are handled by fat with ->compat_ioctl, but we don't want warnings on other file systems. So declare them as compatible here. */ #define VFAT_IOCTL_READDIR_BOTH32 _IOR('r', 1, struct compat_dirent[2]) #define VFAT_IOCTL_READDIR_SHORT32 _IOR('r', 2, struct compat_dirent[2]) IGNORE_IOCTL(VFAT_IOCTL_READDIR_BOTH32) IGNORE_IOCTL(VFAT_IOCTL_READDIR_SHORT32) #ifdef CONFIG_SPARC /* Sparc framebuffers, handled in sbusfb_compat_ioctl() */ IGNORE_IOCTL(FBIOGTYPE) IGNORE_IOCTL(FBIOSATTR) IGNORE_IOCTL(FBIOGATTR) IGNORE_IOCTL(FBIOSVIDEO) IGNORE_IOCTL(FBIOGVIDEO) IGNORE_IOCTL(FBIOSCURPOS) IGNORE_IOCTL(FBIOGCURPOS) IGNORE_IOCTL(FBIOGCURMAX) IGNORE_IOCTL(FBIOPUTCMAP32) IGNORE_IOCTL(FBIOGETCMAP32) IGNORE_IOCTL(FBIOSCURSOR32) IGNORE_IOCTL(FBIOGCURSOR32) #endif }; /* * Convert common ioctl arguments based on their command number * * Please do not add any code in here. Instead, implement * a compat_ioctl operation in the place that handleѕ the * ioctl for the native case. */ static long do_ioctl_trans(unsigned int cmd, unsigned long arg, struct file *file) { void __user *argp = compat_ptr(arg); switch (cmd) { case PPPIOCGIDLE32: return ppp_gidle(file, cmd, argp); case PPPIOCSCOMPRESS32: return ppp_scompress(file, cmd, argp); case PPPIOCSPASS32: case PPPIOCSACTIVE32: return ppp_sock_fprog_ioctl_trans(file, cmd, argp); #ifdef CONFIG_BLOCK case SG_IO: return sg_ioctl_trans(file, cmd, argp); case SG_GET_REQUEST_TABLE: return sg_grt_trans(file, cmd, argp); case MTIOCGET32: case MTIOCPOS32: return mt_ioctl_trans(file, cmd, argp); #endif /* Serial */ case TIOCGSERIAL: case TIOCSSERIAL: return serial_struct_ioctl(file, cmd, argp); /* Not implemented in the native kernel */ case RTC_IRQP_READ32: case RTC_IRQP_SET32: case RTC_EPOCH_READ32: case RTC_EPOCH_SET32: return rtc_ioctl(file, cmd, argp); /* dvb */ case VIDEO_GET_EVENT: return do_video_get_event(file, cmd, argp); case VIDEO_STILLPICTURE: return do_video_stillpicture(file, cmd, argp); } /* * These take an integer instead of a pointer as 'arg', * so we must not do a compat_ptr() translation. */ switch (cmd) { /* Big T */ case TCSBRKP: case TIOCMIWAIT: case TIOCSCTTY: /* RAID */ case HOT_REMOVE_DISK: case HOT_ADD_DISK: case SET_DISK_FAULTY: case SET_BITMAP_FILE: /* Big K */ case KDSIGACCEPT: case KIOCSOUND: case KDMKTONE: case KDSETMODE: case KDSKBMODE: case KDSKBMETA: case KDSKBLED: case KDSETLED: return vfs_ioctl(file, cmd, arg); } return -ENOIOCTLCMD; } static int compat_ioctl_check_table(unsigned int xcmd) { int i; const int max = ARRAY_SIZE(ioctl_pointer) - 1; BUILD_BUG_ON(max >= (1 << 16)); /* guess initial offset into table, assuming a normalized distribution */ i = ((xcmd >> 16) * max) >> 16; /* do linear search up first, until greater or equal */ while (ioctl_pointer[i] < xcmd && i < max) i++; /* then do linear search down */ while (ioctl_pointer[i] > xcmd && i > 0) i--; return ioctl_pointer[i] == xcmd; } COMPAT_SYSCALL_DEFINE3(ioctl, unsigned int, fd, unsigned int, cmd, compat_ulong_t, arg32) { unsigned long arg = arg32; struct fd f = fdget(fd); int error = -EBADF; if (!f.file) goto out; /* RED-PEN how should LSM module know it's handling 32bit? */ error = security_file_ioctl(f.file, cmd, arg); if (error) goto out_fput; /* * To allow the compat_ioctl handlers to be self contained * we need to check the common ioctls here first. * Just handle them with the standard handlers below. */ switch (cmd) { case FIOCLEX: case FIONCLEX: case FIONBIO: case FIOASYNC: case FIOQSIZE: break; #if defined(CONFIG_IA64) || defined(CONFIG_X86_64) case FS_IOC_RESVSP_32: case FS_IOC_RESVSP64_32: error = compat_ioctl_preallocate(f.file, compat_ptr(arg)); goto out_fput; #else case FS_IOC_RESVSP: case FS_IOC_RESVSP64: error = ioctl_preallocate(f.file, compat_ptr(arg)); goto out_fput; #endif case FICLONE: case FICLONERANGE: case FIDEDUPERANGE: case FS_IOC_FIEMAP: goto do_ioctl; case FIBMAP: case FIGETBSZ: case FIONREAD: if (S_ISREG(file_inode(f.file)->i_mode)) break; /*FALL THROUGH*/ default: if (f.file->f_op->compat_ioctl) { error = f.file->f_op->compat_ioctl(f.file, cmd, arg); if (error != -ENOIOCTLCMD) goto out_fput; } if (!f.file->f_op->unlocked_ioctl) goto do_ioctl; break; } if (compat_ioctl_check_table(XFORM(cmd))) goto found_handler; error = do_ioctl_trans(cmd, arg, f.file); if (error == -ENOIOCTLCMD) error = -ENOTTY; goto out_fput; found_handler: arg = (unsigned long)compat_ptr(arg); do_ioctl: error = do_vfs_ioctl(f.file, fd, cmd, arg); out_fput: fdput(f); out: return error; } static int __init init_sys32_ioctl_cmp(const void *p, const void *q) { unsigned int a, b; a = *(unsigned int *)p; b = *(unsigned int *)q; if (a > b) return 1; if (a < b) return -1; return 0; } static int __init init_sys32_ioctl(void) { sort(ioctl_pointer, ARRAY_SIZE(ioctl_pointer), sizeof(*ioctl_pointer), init_sys32_ioctl_cmp, NULL); return 0; } __initcall(init_sys32_ioctl);