/* * Lock-less NULL terminated single linked list * * The basic atomic operation of this list is cmpxchg on long. On * architectures that don't have NMI-safe cmpxchg implementation, the * list can NOT be used in NMI handlers. So code that uses the list in * an NMI handler should depend on CONFIG_ARCH_HAVE_NMI_SAFE_CMPXCHG. * * Copyright 2010,2011 Intel Corp. * Author: Huang Ying * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License version * 2 as published by the Free Software Foundation; * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA */ #include #include #include /** * llist_add_batch - add several linked entries in batch * @new_first: first entry in batch to be added * @new_last: last entry in batch to be added * @head: the head for your lock-less list * * Return whether list is empty before adding. */ bool llist_add_batch(struct llist_node *new_first, struct llist_node *new_last, struct llist_head *head) { struct llist_node *first; do { new_last->next = first = READ_ONCE(head->first); } while (cmpxchg(&head->first, first, new_first) != first); return !first; } EXPORT_SYMBOL_GPL(llist_add_batch); /** * llist_del_first - delete the first entry of lock-less list * @head: the head for your lock-less list * * If list is empty, return NULL, otherwise, return the first entry * deleted, this is the newest added one. * * Only one llist_del_first user can be used simultaneously with * multiple llist_add users without lock. Because otherwise * llist_del_first, llist_add, llist_add (or llist_del_all, llist_add, * llist_add) sequence in another user may change @head->first->next, * but keep @head->first. If multiple consumers are needed, please * use llist_del_all or use lock between consumers. */ struct llist_node *llist_del_first(struct llist_head *head) { struct llist_node *entry, *old_entry, *next; entry = smp_load_acquire(&head->first); for (;;) { if (entry == NULL) return NULL; old_entry = entry; next = READ_ONCE(entry->next); entry = cmpxchg(&head->first, old_entry, next); if (entry == old_entry) break; } return entry; } EXPORT_SYMBOL_GPL(llist_del_first); /** * llist_reverse_order - reverse order of a llist chain * @head: first item of the list to be reversed * * Reverse the order of a chain of llist entries and return the * new first entry. */ struct llist_node *llist_reverse_order(struct llist_node *head) { struct llist_node *new_head = NULL; while (head) { struct llist_node *tmp = head; head = head->next; tmp->next = new_head; new_head = tmp; } return new_head; } EXPORT_SYMBOL_GPL(llist_reverse_order);