/* * kvm asynchronous fault support * * Copyright 2010 Red Hat, Inc. * * Author: * Gleb Natapov * * This file is free software; you can redistribute it and/or modify * it under the terms of version 2 of the GNU General Public License * as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software Foundation, * Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301, USA. */ #ifndef __KVM_ASYNC_PF_H__ #define __KVM_ASYNC_PF_H__ #ifdef CONFIG_KVM_ASYNC_PF int kvm_async_pf_init(void); void kvm_async_pf_deinit(void); void kvm_async_pf_vcpu_init(struct kvm_vcpu *vcpu); #else #define kvm_async_pf_init() (0) #define kvm_async_pf_deinit() do {} while (0) #define kvm_async_pf_vcpu_init(C) do {} while (0) #endif #endif