/* * kvm eventfd support - use eventfd objects to signal various KVM events * * Copyright 2009 Novell. All Rights Reserved. * Copyright 2010 Red Hat, Inc. and/or its affiliates. * * Author: * Gregory Haskins * * This file is free software; you can redistribute it and/or modify * it under the terms of version 2 of the GNU General Public License * as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software Foundation, * Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301, USA. */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #ifdef CONFIG_HAVE_KVM_IRQFD static struct workqueue_struct *irqfd_cleanup_wq; static void irqfd_inject(struct work_struct *work) { struct kvm_kernel_irqfd *irqfd = container_of(work, struct kvm_kernel_irqfd, inject); struct kvm *kvm = irqfd->kvm; if (!irqfd->resampler) { kvm_set_irq(kvm, KVM_USERSPACE_IRQ_SOURCE_ID, irqfd->gsi, 1, false); kvm_set_irq(kvm, KVM_USERSPACE_IRQ_SOURCE_ID, irqfd->gsi, 0, false); } else kvm_set_irq(kvm, KVM_IRQFD_RESAMPLE_IRQ_SOURCE_ID, irqfd->gsi, 1, false); } /* * Since resampler irqfds share an IRQ source ID, we de-assert once * then notify all of the resampler irqfds using this GSI. We can't * do multiple de-asserts or we risk racing with incoming re-asserts. */ static void irqfd_resampler_ack(struct kvm_irq_ack_notifier *kian) { struct kvm_kernel_irqfd_resampler *resampler; struct kvm *kvm; struct kvm_kernel_irqfd *irqfd; int idx; resampler = container_of(kian, struct kvm_kernel_irqfd_resampler, notifier); kvm = resampler->kvm; kvm_set_irq(kvm, KVM_IRQFD_RESAMPLE_IRQ_SOURCE_ID, resampler->notifier.gsi, 0, false); idx = srcu_read_lock(&kvm->irq_srcu); list_for_each_entry_rcu(irqfd, &resampler->list, resampler_link) eventfd_signal(irqfd->resamplefd, 1); srcu_read_unlock(&kvm->irq_srcu, idx); } static void irqfd_resampler_shutdown(struct kvm_kernel_irqfd *irqfd) { struct kvm_kernel_irqfd_resampler *resampler = irqfd->resampler; struct kvm *kvm = resampler->kvm; mutex_lock(&kvm->irqfds.resampler_lock); list_del_rcu(&irqfd->resampler_link); synchronize_srcu(&kvm->irq_srcu); if (list_empty(&resampler->list)) { list_del(&resampler->link); kvm_unregister_irq_ack_notifier(kvm, &resampler->notifier); kvm_set_irq(kvm, KVM_IRQFD_RESAMPLE_IRQ_SOURCE_ID, resampler->notifier.gsi, 0, false); kfree(resampler); } mutex_unlock(&kvm->irqfds.resampler_lock); } /* * Race-free decouple logic (ordering is critical) */ static void irqfd_shutdown(struct work_struct *work) { struct kvm_kernel_irqfd *irqfd = container_of(work, struct kvm_kernel_irqfd, shutdown); struct kvm *kvm = irqfd->kvm; u64 cnt; /* Make sure irqfd has been initalized in assign path. */ synchronize_srcu(&kvm->irq_srcu); /* * Synchronize with the wait-queue and unhook ourselves to prevent * further events. */ eventfd_ctx_remove_wait_queue(irqfd->eventfd, &irqfd->wait, &cnt); /* * We know no new events will be scheduled at this point, so block * until all previously outstanding events have completed */ flush_work(&irqfd->inject); if (irqfd->resampler) { irqfd_resampler_shutdown(irqfd); eventfd_ctx_put(irqfd->resamplefd); } /* * It is now safe to release the object's resources */ #ifdef CONFIG_HAVE_KVM_IRQ_BYPASS irq_bypass_unregister_consumer(&irqfd->consumer); #endif eventfd_ctx_put(irqfd->eventfd); kfree(irqfd); } /* assumes kvm->irqfds.lock is held */ static bool irqfd_is_active(struct kvm_kernel_irqfd *irqfd) { return list_empty(&irqfd->list) ? false : true; } /* * Mark the irqfd as inactive and schedule it for removal * * assumes kvm->irqfds.lock is held */ static void irqfd_deactivate(struct kvm_kernel_irqfd *irqfd) { BUG_ON(!irqfd_is_active(irqfd)); list_del_init(&irqfd->list); queue_work(irqfd_cleanup_wq, &irqfd->shutdown); } int __attribute__((weak)) kvm_arch_set_irq_inatomic( struct kvm_kernel_irq_routing_entry *irq, struct kvm *kvm, int irq_source_id, int level, bool line_status) { return -EWOULDBLOCK; } /* * Called with wqh->lock held and interrupts disabled */ static int irqfd_wakeup(wait_queue_entry_t *wait, unsigned mode, int sync, void *key) { struct kvm_kernel_irqfd *irqfd = container_of(wait, struct kvm_kernel_irqfd, wait); __poll_t flags = key_to_poll(key); struct kvm_kernel_irq_routing_entry irq; struct kvm *kvm = irqfd->kvm; unsigned seq; int idx; if (flags & EPOLLIN) { idx = srcu_read_lock(&kvm->irq_srcu); do { seq = read_seqcount_begin(&irqfd->irq_entry_sc); irq = irqfd->irq_entry; } while (read_seqcount_retry(&irqfd->irq_entry_sc, seq)); /* An event has been signaled, inject an interrupt */ if (kvm_arch_set_irq_inatomic(&irq, kvm, KVM_USERSPACE_IRQ_SOURCE_ID, 1, false) == -EWOULDBLOCK) schedule_work(&irqfd->inject); srcu_read_unlock(&kvm->irq_srcu, idx); } if (flags & EPOLLHUP) { /* The eventfd is closing, detach from KVM */ unsigned long flags; spin_lock_irqsave(&kvm->irqfds.lock, flags); /* * We must check if someone deactivated the irqfd before * we could acquire the irqfds.lock since the item is * deactivated from the KVM side before it is unhooked from * the wait-queue. If it is already deactivated, we can * simply return knowing the other side will cleanup for us. * We cannot race against the irqfd going away since the * other side is required to acquire wqh->lock, which we hold */ if (irqfd_is_active(irqfd)) irqfd_deactivate(irqfd); spin_unlock_irqrestore(&kvm->irqfds.lock, flags); } return 0; } static void irqfd_ptable_queue_proc(struct file *file, wait_queue_head_t *wqh, poll_table *pt) { struct kvm_kernel_irqfd *irqfd = container_of(pt, struct kvm_kernel_irqfd, pt); add_wait_queue(wqh, &irqfd->wait); } /* Must be called under irqfds.lock */ static void irqfd_update(struct kvm *kvm, struct kvm_kernel_irqfd *irqfd) { struct kvm_kernel_irq_routing_entry *e; struct kvm_kernel_irq_routing_entry entries[KVM_NR_IRQCHIPS]; int n_entries; n_entries = kvm_irq_map_gsi(kvm, entries, irqfd->gsi); write_seqcount_begin(&irqfd->irq_entry_sc); e = entries; if (n_entries == 1) irqfd->irq_entry = *e; else irqfd->irq_entry.type = 0; write_seqcount_end(&irqfd->irq_entry_sc); } #ifdef CONFIG_HAVE_KVM_IRQ_BYPASS void __attribute__((weak)) kvm_arch_irq_bypass_stop( struct irq_bypass_consumer *cons) { } void __attribute__((weak)) kvm_arch_irq_bypass_start( struct irq_bypass_consumer *cons) { } int __attribute__((weak)) kvm_arch_update_irqfd_routing( struct kvm *kvm, unsigned int host_irq, uint32_t guest_irq, bool set) { return 0; } #endif static int kvm_irqfd_assign(struct kvm *kvm, struct kvm_irqfd *args) { struct kvm_kernel_irqfd *irqfd, *tmp; struct fd f; struct eventfd_ctx *eventfd = NULL, *resamplefd = NULL; int ret; __poll_t events; int idx; if (!kvm_arch_intc_initialized(kvm)) return -EAGAIN; irqfd = kzalloc(sizeof(*irqfd), GFP_KERNEL); if (!irqfd) return -ENOMEM; irqfd->kvm = kvm; irqfd->gsi = args->gsi; INIT_LIST_HEAD(&irqfd->list); INIT_WORK(&irqfd->inject, irqfd_inject); INIT_WORK(&irqfd->shutdown, irqfd_shutdown); seqcount_init(&irqfd->irq_entry_sc); f = fdget(args->fd); if (!f.file) { ret = -EBADF; goto out; } eventfd = eventfd_ctx_fileget(f.file); if (IS_ERR(eventfd)) { ret = PTR_ERR(eventfd); goto fail; } irqfd->eventfd = eventfd; if (args->flags & KVM_IRQFD_FLAG_RESAMPLE) { struct kvm_kernel_irqfd_resampler *resampler; resamplefd = eventfd_ctx_fdget(args->resamplefd); if (IS_ERR(resamplefd)) { ret = PTR_ERR(resamplefd); goto fail; } irqfd->resamplefd = resamplefd; INIT_LIST_HEAD(&irqfd->resampler_link); mutex_lock(&kvm->irqfds.resampler_lock); list_for_each_entry(resampler, &kvm->irqfds.resampler_list, link) { if (resampler->notifier.gsi == irqfd->gsi) { irqfd->resampler = resampler; break; } } if (!irqfd->resampler) { resampler = kzalloc(sizeof(*resampler), GFP_KERNEL); if (!resampler) { ret = -ENOMEM; mutex_unlock(&kvm->irqfds.resampler_lock); goto fail; } resampler->kvm = kvm; INIT_LIST_HEAD(&resampler->list); resampler->notifier.gsi = irqfd->gsi; resampler->notifier.irq_acked = irqfd_resampler_ack; INIT_LIST_HEAD(&resampler->link); list_add(&resampler->link, &kvm->irqfds.resampler_list); kvm_register_irq_ack_notifier(kvm, &resampler->notifier); irqfd->resampler = resampler; } list_add_rcu(&irqfd->resampler_link, &irqfd->resampler->list); synchronize_srcu(&kvm->irq_srcu); mutex_unlock(&kvm->irqfds.resampler_lock); } /* * Install our own custom wake-up handling so we are notified via * a callback whenever someone signals the underlying eventfd */ init_waitqueue_func_entry(&irqfd->wait, irqfd_wakeup); init_poll_funcptr(&irqfd->pt, irqfd_ptable_queue_proc); spin_lock_irq(&kvm->irqfds.lock); ret = 0; list_for_each_entry(tmp, &kvm->irqfds.items, list) { if (irqfd->eventfd != tmp->eventfd) continue; /* This fd is used for another irq already. */ ret = -EBUSY; spin_unlock_irq(&kvm->irqfds.lock); goto fail; } idx = srcu_read_lock(&kvm->irq_srcu); irqfd_update(kvm, irqfd); list_add_tail(&irqfd->list, &kvm->irqfds.items); spin_unlock_irq(&kvm->irqfds.lock); /* * Check if there was an event already pending on the eventfd * before we registered, and trigger it as if we didn't miss it. */ events = vfs_poll(f.file, &irqfd->pt); if (events & EPOLLIN) schedule_work(&irqfd->inject); #ifdef CONFIG_HAVE_KVM_IRQ_BYPASS if (kvm_arch_has_irq_bypass()) { irqfd->consumer.token = (void *)irqfd->eventfd; irqfd->consumer.add_producer = kvm_arch_irq_bypass_add_producer; irqfd->consumer.del_producer = kvm_arch_irq_bypass_del_producer; irqfd->consumer.stop = kvm_arch_irq_bypass_stop; irqfd->consumer.start = kvm_arch_irq_bypass_start; ret = irq_bypass_register_consumer(&irqfd->consumer); if (ret) pr_info("irq bypass consumer (token %p) registration fails: %d\n", irqfd->consumer.token, ret); } #endif srcu_read_unlock(&kvm->irq_srcu, idx); /* * do not drop the file until the irqfd is fully initialized, otherwise * we might race against the EPOLLHUP */ fdput(f); return 0; fail: if (irqfd->resampler) irqfd_resampler_shutdown(irqfd); if (resamplefd && !IS_ERR(resamplefd)) eventfd_ctx_put(resamplefd); if (eventfd && !IS_ERR(eventfd)) eventfd_ctx_put(eventfd); fdput(f); out: kfree(irqfd); return ret; } bool kvm_irq_has_notifier(struct kvm *kvm, unsigned irqchip, unsigned pin) { struct kvm_irq_ack_notifier *kian; int gsi, idx; idx = srcu_read_lock(&kvm->irq_srcu); gsi = kvm_irq_map_chip_pin(kvm, irqchip, pin); if (gsi != -1) hlist_for_each_entry_rcu(kian, &kvm->irq_ack_notifier_list, link) if (kian->gsi == gsi) { srcu_read_unlock(&kvm->irq_srcu, idx); return true; } srcu_read_unlock(&kvm->irq_srcu, idx); return false; } EXPORT_SYMBOL_GPL(kvm_irq_has_notifier); void kvm_notify_acked_gsi(struct kvm *kvm, int gsi) { struct kvm_irq_ack_notifier *kian; hlist_for_each_entry_rcu(kian, &kvm->irq_ack_notifier_list, link) if (kian->gsi == gsi) kian->irq_acked(kian); } void kvm_notify_acked_irq(struct kvm *kvm, unsigned irqchip, unsigned pin) { int gsi, idx; trace_kvm_ack_irq(irqchip, pin); idx = srcu_read_lock(&kvm->irq_srcu); gsi = kvm_irq_map_chip_pin(kvm, irqchip, pin); if (gsi != -1) kvm_notify_acked_gsi(kvm, gsi); srcu_read_unlock(&kvm->irq_srcu, idx); } void kvm_register_irq_ack_notifier(struct kvm *kvm, struct kvm_irq_ack_notifier *kian) { mutex_lock(&kvm->irq_lock); hlist_add_head_rcu(&kian->link, &kvm->irq_ack_notifier_list); mutex_unlock(&kvm->irq_lock); kvm_arch_post_irq_ack_notifier_list_update(kvm); } void kvm_unregister_irq_ack_notifier(struct kvm *kvm, struct kvm_irq_ack_notifier *kian) { mutex_lock(&kvm->irq_lock); hlist_del_init_rcu(&kian->link); mutex_unlock(&kvm->irq_lock); synchronize_srcu(&kvm->irq_srcu); kvm_arch_post_irq_ack_notifier_list_update(kvm); } #endif void kvm_eventfd_init(struct kvm *kvm) { #ifdef CONFIG_HAVE_KVM_IRQFD spin_lock_init(&kvm->irqfds.lock); INIT_LIST_HEAD(&kvm->irqfds.items); INIT_LIST_HEAD(&kvm->irqfds.resampler_list); mutex_init(&kvm->irqfds.resampler_lock); #endif INIT_LIST_HEAD(&kvm->ioeventfds); } #ifdef CONFIG_HAVE_KVM_IRQFD /* * shutdown any irqfd's that match fd+gsi */ static int kvm_irqfd_deassign(struct kvm *kvm, struct kvm_irqfd *args) { struct kvm_kernel_irqfd *irqfd, *tmp; struct eventfd_ctx *eventfd; eventfd = eventfd_ctx_fdget(args->fd); if (IS_ERR(eventfd)) return PTR_ERR(eventfd); spin_lock_irq(&kvm->irqfds.lock); list_for_each_entry_safe(irqfd, tmp, &kvm->irqfds.items, list) { if (irqfd->eventfd == eventfd && irqfd->gsi == args->gsi) { /* * This clearing of irq_entry.type is needed for when * another thread calls kvm_irq_routing_update before * we flush workqueue below (we synchronize with * kvm_irq_routing_update using irqfds.lock). */ write_seqcount_begin(&irqfd->irq_entry_sc); irqfd->irq_entry.type = 0; write_seqcount_end(&irqfd->irq_entry_sc); irqfd_deactivate(irqfd); } } spin_unlock_irq(&kvm->irqfds.lock); eventfd_ctx_put(eventfd); /* * Block until we know all outstanding shutdown jobs have completed * so that we guarantee there will not be any more interrupts on this * gsi once this deassign function returns. */ flush_workqueue(irqfd_cleanup_wq); return 0; } int kvm_irqfd(struct kvm *kvm, struct kvm_irqfd *args) { if (args->flags & ~(KVM_IRQFD_FLAG_DEASSIGN | KVM_IRQFD_FLAG_RESAMPLE)) return -EINVAL; if (args->flags & KVM_IRQFD_FLAG_DEASSIGN) return kvm_irqfd_deassign(kvm, args); return kvm_irqfd_assign(kvm, args); } /* * This function is called as the kvm VM fd is being released. Shutdown all * irqfds that still remain open */ void kvm_irqfd_release(struct kvm *kvm) { struct kvm_kernel_irqfd *irqfd, *tmp; spin_lock_irq(&kvm->irqfds.lock); list_for_each_entry_safe(irqfd, tmp, &kvm->irqfds.items, list) irqfd_deactivate(irqfd); spin_unlock_irq(&kvm->irqfds.lock); /* * Block until we know all outstanding shutdown jobs have completed * since we do not take a kvm* reference. */ flush_workqueue(irqfd_cleanup_wq); } /* * Take note of a change in irq routing. * Caller must invoke synchronize_srcu(&kvm->irq_srcu) afterwards. */ void kvm_irq_routing_update(struct kvm *kvm) { struct kvm_kernel_irqfd *irqfd; spin_lock_irq(&kvm->irqfds.lock); list_for_each_entry(irqfd, &kvm->irqfds.items, list) { irqfd_update(kvm, irqfd); #ifdef CONFIG_HAVE_KVM_IRQ_BYPASS if (irqfd->producer) { int ret = kvm_arch_update_irqfd_routing( irqfd->kvm, irqfd->producer->irq, irqfd->gsi, 1); WARN_ON(ret); } #endif } spin_unlock_irq(&kvm->irqfds.lock); } /* * create a host-wide workqueue for issuing deferred shutdown requests * aggregated from all vm* instances. We need our own isolated * queue to ease flushing work items when a VM exits. */ int kvm_irqfd_init(void) { irqfd_cleanup_wq = alloc_workqueue("kvm-irqfd-cleanup", 0, 0); if (!irqfd_cleanup_wq) return -ENOMEM; return 0; } void kvm_irqfd_exit(void) { destroy_workqueue(irqfd_cleanup_wq); } #endif /* * -------------------------------------------------------------------- * ioeventfd: translate a PIO/MMIO memory write to an eventfd signal. * * userspace can register a PIO/MMIO address with an eventfd for receiving * notification when the memory has been touched. * -------------------------------------------------------------------- */ struct _ioeventfd { struct list_head list; u64 addr; int length; struct eventfd_ctx *eventfd; u64 datamatch; struct kvm_io_device dev; u8 bus_idx; bool wildcard; }; static inline struct _ioeventfd * to_ioeventfd(struct kvm_io_device *dev) { return container_of(dev, struct _ioeventfd, dev); } static void ioeventfd_release(struct _ioeventfd *p) { eventfd_ctx_put(p->eventfd); list_del(&p->list); kfree(p); } static bool ioeventfd_in_range(struct _ioeventfd *p, gpa_t addr, int len, const void *val) { u64 _val; if (addr != p->addr) /* address must be precise for a hit */ return false; if (!p->length) /* length = 0 means only look at the address, so always a hit */ return true; if (len != p->length) /* address-range must be precise for a hit */ return false; if (p->wildcard) /* all else equal, wildcard is always a hit */ return true; /* otherwise, we have to actually compare the data */ BUG_ON(!IS_ALIGNED((unsigned long)val, len)); switch (len) { case 1: _val = *(u8 *)val; break; case 2: _val = *(u16 *)val; break; case 4: _val = *(u32 *)val; break; case 8: _val = *(u64 *)val; break; default: return false; } return _val == p->datamatch ? true : false; } /* MMIO/PIO writes trigger an event if the addr/val match */ static int ioeventfd_write(struct kvm_vcpu *vcpu, struct kvm_io_device *this, gpa_t addr, int len, const void *val) { struct _ioeventfd *p = to_ioeventfd(this); if (!ioeventfd_in_range(p, addr, len, val)) return -EOPNOTSUPP; eventfd_signal(p->eventfd, 1); return 0; } /* * This function is called as KVM is completely shutting down. We do not * need to worry about locking just nuke anything we have as quickly as possible */ static void ioeventfd_destructor(struct kvm_io_device *this) { struct _ioeventfd *p = to_ioeventfd(this); ioeventfd_release(p); } static const struct kvm_io_device_ops ioeventfd_ops = { .write = ioeventfd_write, .destructor = ioeventfd_destructor, }; /* assumes kvm->slots_lock held */ static bool ioeventfd_check_collision(struct kvm *kvm, struct _ioeventfd *p) { struct _ioeventfd *_p; list_for_each_entry(_p, &kvm->ioeventfds, list) if (_p->bus_idx == p->bus_idx && _p->addr == p->addr && (!_p->length || !p->length || (_p->length == p->length && (_p->wildcard || p->wildcard || _p->datamatch == p->datamatch)))) return true; return false; } static enum kvm_bus ioeventfd_bus_from_flags(__u32 flags) { if (flags & KVM_IOEVENTFD_FLAG_PIO) return KVM_PIO_BUS; if (flags & KVM_IOEVENTFD_FLAG_VIRTIO_CCW_NOTIFY) return KVM_VIRTIO_CCW_NOTIFY_BUS; return KVM_MMIO_BUS; } static int kvm_assign_ioeventfd_idx(struct kvm *kvm, enum kvm_bus bus_idx, struct kvm_ioeventfd *args) { struct eventfd_ctx *eventfd; struct _ioeventfd *p; int ret; eventfd = eventfd_ctx_fdget(args->fd); if (IS_ERR(eventfd)) return PTR_ERR(eventfd); p = kzalloc(sizeof(*p), GFP_KERNEL); if (!p) { ret = -ENOMEM; goto fail; } INIT_LIST_HEAD(&p->list); p->addr = args->addr; p->bus_idx = bus_idx; p->length = args->len; p->eventfd = eventfd; /* The datamatch feature is optional, otherwise this is a wildcard */ if (args->flags & KVM_IOEVENTFD_FLAG_DATAMATCH) p->datamatch = args->datamatch; else p->wildcard = true; mutex_lock(&kvm->slots_lock); /* Verify that there isn't a match already */ if (ioeventfd_check_collision(kvm, p)) { ret = -EEXIST; goto unlock_fail; } kvm_iodevice_init(&p->dev, &ioeventfd_ops); ret = kvm_io_bus_register_dev(kvm, bus_idx, p->addr, p->length, &p->dev); if (ret < 0) goto unlock_fail; kvm_get_bus(kvm, bus_idx)->ioeventfd_count++; list_add_tail(&p->list, &kvm->ioeventfds); mutex_unlock(&kvm->slots_lock); return 0; unlock_fail: mutex_unlock(&kvm->slots_lock); fail: kfree(p); eventfd_ctx_put(eventfd); return ret; } static int kvm_deassign_ioeventfd_idx(struct kvm *kvm, enum kvm_bus bus_idx, struct kvm_ioeventfd *args) { struct _ioeventfd *p, *tmp; struct eventfd_ctx *eventfd; struct kvm_io_bus *bus; int ret = -ENOENT; eventfd = eventfd_ctx_fdget(args->fd); if (IS_ERR(eventfd)) return PTR_ERR(eventfd); mutex_lock(&kvm->slots_lock); list_for_each_entry_safe(p, tmp, &kvm->ioeventfds, list) { bool wildcard = !(args->flags & KVM_IOEVENTFD_FLAG_DATAMATCH); if (p->bus_idx != bus_idx || p->eventfd != eventfd || p->addr != args->addr || p->length != args->len || p->wildcard != wildcard) continue; if (!p->wildcard && p->datamatch != args->datamatch) continue; kvm_io_bus_unregister_dev(kvm, bus_idx, &p->dev); bus = kvm_get_bus(kvm, bus_idx); if (bus) bus->ioeventfd_count--; ioeventfd_release(p); ret = 0; break; } mutex_unlock(&kvm->slots_lock); eventfd_ctx_put(eventfd); return ret; } static int kvm_deassign_ioeventfd(struct kvm *kvm, struct kvm_ioeventfd *args) { enum kvm_bus bus_idx = ioeventfd_bus_from_flags(args->flags); int ret = kvm_deassign_ioeventfd_idx(kvm, bus_idx, args); if (!args->len && bus_idx == KVM_MMIO_BUS) kvm_deassign_ioeventfd_idx(kvm, KVM_FAST_MMIO_BUS, args); return ret; } static int kvm_assign_ioeventfd(struct kvm *kvm, struct kvm_ioeventfd *args) { enum kvm_bus bus_idx; int ret; bus_idx = ioeventfd_bus_from_flags(args->flags); /* must be natural-word sized, or 0 to ignore length */ switch (args->len) { case 0: case 1: case 2: case 4: case 8: break; default: return -EINVAL; } /* check for range overflow */ if (args->addr + args->len < args->addr) return -EINVAL; /* check for extra flags that we don't understand */ if (args->flags & ~KVM_IOEVENTFD_VALID_FLAG_MASK) return -EINVAL; /* ioeventfd with no length can't be combined with DATAMATCH */ if (!args->len && (args->flags & KVM_IOEVENTFD_FLAG_DATAMATCH)) return -EINVAL; ret = kvm_assign_ioeventfd_idx(kvm, bus_idx, args); if (ret) goto fail; /* When length is ignored, MMIO is also put on a separate bus, for * faster lookups. */ if (!args->len && bus_idx == KVM_MMIO_BUS) { ret = kvm_assign_ioeventfd_idx(kvm, KVM_FAST_MMIO_BUS, args); if (ret < 0) goto fast_fail; } return 0; fast_fail: kvm_deassign_ioeventfd_idx(kvm, bus_idx, args); fail: return ret; } int kvm_ioeventfd(struct kvm *kvm, struct kvm_ioeventfd *args) { if (args->flags & KVM_IOEVENTFD_FLAG_DEASSIGN) return kvm_deassign_ioeventfd(kvm, args); return kvm_assign_ioeventfd(kvm, args); }