index a24ec89ba4420ad38e8848422ca5f69baa5ffe1c..67fc7a8badaff655f259af742cd0bc289b6644c5 100644 (file)
--- a/README
+++ b/README
- Linux kernel release 3.x <http://kernel.org/>
+ Linux kernel release 4.x <http://kernel.org/>
-These are the release notes for Linux version 3. Read them carefully,
+These are the release notes for Linux version 4. Read them carefully,
as they tell you what this is all about, explain how to install the
kernel, and what to do if something goes wrong.
directory where you have permissions (eg. your home directory) and
unpack it:
- gzip -cd linux-3.X.tar.gz | tar xvf -
+ gzip -cd linux-4.X.tar.gz | tar xvf -
or
- bzip2 -dc linux-3.X.tar.bz2 | tar xvf -
+ bzip2 -dc linux-4.X.tar.bz2 | tar xvf -
Replace "X" with the version number of the latest kernel.
files. They should match the library, and not get messed up by
whatever the kernel-du-jour happens to be.
- - You can also upgrade between 3.x releases by patching. Patches are
+ - You can also upgrade between 4.x releases by patching. Patches are
distributed in the traditional gzip and the newer bzip2 format. To
install by patching, get all the newer patch files, enter the
- top level directory of the kernel source (linux-3.X) and execute:
+ top level directory of the kernel source (linux-4.X) and execute:
- gzip -cd ../patch-3.x.gz | patch -p1
+ gzip -cd ../patch-4.x.gz | patch -p1
or
- bzip2 -dc ../patch-3.x.bz2 | patch -p1
+ bzip2 -dc ../patch-4.x.bz2 | patch -p1
Replace "x" for all versions bigger than the version "X" of your current
source tree, _in_order_, and you should be ok. You may want to remove
that there are no failed patches (some-file-name# or some-file-name.rej).
If there are, either you or I have made a mistake.
- Unlike patches for the 3.x kernels, patches for the 3.x.y kernels
+ Unlike patches for the 4.x kernels, patches for the 4.x.y kernels
(also known as the -stable kernels) are not incremental but instead apply
- directly to the base 3.x kernel. For example, if your base kernel is 3.0
- and you want to apply the 3.0.3 patch, you must not first apply the 3.0.1
- and 3.0.2 patches. Similarly, if you are running kernel version 3.0.2 and
- want to jump to 3.0.3, you must first reverse the 3.0.2 patch (that is,
- patch -R) _before_ applying the 3.0.3 patch. You can read more on this in
+ directly to the base 4.x kernel. For example, if your base kernel is 4.0
+ and you want to apply the 4.0.3 patch, you must not first apply the 4.0.1
+ and 4.0.2 patches. Similarly, if you are running kernel version 4.0.2 and
+ want to jump to 4.0.3, you must first reverse the 4.0.2 patch (that is,
+ patch -R) _before_ applying the 4.0.3 patch. You can read more on this in
Documentation/applying-patches.txt
Alternatively, the script patch-kernel can be used to automate this
SOFTWARE REQUIREMENTS
- Compiling and running the 3.x kernels requires up-to-date
+ Compiling and running the 4.x kernels requires up-to-date
versions of various software packages. Consult
Documentation/Changes for the minimum version numbers required
and how to get updates for these packages. Beware that using
place for the output files (including .config).
Example:
- kernel source code: /usr/src/linux-3.X
+ kernel source code: /usr/src/linux-4.X
build directory: /home/name/build/kernel
To configure and build the kernel, use:
- cd /usr/src/linux-3.X
+ cd /usr/src/linux-4.X
make O=/home/name/build/kernel menuconfig
make O=/home/name/build/kernel
sudo make O=/home/name/build/kernel modules_install install