index afc4f0d81ee1798d400a173b287709e6ea07babc..e8c8a6dc1c2bc9713eab305dc9a63001abef7049 100644 (file)
--- a/README
+++ b/README
These are the release notes for Linux version 4. Read them carefully,
as they tell you what this is all about, explain how to install the
-kernel, and what to do if something goes wrong.
+kernel, and what to do if something goes wrong.
WHAT IS LINUX?
and multistack networking including IPv4 and IPv6.
It is distributed under the GNU General Public License - see the
- accompanying COPYING file for more details.
+ accompanying COPYING file for more details.
ON WHAT HARDWARE DOES IT RUN?
system: there are much better sources available.
- There are various README files in the Documentation/ subdirectory:
- these typically contain kernel-specific installation notes for some
+ these typically contain kernel-specific installation notes for some
drivers for example. See Documentation/00-INDEX for a list of what
is contained in each file. Please read the Changes file, as it
contains information about the problems, which may result by upgrading
To have the build system also tell the reason for the rebuild of each
target, use "V=2". The default is "V=0".
- - Keep a backup kernel handy in case something goes wrong. This is
+ - Keep a backup kernel handy in case something goes wrong. This is
especially true for the development releases, since each new release
contains new code which has not been debugged. Make sure you keep a
backup of the modules corresponding to that kernel, as well. If you
- In order to boot your new kernel, you'll need to copy the kernel
image (e.g. .../linux/arch/i386/boot/bzImage after compilation)
- to the place where your regular bootable kernel is found.
+ to the place where your regular bootable kernel is found.
- Booting a kernel directly from a floppy without the assistance of a
bootloader such as LILO, is no longer supported.
to update the loading map! If you don't, you won't be able to boot
the new kernel image.
- Reinstalling LILO is usually a matter of running /sbin/lilo.
+ Reinstalling LILO is usually a matter of running /sbin/lilo.
You may wish to edit /etc/lilo.conf to specify an entry for your
old kernel image (say, /vmlinux.old) in case the new one does not
- work. See the LILO docs for more information.
+ work. See the LILO docs for more information.
After reinstalling LILO, you should be all set. Shutdown the system,
reboot, and enjoy!
If you ever need to change the default root device, video mode,
ramdisk size, etc. in the kernel image, use the 'rdev' program (or
alternatively the LILO boot options when appropriate). No need to
- recompile the kernel to change these parameters.
+ recompile the kernel to change these parameters.
- - Reboot with the new kernel and enjoy.
+ - Reboot with the new kernel and enjoy.
IF SOMETHING GOES WRONG:
is followed by a function with a higher address you will find the one
you want. In fact, it may be a good idea to include a bit of
"context" in your problem report, giving a few lines around the
- interesting one.
+ interesting one.
If you for some reason cannot do the above (you have a pre-compiled
kernel image or similar), telling me as much about your setup as