diff --git a/virt/kvm/arm/mmu.c b/virt/kvm/arm/mmu.c
index 1d90d79706bd5b71d3914ecd808d2bd6c127286c..91aaf73b00df8a385a28c2a221505b6ba82062b1 100644 (file)
--- a/virt/kvm/arm/mmu.c
+++ b/virt/kvm/arm/mmu.c
@@ -177,6 +177,35 @@ static void clear_stage2_pmd_entry(struct kvm *kvm, pmd_t *pmd, phys_addr_t addr
put_page(virt_to_page(pmd));
}
+static inline void kvm_set_pte(pte_t *ptep, pte_t new_pte)
+{
+ WRITE_ONCE(*ptep, new_pte);
+ dsb(ishst);
+}
+
+static inline void kvm_set_pmd(pmd_t *pmdp, pmd_t new_pmd)
+{
+ WRITE_ONCE(*pmdp, new_pmd);
+ dsb(ishst);
+}
+
+static inline void kvm_pmd_populate(pmd_t *pmdp, pte_t *ptep)
+{
+ kvm_set_pmd(pmdp, kvm_mk_pmd(ptep));
+}
+
+static inline void kvm_pud_populate(pud_t *pudp, pmd_t *pmdp)
+{
+ WRITE_ONCE(*pudp, kvm_mk_pud(pmdp));
+ dsb(ishst);
+}
+
+static inline void kvm_pgd_populate(pgd_t *pgdp, pud_t *pudp)
+{
+ WRITE_ONCE(*pgdp, kvm_mk_pgd(pudp));
+ dsb(ishst);
+}
+
/*
* Unmapping vs dcache management:
*
@@ -196,6 +225,10 @@ static void clear_stage2_pmd_entry(struct kvm *kvm, pmd_t *pmd, phys_addr_t addr
* This is why right after unmapping a page/section and invalidating
* the corresponding TLBs, we call kvm_flush_dcache_p*() to make sure
* the IO subsystem will never hit in the cache.
+ *
+ * This is all avoided on systems that have ARM64_HAS_STAGE2_FWB, as
+ * we then fully enforce cacheability of RAM, no matter what the guest
+ * does.
*/
static void unmap_stage2_ptes(struct kvm *kvm, pmd_t *pmd,
phys_addr_t addr, phys_addr_t end)
pte = pte_offset_kernel(pmd, addr);
kvm_set_pte(pte, pfn_pte(pfn, prot));
get_page(virt_to_page(pte));
- kvm_flush_dcache_to_poc(pte, sizeof(*pte));
pfn++;
} while (addr += PAGE_SIZE, addr != end);
}
kvm_err("Cannot allocate Hyp pte\n");
return -ENOMEM;
}
- pmd_populate_kernel(NULL, pmd, pte);
+ kvm_pmd_populate(pmd, pte);
get_page(virt_to_page(pmd));
- kvm_flush_dcache_to_poc(pmd, sizeof(*pmd));
}
next = pmd_addr_end(addr, end);
kvm_err("Cannot allocate Hyp pmd\n");
return -ENOMEM;
}
- pud_populate(NULL, pud, pmd);
+ kvm_pud_populate(pud, pmd);
get_page(virt_to_page(pud));
- kvm_flush_dcache_to_poc(pud, sizeof(*pud));
}
next = pud_addr_end(addr, end);
err = -ENOMEM;
goto out;
}
- pgd_populate(NULL, pgd, pud);
+ kvm_pgd_populate(pgd, pud);
get_page(virt_to_page(pgd));
- kvm_flush_dcache_to_poc(pgd, sizeof(*pgd));
}
next = pgd_addr_end(addr, end);
pmd = stage2_get_pmd(kvm, cache, addr);
VM_BUG_ON(!pmd);
- /*
- * Mapping in huge pages should only happen through a fault. If a
- * page is merged into a transparent huge page, the individual
- * subpages of that huge page should be unmapped through MMU
- * notifiers before we get here.
- *
- * Merging of CompoundPages is not supported; they should become
- * splitting first, unmapped, merged, and mapped back in on-demand.
- */
- VM_BUG_ON(pmd_present(*pmd) && pmd_pfn(*pmd) != pmd_pfn(*new_pmd));
-
old_pmd = *pmd;
if (pmd_present(old_pmd)) {
+ /*
+ * Multiple vcpus faulting on the same PMD entry, can
+ * lead to them sequentially updating the PMD with the
+ * same value. Following the break-before-make
+ * (pmd_clear() followed by tlb_flush()) process can
+ * hinder forward progress due to refaults generated
+ * on missing translations.
+ *
+ * Skip updating the page table if the entry is
+ * unchanged.
+ */
+ if (pmd_val(old_pmd) == pmd_val(*new_pmd))
+ return 0;
+
+ /*
+ * Mapping in huge pages should only happen through a
+ * fault. If a page is merged into a transparent huge
+ * page, the individual subpages of that huge page
+ * should be unmapped through MMU notifiers before we
+ * get here.
+ *
+ * Merging of CompoundPages is not supported; they
+ * should become splitting first, unmapped, merged,
+ * and mapped back in on-demand.
+ */
+ VM_BUG_ON(pmd_pfn(old_pmd) != pmd_pfn(*new_pmd));
+
pmd_clear(pmd);
kvm_tlb_flush_vmid_ipa(kvm, addr);
} else {
@@ -1090,7 +1135,7 @@ static int stage2_set_pte(struct kvm *kvm, struct kvm_mmu_memory_cache *cache,
if (!cache)
return 0; /* ignore calls from kvm_set_spte_hva */
pte = mmu_memory_cache_alloc(cache);
- pmd_populate_kernel(NULL, pmd, pte);
+ kvm_pmd_populate(pmd, pte);
get_page(virt_to_page(pmd));
}
@@ -1102,6 +1147,10 @@ static int stage2_set_pte(struct kvm *kvm, struct kvm_mmu_memory_cache *cache,
/* Create 2nd stage page table mapping - Level 3 */
old_pte = *pte;
if (pte_present(old_pte)) {
+ /* Skip page table update if there is no change */
+ if (pte_val(old_pte) == pte_val(*new_pte))
+ return 0;
+
kvm_set_pte(pte, __pte(0));
kvm_tlb_flush_vmid_ipa(kvm, addr);
} else {