]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
ARM: dts: am571x-idk: Add CMA pools and enable IPUs & DSP1 rprocs
authorSuman Anna <s-anna@ti.com>
Thu, 22 Feb 2018 17:41:11 +0000 (11:41 -0600)
committerSuman Anna <s-anna@ti.com>
Mon, 4 Mar 2019 16:02:39 +0000 (10:02 -0600)
commit0b6cc121175c83e3a2fc6209f04c6551ffea9280
treeb1cd699bc075b7400cb551ed0e4c6928e6189cac
parentfb756be57b8c1c9cd06f5152a5635d101794d1a5
ARM: dts: am571x-idk: Add CMA pools and enable IPUs & DSP1 rprocs

The CMA reserved memory nodes have been added for both the IPUs and the
DSP1 remoteproc devices on the AM571x IDK board. These nodes are assigned
to the respective rproc device nodes, and both the IPUs and the DSP1
remote processors are enabled for this board.

The current CMA pools and sizes are defined statically for each device.
The addresses chosen are the same as the respective processors on the
DRA72 EVM board to maintain firmware compatibility between the two boards.
The CMA pools and sizes are defined using 64-bit values to support LPAE.
The starting addresses are fixed to meet current dependencies on the
remote processor firmwares, and this will go away when the remote-side
code has been improved to gather this information runtime during its
initialization.

An associated pair of the rproc node and its CMA node can be disabled
later on if there is no use-case defined to use that remote processor.

Signed-off-by: Suman Anna <s-anna@ti.com>
arch/arm/boot/dts/am571x-idk.dts