]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
Merge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
authorLinus Torvalds <torvalds@linux-foundation.org>
Sun, 15 Apr 2018 19:36:31 +0000 (12:36 -0700)
committerLinus Torvalds <torvalds@linux-foundation.org>
Sun, 15 Apr 2018 19:36:31 +0000 (12:36 -0700)
commit174e719439b8224d7cedfbdd9529de396cac01ff
treea1729ca869e7dedaa47199d0818b2297521076a5
parent19ca90de49c3269874722148edf07083182e23ec
parent32e6e967fb36bf77ed99221ae3ce1909f045d8f9
Merge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip

Pull more perf updates from Thomas Gleixner:
 "A rather large set of perf updates:

  Kernel:

   - Fix various initialization issues

   - Prevent creating [ku]probes for not CAP_SYS_ADMIN users

  Tooling:

   - Show only failing syscalls with 'perf trace --failure' (Arnaldo
     Carvalho de Melo)

            e.g: See what 'openat' syscalls are failing:

        # perf trace --failure -e openat
         762.323 ( 0.007 ms): VideoCapture/4566 openat(dfd: CWD, filename: /dev/video2) = -1 ENOENT No such file or directory
         <SNIP N /dev/videoN open attempts... sigh, where is that improvised camera lid?!? >
         790.228 ( 0.008 ms): VideoCapture/4566 openat(dfd: CWD, filename: /dev/video63) = -1 ENOENT No such file or directory
        ^C#

   - Show information about the event (freq, nr_samples, total
     period/nr_events) in the annotate --tui and --stdio2 'perf
     annotate' output, similar to the first line in the 'perf report
     --tui', but just for the samples for a the annotated symbol
     (Arnaldo Carvalho de Melo)

   - Introduce 'perf version --build-options' to show what features were
     linked, aliased as well as a shorter 'perf -vv' (Jin Yao)

   - Add a "dso_size" sort order (Kim Phillips)

   - Remove redundant ')' in the tracepoint output in 'perf trace'
     (Changbin Du)

   - Synchronize x86's cpufeatures.h, no effect on toolss (Arnaldo
     Carvalho de Melo)

   - Show group details on the title line in the annotate browser and
     'perf annotate --stdio2' output, so that the per-event columns can
     have headers (Arnaldo Carvalho de Melo)

   - Fixup vertical line separating metrics from instructions and
     cleaning unused lines at the bottom, both in the annotate TUI
     browser (Arnaldo Carvalho de Melo)

   - Remove duplicated 'samples' in lost samples warning in
     'perf report' (Arnaldo Carvalho de Melo)

   - Synchronize i915_drm.h, silencing the perf build process,
     automagically adding support for the new DRM_I915_QUERY ioctl
     (Arnaldo Carvalho de Melo)

   - Make auxtrace_queues__add_buffer() allocate struct buffer, from a
     patchkit already applied (Adrian Hunter)

   - Fix the --stdio2/TUI annotate output to include group details, be
     it for a recorded '{a,b,f}' explicit event group or when forcing
     group display using 'perf report --group' for a set of events not
     recorded as a group (Arnaldo Carvalho de Melo)

   - Fix display artifacts in the ui browser (base class for the
     annotate and main report/top TUI browser) related to the extra
     title lines work (Arnaldo Carvalho de Melo)

   - perf auxtrace refactorings, leftovers from a previously partially
     processed patchset (Adrian Hunter)

   - Fix the builtin clang build (Sandipan Das, Arnaldo Carvalho de
     Melo)

   - Synchronize i915_drm.h, silencing a perf build warning and in the
     process automagically adding support for a new ioctl command
     (Arnaldo Carvalho de Melo)

   - Fix a strncpy issue in uprobe tracing"

* 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: (36 commits)
  perf/core: Need CAP_SYS_ADMIN to create k/uprobe with perf_event_open()
  tracing/uprobe_event: Fix strncpy corner case
  perf/core: Fix perf_uprobe_init()
  perf/core: Fix perf_kprobe_init()
  perf/core: Fix use-after-free in uprobe_perf_close()
  perf tests clang: Fix function name for clang IR test
  perf clang: Add support for recent clang versions
  perf tools: Fix perf builds with clang support
  perf tools: No need to include namespaces.h in util.h
  perf hists browser: Remove leftover from row returned from refresh
  perf hists browser: Show extra_title_lines in the 'D' debug hotkey
  perf auxtrace: Make auxtrace_queues__add_buffer() do CPU filtering
  tools headers uapi: Synchronize i915_drm.h
  perf report: Remove duplicated 'samples' in lost samples warning
  perf ui browser: Fixup cleaning unused lines at the bottom
  perf annotate browser: Fixup vertical line separating metrics from instructions
  perf annotate: Show group details on the title line
  perf auxtrace: Make auxtrace_queues__add_buffer() allocate struct buffer
  perf/x86/intel: Move regs->flags EXACT bit init
  perf trace: Remove redundant ')'
  ...
kernel/trace/trace_uprobe.c