]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
ARM: dts: am437x-sk: Enable PRU-ICSS nodes
authorSuman Anna <s-anna@ti.com>
Tue, 30 Jan 2018 19:43:20 +0000 (13:43 -0600)
committerSuman Anna <s-anna@ti.com>
Sun, 24 Feb 2019 01:20:50 +0000 (19:20 -0600)
commit703dc8b679580fa0573bc783c5ae0c8bd1b37269
tree6b5780ac28982412aa7d86be66cb774c06f29db7
parent3be03de0f13b64fe92ed33d27643975de5706a7f
ARM: dts: am437x-sk: Enable PRU-ICSS nodes

The AM437x SK EVM board uses a AM437x SoC that supports two PRU-ICSS
instances. The PRU-ICSS processor bus nodes and subsystem nodes were
left in disabled state in the base am4372.dtsi file. All these nodes
(both PRU-ICSS1 and PRU-ICSS0 instances) have been enabled now. The
PRU nodes are already enabled in the base dts file, and so become
effective automatically with the enabling of these PRU-ICSS nodes.

The corresponding PRU nodes can be disabled later on if there are
no use-cases defined to use a particular PRU core or the whole
PRU-ICSS subsystem itself if both its PRU cores are unused.

Signed-off-by: Suman Anna <s-anna@ti.com>
arch/arm/boot/dts/am437x-sk-evm.dts